powered by CADENAS

Social Share

Amazon

Motorized tricycle (5728 views - Cars & Motorbikes & Trucks)

A motorized tricycle, motor trike, or three-wheeled motorcycle is a three-wheeled vehicle based on the same technology as a bicycle or motorcycle, and powered by an electric motor, motorcycle, scooter or car engine. These are mainly used by old motorcyclists that can not reverse using their feet
Go to Article

Explanation by Hotspot Model

Youtube


    

Motorized tricycle

Motorized tricycle

Motorized tricycle

A motorized tricycle, motor trike, or three-wheeled motorcycle is a three-wheeled vehicle based on the same technology as a bicycle or motorcycle, and powered by an electric motor, motorcycle, scooter or car engine. These are mainly used by old motorcyclists that can not reverse using their feet

Classification

Depending on the design of the vehicle, a motorized trike may be categorized as a motorcycle, motor scooter, or simply the three-wheeled counterpart to a motorized or electric bicycle. The main difference between a motorcycle trike and a scooter trike is that motorcycles are sat on in a "saddle"-style seating (as with a horse), with the legs apart, and motorcycles have manual transmissions. Scooters have a "step-through" seating style, in which the driver sits on a more chair-like seat, with the legs together; as well, scooters have automatic transmissions. Laypersons often associate the engine size as a dividing line between motorcycles and scooters,[citation needed] since a typical scooter has a small 50 cc engine, but scooter engines can also be as large as 650cc as used in the Suzuki Burgman.

Motorcycles with sidecars are not usually considered tricycles. It can be harder to categorize three-wheeled automobiles. While some early prototype automobiles were steam tricycles, three-wheeled cars such as the Morgan 3-Wheeler are often classified as cars rather than motorcycles. Generally, the motorcycle classification will require passengers to sit behind the driver, whereas in the car classification, at least one passenger is able to sit abreast to the driver.

Motorcycle tricycles

A motorized tricycle's wheels may be arranged in either configuration: delta or tadpole. A delta trike has one wheel in front and two in back, and the tadpole trike has two wheels in front and one in back. Occasionally, rear wheel steering is used, although this increases the turning circle and can affect handling (the geometry is similar to a regular trike operating in reverse, but with a steering damper added).

Tadpoles are more stable under braking and more likely to slide instead of roll; front braking hard on a delta requires the vehicle to steer almost straight to avoid tipping. The balance of friction patches and rolling resistance also means that tadpoles tend to oversteer and deltas understeer.

Motor trikes are attractive for those with mobility or balance problems.

Under some local regulations, while riding a three-wheeled vehicle, it may be possible to carry multiple passengers with a motorcycle driving license, to ride a motorcycle-style vehicle with a car license, or to avoid motorcycle helmet use regulations.

These machines are generally custom-built. A common arrangement is to fit chopper-style ("ape hanger") front forks to a VW Beetle engine and transaxle, popular because it is largely self-contained on a single subframe. Similarly, the engine, transmission and rear wheel may be taken from a large motorcycle as a single unit, and used in the construction of a tadpole trike.

Mass-manufactured motor tricycles include the Piaggio MP3; the Piaggio Ape (Italian for Bee) delivery trike (delta); the Harley-Davidson Tri Glide Ultra Classic; the Bombardier Recreational Products Can-Am Spyder (tadpole); the Polaris Slingshot (tadpole); the T-Rex reverse trike; trikes used by municipal authorities in the USA; and, historically, vehicles such as the Scammell Scarab railway dray, a common sight around post-war British railway stations.

Motorized freight trikes

In Asian and Southeast Asian countries, motorized trikes are used as small freight trucks and commercial vehicles. Nicknamed "three-wheelers" or "tuk-tuks" in popular parlance, they are a motorized version of the traditional pulled rickshaw or cycle rickshaw. While they are mostly used as taxis for hire, they are also used for commercial and freight deliveries. They are particularly popular in cities where traffic congestion is a problem.

They usually have a sheet-metal body or open frame that rests on three wheels, a canvas roof with drop-down sides, a small cabin in the front of the vehicle for the driver, an air-cooled scooter version of a two-stroke engine, with handlebar controls instead of a steering wheel. The smaller motorized trikes are used as delivery vehicles for lighter loads. The larger trikes, with more powerful engines, have larger cargo bays, and they can carry freight within a city.

China

Motorized three-wheel freight vehicles are a common sight throughout China. They come in various sizes, from open saddle-style trikes to 'three-wheel trucks' with a fully closed cabin.

Philippines

In the Philippines, a "motorbike and sidecar" is called a tricycle. They are commonly used as a public utility vehicle and for personal transportation.

India

Since 2012, electric tricycles known as e-rickshaws have become popular, replacing other commercial transports. For vehicles other than electric rickshaws, various locally made configurations are used in India. They fall under the category of Jugaad and serve as both passenger and commercial vehicles. The motorized versions are popular for their low cost, because they are put together from salvaged motorcycles and often do not require the operator to have a drivers license.

See also



This article uses material from the Wikipedia article "Motorized tricycle", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer