Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Edmolift AB).
A scissors mechanism uses linked, folding supports in a criss-cross 'X' pattern.[1]
Extension is achieved by applying pressure to the outside of a set of supports located at one end of the mechanism, elongating the crossing pattern. This can be achieved through hydraulic, pneumatic, mechanical or simply muscular means.
It may require no power to return to its original position, but simply a release of the original pressure. Also used in kinematics of mechanisms
This mechanism is used in devices such as lift tables and scissor lifts. Modern low-profile computer keyboards make an extensive use of it as well, installing each key on a scissor support to ensure their smooth vertical movement, allowing the use of a cheap and reliable rubber dome contact set, instead of expensive and complex array of mechanical switches.
This technology-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Scissors mechanism", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,Geneva double,mechanism,kinematics,rotation,translation