Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article includes a list of references, but its sources remain unclear because it has insufficient inline citations. Please help to improve this article by introducing more precise citations. (June 2010) (Learn how and when to remove this template message) |
A muffle furnace (sometimes retort furnace in historical usage) is a furnace in which the subject material is isolated from the fuel and all of the products of combustion, including gases and flying ash.[1] After the development of high-temperature heating elements and widespread electrification in developed countries, new muffle furnaces quickly moved to electric designs.[2]
Today, a muffle furnace is (usually) a front-loading box-type oven or kiln for high-temperature applications such as fusing glass, creating enamel coatings, ceramics and soldering and brazing articles. They are also used in many research facilities, for example by chemists in order to determine what proportion of a sample is non-combustible and non-volatile (i.e., ash). Some digital controllers allow RS232 interface and permit the operator to program up to 126[3] segments, such as ramping, soaking, sintering, and more. Also, advances in materials for heating elements, such as molybdenum disilicide, can now produce working temperatures up to 1,800 degrees Celsius (3,272 degrees Fahrenheit), which facilitate more sophisticated metallurgical applications.[citation needed]
The term muffle furnace may also be used to describe another oven constructed on many of the same principles as the box-type kiln mentioned above, but takes the form of a long, wide, and thin hollow tube used in roll-to-roll manufacturing processes.[citation needed]
Both of the above-mentioned furnaces are usually heated to desired temperatures by conduction, convection, or blackbody radiation from electrical resistance heater elements.[citation needed] Therefore, there is (usually) no combustion involved in the temperature control of the system, which allows for much greater control of temperature uniformity and assures isolation of the material being heated from the byproducts of fuel combustion. Discover an advanced muffle furnace, with a smooth & safe operation even at high-level temperature.
Wikimedia Commons has media related to Muffle furnaces. |
Iron production (Ironworks) |
| ||||||||
---|---|---|---|---|---|---|---|---|---|
Steelmaking (Steel mill) |
| ||||||||
Production by country | |||||||||
Heat treatment methods |
|
This article uses material from the Wikipedia article "Muffle furnace", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced