Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A wide-body aircraft, also known as a twin-aisle aircraft, is a jet airliner with a fuselage wide enough to accommodate two passenger aisles with seven or more seats abreast.[1] The typical fuselage diameter is 5 to 6 m (16 to 20 ft).[2] In the typical wide-body economy cabin, passengers are seated seven to ten abreast,[3] allowing a total capacity of 200 to 850[4] passengers. The largest wide-body aircraft are over 6 m (20 ft) wide, and can accommodate up to eleven passengers abreast in high-density configurations.
By comparison, a typical narrow-body airliner has a diameter of 3 to 4 m (10 to 13 ft), with a single aisle,[1][5] and seats between two and six people abreast.[6]
Wide-body aircraft were originally designed for a combination of efficiency and passenger comfort and to increase the amount of cargo space. However, airlines quickly gave in to economic factors, and reduced the extra passenger space in order to maximize revenue and profits.[7]
Wide-body aircraft are also used for the transport of commercial freight and cargo[8] and other special uses, described further below.
The biggest wide-body aircraft are known as jumbo jets due to their very large size; examples include the Boeing 747 ("jumbo jet"), Airbus A380 ("superjumbo jet"), and upcoming Boeing 777X ("mini jumbo jet").[9][10] The phrase "jumbo jet" derives from Jumbo, a circus elephant in the 19th century.[11][12]
Seven-abreast aircraft typically seat 160 to 260 passengers, eight-abreast 250 to 380, nine- and ten-abreast 350 to 480.[13]
Up to the end of 2017, nearly 8,800 wide-body airplanes had been delivered since 1969, peaking at 412 in 2015.[14]
Following the success of the Boeing 707 and Douglas DC-8 in the late 1950s and early 1960s, airlines began seeking larger aircraft to meet the rising global demand for air travel. Engineers were faced with many challenges as airlines demanded more passenger seats per aircraft, longer ranges and lower operating costs.
Early jet aircraft such as the 707 and DC-8 seated passengers along either side of a single aisle, with no more than six seats per row. Larger aircraft would have to be longer, higher (such as a double deck), or wider in order to accommodate a greater number of passenger seats. Engineers realized having two decks created difficulties in meeting emergency evacuation regulations with the technology available at that time. During the 1960s, it was also believed that supersonic airliners would succeed larger, slower planes. Thus, it was believed that most subsonic aircraft would become obsolete for passenger travel and would be eventually converted to freighters. As a result, airline manufacturers opted for a wider fuselage rather than a taller one (the 747, and eventually the DC-10 and L-1011). By adding a second aisle, the wider aircraft could accommodate as many as 10 seats across, but could also be easily converted to a freighter and carry two eight-by-eight freight pallets abreast.[15]
The engineers also opted for creating "stretched" versions of the DC-8 (61, 62 and 63 models), as well as longer versions of Boeing's 707 (-320B and 320C models) and 727 (-200 model); and Douglas' DC-9 (-30, -40, and -50 models), all of which were capable of accommodating more seats than their shorter predecessor versions.
The wide-body age began in 1970 with the entry into service of the first wide-body airliner, the four-engined, partial double-deck Boeing 747.[16] New trijet wide-body aircraft soon followed, including the McDonnell Douglas DC-10 and the Lockheed L-1011 TriStar. The first wide-body twinjet, the Airbus A300, entered service in 1974. This period came to be known as the "wide-body wars".[17]
After L-1011 TriStars were demonstrated in the USSR,[18] in 1976 the Soviet Union launched its own first four-engined wide--body, the Ilyushin Il-86.[19] The USSR failed to purchase a lot of L-1011 or negotiate their production.[verification needed]
After the success of the early wide-body aircraft, several subsequent designs came to market over the next two decades, including the Boeing 767 and 777, the Airbus A330 and A340, and the McDonnell Douglas MD-11. In the "jumbo" category, the capacity of the Boeing 747 was not surpassed until October 2007, when the Airbus A380 entered commercial service with the nickname "Superjumbo".[20] Both the Boeing 747 and Airbus A380 "jumbo jets" have four engines each (quad-jets), however the upcoming Boeing 777X ("mini jumbo jet") is a twinjet.[9][10]
In the mid-2000s, rising oil costs in a post-9/11 climate caused airlines to look towards newer, more fuel efficient aircraft. Two such examples are the Boeing 787 Dreamliner and Airbus A350 XWB. The proposed Comac C929 and C939 may also share this new wide-body market.
The production of the large Boeing 747-8 and Airbus A380 four-engine, long-haul jets is being cut back as airlines are now preferring the smaller, more efficient A350, B787 and B777 twin-engine, long-range airliners.[21]
Although wide-body aircraft have larger frontal areas (and thus greater form drag) than narrow-body aircraft of similar capacity, they have several advantages over their narrow-body counterparts:
British and Russian designers had proposed wide-body aircraft similar in configuration to the Vickers VC10 and Douglas DC-9, but with a wide-body fuselage. The British Three-Eleven project never left the drawing board, while the Russian Il-86 wide-body proposal eventually gave way to a more conventional wing-mounted engine design, most likely due to the inefficiencies of mounting such large engines on the aft fuselage.
As jet engine power and reliability have increased over the last decades, most of the wide-body aircraft built today have only two engines. A twinjet design is more fuel-efficient than a trijet or four-engined aircraft of similar size.[citation needed] The increased reliability of modern jet engines also allows aircraft to meet the ETOPS certification standard, which calculates reasonable safety margins for flights across oceans. The trijet design was dismissed due to higher maintenance and fuel costs compared to a twinjet.[citation needed] Most modern wide-body aircraft have two engines, although the heaviest wide-body aircraft are built with four engines: the Airbus A380, Boeing 747-8. The upcoming Boeing 777X-9 twinjet is approaching the capacity of the earlier Boeing 747.[9][10]
The Boeing 777 twinjet features the largest and most powerful jet engine, the General Electric GE90.[23] The early variants have a fan diameter of 123 in (312 cm), and the larger GE90-115B has a fan diameter of 128 in (325 cm).[24] This as wide as the 3.30 m (130 in) Fokker 100 fuselage. The GE90 series are physically the largest engines in aviation history.[citation needed] Complete GE90 engines can only be ferried by outsize cargo aircraft such as the Antonov An-124, presenting logistics problems if a 777 is stranded in a place due to emergency diversions without the proper spare parts. If the fan is removed from the core, then the engines may be shipped on a Boeing 747 Freighter.[25]
The 560 t (1,230,000 lb) maximum takeoff weight of the Airbus A380 would not have been possible without the engine technology developed for the Boeing 777 such as contra-rotating spools.[26] Its Trent 900 engine has a fan diameter of 116 in (290 cm), slightly smaller than the GE90 engines on the Boeing 777. The Trent 900 is designed to fit into a Boeing 747-400F freighter for easier transport by air cargo.[27]
The interiors of aircraft, known as the aircraft cabin, have been undergoing evolution since the first passenger aircraft. Today, between one and four classes of travel are available on wide-body aircraft.
Bar and lounge areas which were once installed on wide-body aircraft have mostly disappeared, but a few have returned in first class or business class on the Airbus A340-600,[28] Boeing 777-300ER,[29] and on the Airbus A380.[30] Emirates has installed showers for first-class passengers on the A380; twenty-five minutes are allotted for use of the room, and the shower operates for a maximum of five minutes.[31][32]
Depending on how the airline configures the aircraft, the size and seat pitch of the airline seats will vary significantly.[33] For example, aircraft scheduled for shorter flights are often configured at a higher seat density than long-haul aircraft. Due to current economic pressures on the airline industry, high seating densities in the economy class cabin are likely to continue.[34]
In some of the largest single-deck wide-body aircraft, such as the Boeing 777, the extra space above the cabin is used for crew rest areas and galley storage.
A comparison of interior cabin widths and economy class seating layouts is shown below under wide-body specifications. Further information can be found under external links.
Economy class in an Airbus A350
A350 Business class
First-class in a 747-400 of Cathay Pacific
Aircraft are categorized by ICAO according to the wake turbulence they produce. Because wake turbulence is generally related to the weight of an aircraft, these categories are based on one of four weight categories:[35] light, medium, heavy, and super.[36]
Due to their weight, all current wide-body aircraft are categorized as "heavy", or in the case of the A380 in U.S. airspace, "super".
The wake-turbulence category also is used to guide the separation of aircraft.[37] Super- and heavy-category aircraft require greater separation behind them than those in other categories. In some countries, such as the United States, it is a requirement to suffix the aircraft's call sign with the word heavy (or super) when communicating with air traffic control in certain areas.
Wide-body aircraft are used in science, research, and the military. Two specially modified Boeing 747 aircraft, the Shuttle Carrier Aircraft, were used to transport the U.S. Space Shuttle. Some wide-body aircraft are used as flying command posts by the military like the Ilyushin Il-80[38] or the Boeing E-4, while the Boeing E-767 is used for Airborne Early Warning and Control. New military weapons are tested aboard wide-bodies, as in the laser weapons testing on the Boeing YAL-1. Other wide-body aircraft are used as flying research stations, such as the joint German–U.S. Stratospheric Observatory for Infrared Astronomy (SOFIA). Airbus A340,[39] Airbus A380,[40] and Boeing 747[41] four-engine wide-body aircraft are used to test new generations of aircraft engines in flight. A few aircraft have also been converted for aerial firefighting, such as the DC-10-based[42] Tanker 910 and the 747-based Evergreen Supertanker.[43]
Some wide-body aircraft are used as VIP transport. Canada uses the Airbus A310, while Russia use the Ilyushin Il-96, to transport those holding the highest offices. Germany replaced their Airbus A310 with an Airbus A340 in spring 2011. Specially-modified Boeing 747-200s (Boeing VC-25s) are used to ferry the President of the United States; when one of these aircraft is in use by the President, its call sign is Air Force One. More information can be found under Air transports of heads of state and government.
Model | produced | MTOW (tonnes) |
Length | inside width |
outside width |
economy seats across | seat width[a] |
---|---|---|---|---|---|---|---|
B767[44] | 1981– | 186.9 | 48.51–61.37 m (159.2–201.3 ft) | 4.72 m (186 in) | 5.03 m (198 in) | 7: 2-3-2 (HD, 8: 2-4-2) | 18" (16.4) |
A300[45] | 1974–2007 | 171.7 | 53.61–54.08 m (175.9–177.4 ft) | 5.28 m (208 in) | 5.64 m (222 in) | 8: 2-4-2 (HD, 9: 3-3-3) | 17.2" (16.4") |
A310[46] | 1983–1998 | 164 | 46.66 m (153.1 ft) | 8: 2-4-2 | 17.2" | ||
A330[47] | 1994– | 242 | 58.82–63.67 m (193.0–208.9 ft) | 8: 2-4-2 (9: 3-3-3 on D7[48]) | 18" (16.5") | ||
A340[49] | 1993–2011 | 380 | 59.40–75.36 m (194.9–247.2 ft) | 8: 2-4-2 (9: 3-3-3) | 17.8" (16.4") | ||
B787[50] | 2007– | 252.7 | 56.72–68.28 m (186.1–224.0 ft) | 5.49 m (216 in) | 5.76 m (227 in) | 9: 3-3-3 (8: 2-4-2 on JL[51]) | 17.2" |
CR929[52] | 2023- | 245[53] | 63.755 m (209.17 ft)[53] | 5.61 m (221 in) | 5.92 m (233 in) | 9: 3-3-3 | 17.9" |
A350[54] | 2010– | 268 | 66.61–73.59 m (218.5–241.4 ft) | 5.61 m (221 in) | 5.96 m (235 in) | 9: 3-3-3 (10: 3-4-3 on TX[55]) | 18" (16.5”) |
DC-10[56] | 1971–1989 | 259.5 | 51.97 m (170.5 ft) | 5.69 m (224 in) | 6.02 m (237 in) | 9: 2-4-3, 10: 3-4-3 | 18", 16.5" |
MD-11[57] | 1990–2001 | 286 | 58.65 m (192.4 ft) | 9: 2-5-2, 10: 3-4-3 | 18", 16.5" | ||
L-1011[58] | 1972–1985 | 231.3 | 54.17–50.05 m (177.7–164.2 ft) | 5.77 m (227 in) | 6.02 m (237 in) | 9: 3-4-2/2-5-2, 10: 3-4-3 | 17.7", 16.5" |
Il-86 | 1980–1994 | 206 | 60.21 m (197.5 ft) | 5.70 m (224 in) | 6.08 m (239 in) | 9: 3-3-3[59] | 18" |
Il-96 | 1992- | 270 | 55.3–63.94 m (181.4–209.8 ft) | ||||
B777[60] | 1993– | 351.5 | 63.7–73.9 m (209–242 ft) | 5.86 m (231 in) | 6.19 m (244 in) | 9: 2-5-2/3-3-3, 10: 3-4-3 | 18.5", 17" |
B777X[61] | 2019– | 351.5 | 69.8–76.7 m (229–252 ft) | 5.94 m (234 in) | 10: 3-4-3 | 17.2" | |
B747[62] | 1968– | 447.7 | 56.3–76.25 m (184.7–250.2 ft) | 6.10 m (240 in) up: 3.46 m (136 in) |
6.50 m (256 in) | 10: 3-4-3/9: 3-4-2 (main) 6: 3-3 (upper) |
17.2"/18.5" |
A380[63] | 2005–2021 | 560 | 72.72 m (238.6 ft) | 6.54 m (257 in) up: 5.80 m (228 in) |
7.14 m (281 in) | 10: 3-4-3 (11: 3-5-3 proposed[64]) (main) 8: 2-4-2 (upper) |
18" (18") |
This article uses material from the Wikipedia article "Wide-body aircraft", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht