Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 3.0 (Wheresmysocks).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Variable-message sign" – news · newspapers · books · scholar · JSTOR (May 2015) (Learn how and when to remove this template message) |
A variable- (also changeable-,[1] electronic-, or dynamic-) message sign, often abbreviated VMS, CMS, or DMS, and in the UK known as a matrix sign,[2] is an electronic traffic sign often used on roadways to give travellers information about special events. Such signs warn of traffic congestion, accidents, incidents such as terrorist attacks, AMBER/Silver/Blue Alerts, roadwork zones, or speed limits on a specific highway segment. In urban areas, VMS are used within parking guidance and information systems to guide drivers to available car parking spaces. They may also ask vehicles to take alternative routes, limit travel speed, warn of duration and location of the incidents, or just inform of the traffic conditions.
This section needs expansion. You can help by adding to it. (May 2015) |
VMS's were deployed at least as early as the 1950s on the New Jersey Turnpike.[3] The NJ Turnpike's signs of that period, and up to around 2012, were capable of displaying a few messages in neon, all oriented around warning drivers to slow down: "REDUCE SPEED", followed by a warning of either construction, accident, congestion, ice, snow, or fog at a certain distance ahead.[4] The New Jersey Turnpike Authority replaced those signs (along with 1990s-vintage dot-matrix VMS's along the Garden State Parkway) with more flexible electronic signs between 2010 and 2016.
The current VMS systems are largely deployed on freeways, trunk highways, or in work zones.[citation needed]
On the interchange of I-5 and SR 120 in San Joaquin County, California, an automated visibility and speed warning system was installed in 1996 to warn traffic of reduced visibility due to fog (where tule fog is a common problem in the winter), and of slow or stopped traffic.
Message Signs were deployed in Ontario during the 1990s in the Greater Toronto Area and are now being upgraded on 400 series Highways in the GTA as well as two pilot secondary highways in northeastern Ontario.[5]
Early variable message signs included static signs with words that would illuminate (often using neon tubing) indicating the type of incident that occurred, or signs that used rotating prisms (trilons) to change the message being displayed. These were later replaced by dot matrix displays typically using eggcrate, fiber optic, or flip-disc technology, which were capable of displaying a much wider range of messages than earlier static variable message signs. Since the late 1990s, the most common technology used in new installations for variable message signs are LED displays. In recent years, some newer LED variable message signs have the ability to display colored text and graphics.
Dot-matrix variable message signs are divided into three subgroups: character matrix, row matrix, and full matrix. In a character matrix VMS, each character is given its own matrix with equal horizontal spacing between them, typically with two or three rows of characters. In a full matrix VMS, the entire sign is a single large dot matrix display, allowing the display of different fonts and graphics. A row matrix VMS is a hybrid of the two types, divided into two or three rows like a character matrix display, except each row is a single long dot matrix display instead of being split per character horizontally.
Overhead variable message signs are today available in three form factors: front access, rear access, and walk-in. In a front access variable message sign, maintenance is performed by lifting the sign open from the front. Most smaller VMS are of the front access form factor, and are typically installed today on major arterials. The rear access form factor is similar to the front access form factor, except that maintenance is performed from the rear of the sign, and are commonly used for medium-sized dynamic message signs installed along the roadside of freeways (instead of overhead). The walk-in form factor is a more recent introduction, where maintenance on the sign is performed from the inside of the sign. A key advantage of the walk-in form factor is that lane closures are generally not required to perform maintenance on the sign. Most of the largest VMS units installed today are walk-in units, and are typically installed overhead on freeways.
The NJ Turnpike Authority counts five unique types of variable message signs under its jurisdiction, at least one of which has been replaced by newer signs.[6] They are:
Early models required an operator to be physically present when programming a message, whereas newer models may be reprogrammed remotely via a wired or wireless network or cellphone connection.[citation needed]
A complete message on a panel generally includes a problem statement indicating incident, roadwork, stalled vehicle etc.; a location statement indicating where the incident is located; an effect statement indicating lane closure, delay, etc. and an action statement giving suggestion what to do traffic conditions ahead. These signs are also used for AMBER Alert messages, and in some states, Silver and Blue Alert messages.
In some places, VMSes are set up with permanent, semi-static displays indicating predicted travel times to important traffic destinations such as major cities or interchanges along the route of a highway.
Typical messages provide the following information:
The information comes from a variety of traffic monitoring and surveillance systems. It is expected that by providing real-time information on special events on the oncoming road, VMS can improve motorists' route selection, reduce travel time, mitigate the severity and duration of incidents and improve the performance of the transportation network.
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (July 2016) (Learn how and when to remove this template message) |
Truck-mounted VMSes (also called Portable Changeable Message Signs or PCMS) are sometimes dispatched by highway agencies such as Caltrans to warn traffic of incidents such as accidents in areas where permanent VMSes aren't available or near enough as a preventive measure for reducing secondary accidents. They are often deployed in pairs so that the second VMS truck can take over when the traffic queue overtakes the first truck, requiring the first truck to reposition further upstream from the queue, to be effective. An optional third truck, the team leader, may be utilized for driving by and monitoring the incident itself, traffic patterns and delay times, to make strategic decisions for minimizing delays—analogous to spotter planes used in fighting forest fires.
Trailer-mounted variable-message signs are used to alter traffic patterns near work zones, and for traffic management for special events, natural disasters, and other temporary traffic patterns. The messages displayed on the sign can be programmed locally on the unit's control panel, or units equipped with a cellular modem can be programmed remotely via computer or phone. Most manufacturers produce trailers which comply with the National Transportation Communications for Intelligent Transportation System Protocol (NTCIP) which allows the portable trailer to be integrated with an intelligent transportation system. Trailer-mounted VMS can be equipped with radar, cameras, and other sensing devices as part of a smart work zone deployment..
A variable-message sign figures significantly into the plot of the 1991 film L.A. Story.
A single row matrix LED sign on Katunayake Expressway in Colombo, Sri Lanka
A three row fixed character matrix LED sign warns "Avoid London - Area Closed - Turn On Radio" following the 7 July 2005 London bombings
Europe's largest Dynamic Route Guidance System, in Nuremberg, Germany (hybrid rotating prism and row matrix LED)
A dual row matrix LED sign on National Highway 4, in Bangalore, India
A row matrix LED sign on an interchange of a German Autobahn with side graphics display.
A hybrid row matrix and full matrix sign on Highway 401 in Ontario, Canada
A full matrix walk-in cabinet LED sign (manufactured by Skyline Products) displaying travel times on Interstate 70 north of Evergreen, Colorado.
A dual row matrix LED sign in Manhattan reminding motorists to drive safely
An LED sign on the New Jersey Turnpike displaying a warning about congestion ahead
A set of LED signs on Interstate 90 in Mercer Island, Washington that warn of an upcoming lane closure due to a collision. Normally, these signs display variable speed limits that are adjusted during rush hour.
A variable-message sign tells drivers that a section of the Hidaka Expressway in Hokkaido, Japan is damaged after the 2018 Hokkaido Eastern Iburi earthquake.
This article uses material from the Wikipedia article "Variable-message sign", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer