This article possibly contains original research. Please improve it by verifying the claims made and adding inline citations. Statements consisting only of original research should be removed. (December 2016) (Learn how and when to remove this template message) |
Developer(s) | Amazon |
---|---|
Initial release | November 2014; 4 years ago (2014-11) |
Operating system | Fire OS 5.0 or later, iOS 8.0 or later[1] Android 4.4 or later |
Platform | |
Available in | |
Type | Intelligent personal assistant, cloud-based voice service |
Website | developer |
Amazon Alexa, known simply as Alexa,[2] is a virtual assistant developed by Amazon, first used in the Amazon Echo and the Amazon Echo Dot smart speakers developed by Amazon Lab126. It is capable of voice interaction, music playback, making to-do lists, setting alarms, streaming podcasts, playing audiobooks, and providing weather, traffic, sports, and other real-time information, such as news.[3] Alexa can also control several smart devices using itself as a home automation system. Users are able to extend the Alexa capabilities by installing "skills" (additional functionality developed by third-party vendors, in other settings more commonly called apps such as weather programs and audio features).
Most devices with Alexa allow users to activate the device using a wake-word (such as Alexa); other devices (such as the Amazon mobile app on iOS or Android) require the user to push a button to activate Alexa's listening mode. Currently, interaction and communication with Alexa are only available in English, German, French, Italian, Spanish,[4] and Japanese. In November 2017, Alexa became available in the Canadian market in English only.[5]
As of September 2017[update], Amazon had more than 5,000 employees working on Alexa and related products.[6] In January 2019, Amazon's devices team announced that they had sold over 100 million Alexa-enabled devices.[7]
In November 2014, Amazon announced Alexa alongside the Echo.[8] Alexa was inspired by the computer voice and conversational system on board the Starship Enterprise in science fiction TV series and movies, beginning with Star Trek: The Original Series and Star Trek: The Next Generation.[9] A year prior to the original Star Trek TV series, in 1964, premiered the original Jonny Quest animated series which had desktop computer called UNIC (pronounced /ˈjuːnɪs/ YOO-niss like the name Eunice).[10] UNIC communicated in digital readout and voice response.
The name Alexa was chosen due to the fact that it has a hard consonant with the X and therefore could be recognized with higher precision. The name is also claimed to be reminiscent of the Library of Alexandria, which is also used by Amazon Alexa Internet for the same reason.[11][12][13] In June 2015, Amazon announced Alexa Fund, a program that would invest in companies making voice control skills and technologies. The US$100 million in funds has invested in companies including Ecobee, Orange Chef, Scout Alarm, Garageio, Toymail, MARA, and Mojio.[14] In 2016, the Alexa Prize was announced to advance the technology.
In January 2017, the first Alexa Conference took place in Nashville, Tennessee, an independent gathering of the worldwide community of Alexa developers and enthusiasts.[15][16][17] The follow-up has been announced, to be keynoted by original Amazon Alexa / Connected Home product head Ahmed Bouzid.[18]
At the Amazon Web Services Re:Invent conference in Las Vegas, Amazon announced Alexa for Business and the ability for app developers to have paid add-ons to their skills.
In May 2018, Amazon announced that Alexa will be included into all of the 35,000 new Lennar Corporation homes built this year.[19]
In November 2018, Amazon opened its first Alexa-themed pop-up shop inside of Toronto's Eaton Centre, showcasing the use of home automation products with Amazon's smart speakers.[20] Amazon also sells Alexa devices at Amazon Books and Whole Foods Market locations, in addition to mall-based pop-ups throughout the United States.
A companion app is available from the Apple App Store, Google Play, and Amazon Appstore. The app can be used by owners of Alexa-enabled devices to install skills, control music, manage alarms, and view shopping lists.[21] It also allows users to review the recognized text on the app screen and to send feedback to Amazon concerning whether the recognition was good or bad. A web interface is also available to set up compatible devices (e.g., Amazon Echo, Amazon Dot, Amazon Echo Show).
Alexa offers weather reports provided by AccuWeather and news provided by TuneIn from a variety of sources including local radio stations, NPR, and ESPN.[22] Additionally, Alexa-supported devices stream music from the owner's Amazon Music accounts and have built-in support for Pandora and Spotify accounts.[23] Alexa can play music from streaming services such as Apple Music and Google Play Music from a phone or tablet. Alexa can manage voice-controlled alarms, timers, and shopping and to-do lists, and can access Wikipedia articles.[24] Alexa devices will respond to questions about items in the user's Google Calendar. Alexa's question answering ability is partly powered by the Wolfram Language.[25] When questions are asked, Alexa converts sound waves into text which allows it to gather information from various sources. Behind the scenes, the data gathered is then parsed by Wolfram's technology to generate suitable and accurate answers.[26] Similarly to generating accurate answers to questions, it is possible to design functions for Alexa by what the main line of conversation will be, anticipating "the happy path," which is the most common interactions.[27]As of November 2016[update], the Alexa Appstore had over 5,000 functions ("skills") available for users to download,[28] up from 1,000 functions in June 2016.[29] As of a partnership with fellow technology company, Microsoft's AI Cortana became available to use on Alexa enabled devices as of August 2018[update],[30] Amazon rolled out a new "Brief Mode," wherein Alexa would begin responding with a beep sound rather than saying, "Okay," to confirm receipt of a command.[31] On December 20, 2018, Amazon announced a new integration with the Wolfram Alpha answer engine,[32] which provides enhanced accuracy for users asking questions of Alexa related to math, science, astronomy, engineering, geography, history, and more.
In the home automation space, Alexa can interact with devices from several manufacturers including Belkin, ecobee, Geeni, IFTTT,[33] Insteon, LIFX, LightwaveRF, Nest , Philips Hue, SmartThings, Wink,[34][35] and Yonomi.[36] The Home Automation feature was launched on April 8, 2015.[37] Developers are able to create their own smart home skills using the Alexa Skills Kit.
In September 2018, Amazon announced a microwave oven that can be paired and controlled with an Echo device. It is sold under Amazon's AmazonBasics label.[38]
Take-out food can be ordered using Alexa; as of May 2017[update] food ordering using Alexa is supported by Domino's Pizza, Grubhub, Pizza Hut, Seamless, and Wingstop.[39] Also, users of Alexa in the UK can order meals via Just Eat.[40] In early 2017, Starbucks announced a private beta for placing pick-up orders using Alexa.[41] In addition, users can order meals using Amazon Prime Now via Alexa in 20 major US cities.[42] With the introduction of Amazon Key in November 2017, Alexa also works together with the smart lock and the Alexa Cloud Cam included in the service to allow Amazon couriers to unlock customers' front doors and deliver packages inside.[43]
According to an August 2018 article by The Information, only 2 percent of Alexa owners have used the device to make a purchase during the first seven months of 2018 and of those who made an initial purchase, 90 percent did not make a second purchase.[44]
Alexa supports a multitude of subscription-based and free streaming services on Amazon devices. These streaming services include: Prime Music, Amazon Music, Amazon Music Unlimited, Apple Music, TuneIn, iHeartRadio, Audible, Pandora, and Spotify Premium. However, some of these music services are not available on other Alexa-enabled products that are manufactured by companies external of its services. This unavailability also includes Amazon's own Fire TV devices or tablets.[45]
Alexa is able to stream media and music directly. To do this, Alexa's device should be linked to the Amazon account, which enables access to one's Amazon Music library, in addition to any audiobooks available in one's Audible library. Amazon Prime members have an additional ability to access stations, playlists, and over two million songs free of charge. Amazon Music Unlimited subscribers also have access to a list of millions of songs.
Amazon Music for PC allows one to play personal music from Google Play, iTunes, and others on an Alexa device. This can be done by uploading one's collection to My Music on Amazon from a computer. Up to 250 songs can be uploaded free of charge. Once this is done, Alexa can play this music and control playback through voice command options.
Alexa allows the user to hear updates on supported sports teams. A way to do this is by adding the sports team to the list created under Alexa's Sports Update app section. [46]
The user is able to hear updates on up to 15 supported teams:[46]
There are a number of ways messages can be sent from Alexa's application. Alexa is able to deliver messages to a recipient's Alexa application, as well as to all of their Echo devices that are both supported and associated with their Amazon account. Alexa is able to send typed messages only from Alexa's app. If one sends a message from an associated Echo device, it will be sent as a voice message. Alexa cannot send attachments such as videos and photos.[47]
For households with more than one member, one's Alexa contacts are pooled across all of the devices that are registered to its associated account. However, within Alexa's app one is only able to start conversations with its Alexa contacts.[48] When accessed and supported by an Alexa app or Echo device, Alexa messaging is available to anyone in one's household. These messages can be heard by anyone with access in the household. This messaging feature does not yet contain a password protection or associated PIN. Anyone who has access to one's cell phone number is able to use this feature to contact them through their supported Alexa app or Echo device. The feature to block alerts for messages and calls is available temporarily by utilizing the Do Not Disturb feature.[49]
Alexa for Business is a paid subscription service allowing companies to use Alexa to join conference calls, schedule meeting rooms, and custom skills designed by 3rd-party vendors.[50] At launch, notable skills are available from SAP, Microsoft, and Salesforce.[51]
Amazon allows developers to build and publish skills for Alexa using the Alexa Skills Kit known as Alexa Skills.[52] These third-party developed skills, once published, are available across Alexa-enabled devices. Users can enable these skills using the Alexa app.
A "Smart Home Skill API"[53] is available, meant to be used by hardware manufacturers to allow users to control smart home devices.[54]
Most skills run code almost entirely in the cloud, using Amazon's AWS Lambda service.[55]
In April 2018, Amazon launched Blueprints, a tool for individuals to build skills for their personal use.[56]
In February 2019, Amazon further expanded the capability of Blueprints by allowing customers to publish skills they've built with the templates to its Alexa Skill Store in the US for use by anyone with an Alexa-enabled device. [57]
Amazon allows device manufacturers to integrate Alexa voice capabilities into their own connected products by using the Alexa Voice Service (AVS), a cloud-based service that provides APIs to interface with Alexa. Products built using AVS have access to Alexa's growing list of capabilities including all of the Alexa Skills. AVS provides cloud-based automatic speech recognition (ASR) and natural language understanding (NLU). There are no fees for companies looking to integrate Alexa into their products by using AVS.[58]
The voice of Amazon Alexa is generated by a long short-term memory artificial neural network.[59][60][61]
On November 30, 2016 Amazon announced that they will make the speech recognition and natural language processing technology behind Alexa available for developers under the name of Amazon Lex. This new service would allow developers to create their own chatbots that can interact in a conversational manner, similar to Alexa. Along with the connection to various Amazon services, the initial version will provide connectivity to Facebook Messenger, with Slack and Twilio integration to follow.[62][63]
There are concerns about the access Amazon has to private conversations in the home and other non-verbal indications that can identify who is present in the home with non-stop audio pick-up from Alexa-enabled devices.[64][65] Amazon responds to these concerns by stating that the devices only stream recordings from the user's home when the 'wake word' activates the device.
Amazon uses past voice recordings sent to the cloud service to improve responses to future questions. Users can delete voice recordings that are associated with their account.
Alexa uses an address stored in the companion app when it needs a location.[66] For example, Alexa uses the user's location to respond to requests for nearby restaurants or stores. Similarly, Alexa uses the user's location for mapping-related requests.
Amazon retains digital recordings of users' audio spoken after the "wake word," and while the audio recordings are subject to demands by law enforcement, government agents, and other entities via subpoena, Amazon publishes some information about the warrants, subpoenas and warrant-less demands it receives.[67]
In 2018, Too Many T's, a hip hop group from London received international media attention by being the first artists to feature Amazon Alexa as rapper and singer.[68]
In early 2018, security researchers managed to turn an Echo into a spy device[69]by creating a malicious Alexa Skill that could record unsuspecting users and send the transcription of their conversations to an attacker.[70]
In November 2018, Amazon sent 1700 recordings of an American couple to an unrelated European man. The incident proves that Alexa records people without their knowledge.[71] Although the man who received the recordings reported the anomaly to Amazon, the company did not notify the victim until German magazine c't also contacted them and published a story about the incident. The recipient of the recordings contacted the publication after weeks went by following his report with no response from Amazon (although the company did delete the recordings from its server). When Amazon did finally contact the man whose recordings had been sent to a stranger, they claimed to have discovered the error themselves and offered him a free Prime membership and new Alexa devices by way of apology.[72]
Amazon blamed the incident on "human error" and called it an "isolated single case." However, in May 2018 an Alexa device in Portland, Oregon recorded a family's conversation and sent it to one of their contacts without their knowledge. The company dismissed the incident as an "extremely rare occurrence" and claimed the device "interpreted background conversation" as a sequence of commands to turn on, record, send the recording, and select a specific recipient.[73]
A New Hampshire judge ruled in November 2018 that authorities could examine recordings from an Amazon Echo device recovered from the home of murder victim Christine Sullivan for use as evidence against defendant Timothy Verrill. Investigators believe that the device, which belonged to the victim's boyfriend, could have captured audio of the murder and its aftermath.[74]
During the Chris Watts interrogation/interview video[75] 16:15:15 of recording timestamp, Watts was explained by the interrogator "We know that there's an Alexa in your house, and you know those are trained to record distress." Indicating Alexa may send recordings to Amazon if certain frequencies and decibels (that can only be heard during intense arguments or screams) are detected.[citation needed]
As of November 2018[update], Alexa is available in 41 countries. Most recently, Alexa launched in Mexico on November 12, 2018.[76]
Date | Country |
---|---|
November 6, 2014 (limited) June 28, 2015 (full) |
United States |
September 28, 2016[77] | United Kingdom |
October 26, 2016[77] | Germany |
Austria | |
October 4, 2017 | India |
November 15, 2017[78] | Japan |
December 5, 2017[79] | Canada |
December 8, 2017[80] | Belgium |
Bolivia | |
Bulgaria | |
Chile | |
Colombia | |
Costa Rica | |
Cyprus | |
Czech Republic | |
Ecuador | |
El Salvador | |
Estonia | |
Finland | |
Greece | |
Hungary | |
Iceland | |
Latvia | |
Liechtenstein | |
Lithuania | |
Luxembourg | |
Malta | |
Netherlands | |
Panama | |
Peru | |
Poland | |
Portugal | |
Slovakia | |
Sweden | |
Uruguay | |
January 25, 2018[81] | Ireland |
February 1, 2018[82] | Australia |
New Zealand | |
February 6, 2018[83] | France |
October 30, 2018[84][85] | Italy |
Spain | |
November 12, 2018[86] | Mexico |
As of September 2018[update], over 20,000 devices support interaction with Amazon Alexa.[87] Listed below are commercially available Alexa devices.
In September 2016, a university student competition called the Alexa Prize was announced for November of that year.[165] The prize is equipped with a total of $2.5 million and teams and their universities can win cash and research grants. The process started with team selection in 2016.[166] The 2017 inaugural competition focuses on the challenge of building a socialbot. The University of Washington student team was awarded first place for the 2017 prize.[167] A second year of the competition has been announced.
Given Amazon's strong belief in voice technologies, Amazon announced a US$100 million venture capital fund on June 25, 2015. By specifically targeting developers, device-makers and innovative companies of all sizes, Amazon aims at making digital voice assistants more powerful for its users.[168] Eligible projects for financial funding base on either creating new Alexa capabilities by using the Alexa Skills Kit (ASK) or Alexa Voice Service (AVS).[169]
The final selection of companies originates from the customer perspective and works backwards, specific elements that are considered for potential investments are: level of customer centricity, degree of innovation, motivation of leadership, fit to Alexa product/service line, amount of other funding raised.[169]
Besides financial support, Amazon provides business and technology expertise, help for bringing products to the market, aid for hard- and software development as well as enhanced marketing support on proprietary Amazon platforms.
The list of funded business includes (in alphabetical order): DefinedCrows, Dragon Innovation, Ecobee, Embodied Inc., Garageio, Invoxia, kitt.ai, June, Luma, Mara, Mojio (2x times), Musaic, Nucleus, Orange Chef, Owlet Baby Care, Petnet, Rachio, Ring, Scout, Sutro, Thalmic Labs, Toymail Co., TrackR, and Vesper.[170]
This article uses material from the Wikipedia article "Amazon Alexa", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library