powered by CADENAS

Social Share

Amazon

Open-wheel car (9826 views - Cars & Motorbikes & Trucks)

An open-wheel car (formula car, or often single-seater car in British English) is a car with the wheels outside the car's main body, and usually having only one seat. Open-wheel cars contrast with street cars, sports cars, stock cars, and touring cars, which have their wheels below the body or inside fenders. Open-wheel cars are usually built specifically for road racing, frequently with a higher degree of technological sophistication than in other forms of motor sport. Open-wheel street cars, such as the Ariel Atom, are very scarce as they are often impractical for everyday use.
Go to Article

Explanation by Hotspot Model

Youtube


    

Open-wheel car

Open-wheel car

Open-wheel car
1993 Lola Indy car driven by Nigel Mansell
ClassificationVehicle
ApplicationRecreation, sports
Fuel sourceGasoline, electric, hydrogen
PoweredYes
Self-propelledYes
Wheels4
Axles2-4
InventorRay Harroun

An open-wheel car (formula car, or often single-seater car in British English) is a car with the wheels outside the car's main body, and usually having only one seat. Open-wheel cars contrast with street cars, sports cars, stock cars, and touring cars, which have their wheels below the body or inside fenders. Open-wheel cars are usually built specifically for road racing, frequently with a higher degree of technological sophistication than in other forms of motor sport. Open-wheel street cars, such as the Ariel Atom, are very scarce as they are often impractical for everyday use.[1]

History

American racecar driver and constructor Ray Harroun was an early pioneer of the concept of a lightweight single-seater, open-wheel "monoposto" racecar.[2] After working as a mechanic in the automotive industry, Harroun began competitive professional racing in 1906, winning the AAA National Championship in 1910. He was then hired by the Marmon Motor Car Company as chief engineer, charged with building a racecar intended to race at the very first Indianapolis 500, which he went on to win. He developed a revolutionary concept which would become the originator and forefather of the single-seater (i.e. monoposto) racecar design.[3][4] Harroun has also been credited by some as pioneering the rear-view mirror which appeared on his 1911 Indianapolis 500 winning car, though he himself claimed he got the idea from seeing a mirror used for a similar purpose on a horse-drawn vehicle in 1904.[5]

Design

A typical open-wheeler has a minimal cockpit sufficient only to enclose the driver's body, with the head exposed to the air. In the Whelen Modified Tour and other short track modified series, the driver's head is contained in the car. In modern cars the engine is often located directly behind the driver, and drives the rear wheels; except in asphalt modified cars, such as the Whelen Modified Tour, where the engine is in front of the driver. Depending on the rules of the class, many types of open-wheelers have wings at the front and rear of the vehicle, as well as a very low and virtually flat undertray that helps achieve additional aerodynamic downforce pushing the car onto the road.

Some major races, such as the Singapore Grand Prix, Monaco Grand Prix (sanctioned by Formula One) and the Long Beach Grand Prix (sanctioned by IndyCar), are held on temporary street circuits. However, most open-wheel races are on dedicated road courses, such as Watkins Glen International in the US, Nürburgring in Germany, Spa-Francorchamps in Belgium and Silverstone in Great Britain. In the United States some top-level open-wheel events are held on ovals, of both short track and superspeedway variety, with an emphasis being placed more on speed and endurance than the maneuverability inherently required by road and street course events. The Whelen Modified Tour is the only opened wheeled race car series endorsed by NASCAR. This series races on most of NASCAR's most famous tracks in the United States. Other asphalt modified series race on short tracks in the United States and Canada, such as Wyoming County International Speedway in New York. The most well-attended oval race in the world is the annual Indianapolis 500 (Indy 500) in Speedway, Indiana, sanctioned by IndyCar; in the United States, it is quite common to refer to open-wheel cars as IndyCars, or Champ Cars, because of their recognizable appearance and widespread popularity across America at the Indy 500.

Driving

Open-wheeled racing is among the fastest in the world. Formula 1 cars can reach speeds in excess of 360 kilometres per hour (220 mph). At Autodromo Nazionale Monza, Antônio Pizzonia of BMW Williams F1 team recorded a top speed of 369.9 kilometres per hour (229.8 mph) in the 2004 Italian Grand Prix. Since the end of the V10 era in 2006 speeds like this have not been reached, with contemporary machinery reaching around 360 kilometres per hour (220 mph).[6] It is difficult to give precise figures for the absolute top speeds of Formula 1 cars, as the cars do not have speedometers as such and the data are not generally released by teams. The 'speed traps' on fast circuits such as Monza give a good indication, but are not necessarily located at the point on the track where the car is travelling at its fastest. BAR Honda team recorded an average top speed of 400 kilometres per hour (250 mph) in 2006 at Bonneville Salt Flats with unofficial top speed reaching 413 kilometres per hour (257 mph) using modified BAR 007 Formula 1 car. Speeds on ovals can range in constant excess of 210–220 miles per hour (340–350 km/h), and at Indianapolis in excess of 230 miles per hour (370 km/h). Some sources claim that in 1996, Paul Tracy recorded a trap speed of 256.948 miles per hour (413.518 km/h) at Michigan International Speedway.[citation needed] In 2000, Gil de Ferran set the one-lap qualifying record of 241.428 miles per hour (388.541 km/h) at California Speedway.[7] Even on tight non-oval street circuits such as the Grand Prix of Toronto, open-wheel Indy Cars attain speeds of 190 miles per hour (310 km/h).

Driving an open-wheel car is substantially different from driving a car with fenders. Virtually all Formula One and Indycar drivers spent some time in various open-wheel categories before joining either top series. Open-wheel vehicles, due to their light weight, aerodynamic capabilities, and powerful engines, are often considered the fastest racing vehicles available and among the most challenging to master. Wheel-to-wheel contact is dangerous, particularly when the forward edge of one tire contacts the rear of another tire: since the treads are moving in opposite directions (one upward, one downward) at the point of contact, both wheels rapidly decelerate, torquing the chassis of both cars and often causing one or both vehicles to be suddenly and powerfully flung upwards (the rear car tends to pitch forward, and the front car tends to pitch back.) An example of this is the 2005 Chicagoland crash of Ryan Briscoe with Alex Barron.

The lower weight of an open-wheel racecar allows for better performance. While the exposure of the wheels to the airstream causes a very high aerodynamic drag at high speeds, it allows improved cooling of the brakes, which is important on road courses with their frequent changes of pace.

Gallery

Safety

In 2018, several single seater series such as Formula One, Formula 2 (with their new Dallara F2 2018 chassis), and Formula E (with their new Spark SRT05e chassis) introduced a protection system to the cockpit called the "halo", a wishbone-shaped frame aimed to deflect debris away from a driver's head. Despite initial criticism, it showed some praise in the Formula 2 sprint race in Catalunya when Nirei Fukuzumi spun and had the back of his car land on fellow countryman Tadasuke Makino's halo. In the Formula 1 Belgian Grand Prix, McLaren driver Fernando Alonso was sent airborne after being hit from behind by the Renault of Nico Hülkenberg and struck the halo of Sauber driver Charles Leclerc, thereby saving the Monegasque driver from a very nasty incident.

In 2019, the newly-formed FIA Formula 3 Championship will introduce a halo to their new chassis which was unveiled at the 2018 Abu Dhabi Grand Prix.

  1. ^ Eric Brandt (11 July 2018). "Ariel Atom 4 Roadster Unveiled Packing 320-HP Honda Type R Engine". The Drive. Retrieved 9 August 2018.
  2. ^ swatson. "Harroun, Ray - Historic - 2000". Retrieved 17 April 2016.
  3. ^ "Ray Harroun Checks his Rear View Mirror". Retrieved 17 April 2016.
  4. ^ "1911 Marmon Wasp - Conceptcarz". conceptcarz.com. Retrieved 17 April 2016.
  5. ^ Davidson, Donald The Talk of Gasoline Alley (radio program). Accessed via WIBC (FM), 28 May 200
  6. ^ "Drivers hit record speeds in Mexico". Formula One Digital Media. Formula1.com. Oct 30, 2015. Retrieved 4 June 2016.
  7. ^ "De Ferran wins pole, sets record". Las Vegas Sun. October 28, 2000. Archived from the original on November 10, 2013.

See also



This article uses material from the Wikipedia article "Open-wheel car", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer