powered by CADENAS

Social Share

Amazon

Wireless router (9951 views - Electrical Engineering)

A wireless router is a device that performs the functions of a router and also includes the functions of a wireless access point. It is used to provide access to the Internet or a private computer network. Depending on the manufacturer and model, it can function in a wired local area network, in a wireless-only LAN, or in a mixed wired and wireless network.
Go to Article

Explanation by Hotspot Model

Youtube


    

Wireless router

Wireless router

A wireless router is a device that performs the functions of a router and also includes the functions of a wireless access point. It is used to provide access to the Internet or a private computer network. Depending on the manufacturer and model, it can function in a wired local area network, in a wireless-only LAN, or in a mixed wired and wireless network.

Features

Most current wireless routers have the following characteristics:

  • One or multiple NICs supporting Fast Ethernet or Gigabit Ethernet integrated into the main SoC.
    • Some newer routers feature Link Aggregation allowing two ports to be used together improving throughput and redundancy. [1]
  • One or multiple WNICs supporting a part of the IEEE 802.11-standard family also integrated into the main SoC or as separate chips on the printed circuit board. It also can be a distinct card connected over a MiniPCI or MiniPCIe interface.
    • So far the PHY-Chips for the WNICs are generally distinct chips on the PCB. Dependent on the mode the WNIC supports, i.e. 1T1R, 2T2R or 3T3R, one WNIC have up to 3 PHY-Chips connected to it. Each PHY-Chip is connected to a Hirose U.FL-connector on the PCB. A so-called pigtail cable connects the Hirose U.FL either to a RF connector, in which case the antenna can be changed or directly to the antenna, in which case it is integrated into the casing. Common are single-band (i.e. only for 2.4 GHz or only for 5 GHz), dual-band (i.e. for 2.4 and 5 GHz) and tri-band (i.e. for a single 2.4 GHz and two 5 GHz) antennas.
  • Often an Ethernet switch supporting Gigabit Ethernet or Fast Ethernet, with support for IEEE 802.1Q, integrated into the main SoC (MediaTek SoCs) or as separate Chip on the PCB.
  • Some wireless routers come with either xDSL modem, DOCSIS modem, LTE modem, or fiber optic modem integrated.
  • IEEE 802.11ac compliant or ready.
  • Some dual-band wireless routers operate the 2.4 GHz and 5 GHz bands simultaneously.
  • Many dual-band wireless routers have data transfer rates exceeding 300 Mbit/s (For 2.4 GHz band) and 450 Mbit/s (For 5 GHz band).[2]
  • Some wireless routers provide multiple streams allowing multiples of data transfer rates (i.e. a three-stream wireless router allows transfers of up to 1.3 Gbit/s on the 5 GHz bands).
  • The Wi-Fi clone button simplifies Wi-Fi configuration and builds a seamless unified home network, enabling Super Range Extension, which means it can automatically copy the SSID and Password of your router.[3]
  • Some wireless routers have one or two USB ports. For wireless routers having one USB port, it is designated for either printer or desktop/mobile external hard disk drive. For wireless routers having two USB ports, one is designated for the printer and the other one is designated for either desktop or mobile external hard disk drive.[4]
  • Some wireless routers have a USB port specifically designed for connecting mobile broadband modem,[5] [6] aside from connecting the wireless router to an Ethernet with xDSL or cable modem. So, can be inserted a mobile broadband USB adapter into the router to share the mobile broadband Internet connection through the wireless network.

List of data standards used in wireless routers

There are many data standards that have been introduced for wireless router technology. New standards have been created to accommodate the increasing need for faster wireless connections. Some wireless routers provide backward compatibility with older Wi-Fi technologies as many devices were manufactured for use with older standards. [7]

Notable manufacturers

Operating system

The most common operating system on such embedded devices is Linux. More seldomly, VxWorks is used. The devices are configured over a web user interface served by a light web server software running on the device. It is possible for a computer running a desktop operating system with appropriate software to act as a wireless router. This is commonly referred to as a SoftAP.

In 2003, Linksys was forced to open-source the firmware of its WRT54G router series (the best-selling routers of all time) after people on the Linux kernel mailing list discovered that it used GPL Linux code.[8] In 2008, Cisco was sued in Free Software Foundation, Inc. v. Cisco Systems, Inc due to similar issues with Linksys routers. Since then, various open-source projects have built on this foundation, including OpenWrt, DD-WRT, and Tomato.

In 2016, various manufacturers changed their firmware to block custom installations after an FCC ruling.[9] However, some companies plan to continue to officially support open-source firmware, including Linksys[10] and Asus.[9]

See also



This article uses material from the Wikipedia article "Wireless router", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced