Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Infantry tank | |
---|---|
Churchill tanks during the 2nd Battle of El Alamein | |
Type | Armoured fighting vehicle |
Place of origin | France and the United Kingdom |
Service history | |
In service | 1938–1945 |
Used by | French and British armies |
Wars | Second World War |
Era | |
---|---|
Country | |
Type |
The infantry tank was a concept developed by the United Kingdom and France in the years leading up to World War II. Infantry tanks were designed to support infantrymen in an attack. To achieve this, the vehicles were generally heavily armoured to allow them to operate in close concert with infantry even under heavy fire. The extra armour came at the expense of speed, which was not an issue when supporting relatively slow-moving foot soldiers.
Once an attack supported by infantry tanks had broken through heavily defended areas in the enemy lines, faster tanks such as cruiser or light tanks were expected to use their higher speed and longer range to operate far behind the front and cut lines of supply and communications.
The Infantry Tank was superseded by the Universal Tank concept which could adequately perform the roles of both infantry and cruiser tank, as represented by the Centurion which replaced both the Churchill and any Mediums or Cruisers then in service.
The experimental armoured formations of the British army were mostly equipped with the Vickers Medium Tank Mk I and Medium Mk II, which were judged obsolete by the 1930s; most of the vehicles were at the end of their mechanical life. It was impractical to build more because their road speed of only 18 mph (29 km/h) was too slow for manoeuvre warfare and their armament of a 3-pounder gun lacked the power to penetrate newer foreign tanks.[1] By 1931, experience with the Experimental Mechanized Force led to the report of the Kirke Committee and specifications for three types of tank, a medium tank with a small-calibre anti-tank gun and a machine-gun, a light tank armed with machine-guns for reconnaissance and to co-operate with medium tanks by engaging anti-tank guns. A close support tank armed with a gun firing high explosive and smoke shells to give covering fire for tank attacks was also specified.[2] The Wall Street Crash of 1929 and the Great Depression led to big reductions in the funds made available for the army. Money spent on tracked vehicles fell from £357,000 in 1931–32 to £301,000 in the year 1932–33 and exceeded the 1931 figure only in 1934–35.[3]
In May 1934, Lieutenant-General Hugh Elles was appointed Master-General of the Ordnance and Brigadier Percy Hobart, the Inspector, Royal Tank Corps, asked Vickers to design a tank for infantry co-operation, that could survive all existing anti-tank weapons and be cheap enough for mass production in peacetime. The next year, Vickers had a two-man tank design, with a machine-gun and powered by a civilian Ford V8 engine of 70 hp (52 kW). The prototype of October 1936 weighted 10 long tons (10 t) had a maximum speed of only 8 mph (13 km/h) but carried 60–65 mm (2.4–2.6 in) of armour and was mechanically reliable. The A11, Infantry Tank Mk I, was the first Infantry tank (I tank) and the first practical expression of the decision to split design into I tanks and cruiser tanks, with different functions and tactics, supplied to separate units and formations.[2][4]
The 1935 edition of the War Office publication, Field Service Regulations (FSR), containing the principles by which the army was to act to achieve objectives, was written by Major-General Archibald Wavell, made breakthrough the responsibility of infantry divisions with the support of Army Tank Battalions, equipped with specialised vehicles for infantry-artillery co-operation, the slow and heavy Infantry tanks. Once a breakthrough had been created, a Mobile Division containing a tank brigade with light and cruiser tanks, would advance through the gap and use the speed and range of its tanks to surprise the defender and attack flanks, headquarters and non-combatant units. By 1939, further amendments to FSR added counter-attacks on an enemy armoured breakthrough. (The codification of the difference between Infantry and cruiser tanks and their functions in FSR 1935, accidentally created an obstacle to all-arms co-operation that lasted long into the Second World War.) Defence against tanks could be achieved by troops finding physical obstacles and by controlling their own anti-tank guns. The obstacles could be woods and rivers or minefields as long as they were covered by fire from other weapons. In places lacking convenient terrain features, lines-of-communication troops would also need anti-tank guns and be trained to set up localities suitable for all-round defence[5]
The need for economy in the design and production of the A11, which was too small for a radio, led to work on a successor, the A12, Infantry Tank Mk II in 1936. Capable of 15 mph (24 km/h), the A12 was still slow but had 60–70 mm (2.4–2.8 in) of armour, making it almost invulnerable to tank guns and standard foreign guns like the German 37 mm Pak 36 anti-tank gun. The tank had a four-man crew and a turret big enough for a radio and a Ordnance QF 2-pounder high-velocity gun, firing solid projectiles capable of penetrating all 1939–1940 German tanks. Vickers and government factories could not take on the work and it was farmed out to a civilian firm, which lacked experience, designers and draftsmen. It took until 1939 to bring the A12 into production as the "Matilda II" and it had not gone into service when the war began, only 67 A11s having been delivered. When the Matilda was supplied to Army Tank Battalions it was an effective tank in the Battle of France and in the Western Desert Campaign, where it outclassed Italian tanks and was effective against standard Italian and German anti-tank guns from 1940–1941 but was later found to be too slow for the fast tempo that German panzer units could achieve and unable to engage the more powerful German anti-tank guns from long range with high explosive shells.[6][7][8]
Using later terminology, the infantry tank has been compared to a heavy tank, while the cruisers were compared to mediums, lights, or even armoured cars. This comparison can be misleading; late Second World War heavy tanks were intended to have superior anti-tank capabilities, which wasn't a focus of the traditional infantry tank.
The infantry tank was different from either the "heavy tank" or "breakthrough tank" concepts, although some pre-war multi-turreted heavy machines such as the Soviet T-35 and the German Neubaufahrzeug ( both taking some of their inspiration from the 1926 Vickers A1E1 Independent - an idea which was abandoned by the War Office in the late 1920s for lack of funding), which were similar, and with similar doctrines for their use. The Neubaufahrzeug was considered too slow for Blitzkrieg tactics and fell from favour. German, and to some extent Soviet, wartime doctrine shifted towards faster medium and heavy tanks fighting large multi-tank battles, with the role of the infantry tank in the assault taken by simpler Sturmgeschütz self-propelled gun.
An important difference, however, was that heavy tanks were generally very well armed, while infantry tanks were not necessarily better armed than other types. For example, the Soviet 45-ton KV-1 heavy tank and 25-ton British Matilda II infantry tank were deployed at about the same time in 1940. These two models had similar levels of armour protection and mobility, but the KV's (low velocity) 76.2 mm main gun was much larger than the Matilda's 2-pounder (40mm).
In British practice, the main armament of the infantry tank went in three phases. The pre-Dunkirk British Army Matilda I had only a single heavy Vickers machine gun, a compromise forced by the lightness of its chassis and its target cost. The Matilda II gained a capable anti-tank capacity for its time, with the 2-pounder, but these were only issued with solid-shot (i.e. non-explosive) for anti-tank use and had little effect as artillery when providing close support for the infantry. A separate variant of the Matilda was fitted with a 3-inch howitzer. The ultimate evolution of the British infantry tank concept began with the Churchill Mk I, where a hull-mounted 3-inch howitzer could support infantry assaults with HE shells while the turret had a 2-pdr for use against other tanks.[a] As the increasing size of tanks, and their turret ring diameters, allowed such a howitzer to be turret-mounted in vehicles such as the Crusader Close Support (CS) and Centaur CS cruiser tanks.[b]
Year | Light | I tank/ Cruiser |
Total |
---|---|---|---|
1938 4th Qtr |
169 | 29 | 198 |
1939 | 734 | 235 | 969 |
1940 to June |
140 | 418 | 558 |
Total | 1,043 | 682 | 1,725 |
Since infantry tanks were to work at the pace of infantry units which would be attacking on foot, high speed was not a requirement and they were able to carry heavier armour. The first two purpose-designed infantry tanks, the A.11 Matilda Mark I armed with a heavy machine-gun and A.12 Matilda Mark II with a heavy machine gun and 2-pounder anti-tank gun. The Mark I had been ordered in 1938, but it had become clear that a better-armed tank would be needed and the Mark II, was already under design and would be ordered in mid-1938.
The two saw action in the Battle of France where in the Battle of Arras they caused a shock to the German panzer units. Losses of the Mark I in France were not replaced but the Mark II Matilda remained in production.
Infantry and cruiser tanks were expected to engage enemy tanks, hence the use of both the 2-pounder and then 6-pounder on both.[10]
They were followed into service by the Infantry tank Mk III Valentine tank and A.22 Infantry Tank Mk IV Churchill designs. The Valentine proved to be difficult to develop further but the Churchill went through successive variants and served up to the end of the war.
As British cruiser tank designs developed into larger vehicles with more powerful engines, they could carry bigger guns and more armour and yet still achieve high speeds. At the end of the war the cruiser tank lineage led to the "universal tank" in the form of the Centurion.[11]
In practice the British did not operate only infantry and cruiser tanks. Lack of production capacity meant the large scale adoption of US medium tanks.
During the inter-war years, the French Army adopted three light tanks in the infantry tank role. These were the Hotchkiss H35, the Renault R35 and the FCM 36. All three had two–man crews and were similar to the Matilda I in terms of size, weight and armour. However, they were better armed, having 37mm guns as well as co-axial machine guns.
In practice, although able to resist hits from other tanks and anti-tank guns, and designed for good, albeit slow, cross-country performance, the separation of tank functions into specialised areas such as infantry and cruiser types was not effective. Invariably the cruisers ended up meeting enemy tanks in combat, while the infantry tanks were the only ones present when a breakthrough was accomplished. The infantry tank idea faded as tank design progressed during the war. It was eventually replaced outright with the general acceptance of the 'universal tank' idea.
The concept was also employed by the other big tank-producing nation of the 1930s: the Soviet Union, as exemplified by the T-26. The T-26 was a light tank assigned to infantry units and thus fulfilled the infantry tank role. It had the relatively thin armour of a light tank, but with a potent 45 mm gun. Their BT tanks were the fast cruiser types.
Germany had its separate Panzerwaffe; the German infantry used phased out Panzerkampfwagen Is in its Independent Tank Brigades. This is often seen as reflecting some explicit doctrine; in reality it was simply caused by a lack of funds, tank production not having any priority. When more money became available the Sturmgeschütz III was taken into use by the artillery, in its original role of an infantry close support vehicle—the counterpart of the Allied Infantry tanks.
The U.S. disbanded its Tank Corps in 1919 and the National Defense Act 1920 defined tanks as an infantry responsibility and their purpose was to support the infantry. Few funds were available for tank development and only around two experimental tanks were produced a year. In the early 1930s, the promotion of mechanisation of the cavalry began. For political expediency and to avoid conflicting with the 1920 law, the tanks developed for the cavalry based on the infantry's light tanks were called "Combat Cars".[12]
Medium tank designs produced were focused on infantry support. The M2 Medium Tank designed in the late 1930s had multiple machine guns to give all round fire and a 37 mm anti-tank gun. However before mass production could start the Battle of France had already shown that a 75 mm gun was needed.[13]
The Japanese Imperial Army used tankettes as infantry support in the 1930s and into World War II. These small light tanks were also referred to as armoured cars (though they usually only held a crew of two and appeared like miniature tanks) and included the Type 92, Type 94, and Type 97 "TK" vehicles. Japanese troops would ride on the fast-moving tankettes, use them as tractors to pull equipment, or otherwise use them in support roles. Only later versions of the tankettes came equipped with anything other than machine guns. These vehicles were successful supporting infantry in campaigns against China in the 1930s but were not designed to engage other tanks with armour that was meant to repel only small arms fire.
The Fiat 3000 was the first tank to be produced in series in Italy. It was to be the standard tank of the emerging Italian armored units after World War I. The 3000 was based on the French Renault FT. The design was accepted with deliveries to begin in May 1919, but the end of the war caused the original order to be cancelled and only 100 were delivered. The first Fiat 3000s entered service in 1921 and were officially designated as the carro d'assalto Fiat 3000, Mod. 21. ("Fiat 3000 assault tank, Model 21").The up-gunned version of the Fiat 3000, armed with a 37/40 gun, was tested in 1929 and was officially adopted in 1930 with the designation of carro d'assalto Fiat 3000, Mod. 30. The Model 30, in addition to its improved armament, also differed from the Model 21 in that it had a more powerful engine, improved suspension, different engine compartment silhouette, and the external stores were stowed differently. Some Model 30s were also produced with two 6.5 mm machine guns as main armament, as on the Model 21, in lieu of the 37 mm gun. A limited number of Model 21 vehicles were exported to Albania, Latvia and Abyssinia (Ethiopia) prior to 1930. Some self-propelled guns were used for close support purposes.
During the first few years of the war, the Panzer III and Panzer IV functioned in the same way as a cruiser tank and infantry tank respectively, with the Panzer III's 37mm and 50mm cannons used to attack enemy tanks, and the Panzer IV's short 75mm cannon used to support infantry attacks. These roles began to break down during Operation Barbarossa when German forces met the Russian T-34 and KV-1 tanks and struggled to penetrate their armor, forcing design and production changes.
This led to the up-arming of the Panzer IV to a long barreled 75mm cannon, which could fire both armor piercing rounds and high explosive rounds, giving the tank a dual role. The Panzer III was progressively removed from frontline armor units and relegated to a support role, with production ending in 1943.
Despite the concept of splitting tanks into infantry and cruiser roles being an instance of the general economic principle of division of labour in mechanisation, during World War II, its application in mechanised warfare proved to be hugely inefficient in terms of technical development, production, maintenance, logistics and — worst of all — tactical flexibility. Therefore it was not surprising that during the war, it was progressively abandoned by all the major belligerent countries.[citation needed]
This article uses material from the Wikipedia article "Infantry tank", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht