Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 2.0 de (Lothar Spurzem).
Microcar is a term often used for the smallest size of cars,[1] with three or four wheels and often an engine smaller than 700 cc (43 cu in). Specific types of microcars include bubble cars, cycle cars, quadricycles and voiturettes, and the Japanese equivalent is the kei car.
Microcars are often covered by separate regulations to normal cars, having relaxed requirements for registration and licensing. Most microcars are powered by petrol or diesel engines, however electric-powered microcars have become more common in recent years.
Voiturette is a term used by some small cars and tricycles manufactured from 1895 to 1910.
Cyclecars are a type of small, lightweight and inexpensive car manufactured mainly between 1910 and the late 1920s.
The first cars to be described as microcars (earlier equivalents were called voiturettes or cyclecars) were built in the United Kingdom and Germany following World War II and remained popular until the 1960s. These cars were originally called minicars, however they later became known as microcars.
France also produced large numbers of similar tiny vehicles called voiturettes, however these were rarely sold abroad.
A common characteristic of these microcars is an engine displacement of less than 700 cc (43 cu in),[2][3][4] although several cars with engines up to 1,000 cc (61 cu in) are also considered to be microcars.[5][1](p7) Often the engine was originally designed for a motorcycle.[6] Microcars have three or four wheels.[3]
The origin of these microcars is in the years following World War II, when motorcycles were common.[7](p7) To provide better weather protection, three-wheeled microcars began increasing in popularity in the United Kingdom, where they could be driven using a motorcycle licence.[3][8] Microcars also became popular in Europe, due to their greater fuel efficiency than larger cars.[6][9] One of the first microcars was the 1949 Bond Minicar.
Micro cars became popular in Europe at that time as a demand for cheap personal motorised transport emerged and fuel prices were high due in part to the 1956 Suez Crisis. Most of them were three-wheelers, which in many places qualified them for inexpensive taxes and licensing as motorcycles.
The microcar boom lasted until the late 1950s, when larger cars regained popularity[9][10] The 1959 introduction of the Mini, which provided greater size and performance at an affordable price, contributed to the decline in popularity of microcars.[3] Production of microcars had largely ceased by the end of the 1960s, due to competition from the Mini, Citroen 2CV, Fiat 500 and Renault 4.
Several microcars of the 1950s and 1960s— mostly produced in Germany— were nicknamed bubble cars.[11][12] This was due to the aircraft-style bubble canopies of cars like the Messerschmitt KR175, Messerschmitt KR200 and the FMR Tg500. Other microcars, such as the Isetta, also had a bubble-like appearance.
German manufacturers bubble cars included former military aircraft manufacturers Messerschmitt and Heinkel. BMW manufactured the Italian Iso Rivolta Isetta under licence, using an engine from one of their own motorcycles.
The United Kingdom had licence-built right-hand drive versions of the Heinkel Kabine and the Isetta. The British version of the Isetta was built with only one rear wheel instead of the narrow-tracked pair of wheels in the normal Isetta design in order to take advantage of the three-wheel vehicle laws in the United Kingdom. There were also indigenous British three-wheeled microcars, including the Peel Trident.
Examples include the Citroën Prototype C, FMR Tg500, Fuldamobil, Heinkel Kabine, Isetta, Messerschmitt KR175, Messerschmitt KR200, Peel P50, Peel Trident and Trojan 200.
Recent microcars include the 2001 Aixam 5xx series. The Smart Fortwo is often called a microcar in the United States;[13][14] however it requires a car licence to drive, unlike most microcars.
Electric-powered microcars which have reached production include the 1987 CityEl, the 1990 Automobiles ERAD Spacia, the 1999 Corbin Sparrow, the 2001 REVAi, the 2009 Tazzari Zero and the 2011 Peel P50.
The European Union introduced the quadricycle category in 1992. In several European countries since then, microcars are classified by governments separately to normal cars, sometimes using the same regulations as motorcycles or mopeds. Therefore, compared with normal cars, microcars often have relaxed requirements for registration and licensing, and can be subject to lower taxes and insurance costs.
Kei car is the Japanese legal category for the smallest and most limited power, highway-legal motor vehicles, including passenger cars (kei cars or kei-class cars), microvans, and Kei trucks (kei-class pickup trucks).
There are also a variety of microcar trucks, usually of the "forward control" or van style to provide more cargo room. These might be used for local deliveries on narrow streets that are unsuited to larger vehicles. The Piaggio Ape is a three-wheeled example.[15]
Wikimedia Commons has media related to Microcars. |
This article uses material from the Wikipedia article "Microcar", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer