Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 4.0 (Photograph by D Ramey Logan).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Air racing" – news · newspapers · books · scholar · JSTOR (October 2017) (Learn how and when to remove this template message) |
Air racing is a highly specialised type of motorsport that involves airplanes or other types of aircraft that compete over a fixed course, with the winner either returning the shortest time, the one to complete it with the most points, or to come closest to a previously estimated time.
The first 'heavier-than-air' air race was held on 23 May 1909 - the Prix de Lagatinerie, at the Port-Aviation airport south of Paris, France. Four pilots entered the race, two started, but nobody completed the full race distance; though this was not unexpected, as the rules specified that whoever travelled furthest would be the winner if no-one completed the race. Léon Delagrange, who covered slightly more than half of the ten 1.2-kilometre (0.75 mi; 0.65 nmi) laps was declared the winner.[1]
Some other minor events were held before the Grande Semaine d'Aviation de la Champagne in 22-29 August 1909 at Reims, France. This was the first major international flying event, drawing the most important aircraft makers and pilots of the era, as well as celebrities and royalty. The premier event — the first Gordon Bennett Trophy competition — was won by Glenn Curtiss, who beat second-place finisher Louis Blériot by five seconds. Curtiss was named 'Champion Air Racer of the World'.
The first air race in the United States was held at Dominguez Field, just south of Los Angeles, from 10 to 20 January 1910, organised by pilots A. Roy Knabenshue and Charles Willard. Funding was raised from railroad magnate Henry Huntington, and the Los Angeles Merchants and Manufacturers Association. William Randolph Hearst carried coverage of the event in his Los Angeles Examiner, and hired a hot air balloon with a promotional parse touting his newspaper. The event attracted 43 entrants, of which 16 appeared. It was there that aviation pioneer and military pilot Jimmy Doolittle, then thirteen, saw his first airplane.[2]
In the years before the First World War, popular interest in aviation led to a large number of air races in Europe; including the 1911 Circuit of Europe race, the Daily Mail Circuit of Britain Air Race, and the Aerial Derby.
In 1913, the first Schneider Trophy seaplane race was held. When the competition was resumed after the war, it was significant in advancing aeroplane design, particularly in the fields of aerodynamics and engine design, and would show its results in the best fighters of World War II.
On 19 October 1919, the Army Transcontinental Air Race began along a 2,700 mi (2,346 nmi; 4,345 km) route from Long Island, New York to San Francisco, California, and back, which would see widespread carnage; including seven fatalities (two en route to the race). Of the 48 aircraft that started, 33 would complete the double crossing of the continent.[3]
In 1921, the United States instituted the National Air Meets, which became the National Air Races in 1924. In 1929, the Women's Air Derby, nicknamed the 'Powder Puff Derby', became a part of the National Air Races circuit. The National Air Races lasted until 1949. The Cleveland Air Races was another important event. In 1947, an All-Woman Transcontinental Air Race, also dubbed the Powder Puff Derby was established, running until 1977.
In 1934, the MacRobertson Air Race from England to Australia took place, with the winning de Havilland Comet flown by C. W. A. Scott and Tom Campbell Black.
In 1964, Bill Stead, a Nevada rancher, pilot, and unlimited hydroplane racing champion, organised the first Reno Air Races at a small dirt strip called the Sky Ranch, located between Sparks, Nevada, and Pyramid Lake. The National Championship Air Races were soon moved to the Reno Stead Airport, and have been held there every September since 1966. The five-day event attracts around 200,000 people, and includes racing around courses marked out by pylons for six classes of aircraft: Unlimited, Formula One, Sport Biplane, AT-6, Sport, and Jet. It also features civil airshow acts, military flight demonstrations, and a large static aircraft display. Other promoters have run pylon racing events across the USA and Canada, including races in Las Vegas, NV in 1965, Lancaster, CA in 1965 and 1966, Mojave, California in 1970-71, and 1973–79; at Cape May, NJ in 1971, San Diego, CA in 1971, Miami, FL in 1973 and 1979, Moose Jaw, Saskatchewan in 1984; Hamilton Field, California, in 1988; at Dallas, TX in 1990, in Denver, CO in 1990 and 1992, in Kansas City in 1993, in Phoenix, Arizona in 1994 and 1995; and in Tunica, Mississippi in 2005. Numerous other venues across the United States, Canada, and Mexico have also hosted events featuring the smaller Formula One and Biplane classes.
In 1970, American Formula One racing was exported to Europe (Great Britain, and then to France), where almost as many races have been held as in the U.S.A. Also in 1970, the California 1000 Air Race started at the Mojave Airport with a 66 lap unlimited air race that featured a Douglas DC-7, with one aircraft completing the circuit.[4][5]
Red Bull has created a series called the Red Bull Air Race World Championship, in which competitors fly individually between pairs of pylons, while performing prescribed manoeuvres. Usually held over water near large cities, the sport has attracted large crowds and renewed media interest in air racing.
Aero GP has multiple aircraft racing together pik around pylons, and is based in Europe where it has held an air race each year since 2005.
Powered paragliding or paramotor races have been organised by the Parabatix Sky Racers made up of the world's top paramotor pilots. The first occurring on 4 September 2010 in an airfield in Montauban, Southern France. These are foot-launched ram-air wings powered by small two-stroke engines, and allow for much smaller race venues such as city parks or beaches, where the audience can see the pilots up close as they carry out spectacular manoeuvres swooping close to the ground-pylons during the race.[6]
competition | 1st race |
primary description | course | field | sanctioning body |
---|---|---|---|---|---|
Gordon Bennett Trophy | 1909 | time trials | Pilon, rally (1920) | open | |
Daily Mail aviation prizes | 1910 | various events to encourage aviation | point to point & circuit | open | Daily Mail |
Coupe Deutsch de la Meurthe | 1912 | encourage aviation | cross-country circuit | open | Aéro-Club de France |
Schneider Trophy | 1913 | encourage seaplane development | triangle | seaplanes | Fédération Aéronautique Internationale (FAI) |
Pulitzer & National Air Races | 1920 | unlimited | pylon | open | |
King's Cup Race | 1922 | handicapped race for light aircraft | cross-country (UK) | British pilots | King George V |
Dole Derby | 1927 | California to Hawaii | point to point | open | National Aeronautic Association (NAA) |
Challenge International de Tourisme | 1929 | encourage light aircraft development | technical trials & rally | light aircraft | Fédération Aéronautique Internationale (FAI) |
Thompson Trophy | 1929 | unlimited | pylon | open | National Aeronautics Association (NAA) |
Women's Air Derby | 1929 | unlimited | transcontinental (US) | female pilots | |
Bendix Trophy | 1931 | unlimited | transcontinental (US) | open | |
MacRobertson Air Race | 1934 | commemorate 1934 Melbourne Centennial | intercontinental (UK to Australia) | open | Royal Aero Club (RAC) |
Formula V Air Racing | 1977 | provide affordable racing | circuit | formula aircraft | Formula V Air Racing Association |
race | 1st race |
description | sanctioning body |
---|---|---|---|
Aero GP | 2005 | pylon races plus additional disciplines | |
Air Race Classic | 1977 | All women's cross country race, with handicapped speed planes; courses change every year with at min. 2100 NM routes, completed within 4 days; previously known as the All Women's Transcontinental Air Race (AWTAR) which in turn was popularly known as the Powder Puff Derby - founded after the first Women's Air Derby of 1929 | |
Air Race 1 World Cup | 2014 | pylon races, 8 aircraft together, first one across the line wins | |
Air Race E | 2020 | Airbus-sponsored, similar to the Air Race 1 with experimental electric aircraft | |
British Air Racing Championship | 1952 | handicapped air races | Royal Aero Club Records Racing and Rally Association |
European Air Racing Championship | 2000 | handicapped air races | Royal Aero Club Records Racing and Rally Association |
Hayward Rally | 1965 | air race in Western U.S., courses vary every year | |
Parabatix Sky Racers | 2010 | Paramotor precision air races, pylon racing, interactive ground obstacles, one & two aircraft at a time | |
Red Bull Air Race World Championship | 2003 | pylon races, one plane at a time | |
Reno Air Races | 1964 | only remaining unlimited class pylon race, also includes the famous class of Formula One air races | |
Schneider Trophy | 1981 | landplanes, revived commemoration of original races | Royal Aero Club Records Racing and Rally Association |
Restricting aircraft to a specific type or design creates a competition that focuses on pilot skill. Air racing events such as the Reno air races, incorporate multiple classes or aircraft. These may be defined by the race organiser, or by a sanctioned group. Some air races are limited to a single class.[7] Classes used at the Reno races are as follows:
class | first race |
primary description | course | sanctioning body |
---|---|---|---|---|
T-6 Air Racing | 1946 | T-6/Harvard/SNJ with a P&W R-1340-AN-1 engine | pylon | |
Biplane Air Racing | 1964 | 360 cubic inches (5,899 cubic centimetres) engines, mostly Pitts Specials | pylon | Professional Race Pilots Association biplane division |
Formula One Air Racing | 1970 | 200 cubic inches (3,277 cubic centimetres) engines | pylon | Fédération Aéronautique Internationale (FAI) |
Formula V Air Racing | 1972 | 98 cubic inches (1,606 cubic centimetres) Volkswagen engines | pylon | (defunct) |
Sport Class Racing | 1998 | experimental piston powered aircraft with engines up to 1,000 Cubic Inches and capable of a 200 MPH minimum qualification lap speed. | pylon | Sport Class |
Unlimited Air Racing | 1964 | Generally standard or modified WWII fighters, i.e., P-51 Mustang, F-8F Bearcat, Hawker Sea Furys | pylon | NAG[expand acronym] |
Jet Air Racing | 2002 | L-39, L-29 Provost, Iskra, and de Havilland Vampires | pylon | Racing Jets, Inc. |
This article uses material from the Wikipedia article "Air racing", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht