powered by CADENAS

Social Share

Amazon

Koenigsegg Agera (13305 views - Cars & Motorbikes & Trucks)

The Koenigsegg Agera is a mid-engined sports car produced by Swedish car manufacturer Koenigsegg. It is a successor to the Koenigsegg CCX/CCXR. The name comes from the Swedish verb 'agera' which means "to act" or in imperative form "(You) act!". It was named Hypercar of the Year in 2010 by Top Gear magazine. The Agera RS model is the world's fastest production car, setting a record in 2017 with a GPS-verified two-way average top speed of 447 km/h (278 mph) and a fastest straight-line speed of 458 km/h (285 mph).The Agera ceased production in July 2018 with the unveiling of the two final edition cars at the 2018 Goodwood Festival of Speed.
Go to Article

Explanation by Hotspot Model

Youtube


    

Koenigsegg Agera

Koenigsegg Agera

Koenigsegg Agera

Licensed under Creative Commons Attribution 2.0 (Edvvc from London, UK).

Koenigsegg Agera
Overview
ManufacturerKoenigsegg Automotive AB
ProductionMarch 2011– July 2018
AssemblyÄngelholm, Sweden
DesignerChristian von Koenigsegg
Body and chassis
ClassSports car (S)
Body style2-door targa top
LayoutRear mid-engine, rear-wheel-drive
DoorsDihedral synchro-helix actuation
Powertrain
Engine5.0 L (305 cu in; 5,000 cc) twin-turbocharged V8
Power output
  • Standard: 960 PS (706 kW; 947 hp)
  • Agera R: 1,140 PS (838 kW; 1,124 hp)
  • Agera S: 1,030 PS (758 kW; 1,016 hp)
  • Agera RS: 1,176 PS (865 kW; 1,160 hp)
    1,360 PS (1,000 kW; 1,341 hp) (with optional 1MW package)
  • One:1 / Agera Final: 1,360 PS (1,000 kW; 1,341 hp)
Transmission7-speed dual clutch
Dimensions
Wheelbase2,662 mm (104.8 in)
Length4,293 mm (169.0 in)
Width1,996 mm (78.6 in)
Height1,120 mm (44.1 in)
Curb weight
  • Standard/Agera R/Agera S:
    1,435 kg (3,164 lb)
    1,330 kg (2,932 lb) dry[1]
  • One:1:
    1,360 kg (2,998 lb)[2]
  • Agera RS / Agera Final:
    1,395 kg (3,075 lb)
    1,295 kg (2,855 lb) dry[3]
Chronology
PredecessorKoenigsegg CCX

The Koenigsegg Agera is a mid-engined sports car produced by Swedish car manufacturer Koenigsegg. It is a successor to the Koenigsegg CCX/CCXR. The name comes from the Swedish verb 'agera' which means "to act" or in imperative form "(You) act!".

It was named Hypercar of the Year in 2010 by Top Gear magazine.[4] The Agera RS model is the world's fastest production car, setting a record in 2017 with a GPS-verified two-way average top speed of 447 km/h (278 mph) and a fastest straight-line speed of 458 km/h (285 mph).[5]

The Agera ceased production in July 2018 with the unveiling of the two final edition cars at the 2018 Goodwood Festival of Speed.[6]

Specifications and performance

Early development

In early development, the car was fitted with a 4.7-litre V8 engine with fixed-vane twin-turbochargers,[7] but the engine was replaced with a 5.0-litre twin-turbocharged V8 for the production version of the car.

Engine and transmission

The Agera is powered by an in-house developed 5.0-litre twin-turbocharged V8 engine which generates a maximum power output of 960 PS (947 hp; 706 kW) at 6,900 rpm and 1,100 N⋅m (811 lbf⋅ft) of torque at 4,000 rpm.[8] The total weight of the engine is only 197 kg (434 lb) due to a carbon fibre inlet manifold and aluminium construction.[9] The transmission is a specially developed 7-speed dual-clutch with paddle shifters. It is the first dual-clutch transmission to feature only one input shaft. The second clutch slows down the input shaft during up shifts in order to reduce the time it takes to synchronise the next gear, resulting in faster shift times. Most notably, the transmission weighs only 81 kg (179 lb).[9]

Performance (manufacturer claimed data)

  • 0–100 km/h (0–62 mph) in 2.8 seconds[10]
  • 0–200 km/h (0–124 mph) in 8.0 seconds[10]
  • 0–200–0 km/h (0–124–0 mph) in 13.5 seconds[10]

The top speed for the production model is claimed to be 400 km/h (249 mph).[8]

Exterior and interior

The Agera has a body made from impregnated carbon fibre/kevlar with lightweight reinforcements. The car's hardtop roof is stowable under the front hood lid. The chassis is also made out of carbon fibre with an aluminum honeycomb structure that comes with integrated fuel tanks for optimal weight distribution and safety. The rear wing is electronically adjustable with auto setting or manual control in order to have as little compromise as possible between low drag and downforce, depending on driving conditions.[11] The Agera comes with forged aluminum wheels with centre locking nuts, measuring 19-inch on the front and 20-inch on the rear and wrapped in a set of Michelin Super Sport tyres that can be used for speeds of up to 420 km/h (260 mph). Other notable features include the trademark Dihedral synchro helix actuation doors, a new traction control system, LED lighting, blue hood stripes that continue on through the cockpit of the car and a custom interior with a new "Ghost light" lighting system, which uses carbon nanotubes in a unique configuration to shine through the car's aluminum buttons.[12]

Variants

Koenigsegg Agera R (2011–2014)

The Agera R made its debut at the March 2011 Geneva Motor Show with a Speed Racer livery, and special Michelin tyres. It can accelerate from 0–100 km/h (0–62 mph) in 2.8 seconds and reach a theoretical top speed of 439 km/h (273 mph). The Agera R has a drag coefficient of Cd=0.37, or Cd=0.33 at high speed due to its adaptive rear wing, while producing 300 kg (660 lb) of downforce at 250 km/h (155 mph). This adaptive rear wing system is lighter than conventional hydraulic/electrical adaptive systems, and has the unique ability to compensate for head/tailwind due to its spring-loaded design. Furthermore, the pylons holding the wing play not only a role in the Agera R's aerodynamic performance, but also assist in extracting hot air from the engine bay.[10]

On 2 September 2011, during test sessions in Ängelholm, the Agera R broke six world land speed records for a production car, including 0–300 km/h (0–186 mph) in 14.53 seconds, and 0–300–0 km/h in only 21.19 seconds.[13] The braking performance required to maintain this record is enabled in part by the Agera's stability, demonstrated by Koenigsegg test driver and drivetrain technician Robert Serwanski, who was recorded by passenger Rob Ferretti (founder of the group "Super Speeders") braking from 300 km/h to 0 without holding the steering wheel.[14]

The Agera R can produce lateral cornering forces of 1.60 G,[15] due to a combination of mechanical balance and high levels of grip from the specially developed Michelin Supersport tyres.

The 2013 version of the Agera R premiered at the 2012 Geneva Motor Show. Upgrades included carbon fibre wheels, enhanced aerodynamics, and engine upgrades allowing the Agera R's twin-turbo V8 engine to produce 1,140 PS (1,124 hp; 838 kW) at 7,100 rpm and 1,200 N⋅m (885 lb⋅ft) of torque at 4,100 rpm on E85 fuel.[16] Koenigsegg's Flex Fuel Sensor technology allows the ECU to respond to varying fuel qualities and alcohol content by reducing power levels as a means of protecting the engine. On standard low-octane fuels, power is reduced to 960 PS (706 kW; 947 hp).[15]

The Agera R was featured prominently in the Need for Speed franchise, prominently in Criterion Games' Need for Speed: Most Wanted (2012), Ghost Games' Need for Speed Rivals (2013), and the 2014 film Need for Speed. It is also featured in the 2013 mobile game Real Racing 3. All the three Agera R's featured in the film Need for Speed were replicas.[17]

Koenigsegg Agera S (2013–2014)

Koenigsegg presented the Agera S model in 2013. Built for markets lacking E85 biofuel, the Agera S has most of the upgrades of the Agera R compared to the normal Agera including the dynamic wing, but is optimised for running on low-octane petrol generating a maximum power output of 1,030 PS; 758 kW (1,016 hp) and 1,100 N⋅m (811 lbf⋅ft) compared to the 960 PS; 706 kW (947 hp) and 1,100 N⋅m (811 lbf⋅ft) of an Agera R running on the same fuel.[18] In 2013, one Agera S was the 100th Koenigsegg ever produced, celebrated by a specially-built car with gold leaf inlays named "Hundra" (Swedish for hundred).[19]

On 10 June 2014, NAZA Swedish Motors launched the Agera S in Malaysia. It was the second Koenigsegg after the CCXR to arrive in the country, thus setting a new market for Koenigsegg. It was priced at RM5,000,000 before taxes and it was estimated that it will be priced at RM15,000,000 with government tax and duties—making it one of the most expensive cars in the country. The Agera S is the only model offered in Malaysia due to the absence of E85 biofuel there.[20]

Koenigsegg One:1 (2014–2016)

The Koenigsegg One:1 was presented at the March 2014 Geneva Motor Show.[21] Koenigsegg built six cars apart from the car presented at the Geneva Motor Show. All of which were already sold. Koenigsegg took two cars to the 2014 Goodwood Festival of Speed, where they were displayed alongside other hypercars such as the McLaren P1, the Ferrari LaFerrari, the Porsche 918 Spyder and the Pagani Huayra.

The car is fitted with a variant of the same 5.0 L twin-turbocharged V8 engine used in the other Agera variants. It generates a maximum power output of 1,360 PS (1,000 kW; 1,341 hp) at 7,500 rpm and 1,371 N⋅m (1,011 lb⋅ft) of torque at 6,000 rpm.[22] The transmission is a 7-speed dual clutch paddle shift as used in other variants of the Agera.

The name One:1 comes from the power-to-weight ratio (1,360 PS to 1360 kg) giving the car 1 PS per 1 kg weight. The 1,360 PS power output is the equivalent of one megawatt, which Koenigsegg claims makes the One:1 the 'world's first megacar'. The car is track focused as opposed to the previous cars made by Koenigsegg. Koenigsegg had to sacrifice a few things to be able to achieve their goal with the car. There is an airscoop on the removable roof and an extra set of radiators in the front compartment, so it would not have been possible to stow the roof in the boot like previous models. As such, Koenigsegg have taken advantage of this and modelled the front to create more downforce, which reduces boot capacity by 40%.

Koenigsegg Agera RS (2015–2018)

The Koenigsegg Agera RS was unveiled at the 2015 Geneva Motor Show, along with the prototype version of the Koenigsegg Regera. The Agera RS is an advanced version of the Agera R, implementing some of the new technology and features of the One:1 and combining the features of the Agera R and the Agera S.[23] Koenigsegg billed it as "the ultimate track tool" due to its lightweight features and track optimised technologies. The Agera RS produces 450 kg of downforce at 250 km/h. The 5.0-litre V8 engine now produces 1,176 PS; 865 kW (1,160 hp) on regular pump gasoline. The optional 1-megawatt package increases the engine's power to 1,360 PS; 1,000 kW (1,341 bhp). The Agera RS is limited to 25 units. Each Agera RS can be fully customised by its owner. Some of the customised versions of the Agera RS include: Agera RS Draken, Agera XS, Agera RS Gryphon, Agera RSR, Agera RS Naraya, Agera RS1 and Agera RS ML.

The 2018 Koenigsegg Agera RS has the following fuel economy in miles per gallon: 11 in the city and 18 on the highway (which averages to 13 MPG).[24]

The last Agera RS rolled off the production line on 4 April 2018.[25]

Koenigsegg Agera Final Edition (2016–2018)

At the 2016 Geneva Motor Show, a final three-car series of the Agera was announced as a final celebration of the Agera range and as the last models to wear the Agera badge. The cars can be fully customised and combined the Agera RS chassis with the One:1 engine. The first car to be unveiled was dubbed the 'One of One' and it featured a unique orange paint scheme with bare carbon and blue accents. The exterior of the car was complemented with a large adjustable rear wing from the One:1 and triple front canards along with a large front splitter.[26][27]

The other two distinct final edition cars were unveiled online in July 2018, dubbed as 'Agera FE Thor' and 'Agera FE Vader' respectively. Thor features a custom two-tone black paintwork consisting of crushed diamonds and white accents. The exterior features a large rear wing reminiscent to the one found on the Agera XS, and a different set of front canards, along with a large front splitter and a Le Mans-style central fin for improved downforce, setting it apart from the rest of the Agera models. Vader features the same crushed diamond paintwork with a bare carbon fibre centre along with white accents, incorporating the same rear wing as Thor but excludes the central fin. Both cars made their public appearance at the 2018 Goodwood Festival of Speed.[6]

Other special editions

There have been a number of special editions of the Agera built on customer request. Such special editions include:

  • Agera N[28]
  • Agera X[29]
  • Agera S Hundra (built to celebrate the production of 100 cars)[19]
  • Agera HH[30]
  • Agera RS Naraya[31]
  • Agera RS Draken[32]
  • Agera RS Valhall[33]
  • Agera RS1[32]
  • Agera RSR (3 special-edition Agera RS built for Japanese customers)[32]
  • Agera ML[34]
  • Agera HM[35]
  • Agera XS (2 special-edition Agera RS built for two US customers)[31]
  • Agera RSN[36]
  • Agera RS Phoenix[37]
  • Agera R Zijin[38]

Technical data

Koenigsegg Agera Koenigsegg Agera R Koenigsegg Agera S Koenigsegg One:1 Koenigsegg Agera RS Koenigsegg Agera Final
Production 2011 2011–2014 2012–2014 2014–2015 2015–2018 2016–2018
Engine 5.0L V8, Twin-turbo
Displacement 5,032 cm³ 5,065 cm³
Transmission Specially developed 7-speed dual-clutch
1 input shaft transmission with paddle-shift
Electronic differential
Power 960 PS (947 bhp; 706 kW) at 7,100 1,140 PS (1,124 bhp; 838 kW) at 6,900 1,030 PS (1,016 bhp; 758 kW) at 7,100 1,360 PS (1,341 bhp; 1,000 kW) at 7,500 1,176 PS (1,160 bhp; 865 kW) at 7,800
1,360 PS (1,341 bhp; 1,000 kW) at 7,500 (1 MW upgrade)
1,360 PS (1,341 bhp; 1,000 kW) at 7,500
Torque 1,100 N⋅m (811 lbf⋅ft) at 4,000 1,200 N⋅m (885 lbf⋅ft) at 4,100 1,100 N⋅m (811 lbf⋅ft) at 4,100 1,370 N⋅m (1,010 lbf⋅ft) at 6,000 1,280 N⋅m (944 lbf⋅ft) at 4,100
1,370 N⋅m (1,010 lbf⋅ft) at 6,000 (1 MW upgrade)
1,370 N⋅m (1,010 lbf⋅ft) at 6,000
RPM limiter 7,500/min 8,250/min
0–100 km/h

(62 mph)

3 sec 2.8 sec 2.9 sec ~ 2.8 sec ~ 2.9 sec[39] (1 MW upgrade)
0–200 km/h

(124 mph)

8 sec 7.8 sec 7.9 sec 6.6 sec ~6.9 sec[39](1 MW upgrade)
0–300 km/h

(186 mph)

14.5 sec 11.92 sec
Curb weight (kg) / (lb)
All fluids, 50% fuel
1,435 / 3,163 1,435 / 3,163 1,415 / 3,120 1,360 / 2,998 1,395 / 3,075 1,395 / 3,075

World records

World records set on 8 June 2015 with a Koenigsegg One:1[40][41]

Record Time
0–300 km/h 11.92 sec
0–200 mph 14.328 sec
300–0 km/h 6.03 sec
200–0 mph 6.384 sec
0–300–0 km/h 17.95 sec
0–200–0 mph 20.71 sec

On 1 October 2017, the Agera RS made the 0–400–0 km/h (0–249–0 mph) record in 36.44 seconds, 5.56 seconds faster than the record made by the Bugatti Chiron. The record was achieved on an old Danish air base in Vandel, Denmark. The car was driven by Koenigsegg test driver Niklas Lilja. Koenigsegg mentioned that during the record run, the car accelerated from 0–400 km/h in 26.88 seconds over a distance of 1,958 metres and decelerated in 9.56 seconds over a distance of 483 metres. The total distance used for the record was 2,441 metres. During the speed record run on 4 November 2017, Koenigsegg also broke their previous 0–400–0 km/h record by 2.57 seconds.[42]

Record Time
0–400–0 km/h 36.44 sec
0–400–0 km/h 33.29 sec

On 4 November 2017, Koenigsegg made the production car speed record with an Agera RS recording an average speed of 447 km/h (278 mph). The car achieved a speed of 458 km/h (285 mph) during its northbound run and 436 km/h (271 mph) during its southbound (return run). Official confirmation of the record by Guinness World Records still awaits. The car was driven by Koenigsegg test driver Niklas Lilja. The record run was made in opposite directions on an 18-kilometre (11 mi) section of Nevada State Route 160 between Las Vegas and Pahrump in the United States which was closed specifically for that purpose.[43]

Record Speed (average)
Agera RS 277.9 mph (447.2 km/h)[44]

Successor

The successor of the Agera will be unveiled at the 2019 Geneva Motor Show. The potential replacement was shown to prospective buyers via VR in an event held in Australia by the company.[45]

  1. ^ "Koenigsegg Agera". Koenigsegg Automotive AB. Retrieved 4 March 2015.
  2. ^ "Koenigsegg One:1". Koenigsegg Automotive AB. Retrieved 4 March 2015.
  3. ^ "Koenigsegg Agera RS". Koenigsegg Automotive AB. Retrieved 4 March 2015.
  4. ^ Philip, Sam (20 April 2011). "2010 TopGear Awards: Hypercar of the Year". Top Gear. Retrieved 5 September 2011.
  5. ^ "Koenigsegg's Top Speed Was 285 MPH on the Nevada Highway". Road and Track. Retrieved 29 December 2017.
  6. ^ a b Jeff Glucker (10 July 2018). "Final Koenigsegg Ageras named Thor and Vader". Motorauthority. Retrieved 17 July 2018.
  7. ^ Thomas, Bill (1 December 2010). "Bug catcher: Koenigsegg Agera". Top Gear. Retrieved 5 September 2011.
  8. ^ a b "Specifications, Agera". Retrieved 31 December 2017.
  9. ^ a b Card, Harrison (5 July 2011). "Koenigsegg Agera Rocks the Super Car World". Auto Trends. Archived from the original on 10 September 2011. Retrieved 5 September 2011.
  10. ^ a b c d "Koenigsegg Agera". Koenigsegg. Retrieved 8 May 2012.
  11. ^ "Koenigsegg Agera Price, Specs & More". RSportsCars.com. Archived from the original on 7 October 2011. Retrieved 10 October 2011.
  12. ^ Wood, Colum (3 March 2010). "Geneva 2010: Koenigsegg Agera Celebrates 15 Years of a Timeless Design". Auto Guide. Retrieved 5 September 2011.
  13. ^ Korzeniewski, Jeremy (30 November 2011). "Koenigsegg Agera gets official Guinness World Record for quickest 0-300-0 km/h". Retrieved 28 April 2014..
  14. ^ Okulski, Travis (16 October 2013). "Agera R Is Basically Idiot Proof". Jalopnik. Retrieved 29 April 2014.
  15. ^ a b "Koenigsegg Agera R". Koenigsegg. 9 March 2013. Retrieved 9 March 2013.
  16. ^ Hall, Nick (1 July 2011). "FIRST DRIVE: KOENIGSEGG AGERA". Motor Trend. Retrieved 13 September 2018.
  17. ^ Anderson, Brad (3 February 2014). "Replica Agera R's in the Need for Speed movie". GT Spirit. Retrieved 8 November 2017.
  18. ^ "Koenigsegg Agera S". Koenigsegg. Retrieved 18 October 2014.
  19. ^ a b "Koenigsegg from 0 to 100 in 10 Years". Koenigsegg. 10 March 2013. Archived from the original on 12 March 2013. Retrieved 10 March 2013.
  20. ^ Lim, Anthony (10 June 2014). "Koenigsegg Agera S arrives in Malaysia - RM5 million before tax". paultan.org. Retrieved 16 June 2014.
  21. ^ Dobie, Stephen (4 March 2014). "Koenigsegg One:1 supercar: Geneva 2014". Evo. Retrieved 4 March 2014.
  22. ^ "2014 Koenigsegg One:1". automobile-catalog.com. Retrieved 29 June 2018.
  23. ^ "Geneva 2015: Koenigsegg Agera RS". GTspirit.com. 3 March 2015. Retrieved 3 March 2015.
  24. ^ "2018 Koenigsegg Agera RS". www.fueleconomy.gov.
  25. ^ "Agera RS Production is Complete". Koenigsegg. 4 April 2018. Retrieved 11 April 2018.
  26. ^ Burkart, Tom (29 February 2016). "Geneva Debuts – 2016 Koenigsegg AGERA RS and AGERA Finale". Car-Revs-Daily. Retrieved 2 March 2016.
  27. ^ "Koenigsegg Presents Production Spec Regera, 'Agera Final' and Agera RS at Geneva 2016" (Press release). Koenigsegg. 29 February 2016. Retrieved 2 March 2016.
  28. ^ Anderson, Brad (30 August 2015). "The Story Behind the Koenigsegg Agera 'N' - GTspirit". GTspirit. Retrieved 3 February 2018.
  29. ^ "One-Off Koenigsegg Agera X Up For Sale". Motor Authority. Retrieved 3 February 2018.
  30. ^ "The Koenigsegg Agera HH & the Pagani Zonda HH", The Billionaire Shop, 22 October 2014, retrieved 21 June 2018
  31. ^ a b "Koenigsegg at Salon Privé 2016". Koenigsegg (Press release). 30 August 2016. Retrieved 3 February 2018.
  32. ^ a b c "The 11 Koenigseggs of Monterey Car Week, 2017". Koenigsegg (Press release). 23 August 2017. Retrieved 3 February 2018.
  33. ^ "#135". koenigsegg-registry.net. Retrieved 3 February 2018.
  34. ^ "1:18 Agera RS "ML"" (Press release). Koenigsegg. Retrieved 3 February 2018.
  35. ^ "#115". koenigsegg-registry.net. Retrieved 3 February 2018.
  36. ^ Tutu, Andrei (21 March 2018). "Koenigsegg Secretly Built an 1,360 HP Agera RSN with a Two-Tone Blue Finish". autoevolution. Retrieved 20 August 2018.
  37. ^ "Manny Khoshbin Takes Delivery Of Final Koenigsegg Agera RS". Autofluence. 7 May 2018. Retrieved 20 August 2018.
  38. ^ Nedelea, Andrei (22 January 2013). "China-Only Koenigsegg Agera R Zijin Spotted - Gets Solid Gold-Plated Interior!". autoevolution. Retrieved 20 August 2018.
  39. ^ a b Koenigsegg Agera RS 0-400-0. Koenigsegg. Retrieved 5 October 2017 – via YouTube.
  40. ^ Potter, Brian (2 September 2011). "Koenigsegg Agera R sets Guiness [sic] world record for 0-300-0 km/h". worldcarfans. Retrieved 5 August 2013.
  41. ^ Koenigsegg One:1 vs 0-300-0 kmh. 17 June 2015 – via YouTube.
  42. ^ "Koenigsegg Agera RS completes 0-400-0 km/h in 36.44 seconds". Koenigsegg. 5 October 2017. Retrieved 5 October 2017.
  43. ^ Okulski, Travis (5 November 2017). "Koenigsegg Agera RS is the world's fastest car". Road and Track. Retrieved 5 November 2017.
  44. ^ "Koenigsegg Agera RS Achieves Multiple Production Car World Speed Records" (Press release). Koenigsegg. 7 November 2017. Retrieved 14 November 2017.
  45. ^ "These are the last ever Koenigsegg Agera RS hypercars". TopGear.com. Retrieved 13 September 2018.


This article uses material from the Wikipedia article "Koenigsegg Agera", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer