powered by CADENAS

Social Share

Amazon

Action game (11723 views - Game & Play & Gamification)

The action game is a video game genre that emphasizes physical challenges, including hand–eye coordination and reaction-time. The genre includes a large variety of sub-genres, such as fighting games, beat 'em ups, shooter games and platform games. Some multiplayer online battle arena and real-time strategy games are also considered action games. In an action game, the player typically controls a character often in the form of a protagonist or avatar. This player character must navigate a level, collecting objects, avoiding obstacles, and battling enemies with their natural skills as well as weapons and other tools at their disposal. At the end of a level or group of levels, the player must often defeat a boss enemy that is more challenging and often a major antagonist in the game's story. Enemy attacks and obstacles deplete the player character's health and lives, and the player receives a Game over when they run out of lives. Alternatively, the player gets to the end of the game by finishing a sequence of levels and seeing the credits. But some action games, such as early arcade games, are unbeatable and have an indefinite number of levels; with the player's only goal being to get as far as they can to maximize their score.
Go to Article

Explanation by Hotspot Model

Youtube


    

Action game

Action game

Part of a series on
Action games

The action game is a video game genre that emphasizes physical challenges, including hand–eye coordination and reaction-time. The genre includes a large variety of sub-genres, such as fighting games, beat 'em ups, shooter games and platform games. Some multiplayer online battle arena and real-time strategy games are also considered action games.

In an action game, the player typically controls a character often in the form of a protagonist or avatar. This player character must navigate a level, collecting objects, avoiding obstacles, and battling enemies with their natural skills as well as weapons and other tools at their disposal. At the end of a level or group of levels, the player must often defeat a boss enemy that is more challenging and often a major antagonist in the game's story. Enemy attacks and obstacles deplete the player character's health and lives, and the player receives a Game over when they run out of lives. Alternatively, the player gets to the end of the game by finishing a sequence of levels and seeing the credits. But some action games, such as early arcade games, are unbeatable and have an indefinite number of levels; with the player's only goal being to get as far as they can to maximize their score.

Defining elements

The action genre includes any game where the player overcomes challenges by physical means such as precise aim and quick response times.[1] Action games can sometimes incorporate other challenges such as races, puzzles, or collecting objects, but they are not central to the genre. Players may also encounter tactical and exploration challenges, but these games first-and-foremost require high reaction speed and good hand–eye coordination. The player is often under time pressure, and there is not enough time for complex strategic planning. In general, faster action games are more challenging. Action games may sometimes involve puzzle solving, but they are usually quite simple because the player is under immense time pressure.[2]

Game design

Levels

Players advance through an action game by completing a series of levels. Levels are often grouped by theme, with similar graphics and enemies called a world. Each level involves a variety of challenges, whether dancing in a dance game or shooting things in a shooter, which the player must overcome to win the game. Older games force players to restart a level after dying, although action games evolved to offer saved games and checkpoints to allow the player to restart partway through a level. Increasingly, though, some games allow for 'resurrection' or 'cloning' and the opportunity to regain lost items upon death for a certain sum of ingame currency, typically increasing exponentially the more times the player dies. The obstacles and enemies in a level do not usually vary between play sessions, allowing players to learn by trial and error. However, levels sometimes add an element of randomness, such as an enemy that randomly appears or that takes an unpredictable path.[2]

Levels in an action game may be linear or nonlinear, and sometimes include shortcuts. For levels that require exploration, the player may need to search for a level exit that is hidden or guarded by enemies. Such levels can also contain secrets—hidden or hard-to-reach objects or places that contain something valuable. The prize can be a bonus (see below) or a non-standard exit that allows a player to access a hidden level, or jump ahead several levels. Action games sometimes offer a teleporter that will cause the player's avatar to re-appear elsewhere in the same level. Levels often make use of locked doors that can only be opened with a specific key found elsewhere in the level.[2]

Action games sometimes make use of time restrictions to increase the challenge. However, game levels typically do not react to time passing, and day/night cycles are rare.[2] When the timer expires, the player typically loses a life, although some games generate a difficult enemy or challenge. If the level is completed with time remaining, this usually adds to the player's score.[2]

Character abilities

In most action games, the player controls a single avatar as the protagonist.[2] The avatar has the ability to navigate and maneuver, and often collects or manipulates objects. They have a range of defenses and attacks, such as shooting or punching. Many action games make use of a powerful attack that destroys all enemies within a limited range, but this attack is rare.[2]

Players may find a power-up within the game world that grants temporary or permanent improvements to their abilities. For example, the avatar may gain an increase in speed, more powerful attacks, or a temporary shield from attacks. Some action games even allow players to spend upgrade points on the power ups of their choice.[2]

Obstacles and enemies

In action games that involve navigating a space, players will encounter obstacles, traps, and enemies. Enemies typically follow fixed patterns and attack the player, although newer action games may make use of more complex artificial intelligence to pursue the player. Enemies sometimes appears in groups or waves, with enemies increasing in strength and number until the end of the level. Enemies may also appear out of thin air. This can involve an invisible spawn point, or a visible generator which can be destroyed by the player. These points may generate enemies indefinitely, or only up to a certain number.[2] At the end of a level or group of themed levels, players often encounter a boss. This boss enemy will often resemble a larger or more difficult version of a regular enemy. A boss may require a special weapon or attack method, such as striking when the boss opens their mouth or attacking particular part of the Boss.[2]

Health and lives

In many action games, the avatar has a certain number of hit-markers or health, which are depleted by enemy attacks and other hazards. Sometimes health can be replenished by collecting an in-game object. When the player runs out of health, the player dies. The player's avatar is often given a small number of chances to retry after death, typically referred to as lives. Upon beginning a new life, the player resumes the game either from the same location they died, a checkpoint, or the start of the level. Upon starting a new life, the avatar is typically invincible for a few seconds to allow the player to re-orient themselves. Players may earn extra lives by reaching a certain score or by finding an in-game object. Arcade games still limit the number of player lives, while home video games have shifted increasingly to unlimited lives.[2]

Graphics and interface

Action games take place in either 2D or 3D from a variety of perspectives. 2D action games typically use a side view or top-down view. The screen frequently scrolls as the player explores the level, although many games scroll through the level automatically to push the player forward. In 3D action games, the perspective is usually tied to the avatar from a first-person or third-person perspective. However, some 3D games offer a context-sensitive perspective that is controlled by an artificial intelligence camera. Most of what the player needs to know is contained within a single screen, although action games frequently make use of a heads-up display that display important information such as health or ammunition. Action games sometimes make use of maps which can be accessed during lulls in action, or a mini-map that is always visible.[2]

Scoring and victory

Action games tend to set simple goals, and reaching them is obvious.[2] A common goal is to defeat the end-of-game boss. This is often presented in the form of a structured story, with a happy ending upon winning the game. In some games, the goal changes as the player reveals more of the story.[2]

Many action games keep track of the player's score. Points are awarded for completing certain challenges, or defeating certain enemies. Skillful play is often rewarded with point multipliers, such as in Pac-Man where each ghost that the avatar eats will generate twice as many points as the last. Sometimes action games will offer bonus objects that increase the player's score. There is no penalty for failing to collect them, although these bonus objects may unlock hidden levels or special events. In many action games, achieving a high score is the only goal, and levels increase in difficulty until the player loses. Arcade games are more likely to be unbeatable, as they make their money by forcing the player to lose the game. On the other hand, games sold at home are more likely to have discrete victory conditions, since a publisher wants the player to purchase another game when they are done.[2]

Subgenres

Action games have several major subgenres. However, there are many action games without any clear subgenre, such as Frogger, as well as other types of genres like Adventure or Strategy that have action elements.[2]

Action-adventure games mix elements of both action and adventure genres, examples include The Legend of Zelda, Assassin's Creed and Grand Theft Auto series.

Beat 'em ups are games that involve fighting through a side-scrolling stage of multiple adversaries, using martial arts or other close-range fighting techniques.[3][4]

Fighting games feature combat between pairs of fighters, usually using martial arts moves. Actions are limited to various attacks and defenses, and matches end when a fighter's health is reduced to zero. They often make use of special moves and combos. There are both 2D and 3D fighting games, but most 3D fighting games largely take place in a 2D plane and occasionally include side-stepping. They are distinct from sports games such as boxing and wrestling games which attempt to model movements and techniques more realistically.[2]

Maze games such as Pac-Man involve navigating a maze to avoid or chase adversaries.[5]

Platform games involve jumping between platforms of different heights, while battling enemies and avoiding obstacles. Physics are often unrealistic, and game levels are often vertically exaggerated. They exist in both 2D and 3D forms.[2]

Rhythm action games challenge the player's sense of rhythm, and award points for accurately pressing certain buttons in sync with a musical beat. This is a relatively new subgenre of action game.[2] Rhythm games are sometimes classified as a type of music game.[6]

Shooter games allow the player to take action at a distance using a ranged weapon, challenging them to aim with accuracy. Although shooting is usually a form of violence, non-violent shooters exist as well, such as Splatoon. This subgenre includes first-person shooters and third-person shooters, as well as a plethora of other shoot 'em up games taking place from a top-down or side-view perspective.[2]

Survival games start the player off with minimal resources, in a hostile, open-world environment, and require them to collect resources, craft tools, weapons, and shelter, in order to survive as long as possible. Many are set in procedurally-generated environments, and are open-ended with no set goals. They may overlap with the survival horror genre, in which the player must survive within a supernatural setting, such as a zombie apocalypse. A specific subgenre of survival game is battle royale.

Physical impact

Studies have shown that people can improve their eyesight by playing action video games. Tests by scientists at the University of Rochester on college students showed that over a period of a month, performance in eye examinations improved by about 20% in those playing Unreal Tournament compared to those playing Tetris.[7] Most arcade games are action games, because they can be difficult for unskilled players, and thus make more money quickly.[2]

Researchers from Helsinki School of Economics have shown that people playing a first-person shooter might secretly enjoy that their character gets killed in the game, although their expressions might show the contrary. The game used in the study was James Bond 007: Nightfire.[8]

History

A major turning point for action games came with the 1978 release of the shoot 'em up game Space Invaders,[9] which marked the beginning of the golden age of arcade video games.[10] As a result of Space Invaders' mainstream success, the industry came to be dominated by action games,[9] which have remained the most dominant genre in video arcades and on game consoles through to the present day.[11] Along with Space Invaders,[12] Asteroids from 1979[13] and Pac-Man from 1980[14] have also become iconic examples from the action genre.[2] Robotron: 2084, released in arcades in 1982, also became a classic in the shooter subgenre.[2]

In much the same way Space Invaders set the template for the shooter game subgenre,[9][15] Donkey Kong did the same for the platform game subgenre when it released in 1981.[16] 1984 saw the emergence of martial arts themed games, with Karate Champ establishing the one-on-one fighting game subgenre,[17] and Kung-Fu Master laying the foundations for the side-scrolling beat 'em up subgenre.[18][19]

  1. ^ "The Next Generation 1996 Lexicon A to Z". Next Generation. No. 15. Imagine Media. March 1996. pp. 28–42. Action game - A game characterized by simple action and response gameplay. ... the defining characteristic is that enemies and obstacles are overcome by 'physical' means, rather than involved intellectual problem solving.
  2. ^ a b c d e f g h i j k l m n o p q r s t u v w Rollings, Andrew; Ernest Adams (2006). Fundamentals of Game Design. Prentice Hall.
  3. ^ Spanner Spencer (2008-02-06). "The Tao of Beat-'em-ups". EuroGamer. Retrieved 2009-02-18.
  4. ^ Subskin. "Reviews - Fighting Force 2". GameSpy. Archived from the original on 2008-06-04. Retrieved 2009-02-18.
  5. ^ Robert J. Sternberg, David Preiss (2005). Intelligence and Technology. Routledge.
  6. ^ Stephen Totilo (2008-10-27). "One-On-One With Shigeru Miyamoto: From 'Wii Music' To Bowser To… MotionPlus?". MTV. Archived from the original on 15 January 2009. Retrieved 2009-02-20.
  7. ^ "Action computer games can sharpen eyesight" retrieved from NewScientestTech
  8. ^ "Gamers secretly enjoy getting killed " retrieved from NewScientestTech
  9. ^ a b c "Essential 50: Space Invaders". 1UP.com. Archived from the original on 2012-10-18. Retrieved 2011-03-26.
  10. ^ Jason Whittaker (2004), The cyberspace handbook, Routledge, p. 122, ISBN 0-415-16835-X
  11. ^ Jason Whittaker (2004), The cyberspace handbook, Routledge, p. 129, ISBN 0-415-16835-X
  12. ^ Kevin Bowen. "The Gamespy Hall of Fame: Space Invaders". GameSpy. Archived from the original on 2008-04-08. Retrieved 2009-02-17.
  13. ^ Nate Ahearn (2007-11-29). "Asteroids Deluxe Review". IGN. Archived from the original on 2012-03-03. Retrieved 2009-02-17.
  14. ^ Namco Bandai Games Inc. (2005-06-02). "Bandai Namco press release for 25th Anniversary Edition" (in Japanese). bandainamcogames.co.jp/. Archived from the original on 2007-12-30. Retrieved 2007-10-10. 2005年5月22日で生誕25周年を迎えた『パックマン』。 ("Pac-Man celebrates his 25th anniversary on May 22, 2005", seen in image caption)
  15. ^ Edwards, Benj. "Ten Things Everyone Should Know About Space Invaders". 1UP.com. Archived from the original on 2009-02-26. Retrieved 2008-07-11.
  16. ^ "Gaming's most important evolutions". GamesRadar. October 8, 2010. Retrieved 2011-03-31.
  17. ^ Ryan Geddes & Daemon Hatfield (2007-12-10). "IGN's Top 10 Most Influential Games". IGN. Retrieved 2009-04-14.
  18. ^ Spencer, Spanner, The Tao of Beat-'em-ups, Eurogamer, Feb 6, 2008, Accessed Mar 18, 2009
  19. ^ Kunkel, Bill; Worley, Joyce; Katz, Arnie, "The Furious Fists of Sega!", Computer Gaming World, Oct 1988, pp. 48-49


This article uses material from the Wikipedia article "Action game", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Game & Play & Gamification

3d,model,playground,board games,computer,strategy,thinktank