powered by CADENAS

Social Share

Amazon

Film format (10906 views - Movie)

A film format is a technical definition of a set of standard characteristics regarding image capture on photographic film, for either stills or filmmaking. It can also apply to projected film, either slides or movies. The primary characteristic of a film format is its size and shape. In the case of motion picture film, the format may also include audio parameters (though often not). Other characteristics usually include the film gauge, pulldown method, lens anamorphosis (or lack thereof), and film gate or projector aperture dimensions, all of which need to be defined for photography as well as projection, as they may differ.
Go to Article

Explanation by Hotspot Model

Youtube


    

Film format

Film format

Film format

A film format is a technical definition of a set of standard characteristics regarding image capture on photographic film, for either stills or filmmaking. It can also apply to projected film, either slides or movies. The primary characteristic of a film format is its size and shape.

In the case of motion picture film, the format may also include audio parameters (though often not). Other characteristics usually include the film gauge, pulldown method, lens anamorphosis (or lack thereof), and film gate or projector aperture dimensions, all of which need to be defined for photography as well as projection, as they may differ.

Motion picture film formats

Digital camera formats

Still photography film formats

Multiple image

Designation[a] Type Introduced Discontinued Image size Exposures Comment
101 roll film 1895 1956 3½" × 3½"
102 roll film 1896 1933 1½" × 2" One flange has gear teeth
103 roll film 1896 1949 10cm × 12.5cm
104 roll film 1897 1949 4¾" × 3¾"
105 roll film 1897 1949 2¼" × 3¼" Like 120 film with 116-size flanges
106 for roll holder 1898 1924 3½" × 3½" Roll holder films were wound inside out
107 for roll holder 1898 1924 3¼" × 4¼"
108 for roll holder 1898 1929 4¼" × 3¼"
109 for roll holder 1898 1924 4" × 5"
110
(early roll film)
for roll holder 1898 1929 5" × 4" No relation to the later 110 cartridge format.
110
("Pocket Instamatic")
cartridge 1972 Present[2] 13 × 17 mm 16 mm stock, registration perforated
Introduced with Kodak's "Pocket Instamatic" series
Daylight, Transparency, Black & White
111 for roll holder 1898 Unknown 6½" × 4¾"
112 for roll holder 1898 1924 7" × 5"
113 for roll holder 1898 Unknown 9 × 12 cm
114 for roll holder 1898 Unknown 12 × 9 cm
115 roll film 1898 1949 6¾" × 4¾"
116 roll film 1899 1984 2½" × 4¼" Like 616 film with wider flanges
117 roll film 1900 1949 2¼" × 2¼" 12 Like 620 spool with 120 keyslot
118 roll film 1900 1961 3¼" × 4¼" 3.474" spool
119 roll film 1900 1940 4¼" × 3¼"
120 roll film 1901 Present 2¼" × 3¼"
56 × 70 mm
2¼" × 2¼"
2¼" × 1⅝"
8
10
12-13
15-16
2.4 inch (60.96 mm) stock, unperforated, paper-backed
121 roll film 1902 1941 1⅝" × 2½"
122 roll film 1903 1971 3¼" × 5½" 6 or 10 Postcard format
123 roll film 1904 1949 4" × 5"
124 roll film 1905 1961 3¼" × 4¼" 3.716" spool - same picture size as 118 with longer spool
125 roll film 1905 1949 3¼" × 5½" like 122 on longer spool; also for stereo pairs, 3¼" × 2½" x 2
126
(early roll film)
roll film 1906 1949 4¼" × 6½" No relation to the 126 cartridge format introduced in 1963.
126
("Instamatic")
cartridge 1963 2008 26.5 × 26.5 mm 12, 20 (later 24) 35 mm stock, registration perforated
Introduced with first "Instamatic" cameras under the name "Kodapak"
127 roll film 1912 Present 1⅝" × 2½"
1⅝" × 1⅝"
1⅝" × 1¼"
8
12
16
46 mm stock, "Vest Pocket"
128 roll film 1912 1941 1½" × 2¼" for Houghton Ensignette #E1[3]
129 roll film 1912 1951 1⅞" × 3" for Houghton Ensignette #E2
130 roll film 1916 1961 2⅞" × 4⅞"
135 cartridge 1934 Present 24 × 36 mm 24 or 36 35 mm stock, double perforated
formerly available in 12, 18, 20, or 72 exposures[4]
220 roll film 1965 Present 2¼" × 3¼"
6 × 7 cm
2¼" × 2¼"
2¼" × 1⅝"
18
21
24-27
30-33
2.4 inch (60.96 mm) stock, unperforated, no backing paper
Twice as long as 120
235 loading spool 1934 Unknown 24 × 36 mm 35 mm film in daylight-loading spool
240 / APS cartridge 1996 2011 30.2 × 16.7 mm 15, 25, or 40 24 mm stock, registration perforated
Daylight, Transparency, Black & White (Chromogenic 400CN)
335 stereo pairs 1952 Unknown 24 × 24 mm 20 pairs Special length for Realist format stereo pairs
435 loading spool 1934 Unknown 24 × 36 mm 35 mm film in daylight-loading spool
50 for roll holder 1915 March 1941 3¼" × 2¼" for Graflex rollholder
51 for roll holder 1915 Feb. 1951 4¼" × 3¼" for Graflex rollholder
52 for roll holder 1915 March 1949 5½" × 3¼" for Graflex rollholder
53 for roll holder 1915 Feb. 1951 5" × 4" for Graflex rollholder
54 for roll holder 1915 March 1949 7" × 5" for Graflex rollholder
500 film pack 1911 1948 1¾" × 2⅜" 12 redefined 1921 as 1⅝ x 2⁷/₁₆
515 film pack 1905 1955 5" × 7" 12
516 film pack 1909 1955 2½" × 4¼" 12
518 film pack 1903 1976 3¼" × 4¼" 12 sheets
520 film pack 1906 1976 2¼" × 3¼" 16 sheets
522 film pack 1904 1955 3¼" × 5½" 12 sheets 3A postcard
523 film pack 1904 4" × 5" 12 sheets
526 film pack 1920 1941 4¾ × 6½"
531 film pack 1926 1941 2⁹/₃₂ × 5¹¹/₃₂ 6 cm × 13 cm
540 film pack 1920 1941 1¾ × 4¼
541 film pack 1920 1941 3½ × 4¾ 12 9 cm × 12 cm
542 film pack 1911 1948 3 × 5¼ 7.5 cm × 13.5 cm
543 film pack 1920 1948 3¾ × 5½ 12 10 cm × 15 cm
616 roll film 1931 1984 2½" × 4¼" or 2½" × 2⅛" 6, later 8 Similar to 116 film but on a thinner spool
620 roll film 1932 1995 Similar to 120 film but on a thinner spool
828 roll film 1935 1985 28 × 40 mm, 8 35mm, one perforation per frame Bantam
35 roll film 1916 1933 1¼" × 1¾" 35 mm stock, unperforated
00 UniveX roll film 1933 1½" × 1⅛" 6 made by Gevaert
Hit (for example TONE camera) roll film 1937 unknown 14 × 14 mm 10 [5] 17.5 mm stock; used in imported miniature toy cameras [6]
Disc cassette 1982 1998 8 × 11 mm 15 circular sheet of film attached to rigid carrier
Half-frame cartridge later than 1934 Present 18 × 24 mm 48 or 72 135 film in "half-frame" cameras
Minox cartridge 1938 Present 8 × 11 mm 15, 36 or 50 nominally 9.5 mm wide stock (in reality 9.2-9.3 mm)
Karat cartridge 1936 1963 Early AGFA cartridge for 35 mm film
Rapid cartridge 1964 1990s 12 AGFA cartridge for 35 mm film (replaced Karat, same system)
SL cartridge 1958 1990 24 × 36 mm
24 × 24 mm
18 × 24 mm
12
16
24
Orwo Schnell-Lade Kassette for 35 mm film
Kassette 16 cartridge 1978 1990s 13 × 17 mm 20 Orwo, 16 mm stock, central perforation (holes between frames)
Introduced exclusively for the Pentacon k16 camera
Super 16 (Rollei) cartridge 1963 1981 13 × 17 mm 18 Rollei, 16 mm stock, perforation on both edges?
with kino film (?) only by Rollei for the Rollei 16 camera; also Wirgin Edixa 16 (Franka / alka 16)
Minolta-16 cartridge 1955 1974 10 × 14 mm (orig) & 13 × 17 20 Minolta, 16 mm stock, originally double perforated (single perforated or unperforated film could be loaded), later single perf to allow larger 13 × 17 mm image
  1. ^ Unless otherwise noted, all formats were introduced by Kodak, which began allocating the number series in 1913. Before that, films were simply identified by the name of the cameras they were intended for.[1]

For roll holder means film for cartridge roll holders, allowing roll film to be used with cameras designed to use glass plates. These were spooled with the emulsion facing outward, rather than inward as in film designed for native roll-film cameras. Types 106 to 114 were for Eastman-Walker rollholders, while types 50 to 54 were for Graflex rollholders.

The primary reason there were so many different negative formats in the early days was that prints were made by contact, without use of an enlarger. The film format would thus be exactly the same as the size of the print—so if you wanted large prints, you would have to use a large camera and corresponding film format.

Roll film cross-reference table

Before World War II, each film manufacturer used its own system of numbering for the various sizes of rollfilms they made. The following sortable table shows the corresponding numbers. A blank space means that manufacturer did not make film in that size. Two numbers in one box refers to films available with different numbers of exposures, usually 6 and either 10 or 12. Spool length is measured between inner faces of the flanges; several films of the same image size were available on different spools to fit different cameras.

Eastman AGFA Ansco Ensign Vulcan Seneca Rexo Spool
length
101 H6 8A, 8B 3½ inch 202 303 3.661"
102 1B 1½ inch 204 1.655"
103 K6 10A, 10B 4 inch 206 3.912"
104 L6 12A, 12B 5 inch 208 5.064"
105 C6 5A, 5B 2¼ inch C 210 315 2.509"
115 13A, 13B 7 inch 230 7.126"
116 D6 6A, 6B 2½ inch 232 348 425, 426 2.814"
117 B1 3A 2¼ inch A 234 2.470"
118 E6 7A, 7B 3¼ inch 236 354 430, 431 3.474"
119 11A, 11B 4¼ inch 238 4.490"
120 B2 4A 2¼ inch B 240 360 415 2.466"
121 AB6 2A, 2B 1⅝ inch 242 1.850"
122 G6, G10 18A, 18B 3¼ inch A 244 366 445, 446 3.715"
123 J6 10C, 10D 4 inch A 246 4.693"
124 F6 7C, 7D 3¼ inch B 248 372 435 3.716"
125 18C, 18D 3¼ inch C 250 375 3.912"
126 19A 4¼ inch A 252 4.898"
127 A8 2C Ensignette 1J 254 381 407 1.860"
128 O6 Ensignette 1 1.606"
129 N6 Ensignette 2 2.059"
130 M6 26A, 26B 2⅞ inch 260 390 436, 438 3.132"
616 PD16 2.814"
620 PB20 2.468"

Single image

Size (in inches) Type
1⅝×2⅛ "sixteenth-plate" tintypes
2×2½ "ninth-plate" tintypes
2×3 sheet film
2¼×3¼ sheet film
2½×3½ "sixth-plate" tintypes
3×4 sheet film
3⅛×4⅛ "quarter-plate" tintypes
3¼×4¼ sheet film,[7] "quarter-plate" glass plates
3¼×5½ postcard or 3A
4×5 glass plate,sheet film
4×10 sheet film
4¼×5½ "half-plate" tintypes
4¾×6½ "half-plate" glass plates, sheet film
5×7 sheet film
6½×8½ "whole-plate" glass plates, sheet film, tintypes
7×17 sheet film
8×10 glass plates,sheet film
8×20 sheet film
11×14 sheet film
12×20 sheet film
14×17 sheet film
16×20 sheet film
20×24 sheet film
Size (in cm) Type
6.5 × 9 sheet film
9 × 12 glass plate, sheet film
10 × 15 sheet film
13 × 18 sheet film
18 × 24 sheet film
24 × 30 sheet film

Instant film

Designation Type Introduced Discontinued Image size Exposures Comment
Type 20 Polaroid roll film cartridge 1965 1979 2 1/8" × 2 7/8" 8
Type 30 Polaroid roll film cartridge 1954 1979 2 1/8" × 2 7/8" 8
Type 40 Polaroid roll film cartridge 1948 1972 (color)
1992 (monochrome)
2 7/8" × 3 3/4" 6 or 8
Type 50 Polaroid peel-apart film pack 19?? 2008 4" × 5" Including Type 55
Type 80 Polaroid peel-apart film pack 1971 2006 2 3/4" × 2 7/8" 8 or 10
Type 100 Polaroid peel-apart film pack 1963 2016[8] 2 7/8" × 3 3/4" 8, 10 or 11 Discontinued by Polaroid in 2008. Produced by Fujifilm thereafter.[8]
SX-70,
Type 600
Polaroid integral film pack 1972 3 1/8" × 3 1/8" 8 or 10 Discontinued by Polaroid in 2008. Reintroduced by Impossible Project in 2010.
Kodak Instant Kodak integral film pack 1976 1986 91 mm × 67 mm 10
F Series Fuji integral film pack 1981 c.1990 91 mm × 69 mm Film compatible with Kodak Instant, but in a different cartridge and rated at a (slightly) different speed
Kodamatic Kodak integral film pack c.1980 1986 91 mm × 67 mm 10
Trimprint,
Instagraphic
Kodak peel-apart film pack 1983 1986 4" × 3 1/2" 10 [9][10]
System 800 Fuji integral film pack 2010 91 mm × 69 mm
Spectra,
Type 700,
Type 1200
Polaroid integral film pack 1986 3 5/8" × 2 7/8" 10 or 12 Discontinued by Polaroid in 2008. Reintroduced by Impossible Project in 2010.
Captiva,
Type 500
Polaroid integral film pack 1993 2006 2 7/8" × 2 1/8" 10
InstantACE Fuji integral film pack 2010 91 mm × 69 mm
8x10 Polaroid film pack 19?? 8" × 10" 1 Discontinued by Polaroid. Reintroduced by Impossible Project.
i-Zone
Pocket
Polaroid integral film pack 1997 2006 36 mm × 24 mm 12
Instax Mini,
Mio,
Type 300
Fuji/Polaroid integral film pack 1998[11][12][13] 46 mm × 62 mm 10
Instax Wide Fuji integral film pack 1999[13] 99 mm × 62 mm 10
Instax Pivi Fuji integral film pack 2004 46 mm × 61 mm
I-Type Impossible integral film pack 2016 3 1/8" × 3 1/8" 8 Same image format as Polaroid Type 600, but the film cartridge does not contain a battery
Instax Square Fuji integral film pack 2017 62 mm × 62 mm 10

See also



This article uses material from the Wikipedia article "Film format", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Movie

Movie, Animation, Cartoon