powered by CADENAS

Social Share

Amazon

Tricycle (20256 views - Transportation - Air Water Earth)

A tricycle, often abbreviated to trike, is a human-powered (or gravity-powered) three-wheeled vehicle. Some tricycles, such as cycle rickshaws (for passenger transport) and freight trikes, are used for commercial purposes, especially in the developing world, particularly Africa and Asia. In the West, adult-sized tricycles are used primarily for recreation, shopping, and exercise. Tricycles are favoured by children and senior adults for their apparent stability versus a bicycle; however a conventional trike has poor dynamic lateral stability, and the rider must take care when cornering to avoid tipping the trike over. Unconventional designs such as recumbents have a lower centre of gravity so require less care.
Go to Article

Explanation by Hotspot Model

Youtube


    

Tricycle

Tricycle

A tricycle, often abbreviated to trike,[1][2][3][4] is a human-powered (or gravity-powered) three-wheeled vehicle.

Some tricycles, such as cycle rickshaws (for passenger transport) and freight trikes, are used for commercial purposes, especially in the developing world, particularly Africa and Asia.

In the West, adult-sized tricycles are used primarily for recreation, shopping, and exercise. Tricycles are favoured by children and senior adults for their apparent stability versus a bicycle; however a conventional trike has poor dynamic lateral stability, and the rider must take care when cornering to avoid tipping the trike over. Unconventional designs such as recumbents have a lower centre of gravity so require less care.

History

A three-wheeled wheelchair was built in 1655 or 1680 by a disabled German man, Stephan Farffler, who wanted to be able to maintain his mobility. Since he was a watch-maker, he was able to create a vehicle that was powered by hand cranks.[5][6]

In 1789, two French inventors developed a three-wheeled vehicle, powered by pedals; They called it the tricycle.[5]

In 1818, British inventor Denis Johnson patented his approach to designing tricycles.[clarification needed] In 1876, James Starley developed the Coventry Lever Tricycle, which used two small wheels on the right side and a large drive wheel on the left side; power was supplied by hand levers. In 1877, Starley developed a new vehicle he called the Coventry Rotary, which was "one of the first rotary chain drive tricycles." Starley's inventions started a tricycling craze in Britain; by 1879, there were "twenty types of tricycles and multi-wheel cycles ... produced in Coventry, England, and by 1884, there were over 120 different models produced by 20 manufacturers." The first front steering tricycle was manufactured in 1881 by The Leicester Safety Tricycle Company of Leicester, England, which was brought to the market in 1882 costing £18. They also developed a folding tricycle at the same time.

Tricycles were used by riders who did not feel comfortable on the high wheelers, such as women who wore long, flowing dresses (see rational dress).

Associations

In the UK, upright tricycles are sometimes referred to as "barrows". Many trike enthusiasts in the UK belong to the Tricycle Association, formed in 1929. They participate in day rides, tours, time trials, and a criterium (massed start racing) series. [7]

Wheel configurations

Delta

A delta tricycle has one front wheel and two rear wheels.[8]

Tadpole

A tadpole tricycle has two front wheels and one rear wheel.[9] Rear wheel steering is sometimes used, although this increases the turning circle and can affect handling (the geometry is similar to a regular tricycle operating in reverse, but with a steering damper added).[8]

Other

Some early pedal tricycles from the late 19th century used two wheels in tandem on one side and a larger driving wheel on the other.[10]

An in-line three-wheeled vehicle has two steered wheels, one at the front and the other in the middle or at the rear.[11]

Types

Upright

Upright resembles a two-wheeled bicycle, traditionally diamond frame, or open frame, but with either two widely spaced wheels at the back (called delta) or two wheels at the front (called tadpole). The rider straddles the frame in both delta and tadpole configurations. Steering is through a handlebar directly connected to the front wheel via a conventional bicycle fork in delta, or via a form of Ackermann steering geometry in the case of the upright tadpole.

All non-tilting trikes have stability issues and great care must be used when riding a non tilting upright trike. The center of gravity is quite high compared to recumbent trikes. Because of this, non-tilting trikes are more prone to tipping over in corners and on uneven or sloping terrain. Conversely, the rider enjoys better visibility than on a recumbent because their head is higher.

Recumbent

Recumbent trikes' advantages (over conventional trikes) include stability (through low centre of gravity) and low aerodynamic drag. Disadvantages (compared to bicycles) include greater cost, weight, and width. The very low seat may make entry difficult, and on the road they may be less visible to other traffic.[12][citation needed]

Recumbent delta

Recumbent delta is similar to an upright, with two wheels at the back and one at the front, but has a recumbent layout in which the rider is seated in a chair-like seat. One or both rear wheels can be driven, while the front is used for steering (the usual layout). Steering is either through a linkage, with the handlebars under the seat (under seat steering) or directly to the front wheel with a large handlebar (over seat steering). Some delta trikes can be stored upright by lifting the front wheel and resting the top of the seat on the ground.

Delta trikes generally have higher seats and a tighter turning radius than tadpole trikes. The tight turning radius is necessary if riding on trails with offset barriers, or navigating around closely placed obstacles. The higher seat makes mounting and dismounting easier. Even with the higher seat a delta trike can be quite stable provided most of the weight (including the rider) is shifted back towards the rear wheels. Many delta trikes place the seat too far forward and that takes weight off the two rear wheels and puts more weight onto the front wheel making the trike more unstable.[13][14] The Hase Kettwiesel delta trike has an 18 in (460 mm) high seat that is placed to put most of the weight onto the cambered rear wheels making it more stable.

Delta trikes are suitable to be used as manual scooters for mobility, rehab and/or exercise. The Hase Lepus Comfort is an example of a rehab delta trike designed mainly for comfort and ease of use. It has a lowered front boom and the seat can be adjusted to a height of 20 to 28 in (510 to 710 mm), which aids in mounting and dismounting. It also has rear wheel suspension for comfort. The 56 lb (25 kg) Lepus can be folded for easier storage and transportation.

The weight of a delta trike can be quite close to the weight of a tadpole trike if they are both of a similar quality and similar materials are used. The Hase Kettwiesel Allround delta trike has an aluminium frame and weighs 39.4 lbs (17.9 kg).[15] The Catrike Road tadpole trike has an aluminium frame and weighs 37.5 lbs (17 kg).[16]

Recumbent tadpole

Recumbent tadpole or reverse trike is a recumbent design with two steered wheels at the front and one driven wheel at the back, though one model has the front wheels driven while the rear wheel steers. Steering is either through a single handlebar linked with tie rods to the front wheels' stub axle assemblies (indirect) or with two handlebars (rather, two half-handlebars) each bolted to a steerer tube, usually through a bicycle-type headset and connected to a stub axle assembly (direct). A single tie rod connects the left and right axle assemblies.

The tadpole trike is often used by middle-aged or retiree-age former bicyclists who are tired of the associated pains from normal upright bikes. With its extremely low center of gravity, aerodynamic layout and light weight (for trikes), tadpoles are considered the highest performance trikes.

Most Velomobiles are built in a tadpole trike configuration since a wide front and narrow rear offer superior aerodynamics to a delta trike configuration.

Recumbent hand trike

Hand-crank trikes use a hand-operated crank, either as a sole source of power or a double drive with footpower from pedals and hand-power from the hand crank. The hand-power only trikes can be used by individuals who do not have the use of their legs due to a disability or an injury. They are made by companies including Greenspeed, Invacare, Quickie and Druzin.[citation needed]

In case of paralysis of the legs, more speed and range of distance can be obtained by adding functional electrical stimulation to the legs. The large leg muscles are activated by electrical impulses synchronized with the hand cranking movement.[17]

Recumbent tandem

Recumbent tandem trikes allow two people to ride in a recumbent position with an extra-strong backbone frame to hold the extra weight. Some allow the "captain" (the rider who steers) and "stoker" (the rider who only pedals) to pedal at different speeds. They are often made with couplers so the frames can be broken down into pieces for easier transport. Manufacturers of recumbent trikes include Greenspeed, WhizWheelz and Inspired Cycle Engineering (ICE).[citation needed]

Special purposes

Some tricycles (such as the Christiania and the Pashley load trike) are designed for load carrying. Others are designed for racing or for comfort. Some recumbent tricycles are fully enclosed for all weather use as well as for aerodynamic benefits; these are known as velomobiles. Some tricycles, such as the Zigo Leader, are designed to transport children.

Tricycle rickshaw

Most cycle rickshaws, used for carrying passengers for hire, are tricycles with one steering wheel in the front and two wheels in the back supporting a seating area for one or two passengers. Cycle rickshaws often have a parasol or canopy to protect the passengers from sun and rain. These vehicles are widely used in South Asia and Southeast Asia, where rickshaw driving provides essential employment for recent immigrants from rural areas, generally impoverished men. In the 1990s and first decade of the 21st century, rickshaws became increasingly popular in big cities in Britain, Europe and the United States, where they provide urban transportation, novelty rides, and serve as advertising media.

Spidertrike is a recumbent cycle rickshaw that is used in central London and operated by Eco Chariots. The trike pictured is called the SUV (Sensible Utility Vehicle) and is produced by the company Organic Engines, which operates in Florida in the United States. It is a front wheel drive tricycle, articulated behind the driver seat, and has hydraulic double disc brakes and internal hub gears. The passenger is protected from rain and sun with a canopy.

Freight trike

Urban delivery trikes are designed and constructed for transporting large loads. These trikes include a cargo area consisting of a steel tube carrier, an open or enclosed box, a flat platform, or a large, heavy-duty wire basket. These are usually mounted over one or both wheels, low behind the front wheel, or between parallel wheels at either the front or rear of the vehicle, to keep the center of gravity low. The frame and drivetrain must be constructed to handle loads several times that of an ordinary bicycle; as such, extra low gears may be added. Other specific design considerations include operator visibility and load suspension. Many, but not all, cycles used for the purpose of vending goods such as ice cream cart trikes or hot dog vending trikes are cargo bicycles.[citation needed]

Many freight trikes are of the tadpole configuration, with the cargo box (platform, etc.) mounted between the front wheels. India and China are significant strongholds of the rear-loading "delta" carrier trike. Freight trikes are also designed for indoor use in large warehouses or industrial plants. The advantage of using freight trikes rather than a motor vehicle is that there is no exhaust, which means that the trike can be used inside warehouses. While another option is electric golf cart-style vehicles, freight trikes are human-powered, so they do not have the maintenance required to keep batteries on golf carts charged up.[citation needed]

Common uses include:[citation needed]

  • Delivery services in dense urban environments
  • Food vending in high foot traffic areas (including specialist ice cream bikes)
  • Transporting trade tools, including around large installations such as power stations and CERN
  • Airport cargo handling
  • Recycling collections
  • Warehouse inventory transportation
  • Mail
  • Food collection
  • Child transport (in Amsterdam, freight trikes are used primarily to carry children)

Children's tricycle

Compared to adult trikes, children's model are simpler, without brakes or gears, and often with crude front-drive. Tricycles are typically used by children between the ages of two and five, after which point they usually switch to a bicycle, often with training wheels (stabilisers). Child trikes can be unstable, particularly if the wheelbase or track are insufficient.[18] Some trikes have a push bar so adults can control the trike.[18] Child trikes may have frames made of metal, plastic, or even bamboo.[19]

"Budget" child trikes have pedals directly driving the front wheels, for better control of the bike and braking issues but better models (such as the Pashley Pickle) have chain drive to a single rear wheel. Children's rear-drive trikes lack a differential, so one rear wheel spins free. Rear-drive is preferable to front-drive as most of the rider's weight is on the rear wheels; indeed most front drive trikes are prone to skidding when force is applied to the pedals.[citation needed]

Unlike adult bikes, children's trikes do not always have pneumatic tires, having instead wheels of solid rubber or hollow plastic. While this may add to the weight of the tricycle and reduces the shock-absorbing qualities, it eliminates the possibility of punctures. Pull brakes are rarely fitted to front-drive trikes, but the child can slow the trike down by resisting the forward motion through the pedals.

A peculiar design, called grillo ("cricket" in Italian), with a half chain, has been popular in Italy among children for decades, especially for rental in parks.[20]

Drift trike

Drift trikes are a variety of tricycle with slick rear wheels, enabling them to drift, being countersteered round corners. They are commonly used for gravity-powered descents of paved roads with steep gradients.

Hand and foot trike

With hand and foot trikes, the rider makes a pair of front wheels change directions by shifting the center of weight and moves forward by rotating the rear wheel. The hand and foot trike can be also converted into a manual tricycle designed to be driven with both hands and both feet.[21][22] There are also new hybrids between a handcycle, a recumbent bike and a tricycle, these bikes make it even possible to cycle with legs despite a spinal cord injury.[better source needed][23]

Conversion sets

Tricycle conversion sets or kits convert a bicycle to an upright tricycle. Tricycle kit can remove the front wheel and mounts two wheels under the handlebars for a quick and easy conversion.[24]

The advantages of a trike conversion set include lower cost compared with new hand built tricycles and the freedom to choose almost any donor bicycle frame. Tricycle conversion sets tend to be heavier than a high quality, hand built, sports, touring or racing tricycle. Conversion sets can give the would-be serious tricyclist a taste of triking before making the final decision to purchase a complete tricycle. Conversion sets can also supplied ready to be brazed onto a lightweight, steel bicycle frame to form a complete trike.[citation needed]

Some trike conversion sets can also be used with recumbent bicycles to form recumbent trikes.[citation needed]

Operation

Adults may find upright tricycles difficult to ride because of familiarity with the counter-steering required to balance a bicycle. The variation in the camber of the road is the principal difficulty to be overcome once basic tricycle handling is mastered. Recumbent trikes are less affected by camber and, depending on track width and riding position, capable of very fast cornering. Some trikes are tilting three-wheelers, which lean into corners much as bicycles do.

In the case of delta tricycles, the drive is often to just one of the rear wheels, though in some cases both wheels are driven through a differential. A double freewheel, preferably using no-backlash roller clutches, is considered superior. Trikes with a differential often use an internally geared hub as a gearbox in a 'mid drive' system. A jackshaft drive permits either single or two-wheel drive. Tadpoles generally use a bicycle's rear wheel drive and for that reason are usually lighter, cheaper and easier to replace and repair.

Braking

Some trikes use a geometry (also called center point steering) with the kingpin axis intersecting the ground directly ahead of the tire contact point, producing a normal amount of trail. This arrangement, elsewhere called "zero scrub radius" is used to mitigate the effects of one-sided braking on steering. While zero scrub can reduce steering feel and increase wandering it can also protect novices from spinning out and/or flipping.

Tadpole trikes tend also to use Ackermann steering geometry, perhaps with both front brakes operated by the stronger hand. While the KMX Kart stunt trike with this setup allows the rear brake to be operated separately, letting the rider do "bootlegger turns", the standard setup for most trikes has the front brake for each side operated by each hand. The center-of-mass of most tadpole trikes is close to the front wheels, making the rear brake less useful. The rear brake may instead be connected to a latching brake lever for use as a parking brake when stopped on a hill.

Recumbent trikes often brake one wheel with each hand, allowing the rider to brake one side alone to pull the trike in that direction.

Manufacturers

Specialist makers of upright trikes in the UK include Longstaff Cycles, Higgins (which ceased trading in the 1960s), Trykit and Pashley Cycles. Italian company Di Blasi make a folding upright trike.

Makers of recumbent trikes include KMX; Hase (who make the Kettwiesel delta, improbably named after the British children's programme Catweazle); Inspired Cycle Engineering, who make the Trice range of tadpole trikes; AVD, who build the record-holding Burrows Windcheetah or Speedy, now exhibited in the Metropolitan Museum of Modern Art (MoMA); Australia's Greenspeed, one of the oldest manufacturers; Michigan-based WhizWheelz, whose ten models include a tadpole and a tandem; Big Cat HPV, which builds the eight Catrike models in Florida; and Sidewinder Cycle, which has a front wheel drive system with rear wheel steering builds 3 models all with Electric assist capability located in California.

The largest manufacturer of recumbent trikes is Sun Bicycles of Taiwan who make both tadpole and delta trikes. The deltas are built from designs licensed from Gardner Martin's EasyRacers, a leading builder of recumbent bicycles.

Records

On 1 July 2005, Sudhakar Yadav from India rode the largest tricycle in Hyderabad which had an overall height of 12.67 metres (41.6 ft). The tricycle exhibited at the Sudha Cars Museum entered the Guinness World Records and had wheel diameter of 5.18 metres (17.0 ft) and length of 11.37 metres (37.3 ft).[25][26]

See also



This article uses material from the Wikipedia article "Tricycle", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht