Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (June 2012) (Learn how and when to remove this template message) |
Cruiser tank | |
---|---|
Crusader I with auxiliary turret | |
Type | Armoured fighting vehicle |
Place of origin | Britain |
Service history | |
In service | 1937–1945 |
Used by | British Army |
Wars | Second World War |
Specifications | |
Main armament | 2-Pounder gun |
Secondary armament | 7.9 mm machine-gun |
Era | |
---|---|
Country | |
Type |
The cruiser tank (also called cavalry tank[citation needed] or fast tank[citation needed]) was a British tank concept of the interwar period for tanks designed to function as modernised armoured and mechanised cavalry. Cruiser tanks were developed after the Royal Armoured Corps were not satisfied with many of the medium tank designs of the 1930s. The cruiser tank concept was conceived by Giffard Le Quesne Martel, who preferred many small light tanks to swarm the enemy, instead of a few expensive medium tanks. There were two main types of cruiser tanks: "light" cruiser tanks and "heavy" cruiser tanks. "Light" cruiser tanks were lightly armoured and relatively fast (for example, the Cruiser Mk I), while "heavy" cruiser tanks were more heavily armoured and slightly slower than "light" cruiser tanks (for example, the Cruiser Mk II).
The British cruiser tank series started in 1938 with the A9 and A10 cruiser tanks, followed by the A13, A13 Mark II, the A13 Mark III "Covenanter" in 1940 and the A15 Crusader which entered service in 1941. The Crusader was superseded by the A27 Cromwell in 1944. The A34 Comet - a better-armed development of Cromwell - began to enter service in late 1944. The Centurion tank of 1946 became the "Universal tank" of the United Kingdom, transcending the cruiser and infantry tank roles and becoming one of the first main battle tanks (MBT).
Dissatisfaction with experimental medium tank designs of the mid-1930s led to the development of specialised fast cruiser tanks, where armour thickness was sacrificed for speed and infantry tanks, in which speed was sacrificed for heavier armour. Financial constraints had made it impossible to produce a vehicle suitable for close support and for exploitation. The thinking was behind several tank designs which saw action during the Second World War. British armoured operations theory flowed from the decision to build two types of tank and equip two types of unit and formation. Cruisers were operated by armoured regiments of the Royal Armoured Corps, established on 4 April 1939, in armoured divisions, some regiments coming from the Royal Tank Regiment (RTR) and some from cavalry regiments converted during the war. Infantry tanks went to Army Tank Battalions, sometimes grouped administratively into Army Tank Brigades of the RTR. Small, fast, lightly armed tanks like the Light Tank Mk VI operated as reconnaissance vehicles.
Giffard Le Quesne Martel originated the cruiser concept while Assistant Director and then Deputy Director of Mechanisation at the War Office in the 1930s. Martel considered that medium tanks were too complicated and expensive for infantry support, where they would be too vulnerable to anti-tank weapons and rejected claims that they could fire accurately when moving, so would gain no benefit from their speed. Martel preferred a large number of smaller and simpler tanks to swamp an opponent, instead of a few comparatively expensive medium tanks. Work should continue on a universal tank in the long term but from 1936 to 1939, Martel gave much thought to the infantry tank; he did not want medium tank development to be split but saw the logic of it, given the constraints on tank development. Tanks were necessary for mobile operations in armoured divisions and for infantry support in attacks on fortified defensive positions; a vehicle satisfactory for both tasks appeared to be impossible to attain. Two types of vehicle led to two theories and procedures, infantry tank thinking coming from the experience of tank operations from 1916 to 1918, when British tanks had been used for infantry support. Armoured division theory emphasised the speed of cruiser tanks and independent action to protect flanks, attack the opponent's flanks and rear, to counter-attack and conduct pursuit operations.
Like naval cruisers, cruiser tanks were fast and mobile for operations independent from slower-moving infantry with their heavier infantry tanks and artillery. When gaps had been forced through the opponent's front by the infantry tanks, cruisers were to penetrate to the rear and attack lines of supply and communication centres in accordance with the theories of J.F.C. Fuller, Percy Hobart and B. H. Liddell Hart. The cruiser tank was designed for use in a manner similar to cavalry, which made speed the most important factor and to achieve this, early cruisers were lightly armoured and armed to save weight.
The emphasis on speed unbalanced the British designs; on limited engine power, the speed was possible only by sacrificing armour protection (by comparison infantry tanks operating at soldiers' pace could carry far more armour). The idea that "speed is armour" was considered most important in the Royal Tank Corps. It was not realised[citation needed] that the principle of mobility was a liability against the German policy of accepting lower speeds for superior armour and armament, ensuring that even one round from a German medium tank could easily destroy a cruiser.
An even bigger problem for most cruiser tanks was the small calibre of their main gun. The first cruisers were armed with the 2-pounder (40 mm) gun. This gun had adequate armour penetration against early war tanks, but was never issued high explosive ammunition. This made the cruisers less able to deal with towed anti-tank guns, which became a major issue with the extended combat ranges of the Desert Campaign. the additional machine gun turret (as mounted on the Crusader) was no substitute for HE rounds. As the armour of German tanks increased British cruisers were up-gunned with the more powerful 57 mm QF 6-pounder gun, starting with the Crusader Mk. III (an interim move pending the introduction of the next cruiser tank). Early marques of what would become the Cromwell were also fitted with the 6-pdr but this gun still did not have a satisfactory HE round. The Cromwell as planned was to have a High Velocity 75 mm gun but the design was not sufficient to mount one and so decided that the new Cromwell tanks would be fitted with the QF 75mm (a bored out 6-pdr design that could take US 75 mm ammunition). The new 75 mm gun providing greater HE capability at the expense of some armour penetration, however it was still adequate to deal with the majority of German armoured vehicles. Part of the Cromwell's success was its high-power to weight ratio, provided by the adoption of the Rolls Royce Merlin engine as the Meteor, which delivered sufficient power for the Cromwell to have a maximum speed around 40 mph (64 km/h) on roads.[a] The new powerplant enabled the tank to be far more heavily armoured and armed than previous cruiser designs.
As the Cromwell could not be fitted with the HV 75 mm, work was undertaken to produce a tank for the powerful 17-pdr anti-tank gun, able to take out the heaviest of German vehicles. To this end the Cruiser Mk VIII Challenger was developed, mounting a 17-pdr gun on a lengthened Cromwell hull and a totally new turret. The Challenger was an unhappy compromise, though it was popular with its crews the cut in armour protection to allow the mounting of the larger gun meant it was not well suited to closer range engagements and it threw its tracks more often than the Cromwell. As the UK had large numbers of US M4 Sherman tanks, an extemporaneous conversion of the Sherman to take a 17-pounder (as the Sherman Firefly) proved effective in providing more 17-pounder gun tanks, the Firefly accompanied Churchills, Shermans and Cromwells generally at a ratio of 1:4. The production of Fireflies greatly outpaced that of the Challenger but in Cromwell-equipped units, the Challenger was generally preferred as the Sherman had a slower road speed and inferior cross-country mobility.
The culmination of British efforts was the Comet tank with a cut down 17-pounder design, the 77 mm HV. The Comet was a further development of the Cromwell, a "heavy" cruiser tank, which sought to remove the need for 17-pdr armoured vehicles, such as the Challenger or Firefly in tank platoons. The Comet reduced its road speed in comparison to the Cromwell to 32 mph (51 km/h), in favour of better armour protection and a weapon able to penetrate the armour of the heavier German tanks whilst not sacrificing HE capability. The tank had a short service life as design for the Centurion was already well underway, with the first prototype arriving in 1945.
Despite the emphasis on high mobility, most cruisers were plagued by mechanical unreliability, notably the Crusader tank in the hot and gritty desert of the North Africa Campaign. This problem was usually caused by rushed development and introduction into service. Most of the early cruiser tank designs were ordered "off the drawing board", particularly given the urgent need for tanks following the fall of France. The Liberty engine which also powered early Cruiser tanks was beginning to show its age and was being pushed to its limit in tanks such as the Crusader. This problem was not fully solved until the débût of the Cromwell tank in 1944, with its powerful, reliable Rolls-Royce Meteor engine.
Year | Light | I tank/ Cruiser |
Total |
---|---|---|---|
1938 4th Qtr |
169 | 29 | 198 |
1939 | 734 | 235 | 969 |
1940 to June |
140 | 418 | 558 |
Total | 1,043 | 682 | 1,725 |
In 1936, the War Office decided on a light tank for the cavalry, a cruiser tank, a medium tank and an infantry or assault tank. By 1938, the medium tank had stagnated as a research project, in favour of heavier cruiser and infantry tanks and after the outbreak of war, the move towards heavy infantry tanks capable of breaking through the Siegfried Line (Westwall) on the German border.[2]
In 1934, Sir John Carden of Vickers-Armstrongs had produced a "Woolworth" medium tank to a 1934 specification (General Staff number A.9) for a close support tank, using elements of the Medium Mk III design (which had been abandoned due to financial reasons) but lighter and using a commercial engine to be cheaper.[3] It was accepted as an interim design for limited production as the Cruiser Tank Mark I. It was expected to be replaced by a Christie suspension design. From 1937–1938, 125 A9s were built. The A9 was lightly armoured but capable of 25 mph (40 km/h) and carried a highly-effective 2-pounder anti-tank gun.
The Cruiser Mk II (A10), was designed by Carden as an infantry tank, built to the same design with added armour for 30 mm (1.2 in) of protection. It was insufficiently armoured for the role but as a "heavy cruiser", it was put into production in July 1938 as another interim design. It had the same gun as the A9, was the first to be equipped with the Besa machine gun and 175 Mk IIs were produced by September 1940.[4] Experience with the A9 during the Battle of France in 1940, revealed shortcomings, including inadequate armour and a lack of space for the crew but it saw useful service in France, the Western desert and Greece in 1941. Orders for the Mk I and Mk II Cruisers were limited, for an advanced and faster cruiser tank which would incorporate Christie suspension designed by J. Walter Christie and have better armour.
In 1936, General Giffard LeQuesne Martel, a pioneer in tank design who had published works on armoured warfare and pioneered the lightly armoured "tankette" concept to enhance infantry mobility, became Assistant Director of Mechanization at the War Office. Later that year, Martel had watched Soviet tanks at the Red Army's autumn manoeuvres including the BT tank, which they had developed from Christie's work. He urged the adoption of a tank that would use the suspension system and also follow the Christie practice of using a lightweight aircraft engine such as the Liberty L-12 engine or a Napier Lion. The government authorised purchase and licensing of a Christie design via the Nuffield Organization.[5][6]
The tank A13 E1 was rudimentary and too small for British use but the Nuffield suspension was most effective and this became the basis of the Cruiser Mk III (A13). Following testing of two Nuffield-built prototypes (A13E2 and A13E3), the A13 was ordered into production and 65 were manufactured by mid-1939.[6] The Mk III weighed 31,400 pounds (14.2 t), had a crew of 4, a 340 hp engine which gave a top speed of 30 mph (48 km/h) and was armed with a 2-pounder (40 mm) gun and a machine gun. When it was introduced in 1937, the army still lacked a formal tank division.[7] The trackless element of the Christie suspension was discarded as adding little value for the extra complexity. The Cruiser Mk IV (A13 Mk II) had heavier armour than the Mk III and production started in 1938.[8]
During the first half of World War II it was used in large numbers in the Western Desert Campaign. The contemporary Covenanter was unreliable and was retained in the UK for training use. The Cavalier, Centaur and Cromwell tanks were the planned successors to the Covenanter and Crusader. Intended to be in production by 1942, the project was delayed and the Crusader was up-gunned as an interim measure with the Mk.III 6-pounder gun; the Cavalier was a development of Crusader. Centaur and Cromwell tanks were an alternative design using the Cavalier engine and the new Rolls-Royce Meteor respectively. The Centaur and Cromwell went into action at the Invasion of Normandy.
The Comet tank was a development from medium tanks.[citation needed] During the war, the development of much more powerful engines and better suspension enabled heavier tanks to approximate the speed of cruisers with the protection of infantry tanks and the concept became obsolete. The Centurion tank was designed to satisfy the "Heavy Cruiser" criterion, by combining the mobility of a cruiser tank and armour of an Infantry tank in one chassis, which evolved into the "Universal tank" concept to "do it all". The Centurion transcended its cruiser tank origins and became the first modern British main battle tank.
The cruiser-tank concept was also employed by the Soviet Union in the 1930s, as exemplified by the BT tank series (Russian: bystrokhodniy tank, [fast tank]).
This article uses material from the Wikipedia article "Cruiser tank", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht