powered by CADENAS

Social Share

Amazon

Medium tank (9500 views - Transportation - Air Water Earth)

Medium tank is a classification of tanks, particularly prevalent during World War II which represented a compromise between the mobility oriented light tanks and the armour and armament oriented heavy tanks. The most widely produced, cost effective and successful tanks of World War II (the Soviet T-34, the American Sherman tank, the Japanese Type 97 and the German Panzer IV) were all medium tank designs, and the success of the concept would later lead to the development of later generations of medium tanks such as the Chieftain. Many of the medium tanks lines became what are called main battle tank in most countries.
Go to Article

Explanation by Hotspot Model

Youtube


    

Medium tank

Medium tank

Medium tank

Medium tank is a classification of tanks, particularly prevalent during World War II which represented a compromise between the mobility oriented light tanks and the armour and armament oriented heavy tanks. The most widely produced, cost effective and successful tanks of World War II (the Soviet T-34, the American Sherman tank, the Japanese Type 97 and the German Panzer IV) were all medium tank designs, and the success of the concept would later lead to the development of later generations of medium tanks such as the Chieftain. Many of the medium tanks lines became what are called main battle tank in most countries.

History

The first tanks to carry the name Medium appeared in the First World War with the British Medium Mark A "Whippet". It was smaller and lighter than the British heavy tanks and only carried machine guns.

The medium tank doctrine came into use in the interwar period. Its existence outlasted the super-heavy tank and heavy tank and gradually transitioned into the main battle tank.

World wars

Medium tanks of the interwar period included the British Vickers Medium Mark II and the Soviet multi-turreted T-28. In the period leading up to World War II, the British stopped using the term Medium for their tanks as the new philosophy of Cruiser tank and Infantry tank which defined tanks by the role rather than size came into use.

There were medium tanks that focused on anti-infantry capabilities (such as in World War II: the Panzer IV short-barrel, and the M4 Sherman), and medium tanks which were more focused on the anti-tank role, mounting high-velocity tank guns. The French cavalry tanks (Chars de Cavalerie) focused on speed in addition to power and protection of the other designs. They were similar to what other countries called medium tanks.

When Soviet tank designers were preparing a successor to the BT tank series, they combined its excellent mobility with thick, sloped armour and the unprecedented[citation needed] firepower of a 76 mm high-velocity gun. The result was the T-34 medium tank, whose superb capabilities shocked the German Wehrmacht when it invaded the Soviet Union. The lessons of Blitzkrieg, first employed by the Germans and eventually adopted by other nations, found their best expression in formations of mutually-supporting medium tanks and motorised infantry. The traditional view of infantry and cavalry tank roles was rendered obsolete.

Both the Soviet Union and the United States benefited from their ability to manufacture a well-balanced medium tank in very large numbers - around 57,000 T-34s and 49,000 M4 Sherman tanks were built during the war period.[citation needed]

Cold War

During and after World War II, the roles of light tanks were gradually taken over by less-expensive armoured cars and specialised reconnaissance vehicles. Heavy tanks, having shown their limitations in combat, experienced a limited post-war arms race of progressively more heavily armed and armoured designs. With the rise of more sophisticated anti-tank missile weapons, to which heavy tanks had demonstrated high vulnerability, these too were eventually phased out.

With advances in technology, aspects such as mobility, armour and weaponry pushed the medium tank to form the core of a countries armoured fighting capability, eventually merging into the Main Battle Tank. Simpler and more economical self-propelled guns, and later anti-tank guided missiles, came to fulfil some fire-support and anti-tank roles, thus shifting the tactical approach how tanks were used.

In the 1990s, medium tanks continued to be use, such as Canadian medium tanks in Kosovo in 1999 which were much better suited to the poor roads and soft ground than the French armoured cars there, but were still able to move along narrow streets and over lighter bridge classifications than the much heavier American Abrams tanks.

Role

The role of medium tanks started with a prioritisation of speed. Medium tanks could travel faster, but needed help to cross trenches, where heavy tanks were large enough to cross unaided. In British use, this evolved into the Cruiser tank class, while other tank doctrines formed around the medium tank making the main advance.

In this later use, medium tanks represent the designer's intent of producing a successful balance of firepower, mobility, and protection. Medium tanks aim to be suitable to the widest variety of roles, with less reliance on other types of tank during normal operations

See also



This article uses material from the Wikipedia article "Medium tank", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht