Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 4.0 (Alexander Migl).
Mercedes-Benz CLS-Class | |
---|---|
Overview | |
Manufacturer |
|
Production | 2004 – present |
Body and chassis | |
Class | Mid-size luxury car |
Body style |
|
Layout | FR / 4WD (4matic) |
The Mercedes-Benz CLS-Class is a series of mid-size luxury cars produced by Mercedes-Benz since 2004.
The original model was a four-door fastback based on the Mercedes E-Class platform, marketed as a four door coupé.[1] An estate (Shooting Brake) model was later added to the model range with the second generation CLS.[2] All models are available as a high performance AMG variant, although it wasn't until the second generation CLS that 4MATIC all-wheel drive was offered.[3]
The CLS range is positioned above the E-Class but below the S-Class in the Mercedes model range[4][5], and models tend to be less practical than the E-Class it is based on.[6]
Marketed as a four-door coupé, the CLS was designed by Michael Fink in 2001[7] who also styled the first generation CLK, the C-SportCoupé, and Maybach 57 and 62.[8] The W219 CLS is based on the W211 E-Class platform, and shares major components including the engines, transmissions, and has an identical wheelbase of 2,854 mm (112 in).[9] IVM Automotive, a subsidiary of German roof system specialist Edscha, developed the entire vehicle from the CLS Vision concept on which the CLS is based on[10], to the production version which debuted at the 2004 New York International Auto Show.[11]
The W218 CLS is the second generation model, and was sold from 2011 to 2018.[12] The body styles of the range are a 4-door coupé (C218 model code), and a 5-door estate (X218 model code, marketed as Shooting Brake). The design of the CLS was based on the Mercedes F800 concept and featured design cues from other models including the Mercedes SLS AMG.[13] Unlike its predecessor, the W218 CLS is available with all-wheel drive and can be optionally configured on CLS63 AMG models as well.[14] In 2014, the CLS underwent a facelift and featured design changes, engine enhancements, and the adoption of the Mercedes 9G-Tronic automatic transmission.[15]
The C257 CLS is the third and current generation model, and is only available as a 4-door sedan and in all-wheel drive (4MATIC) configuration.[16] The Shooting Brake body style was in development for the C257 CLS, but was shortly discontinued due to poor and declining demand overseas for the last generation model.[17] The range of engines consist of a 3.0-litre straight six turbocharged petrol engine and a 2.9-litre straight six turbocharged diesel engine.[18]
The following are the sales figures of the CLS in Europe and in the United States:[19][20]
Year | EU total | US total |
---|---|---|
2004 | 5,543 | - |
2005 | 20,147 | 14,835 |
2006 | 20,262 | 10,763 |
2007 | 17,098 | 7,906 |
2008 | 12,224 | 5,775 |
2009 | 6,083 | 2,527 |
2010 | 3,975 | 2,135 |
2011 | 17,414 | 5,665 |
2012 | 12,797 | 8,065 |
2013 | 15,139 | 8,032 |
2014 | 10,289 | 6,981 |
2015 | 12,600 | 6,152 |
2016 | 7,803 | 4,156 |
2017 | 5,116 | 1,839 |
Wikimedia Commons has media related to Mercedes-Benz CLS-Class. |
This article uses material from the Wikipedia article "Mercedes-Benz CLS-Class", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer