powered by CADENAS

Social Share

Rack unit (14772 views - Electrical Engineering)

A rack unit (abbreviated U or RU) is a unit of measure defined as 44.50 millimetres (1.752 in). It is most frequently used as a measurement of the overall height of 19-inch and 23-inch rack frames, as well as the height of equipment that mounts in these frames, whereby the height of the frame or equipment is expressed as multiples of rack units. For example, a typical full-size rack cage is 42U high, while equipment is typically 1U, 2U, 3U, or 4U high.
Go to Article

Explanation by Hotspot Model

Rack unit

Rack unit

Rack unit

A rack unit (abbreviated U or RU) is a unit of measure defined as 44.50 millimetres (1.752 in). It is most frequently used as a measurement of the overall height of 19-inch and 23-inch rack frames, as well as the height of equipment that mounts in these frames, whereby the height of the frame or equipment is expressed as multiples of rack units. For example, a typical full-size rack cage is 42U high, while equipment is typically 1U, 2U, 3U, or 4U high.

Definition

The rack unit size is based on a standard rack specification as defined in EIA-310. The Eurocard specifies a standard rack unit as the unit of height; it also defines a similar unit, horizontal pitch (HP), used to measure the width of rack-mounted equipment. The standard was adopted worldwide as IEC 60297 Mechanical structures for electronic equipment - Dimensions of mechanical structures of the 482,6 mm (19 in) series, and defines the sizes for rack, subrack (a shelf-like chassis in which cards can be inserted), and the pitch of printed circuit boards/cards providing physical compatibility of technological equipment, typically in telecommunications.

While a rack unit is defined as 44.50 millimetres (1.752 in), a front panel or filler panel in a rack is not an exact multiple of this height. To allow space between adjacent rack-mounted components, a panel is 132 inch (0.03125 in or 0.794 mm) less in height than the full number of rack units would imply. Thus, a 1U front panel would be 1.721 inches (43.7 mm) tall. If n is number of rack units, the formula for panel height is h = (1.751n − 0.031) for calculating in inches, and h = (44.5n − 0.79) for calculating in mm.

The mounting-hole distance (as shown to the right) differs for 19-inch racks and 23-inch racks: The 19-inch racks uses uneven spacings (as shown to the right) while the 23-inch racks uses evenly spaced mounting holes. Although it is called a 19-inch rack unit, the actual mounting dimensions of a 19-inch rack unit are 18516 or 18.3125 inches (465.1 mm)[1] wide, center to center.

Configurations

A typical full size rack is 42U,[2] which means it holds just over 6 feet (1.8 m) of equipment, and a typical "half-height" rack would be 18–22U, or around 3 feet (0.91 m) high.

The term "half-rack" can have different separate meanings: It can describe equipment that fits in a certain number of rack units, but occupy only half the width of a 19-inch rack (9.5 inches (241.30 mm)). These are commonly used when a piece of equipment does not require full rack width, but may require more than 1U of height. For example, a "4U half-rack" DVCAM deck would occupy 4U (7 in) height × 9.5 in width, and in theory, two 4U half-rack decks could be mounted side by side and occupy the 4U space. It can also describe a unit that is 1U high and half the depth of a 4-post rack (such as a network switch, router, KVM switch, or server), such that two units can be mounted in 1U of space (one mounted at the front of the rack and one at the rear). When used to describe the rack enclosure itself, the term "half-rack" typically means a rack enclosure that is half the height (22U tall).

Rack units are universally the same, but the type of thread[3] can vary depending on the rack. Mounting rails can be No. 10-32 tapped (Unified Thread Standard), No. 12-24 tapped, metric M6 threaded or universal square holes. Universal square holes are becoming the most common as these allow the insertion of replaceable cage nuts for the type of thread needed. This prevents stripping of the threading on the rails and allows for more flexibility.

See also



This article uses material from the Wikipedia article "Rack unit", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced