powered by CADENAS

Social Share

Amazon

Hurricane (cocktail) (6087 views - Food Drinks Beverages)

The hurricane is a sweet alcoholic drink made with rum, fruit juice, and syrup or grenadine. It is one of many popular drinks served in New Orleans. The creation of this passion fruit–colored relative of a daiquiri is credited to New Orleans tavern owner Pat O'Brien. The bar allegedly started as a speakeasy called Mr. O'Brien's Club Tipperary and the password was "storm's brewin'".In the 1940s, he needed to create a new drink to help him get rid of all of the less-popular rum that local distributors forced him to buy before he could get a few cases of more popular liquors such as scotch and other whiskeys. He poured the concoction into hurricane lamp–shaped glasses and gave it away to sailors. The drink caught on, and it has been a mainstay in the French Quarter ever since. It is more commonly served in a disposable plastic cup, as New Orleans laws permit drinking in public and leaving a bar with a drink, but the city prohibits public drinking from glass containers.The hurricane cocktail is made differently on the islands of the Bahamas. The drink is composed of various measures of coffee liqueur, 151 rum, Irish cream, and Grand Marnier. It is commonly found in the downtown bars of Nassau.
Go to Article

Explanation by Hotspot Model

Youtube


    

Hurricane (cocktail)

Hurricane (cocktail)

Hurricane
Cocktail
A hurricane served in the typical glass at Pat O'Brien's, New Orleans
TypeCocktail
Primary alcohol by volume
Served"On the rocks"; poured over ice
Standard drinkwarehurricane lamp–shaped glass
Commonly used ingredients
PreparationShake ingredients with ice, then pour into the glass and serve over ice.
Notes+

The hurricane is a sweet alcoholic drink made with rum, fruit juice, and syrup or grenadine. It is one of many popular drinks served in New Orleans.

The creation of this passion fruit–colored relative of a daiquiri is credited to New Orleans tavern owner Pat O'Brien.[1] The bar allegedly started as a speakeasy called Mr. O'Brien's Club Tipperary and the password was "storm's brewin'".[1]

In the 1940s, he needed to create a new drink to help him get rid of all of the less-popular rum that local distributors forced him to buy before he could get a few cases of more popular liquors such as scotch and other whiskeys.[2][3] He poured the concoction into hurricane lamp–shaped glasses and gave it away to sailors.

The drink caught on, and it has been a mainstay in the French Quarter ever since.

A Hurricane in a disposable plastic cup

It is more commonly served in a disposable plastic cup, as New Orleans laws permit drinking in public and leaving a bar with a drink, but the city prohibits public drinking from glass containers.[4]

The hurricane cocktail is made differently on the islands of the Bahamas. The drink is composed of various measures of coffee liqueur, 151 rum, Irish cream, and Grand Marnier. It is commonly found in the downtown bars of Nassau.

See also



This article uses material from the Wikipedia article "Hurricane (cocktail)", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke