Licensed under Creative Commons Attribution 2.0 (Bundeswehr-Fotos).
This article's lead section does not adequately summarize key points of its contents. Please consider expanding the lead to provide an accessible overview of all important aspects of the article. Please discuss this issue on the article's talk page. (September 2012) |
Era | |
---|---|
Country | |
Type |
A main battle tank (MBT), also known as a battle tank or universal tank,[citation needed] is a tank that fills the armor-protected direct fire and maneuver role of many modern armies. Cold War-era development of more powerful engines, better suspension systems and lighter weight composite armor allowed a tank to have the firepower of a super-heavy tank, armor protection of a heavy tank, and mobility of a light tank all in a package with the weight of a medium tank. Through the 1960s, the MBT replaced almost all other tanks, leaving only some specialist roles to be filled by lighter designs or other types of armored fighting vehicles.
Today, main battle tanks are considered a key component of modern armies.[1] Modern MBTs seldom operate alone, as they are organized into armoured units which involve the support of infantry, who may accompany the MBTs in infantry fighting vehicles. They are also often supported by surveillance or ground-attack aircraft.[2]
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2017) (Learn how and when to remove this template message) |
During World War I, combining tracks, armor, and guns into a functional vehicle pushed the limits of mechanical technology. This limited the specific battlefield capabilities any one tank design could be expected to fulfill. A design might have good speed, armour, or firepower, but not all three at the same time.
Facing the deadlock of trench warfare, the first tank designs focused on crossing wide trenches, requiring very long and large vehicles, such as the British Mark I tank; these became known as heavy tanks. Tanks that focused on other combat roles were smaller, like the French Renault FT; these were light tanks or tankettes. Many late-war and inter-war tank designs diverged from these according to new, though mostly untried, concepts for future tank roles and tactics. Each nation tended to create its own list of tank classes with different intended roles, such as "cavalry tanks", "breakthrough tanks", "fast tanks", and "assault tanks". The British maintained cruiser tanks that focused on speed, and infantry tanks that traded speed for more armour.
After years of isolated and divergent development, the various interwar tank concepts were finally tested with the start of World War II. In the chaos of blitzkrieg, tanks designed for a single role often found themselves forced into battlefield situations they were ill-suited for. During the war, limited-role tank designs tended to be replaced by more general-purpose designs, enabled by improving tank technology. Tank classes became mostly based on weight (and the corresponding transport and logistical needs). This led to new definitions of heavy and light tank classes, with medium tanks covering the balance of those between. The German Panzer IV tank, designed before the war as a "heavy" tank for assaulting fixed positions, got redesigned during the war with armour and gun upgrades to allow it to take on anti-tank roles as well, was reclassified as a medium tank.
The second half of World War II saw an increased reliance on general-purpose medium tanks, which became the bulk of the tank combat forces. Generally, these designs massed about 25-30 tonnes, were armed with cannons around 75 mm, and powered by engines in the 400 to 500 hp range. Notable examples include the Soviet T-34 (the most-produced tank to that time) and the US M4 Sherman.
Late war tank development placed increased emphasis on armour, armament, and anti-tank capabilities for medium tanks:
This section needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2017) (Learn how and when to remove this template message) |
In Britain, tank development had continued down the parallel development of cruiser tanks and infantry tanks. Development of the Rolls-Royce Meteor engine for the Cromwell tank, combined with efficiency savings elsewhere in the design, almost doubled the available horsepower for cruiser tanks.[11] This increase led to speculation of a "Universal Tank", able to take on the roles of both a cruiser and an infantry tank by combining both armor and maneuverability.[12]
Field Marshal Bernard Montgomery is acknowledged as the main advocate of the British universal tank concept.[13] Design of a universal tank commenced but was ultimately overtaken by events. Continued development of the basic Cromwell design led eventually to the Centurion. Centurion was designed as a cruiser tank, usually prioritizing mobility and firepower at the expense of armor, but the increase in engine power allowed sufficient armour to be mounted to undertake the Infantry tank role as well.
Development of the universal tank ceased, and Centurion entered service just as World War II finished, becoming a multi-role vehicle forming the main battle tank force of the British army (and other nations through export). The addition of the 20 pounder gun in 1948 gave the tank a significant advantage over other tanks of the era.[14] This paved the way for a new tank classification, the main battle tank, and Centurion is considered by many to be the first MBT as designed.
A surplus of effective WWII-era designs in other forces, notably the US and the Soviet Union, led to slower introductions of similar designs on their part. By the early 1950s, these designs were clearly no longer competitive, especially in a world of shaped charge weapons, and new designs rapidly emerged from most armed forces.
The concept of the medium tank gradually evolved into the MBT in the 1960s,[15] as it was realized that medium tanks could carry guns (such as the US 90 mm, Soviet 100 mm, and especially the British L7 105 mm) that could penetrate any practical level of armour at long range. Also, the heaviest tanks were unable to use most existing bridges. The World War II concept of heavy tanks, armed with the most powerful guns and heaviest armour, became obsolete because the large tanks were too expensive and just as vulnerable to damage by mines, bombs, rockets, and artillery. Likewise, World War II had shown that lightly armed and armoured tanks were of limited value in most roles. Even reconnaissance vehicles had shown a trend towards heavier weight and greater firepower during World War II; speed was not a substitute for armour and firepower.
An increasing variety of anti-tank weapons and the perceived threat of a nuclear war prioritized the need for additional armour. The additional armour prompted the design of even more powerful guns.[16] The main battle tank thus took on the role the British had once called the "universal tank", exemplified by the Centurion, filling almost all battlefield roles. Typical main battle tanks were as well armed as any other vehicle on the battlefield, highly mobile, and well armoured. Yet they were cheap enough to be built in large numbers. The first Soviet main battle tank was the T-64[17] (the T-54/55 and T-62 were considered "medium" tanks)[18] and the first American nomenclature-designated MBT was the M60 Patton.[19]
Anti-tank weapons rapidly outpaced armour developments. By the 1960s anti-tank rounds could penetrate a meter of steel so as to make the application of traditional rolled homogeneous armour unpragmatic. The first solution to this problem was the composite armor of Soviet T-64 tank, which included steel-glass-reinforced textolite-steel sandwich in heavily sloped glacis plates, and steel turret with aluminum inserts, which helped to resist both high-explosive anti-tank (HEAT) and APDS shells of the era. Later came British Chobham armour. This composite armour utilized layers of ceramics and other materials to help attenuate the effects of HEAT munitions. Another threat came by way of the widespread use of helicopters in battle. Before the advent of helicopters, armour was heavily concentrated to the front of the tank. This new threat caused designs to distribute armour on all sides of the tank (also having the effect of protecting the vehicle's occupants from nuclear explosion radiation).[20]
By the late 1970s, MBTs were manufactured by China, France, West Germany, Britain, India, Italy, Japan, the Soviet Union, Sweden, Switzerland, and the United States.[21]
The Soviet Union's war doctrine depended heavily on the main battle tank. Any weapon advancement making the MBT obsolete could have devastated the Soviet Union's fighting capability.[22] The Soviet Union made novel advancements to the weapon systems including mechanical autoloaders and anti-tank guided missiles. Autoloaders were introduced to replace the human loader, permitting the turret to be reduced in size, making the tank smaller and less visible as a target,[16] while missile systems were added to extend the range at which a vehicle could engage a target and thereby enhance the first-round hit probability.[16]
The United States's experience in the Vietnam War contributed to the idea among army leadership that the role of the main battle tank could be fulfilled by attack helicopters. During the Vietnam War, helicopters and missiles competed with MBTs for research money.[23]
Though the Persian Gulf War reaffirmed the role of main battle tanks,[clarification needed] MBTs were outperformed by the attack helicopter.[24] Other strategists considered that the MBT was entirely obsolete in the light of the efficacy and speed with which coalition forces neutralized Iraqi armour.[25]
In asymmetric warfare, threats such as improvised explosive devices and mines have proven effective against MBTs. In response, nations that face asymmetric warfare, such as Israel, are reducing the size of their tank fleet and procuring more advanced models.[26][27]
The United States Army used 1,100 M1 Abrams in the course of the Iraq War. They proved to have an unexpectedly high vulnerability to improvised explosive devices.[28] A relatively new type of remotely detonated mine, the explosively formed penetrator, was used with some success against American armoured vehicles. However, with upgrades to their rear armour, M1s proved to be valuable in urban combat; at the Second Battle of Fallujah the United States Marines brought in two extra companies of M1s.[29] Britain deployed its Challenger 2 tanks to support its operations in southern Iraq.
Advanced armour has not improved vehicle survivability, but has reduced crew fatalities.[30] Small unmanned turrets on top of the cupolas called remote weapon stations armed with machine guns or mortars provide improved defence and enhance crew survivability. Experimental tanks with unmanned turrets locate crew members in the heavily armoured hull, improving survivability and reducing the vehicle's profile.[31]
Technology is reducing the weight and size of the modern MBT.[32] A British military document from 2001 indicated that the British Army would not procure a replacement for the Challenger 2 because of a lack of conventional warfare threats in the foreseeable future. The obsolescence of the tank has been asserted, but the history of the late 20th and early 21st century suggested that MBTs were still necessary.[33]
Main battle tanks remain a useful tool for internal security. States (such as Japan, Bangladesh and Indonesia) lacking expeditionary ambitions, or even credible land-based threats from abroad, are bolstering their ground forces with MBTs for the express purpose of maintaining internal security.[26]
A main battle tank has been officially described by the Organization for Security and Co-operation in Europe as "a self-propelled armoured fighting vehicle, capable of heavy firepower, primarily of a high muzzle velocity direct fire main gun necessary to engage armoured and other targets, with high cross-country mobility, with a high level of self-protection, and which is not designed and equipped primarily to transport combat troops."[34]
|
Originally, most MBTs relied on steel armour to defend against various threats. As newer threats emerged, however, the defensive systems used by MBTs had to evolve to counter them. One of the first new developments was the use of explosive reactive armour (ERA), developed by Israel in the early 1980s to defend against the shaped-charge warheads of modern anti-tank guided missiles and other such high-explosive anti-tank (HEAT) projectiles. This technology was subsequently adopted and expanded upon by the United States and the Soviet Union.
MBT armour is concentrated at the front of the tank, where it is layered up to 33 centimetres (13 in) thick.[35]
Missiles are cheap and cost-effective anti-tank weapons.[36] ERA can be quickly added to vehicles to increase their survivability. However, the detonation of ERA blocks creates a hazard to any supporting infantry near the tank. Despite this drawback, it is still employed on many Russian MBTs, the latest generation Kontakt-5 being capable of defeating both HEAT and kinetic energy penetrator threats. The Soviets also developed Active Protection Systems (APS) designed to more actively neutralize hostile projectiles before they could even strike the tank, namely the Shtora and Arena systems. The United States has also adopted similar technologies in the form of the Missile Countermeasure Device and as part of the Tank Urban Survival Kit used on M1 Abrams tanks serving in Iraq. The latest Russian MBT,according to many forum members the T-14 Armata, incorporates an AESA radar as part of its Afghanit APS and in conjunction with the rest of its armament, can also intercept aircraft and missiles.[37][38]
MBTs can also be protected from radar detection by incorporating stealth technology. The T-14 Armata has a turret designed to be harder to detect with radars and thermal sights.[39] Advanced camouflage, like the Russian Nakidka, will also reduce the radar and thermal signatures of a MBT.[40] The use of electric engines, such as the ones being considered for use on the Turkish Altay, can also reduce the thermal signature of the tank.[41]
Other defensive developments focused on improving the strength of the armour itself; one of the notable advancement coming from the British with the development of Chobham armour in the 1970s. It was first employed on the American M1 Abrams and later the British Challenger 1. Chobham armour uses a lattice of composite and ceramic materials along with metal alloys to defeat incoming threats, and proved highly effective in the conflicts in Iraq in the early 1990s and 2000s; surviving numerous impacts from 1950–60s–era rocket-propelled grenades with negligible damage. It is much less efficient against later models of RPGs. For example, the RPG-29 from the 1980s is able to penetrate the frontal hull armour of the Challenger 2.[42][43]
Main battle tanks are equipped with a main tank gun, and at least one machine gun.
MBT main guns are generally between 100 and 125 mm caliber, and can fire both anti-armour and, more recently, anti-personnel rounds. The cannon serves a dual role, able to engage other armoured targets such as tanks and fortifications, and soft targets such as light vehicles and infantry. It is fixed to the turret, along with the loading and fire mechanism. Modern tanks utilize a sophisticated fire-control system, including rangefinders, computerized fire control, and stabilizers, which are designed to keep the cannon stable and aimed even if the hull is turning or shaking, making it easier for the operators to fire on the move and/or against moving targets. Gun-missile systems are complicated and have been particularly unsatisfactory to the United States who abandoned gun-missile projects such as the M60A2 and MBT-70,[44] but have been diligently developed by the Soviet Union, who even retrofitted them to T-55 tanks, in an effort to double the effective range of the vehicle's fire. The MBT's role could be compromised because of the increasing distances involved and the increased reliance on indirect fire.[31] The tank gun is still useful in urban combat for precisely delivering powerful fire while minimizing collateral damage.[25]
High explosive anti-tank (HEAT), and some form of high velocity kinetic energy penetrator, such as APFSDS (armour-piercing fin stabilized discarding sabot) rounds are carried for anti-armour purposes. Anti-personnel rounds such as high explosive or high explosive fragmentation have dual purpose. Less common rounds are Beehive anti-personnel rounds, and high explosive squash head (HESH) rounds used for both anti-armour and bunker busting. Usually, an MBT carries 30-50 rounds of ammunition for its main gun, usually split between HE, HEAT and kinetic energy penetrator rounds. Some MBTs may also carry smoke or white phosphorus rounds. Some MBTs are equipped with an autoloader, such as the French Leclerc, or the Russian/Ukrainian T-64, T-72, T-80, T-84, T-90, and T-14 and, for this reason, the crew can be reduced to 3 members. MBTs with an autoloader require one less crew member and the autoloader requires less space than its human counterpart, allowing for a reduction in turret size. Further, an autoloader can be designed to handle rounds which would be too difficult for a human to load.[45] This reduces the silhouette which improves the MBT's target profile. However, with a manual loader, the rounds can be isolated within a blowout chamber, rather than a magazine within the turret, which could improve crew survivability. However, the force of a modern depleted uranium armour piercing fin discarding sabot round at the muzzle can exceed 6000 kN (a rough estimate, considering a uranium 60 cm/2 cm rod, 19g/cm3, @ 1,750 m/s). Composite+reactive armour could withstand this kind of force through its deflection and deformation, but with a second hit in the same area, an armour breach is inevitable. As such, the speed of follow up shots is crucial within tank to tank combat.[46]
As secondary weapons, an MBT usually uses between two and four machine guns to engage infantry and light vehicles. Many MBTs mount one heavy caliber anti-aircraft machine gun (AAMG), usually of .50 caliber (like the M2 Browning or DShK), which can be used against helicopters and low flying aircraft. However, their effectiveness is limited in comparison to dedicated anti-aircraft artillery. The tank's machine guns are usually equipped with between 500 and 3000 rounds each.
MBTs, like previous models of tanks, move on continuous tracks, which allow a decent level of mobility over most terrain including sand and mud. They also allow tanks to climb over most obstacles. MBTs can be made water-tight, so they can even dive into shallow water (5 m (16 ft) with snorkel). However, tracks are not as fast as wheels; the maximum speed of a tank is about 65 km/h (40 mph) (72 km/h (45 mph) for the Leopard 2). The extreme weight of vehicles of this type (45-70 tons) also limits their speed. They are usually equipped with a 1,200–1,500 hp (890–1,120 kW) engine (more than 25,000 cc (1,526 cu in)), with an operational range near 500 km (310 mi).
The German Army has prioritized mobility in its Leopard 2 which is considered the fastest MBT in existence.[36]
The MBT is often cumbersome in traffic and frequently obstructs the normal flow of traffic. The tracks can damage some roads after repeated use. Many structures like bridges do not have the load capacity to support an MBT. In the fast pace of combat, it is often impossible to test the sturdiness of these structures. In the 2003 invasion of Iraq, an M1 Abrams attempting to cross a bridge to evade enemy fire plummeted into the Euphrates river when the bridge collapsed.[25] Though appreciated for its excellent off-road characteristics, the MBT can become immobilized in muddy conditions.
The high cost of MBTs can be attributed in part to the high-performance engine-transmission system and to the fire control system. Also, propulsion systems are not produced in high enough quantities to take advantage of economies of scale.[47]
Crew fatigue limits the operational range of MBTs in combat. Reducing the crew to three and relocating all crewmembers from the turret to the hull could provide time to sleep for one off-shift crewmember located in the rear of the hull. In this scenario, crewmembers would rotate shifts regularly and all would require cross-training on all vehicle job functions.[48] Cargo aircraft are instrumental to the timely deployment of MBTs. The absence of sufficient numbers of strategic airlift assets can limit the rate of MBT deployments to the number of aircraft available.[49]
Military planners anticipate that the airlift capability for MBTs will not improve in the future.[50] To date, no helicopter has the capability to lift MBTs.[25] Rail and road are heavily used to move MBTs nearer to the battle, ready to fight in prime condition.[50] Where well maintained roads allow it, wheeled tank transporters can be used.[51]
The difficult task of resupply is usually accomplished with large trucks.[52]
Main battle tanks have internal and external storage space. Internal space is reserved for ammunition. External space enhances independence of logistics and can accommodate extra fuel and some personal equipment of the crew.[53]
The Israeli Merkava can even accommodate crew members displaced from a destroyed vehicle in its ammunition compartment.[48]
Emphasis is placed on selecting and training main battle tank crew members. The crew must perform their tasks faultlessly and harmoniously so commanders select teams taking into consideration personalities and talents.[25]
The main battle tank fulfills the role the British had once called the "universal tank", filling almost all battlefield roles. They were originally designed in the Cold War to combat other MBTs.[31] The modern light tank supplements the MBT in expeditionary roles and situations where all major threats have been neutralized and excess weight in armour and armament would only hinder mobility and cost more money to operate.
Reconnaissance by MBTs is performed in high-intensity conflicts where reconnaissance by light vehicles would be insufficient due to the necessity to "fight" for information.[50]
In asymmetric warfare, main battle tanks are deployed in small, highly concentrated units. MBTs fire only at targets at close range and instead rely on external support such as unmanned aircraft for long range combat.[54]
Main battle tanks have significantly varied characteristics. Procuring too many varieties can place a burden on tactics, training, support and maintenance.[55]
The MBT has a positive morale effect on the infantry it accompanies.[56] It also instills fear in the opposing force who can often hear and even feel their arrival.[25]
MBT production is increasingly being outsourced to wealthy nations. Countries that are just beginning to produce tanks are having difficulties remaining profitable in an industry that is increasingly becoming more expensive through the sophistication of technology. Even some large-scale producers are seeing declines in production. Even China is divesting many of its MBTs.[50]
The production of main battle tanks is limited to manufacturers that specialize in combat vehicles. Commercial manufacturers of civilian vehicles cannot easily be repurposed as MBT production facilities.[57]
Prices for MBTs have more than tripled from 1943 to 2011, although this pales in comparison with the price increase in fighter aircraft from 1943 to 1975.[31]
This section needs expansion. You can help by adding to it. (April 2011) |
Several MBT models, such as the AMX-40 and OF-40, were marketed almost solely as export vehicles.[50] Several tank producers, such as Japan and Israel, choose not to market their creations for export.[50] Others have export control laws in place.
Wikimedia Commons has media related to Main battle tanks. |
This article uses material from the Wikipedia article "Main battle tank", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht