powered by CADENAS

Social Share

Amazon

Panton Chair (7025 views - Interior Design)

The Panton Chair (Danish: Pantonstolen) is an S-shaped plastic chair created by the Danish designer Verner Panton in the 1960s. The world's first moulded plastic chair, it is considered to be one of the masterpieces of Danish design. The chair was included in the 2006 Danish Culture Canon.
Go to Article

Explanation by Hotspot Model

Youtube


    

Panton Chair

Panton Chair

Panton Chair
DesignerVerner Panton (Denmark)
Date1960
MaterialsMoulded plastic
Style / traditionModernist

The Panton Chair (Danish: Pantonstolen) is an S-shaped plastic chair created by the Danish designer Verner Panton in the 1960s. The world's first moulded plastic chair, it is considered to be one of the masterpieces of Danish design. The chair was included in the 2006 Danish Culture Canon.[1]

History

The idea of designing a stackable plastic chair was first expressed by the German architect and designer Ludwig Mies van der Rohe before the Second World War. From the early 1950s, Panton too had dreamt of making a stackable, cantilevered plastic chair all in one piece. It is said he had been inspired in particular by a neatly stacked pile of plastic buckets. In 1956, he designed the S Chair which can be considered a forerunner of the Panton Chair. He saw it as an item of furniture in which the back, seat and legs were made of the continuous piece. It was first produced in 1965.[2][3]

Panton made a series of sketches and design drawings for the Panton Chair in the 1950s. In 1960, he created his first model, a plaster-cast, in collaboration with Dansk Akrylteknik.[2] In the mid-1960s, he met Willi Fehlbaum from the furniture manufacturer Vitra who, unlike many other producers, was fascinated with the drawings of his legless chair in plastic rather than wood, the favoured material of the times. Working closely with Fehlbaum, Panton produced a cold-pressed model using polyester strengthened with fibreglass. For the first time, an entire chair had been designed in one piece, without any legs. It became known as a free-swinger. The first rather heavy model, which required substantial finishing work, was subsequently improved and adapted to industrial production using thermoplastic polystyrene which led to a marked reduction in cost.[4] In 1968, Vitra initiated serial production of the final version which was sold by the Herman Miller Furniture Company. The material used was Baydur, a high-resilience polyurethane foam produced by Bayer in Leverkusen, Germany. It was varnished in seven colors.[5]

In 1979, however, production was halted as it became apparent that polystyrene (reference required, as in the previous section polyurethane was mentioned as the material from 1968 to 1979) was not sufficiently durable and began to look shabby over time. Four years later, the model was again produced as the Panton Chair Classic, this time in the rather more expensive polyurethane structural foam. Finally, in 1999, Vitra used polypropylene for manufacturing the Panton Plastic Chair in a variety of colours.[4]

Exotic appeal

Panton was a contributor to the development of sleek new styles reflecting the "Space Age" of the 1960s which became known as Pop Art. The Panton Chair in particular was seen as being sleek and curvaceous. When it was unveiled in the Danish design journal Mobilia in 1967, it caused a sensation. In 1970, it was featured in the British fashion magazine Nova with a sequence of shots illustrating "How to undress in front of your husband".[6] Perhaps the chair's most famous appearance was in January 1995, when it was featured on the cover of the British edition of Vogue. The photograph by Nick Knight also included a naked Kate Moss.[7]

Museum collections

Over the years, the Panton Chair, initially known as Panton's S Chair, has been widely exhibited in Denmark and abroad. It currently forms part of the permanent collections some of the world's most famous design museums including, New York's Museum of Modern Art, London's Design Museum, Berlin's German Historical Museum and Copenhagen's Danish Museum of Art & Design.[8][9]

See also



This article uses material from the Wikipedia article "Panton Chair", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art