Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 2.0 (Rufino Uribe).
A push-button (also spelled pushbutton) or simply button is a simple switch mechanism for controlling some aspect of a machine or a process. Buttons are typically made out of hard material, usually plastic or metal.[1] The surface is usually flat or shaped to accommodate the human finger or hand, so as to be easily depressed or pushed. Buttons are most often biased switches, although many un-biased buttons (due to their physical nature) still require a spring to return to their un-pushed state. Different people use different terms for the "pushing" of the button, such as press, depress, mash, hit, and punch.
The "push-button" has been utilized in calculators, push-button telephones, kitchen appliances, and various other mechanical and electronic devices, home and commercial. In industrial and commercial applications, push buttons can be connected together by a mechanical linkage so that the act of pushing one button causes the other button to be released. In this way, a stop button can "force" a start button to be released. This method of linkage is used in simple manual operations in which the machine or process has no electrical circuits for control.
In popular culture, the phrase "the button" (sometimes capitalized) refers to a (usually fictional) button that a military or government leader could press to launch nuclear weapons.
To avoid the operator from pushing the wrong button in error, pushbuttons are often color-coded to associate them with their function. Commonly used colors are red for stopping the machine or process and green for starting the machine or process.
Red pushbuttons can also have large heads (called mushroom heads) for easy operation and to facilitate the stopping of a machine. These pushbuttons are called emergency stop buttons and for increased safety are mandated by the electrical code in many jurisdictions. This large mushroom shape can also be found in buttons for use with operators who need to wear gloves for their work and could not actuate a regular flush-mounted push button. As an aid for operators and users in industrial or commercial applications, a pilot light is commonly added to draw the attention of the user and to provide feedback if the button is pushed. Typically this light is included into the center of the pushbutton and a lens replaces the pushbutton hard center disk. The source of the energy to illuminate the light is not directly tied to the contacts on the back of the pushbutton but to the action the pushbutton controls. In this way a start button when pushed will cause the process or machine operation to be started and a secondary contact designed into the operation or process will close to turn on the pilot light and signify the action of pushing the button caused the resultant process or action to start.
Akin to fire alarm switches, some big red buttons, when deployed with suitable visual and audible warnings such as flashing lights and sirens for extreme exigent emergencies, are known as scram switches (as in evacuate, vamoose, "get the hell out"). Generally, such buttons have extended large scale functions, beyond a "mere" fire alarm, such as automated shutdown procedures, complete facility power cut, fire suppression like halogen release, etc. A variant of this is the scramble switch which triggers an alarm to activate emergent personnel to proactively attend to and go to such disasters. An air raid siren at an air base initiates such action, where the fighter pilots are alerted and "scrambled" to their planes to defend the base.
This article uses material from the Wikipedia article "Push-button", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced