Licensed under Creative Commons Attribution 3.0 (Jim Gateley).
Gracht (Dutch pronunciation: [ɣrɑxt]; plural: grachten) is a Dutch word for a canal within a city. Grachten have often a round shape and form a circle around the city cores in the Netherlands, Belgium and northern Germany. Outside the Netherlands, the word grachten mostly refer to the city canals of Amsterdam, for which it is well known.[1][2]
The word gracht cannot be easily translated; for this reason, it is necessary to distinguish between four related terms:[3]
Although the word gracht means "canal" or "waterway" in the general sense, there is no exact equivalent for the term in English.
The word gracht stems from the older word graft, which is derived from graven, to dig. The Dutch language has had a sound shift in which the combination -ft became -cht. Other good examples are lucht (German: Luft, air) and zacht (English: soft). In some regional languages such as Frisian and Gronings, the word graft is still used.
In Dutch, the word gracht is used only when canals are located inside the city, while canals outside a city are called kanaal. However, Venice is an exception. In Dutch, one does not say "de grachten van Venetië" (the city-canals of Venice), but "de kanalen van Venetië" (the canals of Venice).[5]
Toponyms for grachten are usually made by the suffixes -gracht, -singel (which refers to the old circle-shaped canals), -wal (referring to the bank of the gracht), -vest (referring to a fortification), and -kade (Flemish: -kaai; quay). The suffix -diep is used in Groningen where it is a local word for a large canal.
When a gracht is a remake of an old river, the river's name is used.
Grachten were the life-lines of Dutch and Flemish cities. They were used for many purposes: for transportation, for draining, as water supply and as sewers, all at the same time. In heavily populated cities, these combined functions repeatedly proved to be detrimental to the public health.
Most Hanseatic cities have grachten to transport, to load and to land goods in and from ships. In the Netherlands, the northeastern cities of Deventer, Hindeloopen, Kampen, Leeuwarden, Meppel, Sneek, Zutphen and Zwolle are renowned for their historical grachten. Other cities in the Netherlands, in the western part of the country, are also touristic attractions because of their grachten, especially Alkmaar, Amersfoort, Gouda, Hoorn, Leiden, Utrecht and Weesp.
Sometimes grachten were made from older rivers, like in Groningen. There the older river called Drentse Aa was used as a natural part of the grachten. In Delft, the main gracht – Oude Delft – started as a drainage canal for reclaiming land in marshy surroundings: in a period roughly around the year 1100, a canal was delved, making use of a natural creek in the marshy country. This canal was called Delf, later on Delft, from the word delven that is akin to the verb to "delve" in English. This canal was used for draining the land at both sides; later on it also served as a waterway for transport.
Later, a second canal, called the Nieuwe Delft (New Delft) was dug through part of the settlement that had grown around the first. The original canal became known as the Oude Delft (Old Delft), a name it still bears today.
The rural village around Oude and Nieuwe Delft developed into a more urban area and the canals gradually acquired the character of city-canals or grachten. A third canal was dug and also changed into a gracht; it connected with the moat around the marketplace. The city and the grachten grew hand in hand. In 1246, this agglomeration was granted a city charter by the Count of Holland and became the City of Delft. A natural waterway was later incorporated in the city and became a gracht as well. Circular canals or singels were dug and surrounded the city. Fortifications were built along these singels and fixed the shape of the historical inner city of Delft. The characteristic, narrow grachten, perpendicular to the main grachten, developed from ditches that had been dug to drain and delimit the fields which preceded the city.
When it was still a Dutch colony, Cape Town had a network of grachten, that were fed by the springs at the base of Table Mountain. These provided water and sanitation for the infant town. In the ensuing centuries, the grachten were covered over, but many of the prominent streets in the modern city centre still bear their names (notably the Heerengracht, Keizersgracht, Buitengracht and Buitensingel). There is currently a project to restore some of these historic waterways.
A function in almost every city was drainage. Rainwater flowed through these city-canals. Usually they were also used as a sewer. Because these functions are not needed any more, many grachten have been filled in to give access to road traffic. However, these new streets have mostly retained the names of the grachts and singels they covered or replaced.
This article uses material from the Wikipedia article "Gracht", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library