powered by CADENAS

Social Share

Amazon

Triumphal arch (17972 views - Architecure & BIM & MEP)

A triumphal arch is a monumental structure in the shape of an archway with one or more arched passageways, often designed to span a road. In its simplest form a triumphal arch consists of two massive piers connected by an arch, crowned with a flat entablature or attic on which a statue might be mounted or which bears commemorative inscriptions. The main structure is often decorated with carvings, sculpted reliefs, and dedications. More elaborate triumphal arches may have multiple archways. Triumphal arches are one of the most influential and distinctive types of architecture associated with ancient Rome. Thought to have been invented by the Romans, the triumphal arch was used to commemorate victorious generals or significant public events such as the founding of new colonies, the construction of a road or bridge, the death of a member of the imperial family or the accession of a new emperor. The survival of great Roman triumphal arches such as the Arch of Titus inspired many post-Roman states and rulers, up to the present day, to erect their own arches in emulation of the Romans. Arches in the Roman style have been built in many cities around the world, most notably the Arc de Triomphe in Paris, the Narva Triumphal Arch in Saint Petersburg, the Wellington Arch in London, the Arcul de Triumf in Bucharest and India Gate in Delhi. Triumphal arch is also the name given to the arch above the entrance to the chancel of a medieval church where a rood can be placed.
Go to Article

Explanation by Hotspot Model

Youtube


    

Triumphal arch

Triumphal arch

A triumphal arch is a monumental structure in the shape of an archway with one or more arched passageways, often designed to span a road. In its simplest form a triumphal arch consists of two massive piers connected by an arch, crowned with a flat entablature or attic on which a statue might be mounted or which bears commemorative inscriptions. The main structure is often decorated with carvings, sculpted reliefs, and dedications. More elaborate triumphal arches may have multiple archways.

Triumphal arches are one of the most influential and distinctive types of architecture associated with ancient Rome. Thought to have been invented by the Romans, the triumphal arch was used to commemorate victorious generals or significant public events such as the founding of new colonies, the construction of a road or bridge, the death of a member of the imperial family or the accession of a new emperor.

The survival of great Roman triumphal arches such as the Arch of Titus inspired many post-Roman states and rulers, up to the present day, to erect their own arches in emulation of the Romans. Arches in the Roman style have been built in many cities around the world, most notably the Arc de Triomphe in Paris, the Narva Triumphal Arch in Saint Petersburg, the Wellington Arch in London, the Arcul de Triumf in Bucharest and India Gate in Delhi.

Triumphal arch is also the name given to the arch above the entrance to the chancel of a medieval church where a rood can be placed.[1]

Origins and development

Roman triumphal arches

The development of the triumphal arch is often associated with ancient Roman architecture. Roman aqueducts, bridges, amphitheaters and domes employed arch principles and technology.[2][3] The Romans probably borrowed the techniques of arch construction from their Etruscan neighbours.[2] The Etruscans used elaborately decorated single bay arches as gates or portals to their cities; examples of Etruscan arches survive at Perugia and Volterra.[4]

The two key elements of the Roman triumphal arch – a round-topped arch and a square entablature – had long been in use as separate architectural elements in ancient Greece, but the Greeks preferred the use of entablatures in their temples, and almost entirely confined their use of the arch to structures under external pressure, such as tombs and sewers. The Roman triumphal arch combined a round arch and a square entablature in a single free-standing structure. What were originally supporting columns became purely decorative elements on the outer face of arch, while the entablature, liberated from its role as a building support, became the frame for the civic and religious messages that the arch builders wished to convey through the use of statuary and symbolic, narrative and decorative elements.[5]

The modern term "triumphal arch" derives from the notion that this form of architecture was connected to the award and commemoration of a triumph to particularly successful Roman generals, by vote of the Roman senate. The earliest arches set up to commemorate a triumph were made in the time of the Roman Republic.[6] These were called fornices (s. fornix) and bore imagery that described and commemorated the victory and triumph. Lucius Steritinus is known to have erected two such fornices in 196 BC to commemorate his victories in Hispania. Another fornix was built on the Capitoline Hill by Scipio Africanus in 190 BC, and Quintus Fabius Maximus Allobrogicus constructed one in the Roman Forum in 121 BC.[7] None of these structures has survived and little is known about their appearance.[6]

Roman triumphal practices changed significantly at the start of the imperial period when the princeps Augustus decreed that triumphs and triumphal honours were to be confined to members of the Imperial family; in practice, this meant the ruling emperor or his antecedents. The term fornix was replaced by arcus (arch). While Republican fornices could be erected by a triumphator at his own discretion and expense, Imperial triumphal arches were sponsored by decree of the senate, or sometimes by wealthy holders of high office, to honour and promote emperors, their office and the values of empire.[4] Arches were not necessarily built as entrances, but – unlike many modern triumphal arches – they were often erected across roads and were intended to be passed through, not around.[3]

Most Roman triumphal arches were built during the imperial period. By the fourth century AD there were 36 such arches in Rome, of which three have survived - the Arch of Titus (AD 81), the Arch of Septimius Severus (203-205) and the Arch of Constantine (312). Numerous arches were built elsewhere in the Roman Empire.[6] The single arch was the most common, but many triple arches were also built, of which the Triumphal Arch of Orange (circa AD 21) is the earliest surviving example. From the 2nd century AD, many examples of the arcus quadrifrons – a square triumphal arch erected over a crossroads, with arched openings on all four sides – were built, especially in North Africa. Arch-building in Rome and Italy diminished after the time of Trajan (AD 98-117) but remained widespread in the provinces during the 2nd and 3rd centuries AD; they were often erected to commemorate imperial visits.[7]

Little is known about how the Romans viewed triumphal arches. Pliny the Elder, writing in the first century AD, was the only ancient author to discuss them.[8] He wrote that they were intended to "elevate above the ordinary world" an image of an honoured person usually depicted in the form of a statue with a quadriga.[8] However, the designs of Roman imperial triumphal arches – which became increasingly elaborate over time and evolved a regularised set of features – were clearly intended to convey a number of messages to the spectator.

The ornamentation of an arch was intended to serve as a constant visual reminder of the triumph and triumphator. As such, it concentrated on factual imagery rather than allegory. The façade was ornamented with marble columns, and the piers and attics with decorative cornices. Sculpted panels depicted victories and achievements, the deeds of the triumphator, the captured weapons of the enemy or the triumphal procession itself. The spandrels usually depicted flying Victories, while the attic was often inscribed with a dedicatory inscription naming and praising the triumphator. The piers and internal passageways were also decorated with reliefs and free-standing sculptures. The vault was ornamented with coffers. Some triumphal arches were surmounted by a statue or a currus triumphalis, a group of statues depicting the emperor or general in a quadriga.[4][7] The inscriptions on Roman triumphal arches were works of art in themselves, with very finely cut, sometimes gilded letters. The form of each letter and the spacing between them was carefully designed for maximum clarity and simplicity, without any decorative flourishes, emphasizing the Roman taste for restraint and order. This conception of what later became the art of typography remains of fundamental importance down to the present day.[3]

Post-Roman triumphal arches

Roman triumphal arches remained a source of fascination well after the fall of Rome, serving as a reminder of past glories and a symbol of state power. At Lorsch Abbey, the triple-arched Torhalle was built in deliberate imitation of a Roman triumphal arch to signify continuity between the Carolingian Empire and its Roman predecessor. It was not until the coming of the Renaissance, however, that rulers sought to associate themselves systematically with the Roman legacy by building their own triumphal arches. One of the earliest was the "Aragonese Arch" at the Castel Nuovo in Naples, erected by Alfonso V of Aragon in 1443, although like the later Porta Capuana this was engaged as part of the entrance to the castle. By the end of the 16th century the triumphal arch had become closely linked with court theatre, state pageantry and military fortifications. The motif of the triumphal arch was also adapted and incorporated into the facades of public buildings such as city halls and churches.[9]

Temporary triumphal arches made of lath and plaster were often erected for royal entries. Unlike the individual arches erected for Roman conquerors, Renaissance rulers often built a row of arches through which processions were staged. They defined a space for the movement of people and denoted significant sites at which particular messages were conveyed at each stage. Newly elected popes, for instance, processed through the streets of Rome under temporary triumphal arches built specially for the occasion. Arches were also built for dynastic weddings; when Charles Emmanuel I, Duke of Savoy married Infanta Catherine Michelle of Spain in 1585, he processed under temporary triumphal arches that asserted the antiquity of the House of Savoy and associated his dynasty, through the art and architecture of the arches, with the imperial Roman past.[9]

Images of arches gained great importance as well. Although temporary arches were torn down after they had been used, they were recorded in great detail in engravings that were widely distributed and survived long after the original arches had been destroyed. The medium of engraving gave the viewer the opportunity to examine the allegories and inscriptions presented by the arches in a way that would not have been possible during the event.[9] Sometimes the arches depicted were not even real structures but existed entirely as imaginary representations of royal propaganda. One famous example was the Ehrenpforte Maximilians I by Albrecht Dürer, commissioned by the Emperor Maximilian I. It was one of the largest prints ever produced, measuring 3.75 metres (12.3 ft) high and consisting of 192 individual sheets, depicting an arch that was never intended to be built. It was printed in an edition of 700 copies and distributed to be coloured and pasted on the walls of city halls or the palaces of princes.[10]

The French led the way in building new permanent triumphal arches when the imperial ambitions of the Bourbon kings and Napoleon Bonaparte led to a spate of arch-building. By far the most famous arch from this period is the Arc de Triomphe in Paris, built from 1806–36, though it is consciously dissimilar from its Roman predecessors in omitting the customary ornamental columns – a lack that fundamentally changes the balance of the arch and gives it a distinctly "top-heavy" look.[9] Other French arches more closely imitated those of imperial Rome; the Arc de Triomphe du Carrousel in Paris, for instance, is closely modelled on the Arch of Septimius Severus in Rome.[11]

Triumphal arches have continued to be built into the modern era, often as statements of power and self-aggrandizement by dictators. Adolf Hitler planned to build the world's largest triumphal arch in Berlin. The arch would have been vastly larger than any previously built, standing 550 feet (170 m) wide, 92 feet (28 m) deep and 392 feet (119 m) – big enough for the Arc de Triomphe to fit into it 49 times. It was intended to be carved with the names of Germany's 1.8 million dead in the First World War. However, construction was never begun.[12] North Korea's dictator Kim Il Sung built the world's largest triumphal arch in Pyongyang in 1982.[7] It was designed to be substantially bigger than the Arc de Triomphe in Paris and was erected on the site where, on October 14, 1945, Kim Il Sung gave his first public speech to the North Korean people. It is decorated with sculptures and reliefs depicting "the triumphal returning of the victorious Great Leader to the country".[13]

The form of the triumphal arch has also been put to other purposes, notably the construction of monumental memorial arches and city gates such as the Brandenburg Gate in Berlin or the Washington Square Arch in New York City, or simple welcoming arches such as the Barcelona Triumphal Arch, built as an entrance to the fairgrounds for the 1888 World Fair. Although patterned after triumphal arches, these were built for quite different purposes - to memorialise war dead or to provide a monumental entrance to a city, as opposed to celebrating a military success or general.

See also



This article uses material from the Wikipedia article "Triumphal arch", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library