Licensed under Creative Commons Attribution 3.0 (Krish Dulal).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (December 2006) (Learn how and when to remove this template message) |
In telecommunications, transmission (abbreviations: TX, Xmit) is the process of sending and propagating an analogue or digital information signal over a physical point-to-point or point-to-multipoint transmission medium, either wired, optical fiber or wireless.[1][2]
One example of transmission is the sending of a signal with limited duration, for example a block or packet of data, a phone call, or an email. Transmission technologies and schemes typically refer to physical layer protocol duties such as modulation, demodulation, line coding, equalization, error control, bit synchronization and multiplexing, but the term may also involve higher-layer protocol duties, for example, digitizing an analog message signal, and data compression.
Transmission of a digital message, or of a digitized analog signal, is known as digital communication.
This article related to telecommunications is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Transmission (telecommunications)", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced