powered by CADENAS

Social Share

Amazon

Hamann Motorsport (8609 views - Cars & Motorbikes & Trucks)

Hamann Motorsport GmbH is a German car tuning company based in Laupheim. It specialises in Audi, Aston Martin, Bentley, BMW, Mini, Ferrari, Fiat, Jaguar, Land Rover, Maserati, Mercedes, Rolls Royce, Porsche and Lamborghini cars. Hamann Motorsport was founded by Richard Hamann in 1986. The company was founded only to work with cars made in Germany, specifically BMW, but since then, has expanded its business into other car manufacturers such as Lamborghini, Porsche, Aston Martin and Ferrari. It also creates its own, one-of-a-kind cars.Hamann offers cosmetic changes such as low profile spoilers, bodykits, carbon fiber splitters, and multi-piece alloy wheels. Other upgrades include racing LSDs, open racing exhaust systems, twelve-piston disc brakes, and engine remapping. The company orders crate engines from the dealership and then redesigns them.The company designs and builds upon numerous parts of the original car, such as tuning the car's engine, lowering the car, making a new body with more features, and installing racing tires.First car from the Hamann Motorsport was BMW M3 (E30), each producing 348 PS (256 kW) from a 2.3L R4 engine (with Turbocharger). The car accelerate from 0-60 mph in 5.1 seconds and reach top speed of 170 mph (273 km/h). Hamann Motorsports designed a variety of cars, for instance, the Lamborghini Murciélago LP640. Hamann built the engine from scratch to enhance the horsepower to reach 690HP by modifying the engine management system and installing a custom made exhaust system. For the exterior Hamann did not change much, they only installed the matte black wheels.
Go to Article

Explanation by Hotspot Model

Youtube


    

Hamann Motorsport

Hamann Motorsport

Hamann Motorsport

Licensed under Creative Commons Attribution 2.0 (Ed Callow).

Hamann Motorsport GmbH
Public
IndustryAutomotive
Founded1986
HeadquartersLaupheim, Germany
Key people
Richard Hamann
ProductsCars
WebsiteHamann-Motorsport.de

Hamann Motorsport GmbH is a German car tuning company based in Laupheim. It specialises in Audi, Aston Martin, Bentley, BMW, Mini, Ferrari, Fiat, Jaguar, Land Rover, Maserati, Mercedes, Rolls Royce, Porsche and Lamborghini cars. Hamann Motorsport was founded by Richard Hamann in 1986.

The company was founded only to work with cars made in Germany, specifically BMW, but since then, has expanded its business into other car manufacturers such as Lamborghini, Porsche, Aston Martin and Ferrari. It also creates its own, one-of-a-kind cars.[1]

Hamann offers cosmetic changes such as low profile spoilers, bodykits, carbon fiber splitters, and multi-piece alloy wheels. Other upgrades include racing LSDs, open racing exhaust systems, twelve-piston disc brakes, and engine remapping. The company orders crate engines from the dealership and then redesigns them.The company designs and builds upon numerous parts of the original car, such as tuning the car's engine, lowering the car, making a new body with more features, and installing racing tires.[2]

First car from the Hamann Motorsport was BMW M3 (E30), each producing 348 PS (256 kW) from a 2.3L R4 engine (with Turbocharger). The car accelerate from 0-60 mph in 5.1 seconds and reach top speed of 170 mph (273 km/h).

Hamann Motorsports designed a variety of cars, for instance, the Lamborghini Murciélago LP640. Hamann built the engine from scratch to enhance the horsepower to reach 690HP by modifying the engine management system and installing a custom made exhaust system. For the exterior Hamann did not change much, they only installed the matte black wheels.[3]

  1. ^ "The International Frankfurt Auto Show(2010)". Customized Aston Martin from Hamann and video editorial on One-77 from Aston Martin. West Coast Midnight Run. Archived from the original on 2012-03-25. Retrieved December 2010. Check date values in: |accessdate= (help)
  2. ^ "Introduction".
  3. ^ "Lamb". Retrieved 13 August 2013.

See also

  • Mansory, another multi-brand prestigious automobile tuning company
  • Prior Design, multi-brand automobile tuning company, specialises in Audi, BMW, Ford, Jaguar, Lamborghini, Mercedes-Benz, Range Rover and Porsche.


This article uses material from the Wikipedia article "Hamann Motorsport", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer