Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Ultra-high vacuum (UHV) is the vacuum regime characterised by pressures lower than about 10−7 pascal or 100 nanopascals (10−9 mbar, ~10−9 torr). UHV conditions are created by pumping the gas out of a UHV chamber. At these low pressures the mean free path of a gas molecule is greater than approximately 40 km, so the gas is in free molecular flow, and gas molecules will collide with the chamber walls many times before colliding with each other. Almost all molecular interactions therefore take place on various surfaces in the chamber.
UHV conditions are integral to scientific research. Surface science experiments often require a chemically clean sample surface with the absence of any unwanted adsorbates. Surface analysis tools such as X-ray photoelectron spectroscopy and low energy ion scattering require UHV conditions for the transmission of electron or ion beams. For the same reason, beam pipes in particle accelerators such as the Large Hadron Collider are kept at UHV.[1]
Maintaining UHV conditions requires the use of unusual materials for equipment. Heating of the entire system above 100 °C for many hours ("baking") to remove water and other trace gases which adsorb on the surfaces of the chamber is required upon "cycling" the equipment to atmosphere. To save time, energy, and integrity of the UHV volume an "interlock" is often used. The interlock volume has one door or valve facing the UHV side of the volume, and another door against atmospheric pressure through which samples or workpieces are initially introduced. After sample introduction and assuring that the door against atmosphere is closed, the interlock volume is typically pumped down to a medium-high vacuum. In some cases the workpiece itself is baked out or otherwise pre-cleaned under this medium-high vacuum. The gateway to the UHV chamber is then opened, the workpiece transferred to the UHV by robotic means or by other contrivance if necessary, and the UHV valve re-closed. While the initial workpiece is being processed under UHV, a subsequent sample can be introduced into the interlock volume, pre-cleaned, and so-on and so-forth, saving much time. Although a "puff" of gas is generally released into the UHV system when the valve to the interlock volume is opened, the UHV system pumps can generally snatch this gas away before it has time to adsorb onto the UHV surfaces. In a system well designed with suitable interlocks, the UHV components seldom need bakeout and the UHV may improve over time even as workpieces are introduced and removed.
Many common materials are used sparingly if at all due to high vapor pressure, high adsorptivity or absorptivity resulting in subsequent troublesome outgassing, or high permeability in the face of differential pressure (i.e.: "through-gassing"):
Technical limitations:
Ultra-high vacuum is necessary for many surface analytic techniques such as:
UHV is necessary for these applications to reduce surface contamination, by reducing the number of molecules reaching the sample over a given time period. At 0.1 mPa (10−6 Torr), it only takes 1 second to cover a surface with a contaminant, so much lower pressures are needed for long experiments.
UHV is also required for:
and, while not compulsory, can prove beneficial in applications such as:
Typically, UHV requires:
Outgassing is a problem for UHV systems. Outgassing can occur from two sources: surfaces and bulk materials. Outgassing from bulk materials is minimized by selection of materials with low vapor pressures (such as glass, stainless steel, and ceramics) for everything inside the system. Materials which are not generally considered absorbent can outgas, including most plastics and some metals. For example, vessels lined with a highly gas-permeable material such as palladium (which is a high-capacity hydrogen sponge) create special outgassing problems.
Outgassing from surfaces is a subtler problem. At extremely low pressures, more gas molecules are adsorbed on the walls than are floating in the chamber, so the total surface area inside a chamber is more important than its volume for reaching UHV. Water is a significant source of outgassing because a thin layer of water vapor rapidly adsorbs to everything whenever the chamber is opened to air. Water evaporates from surfaces too slowly to be fully removed at room temperature, but just fast enough to present a continuous level of background contamination. Removal of water and similar gases generally requires baking the UHV system at 200 to 400 °C while vacuum pumps are running. During chamber use, the walls of the chamber may be chilled using liquid nitrogen to reduce outgassing further.
Hydrogen and carbon monoxide are the most common background gases in a well-designed, well-baked UHV system. Both Hydrogen and CO diffuse out from the grain boundaries in stainless steel. Helium could diffuse through the steel and glass from the outside air, but this effect is usually negligible due to the low abundance of He in the atmosphere.
There is no single vacuum pump that can operate all the way from atmospheric pressure to ultra-high vacuum. Instead, a series of different pumps is used, according to the appropriate pressure range for each pump. Pumps commonly used to achieve UHV include:
UHV pressures are measured with an ion gauge, either a hot filament or an inverted magnetron type.
Metal seals, with knife edges on both sides cutting into a soft, copper gasket. This all-metal seal can maintain pressures down to 100 pPa (~10−12 Torr).
Measurement of high vacuum is done using a nonabsolute gauge that measures a pressure-related property of the vacuum, for example, its thermal conductivity. See, for example, Pacey.[3] These gauges must be calibrated.[4] The gauges capable of measuring the lowest pressures are magnetic gauges based upon the pressure dependence of the current in a spontaneous gas discharge in intersecting electric and magnetic fields.[5]
A UHV manipulator allows an object which is inside a vacuum chamber and under vacuum to be mechanically positioned. It may provide rotary motion, linear motion, or a combination of both. The most complex devices give motion in three axes and rotations around two of those axes. To generate the mechanical movement inside the chamber, two basic mechanisms are commonly employed: a mechanical coupling through the vacuum wall (using a vacuum-tight seal around the coupling), or a magnetic coupling that transfers motion from air-side to vacuum-side. Various forms of motion control are available for manipulators, such as knobs, handwheels, motors, stepping motors, piezoelectric motors, and pneumatics.
The manipulator or sample holder may include features that allow additional control and testing of a sample, such as the ability to apply heat, cooling, voltage, or a magnetic field. Sample heating can be accomplished by electron bombardment or thermal radiation. For electron bombardment, the sample holder is equipped with a filament which emits electrons when biased at a high negative potential. The impact of the electrons bombarding the sample at high energy causes it to heat. For thermal radiation, a filament is mounted close to the sample and resistively heated to high temperature. The infrared energy from the filament heats the sample.
This article uses material from the Wikipedia article "Ultra-high vacuum", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD