Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (June 2018) (Learn how and when to remove this template message) |
Vacuum engineering deals with technological processes and equipment that use vacuum to achieve better results than those run under atmospheric pressure. The most widespread applications of vacuum technology are:
Vacuum coaters are capable of applying various types of coatings on metal, glass, plastic or ceramic surfaces, providing high quality and uniform thickness and color. Vacuum dryers can be used for delicate materials and save significant quantities of energy due to lower drying temperatures.
Vacuum systems usually consist of gauges, vapor jet and pumps, vapor traps and valves along with other extensional piping’s. A vessel that is operating under vacuum system may be any of these types such as processing tank, steam simulator, particle accelerator, or any other type of space that has an enclosed chamber to maintain the system in less than atmospheric gas pressure. Since a vacuum is created in an enclosed chamber, the consideration of being able to withstand external atmospheric pressure are the usual precaution for this type of design. Along with the effect of buckling or collapsing, the outer shell of vacuum chamber will be carefully evaluated and any sign of deterioration will be corrected by the increase of thickness of the shell itself.The main material used for vacuum design are usually mild steel, stainless steel, and aluminum.Other sections such as glass are used for gauge glass or view ports or sometimes electrical insulation. The interior of vacuum chamber should always be smooth and free of rush and defections. High pressure solvent are usually used to remove any excess oil and contaminants that will affect vacuum in any way.Due to vacuum chamber is in an enclosed space, very specific detergents can be used to prevent any hazards or danger during cleaning. Any vacuum chamber should always have a certain number of access and viewing ports. These are usually served as a flange connection to the attachment of pumps, piping or any other parts required for system operation. The most importance is the fabrication of vacuum chambers sealing capability.The chamber itself must be airtight to maintain perfect vacuum, this is ensure through the process of leaking hunting generally using mass spectrometer leak detector.[1] All openings and connections are also assembled with O rings and gaskets to prevent any further possible leakage of air in the system.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (October 2017) (Learn how and when to remove this template message) |
Vacuum engineering uses techniques and equipment that vary greatly depending on the level of vacuum used. Pressure slightly reduced from atmospheric pressure may be used to control airflow in ventilation systems, or in material handling systems. Lower-pressure vacuums may be used in vacuum evaporation in processing of food stuffs without excessive heating. Higher grades of vacuum are used for degassing, vacuum metallurgy, and in the production of light bulbs and cathode ray tubes. So-called "ultrahigh" vacuums are required for certain semiconductor processing; the "hardest" vacuums with the lowest pressure are produced for experiments in physics, where even a few stray atoms of air would interfere with the experiment in progress.
Apparatus used varies with decreasing pressure. Blowers give way to various kinds of reciprocating and rotary pumps. For some important applications, a steam ejector can quickly evacuate a large process vessel to a rough vacuum, sufficient for some processes or as a preliminary to more complete pumping processes. The invention of the Sprengel pump was a critical step in the development of the incandescent light bulb as it allowed creation of a vacuum that was higher than previously available, which extended the life of the bulbs. At higher vacuum levels (lower pressures), diffusion pumps, absorption, cyrogenic pumps are used. Pumps are more like "compressors" since they gather the rarefied gases in the vacuum vessel and push them into a much higher pressure, smaller volume, exhaust. A chain of two or more different kinds of vacuum pumps may be used in a vacuum system, with one "roughing" pump removing most of the mass of air from the system, and the additional stages handling relatively smaller amounts of air at lower and lower pressures. In some applications, a chemical element is used to combine with the air remaining in an enclosure after pumping. For example, in electronic vacuum tubes, a metallic "getter" was heated by induction to remove the air left after initial pump down and closure of the tubes. The "getter" would also slowly remove any gas evolved within the tube during its remaining life, maintaining sufficiently good vacuum.
Vacuum technology is a method used to evacuate air from a closed volume by creating a pressure differential from the closed volume to some vent, the ultimate vent being the open atmosphere.[2] When using an industrial vacuum system, a vacuum pump or generator creates this pressure differential. A variety of technical inventions were created based on the idea of vacuum discovered during the 17th century. These range from vacuum generation pumps to X-ray tubes, which were later introduced to the medical field for use as sources of X-ray radiation. The vacuum environment has come to play an important role in scientific research as new discoveries are being made by looking back to the basic fundamentals of pressure. The idea of “perfect vacuum” cannot be realized, but very nearly approximated by the technological discoveries of the early 20th century. Vacuum engineering today uses a range of different material, from aluminum to zirconium and just about everything in between. There may be the popular belief that vacuum technology deals only with valves, flanges, and other vacuum components, but novel scientific discoveries are often made with the assistance of these traditional vacuum technologies, especially in the realm of high-tech. Vacuum engineering is used for compound semiconductors, power devices, memory logic, and photovoltaics.
Another technical invention is the vacuum pump. Such invention is used to remove gas molecules from sealed volume thus leaving behind a partial vacuum. More than one vacuum pumps are used in a single application to create fluent flow. Fluent flow is used to allow a clear path made using vacuum to remove any air molecules in the way of the process. Vacuum will be used in this process to attempted to create a perfect vacuum. A type of vacuum such as partial vacuum can be caused by the usage of positive displacement type pumps. A positive displacement pump is able to transfer gas load from the entrance to the exit port, but due to its limitation of design it can only achieve a relatively low vacuum. In order to reach a higher vacuum, other techniques must be used. By using a series of pump such as following up a fast pump down with a positive displacement type pump will create a way better vacuum than using a single pump. These combination of pump used is usually determined by the need of vacuum in the system.
Materials for use in vacuum systems must be carefully evaluated. Many materials have a degree of porosity, unimportant at ordinary pressures, but which would continually admit minute amounts of air into a vacuum system if incorrectly used. Some items, such as rubber and plastic, give off gases into a vacuum that can contaminate the system. At high and ultrahigh vacuum levels, even metals must be carefully selected - air molecules and moisture can cling to the surface of metals, and any trapped gas within the metal may percolate to the surface under vacuum. In some vacuum systems, a simple coating of low-volatile grease is sufficient to seal gaps in joints, but at ultrahigh vacuum, fittings must be carefully machined and polished to minimize trapped gas. It is usual practice to bake components of a high-vacuum system; at high temperatures, any gases or moisture adhering to the surface is driven off. However, this requirement affects which materials can be used.
Particle accelerators are the largest ultrahigh vacuum systems and can be up to kilometres in length.[3]
The word “Vacuum” is originated from the Latin word “vacua”, which is translated to the word “empty”.Physicist use vacuum to describe a partially empty space, where air or some other gases are being removed from one container. The idea of vacuum relating to the empty space has been speculated as early as 5th century from Greek philosophers, Aristotle (384-322 B.C.) was the one who came up with the relation of vacuum being an empty space in nature would be impossible to ever create.[4] This idea had stuck around for over centuries until the 17th century, when vacuum technology and physics was discovered. In the mid 17th century, Evangelista Torricelli studied the properties of a vacuum generated by a mercury column in a glass tube; this became the barometer, an instrument to observe variations in atmospheric air pressure. Otto von Guericke spectacularly demonstrated the effect of atmospheric pressure in 1654, when teams of horses could not separate two 20-inch diameter hemispheres, which had been placed together and evacuated. In 1698, Thomas Savery patented a steam pump that relied on condensation of steam to produce a low-grade vacuum, for pumping water out of mines. The apparatus was improved in the Newcomen atmospheric engine of 1712; while inefficient, it allowed coal mines to be exploited that otherwise would flood by ground water. During the years of 1564-1642, the famous scientist Galileo was one of the first physicist to conduct experiments to develop measured forces to develop vacuum using a piston in a cylinder.This was a big discovery for scientist and was shared among others. French scientist and philosopher Blaise Pascal used the idea that was discovered to look into further research of vacuum. Pascal discoveries were similar to Torricelli’s research as Pascal used similar methods to pull vacuum using mercury. It was until the year 1661, when the mayor of the city of Magdeburg used this discovery to invent or retrofit new ideas. The mayor Otto von Guericke created the first air pump, modified the idea of water pumps, and also modified manometers.Vacuum engineering today, provides the solution for all thin film needs in the mechanical industry. This method of engineering is typically used for R&D needs or large scale material production.
Vacuum was used to propel trains experimentally.
Pump technology hit a plateau until Geissler and Sprengle in the mid 19th century, who finally gave access to the high-vacuum regime. This led to the study of electrical discharges in vacuum, discovery of cathode rays,discovery of X-rays and the discovery of the electron. The photoelectric effect was observed in high vacuum, which was a key discovery that lead to the formulation of quantum mechanics and much of modern physics.
This article uses material from the Wikipedia article "Vacuum engineering", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD