Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under GNU Free Documentation License (Lzur).
Owiesno | |
---|---|
Village | |
Location of Owiesno | |
Coordinates: 50°40′N 16°42′E / 50.667°N 16.700°E / 50.667; 16.700Coordinates: 50°40′N 16°42′E / 50.667°N 16.700°E / 50.667; 16.700 | |
Country | Poland |
Voivodeship | Lower Silesian |
County | Dzierżoniów |
Gmina | Dzierżoniów |
Elevation | 400 m (1,300 ft) |
Population | 580 |
Owiesno [ɔˈvjɛsnɔ] (German: Habendorf) is a village in the administrative district of Gmina Dzierżoniów, within Dzierżoniów County, Lower Silesian Voivodeship, in south-western Poland.[1] It lies approximately 12 km (7 mi) south-east of Dzierżoniów, and 57 km (35 mi) south-west of the regional capital Wrocław. The village has a population of 580.
Owiesno was first mentioned as Ovesonovo in a 1260 deed and as Haverdorph in 1292. In 1945 it fell to Poland.
Upon the foundations of an old Knights Templar castle Przecław of Pogorzeli (Pogarell), the Bishop of Wrocław and chancellor of Emperor Charles IV, had a palace erected in the 14th century. It was rebuilt several times and decayed after 1945 so only ruins remain.
The Holy Trinity church (Polish: Kościół Św. Trójcy) was erected about 1583 and received a Boroque equipment including an altar with a Trinity painting about 1730.
Villages | |
---|---|
Seat (not part of the gmina) |
This Dzierżoniów County location article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Owiesno", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D - 3D Model - 3D CAD - 3D Building - 3D monument - 3D Map - 3D City - 3D GIS - LIDAR - CityGML - Paris London Berlin Rome Sydney Barcelona Vienna Wien Budapest Madrid London