An industrial park (also known as industrial estate, trading estate) is an area zoned and planned for the purpose of industrial development. An industrial park can be thought of as a more "heavyweight" version of a business park or office park, which has offices and light industry, rather than heavy industry.
Industrial parks are usually located on the edges of, or outside the main residential area of a city, and normally provided with good transportation access, including road and rail.[1] One such example would be the large number of industrial estates located along the River Thames in the Thames Gateway area of London. Industrial parks are usually located close to transport facilities, especially where more than one transport modes coincide, including highways, railroads, airports and ports.
This idea of setting land aside through this type of zoning is based on several concepts:
Different industrial parks fulfill these criteria to differing degrees. Many small communities have established industrial parks with only access to a nearby highway, and with only the basic utilities and roadways. Public transportation options may be limited or non-existent. There may be few or no special environmental safeguards.
An industrial park specializing in biotechnology is called a biotechnology industrial park. It may also be known as a bio-industrial park or eco-industrial cluster.
Flatted factories exist in cities like Singapore and Hong Kong, where land is scarce. These are typically similar to flats, but house individual industries instead. Flatted factories have cargo lifts and roads that serve each level, providing access to each factory lot.
UNIDO Viet Nam (United Nations Industrial Development Organization) has compiled a list of Industrial Parks in the ASEAN Economic Community in a report titled "Economic Zones in the ASEAN" written by Arnault Morisson.
This article uses material from the Wikipedia article "Industrial park", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library