powered by CADENAS

Social Share

Amazon

Jupiter-C (11540 views - Astronomy & Astrology)

The Jupiter-C was an American research and development vehicle developed from the Jupiter-A. Jupiter-C was used for three sub-orbital spaceflights in 1956 and 1957 to test re-entry nosecones that were later to be deployed on the more advanced PGM-19 Jupiter mobile missile. A member of the Redstone rocket family, Jupiter-C was designed by the U.S. Army Ballistic Missile Agency (ABMA), under the direction of Wernher von Braun. Three Jupiter-C flights were made followed by three satellite launches (Juno I). All were launched from Cape Canaveral, Florida.
Go to Article

Explanation by Hotspot Model

Youtube


    

Jupiter-C

Jupiter-C

Jupiter-C
Jupiter-C
Jupiter-C on the launch pad at Cape Canaveral
FunctionSounding rocket
ManufacturerChrysler for the ABMA
Country of originUnited States
Size
Height69.9 feet (21.3 m)
Diameter5.8 feet (1.8 m)
Mass64,000 pounds (29,000 kg)
Stages4
Capacity
Payload to
Sub-orbital
11 kg
Launch history
StatusRetired
Launch sitesLC-5 and 6, Cape Canaveral Missile Annex, Florida
Total launches3
Successes1
Failures1
Partial failures1
First flight20 September 1956
Last flight8 August 1957
First stage - Redstone (stretched)
Engines1 North American Aviation (Rocketdyne) 75-110-A-7
Thrust42,439 kgf (416,180 N; 93,560 lbf)
Specific impulse235 sec
Burn time155 seconds
FuelLOX/Hydyne
Second stage Sergeant cluster
Engines11 Solid
Thrust7,480 kgf (73,400 N; 16,500 lbf)
Specific impulse214 sec
Burn time6 seconds
FuelSolid
Third stage - Sergeant cluster
Engines3 Solid
Thrust2,040 kgf (20,000 N; 4,500 lbf)
Specific impulse214 sec
Burn time6 seconds
FuelSolid

The Jupiter-C was an American research and development vehicle[1][2] developed from the Jupiter-A.[3] Jupiter-C was used for three sub-orbital spaceflights in 1956 and 1957 to test re-entry nosecones that were later to be deployed on the more advanced PGM-19 Jupiter mobile missile.

A member of the Redstone rocket family, Jupiter-C was designed by the U.S. Army Ballistic Missile Agency (ABMA), under the direction of Wernher von Braun.[4] Three Jupiter-C flights were made followed by three satellite launches (Juno I).[5][6] All were launched from Cape Canaveral, Florida.

Description

Each vehicle consisted of a modified Redstone ballistic missile with two solid-propellant upper stages. The tanks of the Redstone were lengthened by 8 ft (2.4 m) to provide additional propellant. The instrument compartment was also smaller and lighter than the Redstone's. The second and third stages were clustered in a "tub" atop the vehicle.

Redstone, Jupiter-C and Mercury-Redstone rockets compared
Second stage cluster

The second stage was an outer ring of eleven scaled-down Sergeant rocket engines; the third stage was a cluster of three scaled-down Sergeant rockets grouped within. These were held in position by bulkheads and rings and surrounded by a cylindrical outer shell. The webbed base plate of the shell rested on a ball bearing shaft mounted on the first-stage instrument section. Two electric motors spun in the tub at a rate varying from 450 to 750 rpm to compensate for thrust imbalance when the clustered motors fired. The rate of spin was varied by a programmer so that it did not couple with the changing resonance frequency of the first stage during flight.[7]

The upper-stage tub was visibly spun-up before launch. During first-stage flight, the vehicle was guided by a gyro-controlled autopilot controlling both air-vanes and jet vanes on the first stage by means of servos. Following a vertical launch from a simple steel table, the vehicle was programmed so that it was traveling at an angle of 40 degrees from the horizontal at burnout of the first stage, which occurred 157 seconds after launch.[8]

At first-stage burnout, explosive bolts fired and springs separated the instrument section from the first-stage tankage. The instrument section and the spinning tub were slowly tipped to a horizontal position by means of four air jets located at the base of the instrument section. When the apex of the vertical flight occurred after a coasting flight of about 247 seconds, a radio signal from the ground ignited the eleven-rocket cluster of the second stage, separating the tub from the instrument section. The third stage then fired to raise the apogee. Through this system, designed by Wernher von Braun in 1956 for his proposed Project Orbiter, the Jupiter-C obviated the need for a guidance system in the upper stages.[9]

Juno I

The Juno I was a satellite launch vehicle based on the Jupiter-C, but with the addition of a fourth stage, atop the "tub" of the third stage. The Juno name derived from Von Braun wishing to make the satellite launch appear as peaceable as the Vanguard rocket, which was not a weapon, but was developed from a weather study rocket, the Viking. Since the Juno I was the same height as the Jupiter-C (21.2 meters), with the added fourth stage being hidden inside the shell, this vehicle which successfully launched the first orbital satellite of the United States is often incorrectly referred to as a Jupiter-C.

Encrypted serial number

The Jupiter-C was part of the IRBM project, and the sequence of manufacture of the rockets (which are not necessarily launched in order, and may be uprated as solutions to technical problems are worked out in tests) was considered a military secret. So the designation painted on the sides of the rocket was not a serial number in clear text, but employed a simple transformation cypher that the staff would be sure not to forget. The key was taken from the name of the design and test base: Huntsville, Alabama, giving HUNTSVILE, with duplicated letters dropped: H was used for 1, U for 2, ..., E for 9 and X for 0. For example, the Jupiter-C modified to launch Explorer 1 had "UE" painted on the side, indicating it was S/N 29 (U→2, E→9).[citation needed][10]

General characteristics

  • Weight as configured for Explorer 1 launch, loaded/empty
    • Overall, takeoff: 64,000 lb (29,000 kg)/10,230 lb (4640 kg)
    • Stage 1 62,700 lb (28,400 kg)/9,600 lb (4,400 kg)
    • Stage 2 1,020 lb (460 kg)/490 lb (220 kg)
    • Stage 3 280 lb (130 kg)/140 lb (64 kg)
  • Propulsion
    • Stage 1: Rocketdyne A-7 engine
      • Thrust, 83,000 lbf (370 kN)
      • burning time, 155 s
      • specific impulse, 235 s (2.30 kN·s/kg)
      • propellants, liquid oxygen, as oxidizer, and "Hydyne" (60% unsymmetrical dimethylhydrazine and 40% diethylenetriamine), as fuel
      • propellant feed, turbopump type
      • turbopump drive, 90% hydrogen peroxide decomposed by catalyst bed to produce steam
    • Stage 2: Eleven JPL scaled-down Sergeant rockets
      • Thrust, 16,500 lbf (73 kN)
      • burning time, 6.5 s
      • specific impulse, 220 s (2.16 kN·s/kg)
      • propellant, polysulfide-aluminum and ammonium perchlorate (solid propellant)
    • Stage 3: Three JPL scaled-down Sergeant rockets
      • Thrust, 4,500 lbf (24 kN)
      • burning time, 6.5 s
      • specific impulse, 235 s (2.30 kN·s/kg)
      • propellant, same as for Stage 2

Flight history

  • September 20, 1956: lifted an 86.5-lb (39.2 kg) payload (including a 30-lb (14 kg) dummy satellite) to an altitude of 680 mi (1,100 km), a speed of 16,000 mph (7 km/s), and a range of 3,300 mi (5,300 km) from Cape Canaveral, Florida[4]
  • May 15, 1957: lifted a 300 lb (140 kg) scale Jupiter ablative nose cone to an altitude of 350 mi (560 km) and a range of 710 mi (1,100 km)[4]
  • August 8, 1957: lifted a 1/3-scale Jupiter nose cone to an altitude of 285 mi (460 km) and a range of 1,330 mi (2,140 km); Juno I (four-stage configuration).[4]
  1. ^ "Redstone Arsenal Historical Information - 1957". The United States Army. Retrieved 2015-05-15.
  2. ^ "Redstone Arsenal Historical Information - Jupiter". The United States Army. Retrieved 2015-05-15.
  3. ^ "Rockets and Missiles". www.spaceline.org. Retrieved 2018-04-19.
  4. ^ a b c d "Jupiter-C Explorer-I". NASA.
  5. ^ "Redstone Arsenal Historical Information - Redstone Rocket". The United States Army. Retrieved 2015-05-15.
  6. ^ "Redstone Arsenal Historical Information - Explorer I". The United States Army. Retrieved 2015-05-15.
  7. ^ "ABMA Juno I". Designation-systems.net. Retrieved 2013-03-25.
  8. ^ Juno V Space Vehicle Development Program Report No. DSP-TM-10-58, NASA, October, 1958.
  9. ^ Juno V Space Vehicle Development Program Status Report, DSP-TM-11-58, NASA, November, 1958.
  10. ^ "Rockets and Missiles". www.spaceline.org. Retrieved 2018-04-19.


This article uses material from the Wikipedia article "Jupiter-C", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Astronomy & Astrology

3d,planet,jupiter,erath,venus,astrology,astronomy,esoteric