powered by CADENAS

Social Share

Semi-finished casting products (3505 views - Mechanical Engineering)

Semi-finished casting products are intermediate castings produced in a steel mill that need further processing before being a finished good. There are four types: ingots, blooms, billets, and slabs.
Go to Article

Explanation by Hotspot Model

Youtube


    

Semi-finished casting products

Semi-finished casting products

Semi-finished casting products are intermediate castings produced in a steel mill that need further processing before being a finished good. There are four types: ingots, blooms, billets, and slabs.[1]

Ingot

Ingots are large rough castings designed for storage and transportation. The shape usually resembles a rectangle or square with generous fillets. They are tapered, usually with the big-end-down.[2]

Bloom

In the era of commercial wrought iron, blooms were slag-riddled iron castings poured in a bloomery before being worked into wrought iron. In the era of commercial steel, blooms are intermediate-stage pieces of steel produced by a first pass of rolling (in a blooming mill) that works the ingots down to a smaller cross-sectional area, but still greater than 36 in2 (230 cm2).[1] Blooms are usually further processed via rotary piercing, structural shape rolling and profile rolling. Common final products include structural shapes, rails, rods, and seamless pipes.[3]

Billet

A billet is a length of metal that has a round or square cross-section, with an area less than 36 in2 (230 cm2). Billets are created directly via continuous casting or extrusion or indirectly via hot rolling an ingot or bloom.[1][2][4] Billets are further processed via profile rolling and drawing. Final products include bar stock and wire.[3]

Centrifugal casting is also used to produce short circular tubes as billets, usually to achieve a precise metallurgical structure. They are commonly used as cylinder sleeves where the inner and outer diameters are ground and machined to length. Because their size is not modified significantly, they are not always classified as semi-finished casting products.

In copper production, a billet is a 30' long, about 8" diameter, of pure copper.

Slab

A slab is a length of metal that is rectangular in cross-section. The slab is created directly by continuous casting or indirectly by rolling an ingot on a slabbing mill.[1] Slabs are usually further processed via flat rolling, skelping, and pipe rolling. Common final products include sheet metal, plates, strip metal, pipes, and tubes.[3]

  1. ^ a b c d Glossary, ArcelorMittal, archived from the original on 03-04-2010, retrieved 03-04-2010. Check date values in: |accessdate=, |archivedate= (help)
  2. ^ a b Definition of standard mill terms, archived from the original on 03-04-2010, retrieved 03-04-2010. Check date values in: |accessdate=, |archivedate= (help)
  3. ^ a b c Degarmo, E. Paul; Black, J T.; Kohser, Ronald A. (2003), Materials and Processes in Manufacturing (9th ed.), Wiley, p. 383, ISBN 0-471-65653-4.
  4. ^ Titanium Metal Glossary, archived from the original on 03-04-2010, retrieved 03-04-2010. Check date values in: |accessdate=, |archivedate= (help)


This article uses material from the Wikipedia article "Semi-finished casting products", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD