powered by CADENAS

Social Share

Smelting (12366 views - Plant Design)

Smelting is a process of applying heat to ore in order to extract out a base metal. It is a form of extractive metallurgy. It is used to extract many metals from their ores, including silver, iron, copper, and other base metals. Smelting uses heat and a chemical reducing agent to decompose the ore, driving off other elements as gases or slag and leaving the metal base behind. The reducing agent is commonly a source of carbon, such as coke—or, in earlier times, charcoal.The carbon (or carbon monoxide derived from it) removes oxygen from the ore, leaving the elemental metal. The carbon thus oxidizes in two stages, producing first carbon monoxide and then carbon dioxide. As most ores are impure, it is often necessary to use flux, such as limestone, to remove the accompanying rock gangue as slag. Plants for the electrolytic reduction of aluminium are also generally referred to as aluminium smelters. Labourers working in the smelting industry have reported respiratory illnesses inhibiting their ability to perform the physical tasks demanded by their jobs.
Go to Article

Explanation by Hotspot Model

Youtube


    

Smelting

Smelting

Smelting

Smelting is a process of applying heat to ore in order to extract out a base metal. It is a form of extractive metallurgy. It is used to extract many metals from their ores, including silver, iron, copper, and other base metals. Smelting uses heat and a chemical reducing agent to decompose the ore, driving off other elements as gases or slag and leaving the metal base behind. The reducing agent is commonly a source of carbon, such as coke—or, in earlier times, charcoal.[1]

The carbon (or carbon monoxide derived from it) removes oxygen from the ore, leaving the elemental metal. The carbon thus oxidizes in two stages, producing first carbon monoxide and then carbon dioxide. As most ores are impure, it is often necessary to use flux, such as limestone, to remove the accompanying rock gangue as slag.

Plants for the electrolytic reduction of aluminium are also generally referred to as aluminium smelters.

Labourers working in the smelting industry have reported respiratory illnesses inhibiting their ability to perform the physical tasks demanded by their jobs.[2]

Process

Smelting involves more than just melting the metal out of its ore. Most ores are the chemical compound of the metal and other elements, such as oxygen (as an oxide), sulfur (as a sulfide), or carbon and oxygen together (as a carbonate). To extract the metal, workers must make these compounds undergo a chemical reaction. Smelting therefore consists of using suitable reducing substances that combine with those oxidizing elements to free the metal.

Roasting

In the case of carbonates and sulfides, a process called "roasting" drives out the unwanted carbon or sulfur, leaving an oxide, which can be directly reduced. Roasting is usually carried out in an oxidizing environment. A few practical examples:

  • Malachite, a common ore of copper, is primarily copper carbonate hydroxide Cu2(CO3)(OH)2.[3] This mineral undergoes thermal decomposition to 2CuO, CO2, and H2O[4] in several stages between 250 °C and 350 °C. The carbon dioxide and water are expelled into the atmosphere, leaving copper(II) oxide, which can be directly reduced to copper as described in the following section titled Reduction.
  • Galena, the most common mineral of lead, is primarily lead sulfide (PbS). The sulfide is oxidized to a sulfite (PbSO3), which thermally decomposes into lead oxide and sulfur dioxide gas. (PbO and SO2) The sulfur dioxide is expelled (like the carbon dioxide in the previous example), and the lead oxide is reduced as below.

Reduction

Reduction is the final, high-temperature step in smelting, in which the oxide becomes the elemental metal. A reducing environment (often provided by carbon monoxide, made by incomplete combustion in an air-starved furnace) pulls the final oxygen atoms from the raw metal. The required temperature varies over a very large range, both in absolute terms and in terms of the melting point of the base metal. Examples:

  • Iron oxide becomes metallic iron at roughly 1250 °C (2282 °F or 1523.15 K), almost 300 degrees below iron's melting point of 1538 °C (2800.4 °F or 1811.15 K).
  • Mercuric oxide becomes vaporous mercury near 550 °C (1022 °F or 823.15 K), almost 600 degrees above mercury's melting point of -38 °C (-36.4 °F or 235.15 K).

Flux and slag can provide a secondary service after the reduction step is complete: they provide a molten cover on the purified metal, preventing contact with oxygen while still hot enough to readily oxidize. This prevents impurities from forming in the metal.

Fluxes

Metal workers use fluxes in smelting for several purposes, chief among them catalyzing the desired reactions and chemically binding to unwanted impurities or reaction products. Calcium oxide, in the form of lime, was often used for this purpose, since it could react with the carbon dioxide and sulfur dioxide produced during roasting and smelting to keep them out of the working environment.

History

Of the seven metals known in antiquity, only gold occurred regularly in native form in the natural environment. The others – copper, lead, silver, tin, iron and mercury – occur primarily as minerals, though copper is occasionally found in its native state in commercially significant quantities. These minerals are primarily carbonates, sulfides, or oxides of the metal, mixed with other components such as silica and alumina. Roasting the carbonate and sulfide minerals in air converts them to oxides. The oxides, in turn, are smelted into the metal. Carbon monoxide was (and is) the reducing agent of choice for smelting. It is easily produced during the heating process, and as a gas comes into intimate contact with the ore.

In the Old World, humans learned to smelt metals in prehistoric times, more than 8000 years ago. The discovery and use of the "useful" metals — copper and bronze at first, then iron a few millennia later — had an enormous impact on human society. The impact was so pervasive that scholars traditionally divide ancient history into Stone Age, Bronze Age, and Iron Age.

In the Americas, pre-Inca civilizations of the central Andes in Peru had mastered the smelting of copper and silver at least six centuries before the first Europeans arrived in the 16th century, while never mastering the smelting of metals such as iron for use with weapon-craft.[5]

Tin and lead

In the Old World, the first metals smelted were tin and lead. The earliest known cast lead beads were found in the Çatal Höyük site in Anatolia (Turkey), and dated from about 6500 BC, but the metal may have been known earlier.

Since the discovery happened several millennia before the invention of writing, there is no written record about how it was made. However, tin and lead can be smelted by placing the ores in a wood fire, leaving the possibility that the discovery may have occurred by accident.

Lead is a common metal, but its discovery had relatively little impact in the ancient world. It is too soft to use for structural elements or weapons, though its high density relative to other metals makes it ideal for sling projectiles. However, since it was easy to cast and shape, workers in the classical world of Ancient Greece and Ancient Rome used it extensively to pipe and store water. They also used it as a mortar in stone buildings.

Tin was much less common than lead and is only marginally harder, and had even less impact by itself.

Copper and bronze

After tin and lead, the next metal smelted appears to have been copper. How the discovery came about is debated. Campfires are about 200 °C short of the temperature needed, so some propose that the first smelting of copper may have occurred in pottery kilns. The development of copper smelting in the Andes, which is believed to have occurred independently of the Old World, may have occurred in the same way.[5] The earliest current evidence of copper smelting, dating from between 5500 BC and 5000 BC, has been found in Pločnik and Belovode, Serbia.[6][7] A mace head found in Can Hasan, Turkey and dated to 5000 BC, once thought to be the oldest evidence, now appears to be hammered native copper.[8]

Combining copper with tin and/or arsenic in the right proportions produces bronze, an alloy that is significantly harder than copper. The first copper/arsenic bronzes date from 4200 BC from Asia Minor. The Inca bronze alloys were also of this type. Arsenic is often an impurity in copper ores, so the discovery could have been made by accident. Eventually arsenic-bearing minerals were intentionally added during smelting.[citation needed]

Copper–tin bronzes, harder and more durable, were developed around 3200 BC, also in Asia Minor.[citation needed]

How smiths learned to produce copper/tin bronzes is unknown. The first such bronzes may have been a lucky accident from tin-contaminated copper ores. However, by 2000 BC, people were mining tin on purpose to produce bronze—which is amazing given that tin is a semi-rare metal, and even a rich cassiterite ore only has 5% tin. Also, it takes special skills (or special instruments) to find it and locate richer lodes. However early peoples learned about tin, they understood how to use it to make bronze by 2000 BC.[citation needed]

The discovery of copper and bronze manufacture had a significant impact on the history of the Old World. Metals were hard enough to make weapons that were heavier, stronger, and more resistant to impact damage than wood, bone, or stone equivalents. For several millennia, bronze was the material of choice for weapons such as swords, daggers, battle axes, and spear and arrow points, as well as protective gear such as shields, helmets, greaves (metal shin guards), and other body armor. Bronze also supplanted stone, wood, and organic materials in tools and household utensils—such as chisels, saws, adzes, nails, blade shears, knives, sewing needles and pins, jugs, cooking pots and cauldrons, mirrors, and horse harnesses.[citation needed] Tin and copper also contributed to the establishment of trade networks that spanned large areas of Europe and Asia, and had a major effect on the distribution of wealth among individuals and nations.[citation needed]

Early iron smelting

The earliest evidence for iron-making is a small number of iron fragments with the appropriate amounts of carbon admixture found in the Proto-Hittite layers at Kaman-Kalehöyük and dated to 2200–2000 BC.[9] Souckova-Siegolová (2001) shows that iron implements were made in Central Anatolia in very limited quantities around 1800 BC and were in general use by elites, though not by commoners, during the New Hittite Empire (∼1400–1200 BC).[10]

Archaeologists have found indications of iron working in Ancient Egypt, somewhere between the Third Intermediate Period and 23rd Dynasty (ca. 1100–750 BC). Significantly though, they have found no evidence for iron ore smelting in any (pre-modern) period. There may have been iron smelting and working in West Africa by 1200 BC.[11] In addition, very early instances of carbon steel were in production around 2000 years before the present in northwest Tanzania, based on complex preheating principles. These discoveries are significant for the history of metallurgy.[12]

Most early processes in Europe and Africa involved smelting iron ore in a bloomery, where the temperature is kept low enough so that the iron does not melt. This produces a spongy mass of iron called a bloom, which then must be consolidated with a hammer to produce wrought iron. The earliest evidence to date for the bloomery smelting of iron is found at Tell Hammeh, Jordan ([1]), and dates to 930 BC (C14 dating).

Later iron smelting

From the medieval period, an indirect process began to replace direct reduction in bloomeries. This used a blast furnace to make pig iron, which then had to undergo a further process to make forgeable bar iron. Processes for the second stage include fining in a finery forge and, from the Industrial Revolution, puddling. Both processes are now obsolete, and wrought iron is now rarely made. Instead, mild steel is produced from a bessemer converter or by other means including smelting reduction processes such as the Corex Process.

Base metals

The ores of base metals are often sulfides. In recent centuries, reverberatory furnaces have been used. These keep the fuel and the charge being smelted separate. Traditionally these were used for carrying out the first step: formation of two liquids, one an oxide slag containing most of the impurity elements, and the other a sulfide matte containing the valuable metal sulfide and some impurities. Such "reverb" furnaces are today about 40 m long, 3 m high and 10 m wide. Fuel is burned at one end and the heat melts the dry sulfide concentrates (usually after partial roasting), which are fed through the openings in the roof of the furnace. The slag floats on top of the heavier matte, and is removed and discarded or recycled. The sulfide matte is then sent to the converter. The precise details of the process vary from one furnace to another depending on the mineralogy of the orebody.

While reverberatory furnaces were very good at producing slags containing very little copper, they were relatively energy inefficient and produced a low concentration of sulfur dioxide in their off-gases that made it difficult to capture, and consequently, they have been supplanted by a new generation of copper smelting technologies.[14] More recent furnaces have been designed based upon bath smelting, top jetting lance smelting, flash smelting and blast furnaces. Some examples of bath smelters include the Noranda furnace, the Isasmelt furnace, the Teniente reactor, the Vunyukov smelter and the SKS technology to name a few. Top jetting lance smelters include the Mitsubishi smelting reactor. Flash smelters account for over 50% of the world's copper smelters. There are many more varieties of smelting processes, including the Kivset, Ausmelt, Tamano, EAF, and BF.

Environmental implications

Smelting has serious environmental impacts due to the release of toxic metals in to the atmosphere and the production of excess waste material such as wastewater and slag, during the smelting process. The release of metals in a gaseous form such as copper, silver, iron, cobalt and selenium.[15] Sulfur dioxide is another important gaseous compound that is released and contributed to severe impacts on the environment, due to the fact that as it is released in to the atmosphere, it can lead to the production of acid rain, which can result in soil acidification and the acidification of aquatic environments.[16]

See also



This article uses material from the Wikipedia article "Smelting", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Plant Design

Aveva Tribon, Aveva PDMS, Intergraph Smartplant, Intergraph Smartmarine, Offshore, Onshore, Marine, Shipyard, Plantdesign