powered by CADENAS

Social Share

Pony car (11093 views - Cars & Motorbikes & Trucks)

Not to be confused with the Hyundai Pony. Pony car is an American class of automobile launched and inspired by the Ford Mustang in 1964. It broke all post-World War II automobile sales records, "creating the 'pony car' craze soon adopted by competitors." The term describes an affordable, compact, highly styled car with a sporty or performance-oriented image.
Go to Article

Explanation by Hotspot Model

Youtube


    

Pony car

Pony car

Not to be confused with the Hyundai Pony.

Pony car is an American class of automobile launched and inspired by the Ford Mustang in 1964.[1][2][3][4] It broke all post-World War II automobile sales records, "creating the 'pony car' craze soon adopted by competitors."[5] The term describes an affordable, compact, highly styled car with a sporty or performance-oriented image.[6][7]

Origins of the class

The pony car had its origins when domestic automakers began "noticing the rising interest in small, sporty cars, and the increasing importance of younger customers"[8] Several concept cars were developed. Efforts to entice Ford Motor Company by the Budd Company, the producer of the bodies of the original 2-seater Thunderbird, was a new four-seat car utilizing refurbished tooling from the old model as well as a new two-seat roadster built early 1962 on a Ford Falcon chassis using a modified 4-seat 1957 Thunderbird body.[8] Budd also created an fully operational proof of concept for American Motors Corporation (AMC), the XR-400, featuring a long hood, AMC's 327 cu in (5.4 L) V8, short rear deck, and the look "similar to many European sports cars."[8] The automaker's "management expressed interest in a new car with a sports flair" and work on the Tarpon, a striking 2+2 with an elongated fastback roof, began in early 1963.[8]

Examples of production cars that included sporty and youthful appeal were the 1960 Chevrolet Corvair.[9] Initially positioned as an economy car, the Corvair's plusher-trimmed and sportier Monza model sold around 144,000 units by 1961. The Monza's bucket seats and floor-mounted transmission shifter started a trend toward sportier cars equipped with both in all sizes from compacts to full-size cars. Ford initially responded with Futura and Futura Sprint versions of its Ford Falcon, Chrysler with the Plymouth Valiant Signet and Dodge Dart GT, American Motors with the 440-H and Rogue versions of the Rambler American,[10] and Studebaker with the sporty Daytona version of its compact Lark. Other sporty bucket-seat compact cars that appeared during the early 1960s included the Mercury Comet S-22, Oldsmobile F-85 Cutlass, Buick Special Skylark, and Pontiac Tempest LeMans. Most of these sporty compacts came with the same economical six-cylinder engines as their more mundane counterparts, but in some cases more powerful V8 engines were at least optional along with four-speed manual transmissions and center consoles between the front bucket seats.

Some of the technical developments that debuted in early sporty compact cars in the U.S. (1961–63) included a turbocharged six-cylinder in the rear-engine Corvair Monza Spyder/Corsa (1962–66), turbocharged aluminum V8 on the 1962–63 Oldsmobile Cutlass Jetfire, and a standard 194 cu in (3.2 L) four-cylinder engine/rear transaxle combination on the 1961–63 Pontiac Tempest LeMans (available with an optional high-performance four-barrel carburetor). In 1963, the LeMans introduced a large-for-a-compact-car 326 cu in (5.3 L) V8 option producing up to 280 hp (209 kW).

Although these sporty versions of mundane compact cars were a commercial success for most automakers, some auto executives—led by Ford's Lee Iacocca—believed they only scratched the surface of the potential market. During this period there was a strong influx of young buyers with discretionary income and a taste for vehicles with a younger image than a standard sedan. Iacocca's marketing studies revealed that if a unique-looking sporty car could be offered at an affordable price, it would find many buyers.[11] Ford's response was the Mustang, an enormous success from its April 17, 1964 launch. Year 1 sales forecasts of 100,000 units were shattered on the first day, when Ford dealers took orders for 22,000 vehicles, forcing the company to shift production mid-year. The extended model year sales totaled 618,812 Mustangs.[12]

Defining the class

The 1964 Mustang provided the template for the new class of automobiles.[13][14] The term "pony car" to describe members of its ranks was coined by Car Life magazine editor Dennis Shattuck.[15]

Although the Mustang was based on the Falcon platform, its "long hood, short deck" look was unique. Offered as a two-door coupé and convertible, it was nevertheless mechanically mundane in its basic form, with a 170 cu in (2.8 L) six-cylinder engine coupled to a three-speed manual transmission. Its attractive US$2,368 base price included bucket seats, carpeting, floor shifter, sport steering wheel, and full wheel covers. Importantly, it had an extensive list of options that featured V8 engines, Cruise-O-Matic automatic transmission or four-speed manual gearbox, radios, air conditioning, power steering, and other accessories.[16] A fully dressed V8 Mustang could increase sticker price by up to 60%, which generated excellent profits for Ford.[17]

The cars could carry four people while featuring a sporty design. Many of the offerings came with economical six-cylinder or small V8 engines.[18] The basic two-door "Pony Car" characteristics were thus set:[19][20]

  • Stylish and sporty long hood, short deck, and "open mouth" styling
  • Affordable base price (under $2,500 — in 1965 dollar value)
  • "Off-the-shelf" mass production components
  • Wide range of often lucrative options to individualize each car
  • Youth-oriented marketing and advertising

Tellingly, while most pony cars were available with more powerful engines and performance packages—enough to propel some into the muscle car realm—the vast majority were sold with six-cylinder engines or ordinary V8s.[21] The initial pony cars "were sporty compact cars for the masses."[22] They transformed into performance cars for enthusiasts whose production viability depended on significant sales of economical "secretaries' cars" and low-margin rental fleet models.[22] Similarly as other muscle car versions, for the most part, the high-performance models saw limited sales and were largely limited to drag racing, road racing, or racing homologation purposes.[23]

Pony car competitors

Despite the immediate success of the Mustang, many (including some within Ford) feared that the bubble would soon burst. Even though an early competitor, the Plymouth Barracuda, had actually gone on sale two weeks earlier (on April 1, 1964),[24] other manufacturers were generally relatively slow to respond.

Well aware of the Mustang's upcoming debut, Chrysler had sought a low-cost way to expand the appeal of its mainstream compact Valiant. The company's precarious financial situation meant the resulting Barracuda was compromised, with insufficient distinction from the Valiant and styling that drew mixed reactions. As a result, its sales were a fraction of the Mustang's.[25]

Initially, General Motors believed that the restyled 1965 Corvair would be an adequate challenger for the Mustang. However, when it became clear that the Corvair itself was doomed, the more conventional Chevrolet Camaro was introduced.[20] It appeared in 1967, at the time the Mustang received its first major redesign, and was joined by the Camaro-based Pontiac Firebird and the Mustang-based Mercury Cougar. American Motors made its entry late in 1967 with the Javelin.[26] It was described by race driver Gordon Johncock "as a roomy, comfortable, peppy and handsome example of a so-called pony car, the type of automobile that's showing up more and more on US highways."[27] Although U.S. showrooms were awash in pony cars a final contender appeared in 1970, Dodge's Challenger, essentially an enlarged Barracuda.[28][29]

The pony car market segment was maturing and all four domestic automakers were building versions of the long hood/short deck template that Ford had developed.[30] The term pony car applied to all versions of these nameplates, from base models through high-performance "muscle car" extremes,[31] developed in league with factory supported racing to gain a marketing edge.[32] The competition between the manufacturers was so fierce the Trans-Am Series from 1966 to 1972 is described as "The Pony Car Wars".[33]

While sales were strong throughout the end of the 1960s, pony cars' greater value was in generating brand loyalty, particularly among the crucial youth market. In 1970 Car and Driver reported that while very few pony car drivers bought a second, around 50% purchased another model from the same manufacturer. Even so, by as early as 1969 sales were beginning to slide, dropping to 9% of the total market from a peak of 13% in 1967.

The success Ford experienced with the Mustang also inspired Japanese car maker Toyota to introduce the Celica in 1970.[34] Parroting Ford, Toyota built the first Celica on their compact economy Carina platform. Though the smaller Celica had a generally similar appearance to the Mustang, no Japanese automaker came forward with a V8-powered, rear-drive sporty coupe.[35] Instead they largely stayed with 4- and 6-cylinder models that accentuated practicality at the expense of personality, from the Celica to the Datsun 240Z.[35] The "4-cylinder Honda Preludes of 1978–2001, had no trace of the daring, danger and aggression that appeal to fans of powerful American muscle cars,"[35] reflecting heavy taxes imposed by Japanese Government regulations on engines over 2,000 cc (120 cu in).

In Europe, Ford began production of the Ford Capri,[36] (using the Cortina MkII platform and driveline and a few components from the Escort) while GM of Europe introduced the Opel Manta and Vauxhall Firenza. In April 1970, Ford began selling the Capri in North America via Lincoln-Mercury dealerships as the Mercury Capri (the Mk1 and Mk2 were sold as captives but marketed by Mercury despite the absence of marque badging), as well as in South Africa and Australia.

Expansion and decline

As with most automobile redesigns, each subsequent generation of the pony cars grew larger, heavier, costlier, and more plush. Big-block engines joined the option list, and both performance and comfort options proliferated. Specialty car buyers were better educated and had more money than the average car buyer.[37] These demographic factors contributed to buyer behaviors that included purchasing more optional equipment and moving up the pricing ladder, which resulted in the pony cars becoming larger, more luxurious, and pricier during the late 1960s and early 1970s.[37] The 1973 Mustang, for example, was 8.5 in (216 mm) longer, 5.9 in (150 mm) wider, and over 600 lb (272 kg) heavier than the original 1965 edition. The Dodge Challenger was only slightly smaller outside and lighter than Dodge's own intermediate Coronet four-door sedans. The Cougar abandoned its pony car roots as it became heavier with an emphasis on higher trim levels and convenience appointments. When its Falcon-based platform ended production, the Cougar moved upmarket to the midsize platform used with the Torino.[38] At the same time, the Mustang moved to a subcompact platform. The added bulk left the standard six and V8 engines sorely pressed, while the introduction of powerful big-blocks underscored the limitations of the pony cars' suspension, brakes, and tires.

By 1970 buyers were moving away from the pony cars, either toward smaller compact cars (domestic or imported) or toward larger, more luxurious models. Insurance company pressures combined to assault the pony car market with ever-increasing insurance policy premiums.[39] By 1972, the domestic pony cars were not "selling well at all — neither the current Mustang nor the Camaro, Javelin, Barracuda, Challenger, Firebird, nor Cougar" with the market segment so depressed that industry observers "believed GM would discontinue the Camaro and Firebird after 1972" or perhaps 1973.[40] Performance of the hottest versions of pony cars began to erode as a result of emissions controls. The 1973 oil crisis left the bulky pony cars out of step with the marketplace. The Mustang, which became intermediate size and alienated buyers,[41] was reinvented as the Mustang II and marketed as fuel efficient compact with luxury or sporting trim packages. The new subcompact-sized version was introduced in September 1973, coinciding with the oil embargo and became "in effect, filling the segment the Mustang had created, then abandoned."[42]

The Challenger, Barracuda, and Javelin were cancelled after the 1974 model year, and the Camaro and Firebird were to be discontinued at the same time, although they received last-minute stays of execution. The Cougar, originally billed as an upscale version of the Mustang, remained available as a luxury vehicle despite its upsizing to the platform shared with the Ford Torino, later becoming a corporate twin to the Ford Thunderbird after 1976.

Later developments

Popularity was increased by examples such as the Firebird Trans Am in movies such as Smokey and the Bandit and TV programs such as The Rockford Files and Knight Rider. The GM pony cars experienced a resurgence in popularity in the late 1970s that helped ensure their continuation. The Mustang was redesigned with a renewed sporty image in 1979, prompting Mercury to reenter the pony car market with a Mercury Capri twin based on the new Mustang. Chrysler, beset by financial problems, did not revive the pony car, although it did offer other front-wheel drive performance models with a similar spirit. American Motors brought back its AMX model name to the performance-oriented I6 or V8 powered rear-drive Spirit, a similar car to the Mustang hatchback of that era. Advertising with the line "don't horse around" compared the value of AMC's model in relation to the 1979 Ford Mustang.[43] In 1982, the "Spirit GT became America's first pony car available with a 5-speed gearbox."[44]

Sales of the Mustang remained strong, although in the 1980s Ford gave serious consideration to replacing it with a front-drive model (which eventually appeared as the Ford Probe instead). Emissions and fuel economy concerns led many of the latter-day pony cars to offer four-cylinder engines (sometimes with turbocharging), although they were never as popular as six-cylinder and V8 models.

By the mid-1980s, the pony car survivors (Mustang, Camaro, and Firebird) enjoyed a period of renewed popularity as progressively more and more powerful (yet relatively fuel-efficient) V8 engines were offered in performance-oriented versions of these vehicles. However, declining sales and the growing popularity of rear-wheel drive light trucks and sport utility vehicles ultimately led to the demise of the Firebird and short lived demise of the Camaro after the 2002 model year.

21st-century revival

The dilemma facing automakers in offering pony cars (or their equivalent) going forward is developing a suitable platform that is affordable and capable enough to be viable. Unlike the mid-1960s, the large majority of modern compact cars are front-wheel drive, with four- and six-cylinder engines, and the widespread use of unibody construction makes engineering a specialized body an expensive proposition.

In 2005, Ford introduced a new Mustang based on a dedicated platform. The success of this model inspired Dodge to reintroduce the Challenger in 2008 and Chevrolet to reintroduce the Camaro for 2010, which unlike previous pony cars, were based on full-size car architectures. The Mustang and Camaro were sold with coupe and convertible bodystyles, whereas the Challenger was sold only as a coupe.

The sixth generation Mustang was launched in 2014 and the sixth generation Camaro in 2015. The Mustang was the first model developed as a global car, with fully independent rear suspension and a turbocharged four-cylinder engine. Meanwhile, Dodge will launch the Challenger GT with four-wheel drive.

NASCAR brought pony cars to its second-tier Nationwide Series (now Xfinity) at the Subway Jalepeno 250 at Daytona International Speedway in Daytona, Florida, on Friday, July 2, 2010.[45] Dodge raced its Challenger, and Ford raced the iconic Mustang. The new cars are seen as a move by NASCAR to re-establish brand identity with fans and the cars on the track.[46][47]

Also, silhouettes of the Chevrolet Camaro have competed in the Rolex Sports Car Series, whereas production-based versions of the Camaro, Challenger and Mustang have raced in the SCCA World Challenge and Continental Tire Sports Car Challenge, as well as SCCA and NASA amateur competitions. The Camaro and Mustang have been adapted to GT3 regulations, although not by Chevrolet or Ford themselves. In 2016, Ford unveiled the Mustang GT4.

  1. ^ Mitchell, Larry G. (2000). AMC Muscle Cars. MotorBooks/MBI. p. 17. ISBN 978-0-7603-0761-8. Retrieved 20 May 2017.
  2. ^ Grist, Peter (2009). Dodge Challenger Plymouth Barracuda: Chrysler's Potent Pony Cars. Veloce. p. 6. ISBN 978-1-84584-105-8. Retrieved 20 May 2017.
  3. ^ Linden, Steve (2008). Car Collecting. Motorbooks. p. 8. ISBN 9780760328095. Retrieved 20 May 2017. Mustangs are part of a group of cars called "pony cars" — a term that originated with the Mustang
  4. ^ Witzenburg, Gary L. (1979). Mustang ! The Complete History of America's Pioneer Ponycar. Automobile Quarterly. ISBN 9780525161752.
  5. ^ Maga, Timothy P. (2003). The 1960s (Eyewitness History). Facts on File. p. 324. ISBN 9780816048090. Retrieved 20 May 2017.
  6. ^ Borroz, Tony (17 April 2009). "April 17, 1964: Ford Mustang Starts Galloping". Wired. Archived from the original on 1 January 2014. Retrieved 20 May 2017.
  7. ^ Squatriglia, Chuk (17 April 2009). "Mustang, the Ultimate Pony Car, Turns 45". Wired. Archived from the original on 1 January 2014. Retrieved 20 May 2017.
  8. ^ a b c d McCausland, Evan (2 December 2013). "The Ford Mustang Wasn't The First Pony Car". Automobile Magazine. Retrieved 18 October 2017.
  9. ^ "https://www.hemmings.com/magazine/hcc/2007/08/Corvair-Connoisseurs/1494230.html". www.hemmings.com. Retrieved 2018-09-06. External link in |title= (help)
  10. ^ Severson, Aaron (2010-03-13). "The Sporting American: The History of the AMC Javelin". Ate Up With Motor. Retrieved 2016-01-23. The new Rogue would be AMC's entrée into the emerging "pony car" market.
  11. ^ Fehn, Daniel (7 January 2012). "Pony Car History - The Story Behind America's Smaller Muscle Cars". Timeless Rides. Retrieved 18 October 2017.
  12. ^ Engelman, Emily (2005-03-18). "Ford to Increase Mustang Production to Meet Runaway Consumer Demand" (Press release). Ford Motor. Archived from the original on 2012-03-06. Retrieved 2014-04-03.
  13. ^ Gunnell, John A. (2001). Mustang, America's Favorite Pony Car. Krause Publications. ISBN 978-0-87341-946-8.
  14. ^ Bowling, Brad (2005). Mustang Field Guide: America's Favorite Pony Car. Krause Publications. ISBN 978-0-89689-145-6.
  15. ^ "An evocative event in California — 700 Mustangs appeared at a 20th Anniversary". The Motor. 166: 25. 1984. Retrieved 2014-04-03. A further mark of success is the group of "Pony Cars" (a term, incidentally, that was coined by Dennis Shattuck, who was editor of Car Life magazine at that time) spawned by Mustang: Chevrolet Camaro, Pontiac Firebird, Plymouth Barracuda
  16. ^ Auto Editors of Consumer Guide (2007-02-04). "1965 Mustang Options". auto.howstuffworks.com. Retrieved 2014-04-03.
  17. ^ Auto Editors of Consumer Guide (2007-02-04). "The 1965 Ford Mustang". auto.howstuffworks.com. Retrieved 2014-04-03.
  18. ^ Hakim, Danny (19 April 2002). "DRIVING; As Other Pony Cars Eat Dust, the Mustang Roars On". The New York Times. Retrieved 19 October 2017.
  19. ^ Gartman, David (1994). Auto opium: a social history of American automobile design. Taylor & Francis. p. 197. ISBN 978-0-415-10572-9.
  20. ^ a b Gunnell, John; Heasley, Jerry (2006). The Story of Camaro. Krause Publications. p. 16. ISBN 978-0-89689-432-7. Retrieved 2014-04-03.
  21. ^ "Muscle Car Club definition - Introduction". musclecarclub.com. Retrieved 2016-01-23. These new "pony cars" and compact cars are generally considered muscle cars only if they have the top of the line performance engines and options.
  22. ^ a b DeLorenzo, Matt (2004). Mustang 2005: A New Breed of Pony Car. Motorbooks International. p. 20. ISBN 9780760320396. Retrieved 19 October 2017.
  23. ^ Holmstrom, Darwin (2016). American Muscle Cars: A Full-Throttle History. Motorbooks. p. 81. ISBN 9780760350133. Retrieved 2016-01-23. Most of them were homologation specials built in ultralow volumes to qualify cars and engines for racing programs
  24. ^ "Plymouth 'Cuda History 1964–1974". musclecarclub.com. Retrieved 2016-01-23.
  25. ^ "1964–1966 Barracuda". 74barracuda.com. Archived from the original on 2011-10-02. Retrieved 2011-10-30.
  26. ^ Mueller, Mike (1997). Motor City Muscle: High-Powered History of the American Muscle Car. MotorBooks/MBI. p. 101. ISBN 978-0-7603-0196-8. Retrieved 2011-10-30.
  27. ^ Johncock, Gordon (November 1967). "Gordon Johncock Tests AMC's Javelin". Popular Mechanics. 128 (5): 128–130, 218, 219, 220. Retrieved 2016-01-23.
  28. ^ Mitchell, Larry G. (2000). AMC Muscle Cars. MotorBooks/MBI. p. 33. ISBN 978-0-7603-0761-8. Retrieved 2016-01-23.
  29. ^ Young, Tony (2007). Chrysler, Dodge, Plymouth Muscle. MotorBooks/MBI. p. 47. ISBN 978-0-7603-3204-7. Retrieved 2011-10-30. Dodge was the last of the car manufacturers to join the pony-car race, so the Challenger, introduced in the fall of 1969, was an appropriate name.
  30. ^ Zazarine, Paul (19 September 2014). "The Significant 7 – The Most Notable Of The American Pony Cars". Heacock. Retrieved 20 May 2017.
  31. ^ Leffingwell, Randy; Holmstrom, Darwin; Newhardt, David (2006). Muscle: America's Legendary Performance Cars. MotorBooks/MBI. p. 16. ISBN 978-0-7603-2284-0. Retrieved 2016-01-23.
  32. ^ Holder, William; Kunz, Phil (2006). Extreme Muscle Cars. Krause Publications. p. 14. ISBN 978-0-89689-278-1.
  33. ^ Friedman, Dave (2001). Trans-Am: The Pony Car Wars 1966–1972. MotorBooks/MBI. ISBN 978-0-7603-0943-8.
  34. ^ Long, Brian (2007). Celica & Supra: The Book of Toyota's Sports Coupes. Veloce Publishing. p. 106. ISBN 978-1-904788-13-3. Retrieved 2011-10-30.
  35. ^ a b c Ulrich, Lawrence (2009-04-19). "Japanese Failed to Bet on the Pony Car". The New York Times. Retrieved 2016-01-23.
  36. ^ Lewis, Albert L.; Musciano, Walter A. (1977). Automobiles of the world. Simon & Schuster. p. 608. ISBN 978-0-671-22485-1.
  37. ^ a b Gunnell, John (2005). American Cars of the 1960s: A Decade of Diversity. Krause Publications. p. 47. ISBN 9780896891319. Retrieved 2017-06-14.
  38. ^ Glastonbury, Jim (2010). Ultimate Guide to Muscle Cars. Chartwell Books. p. 297. ISBN 9780785820093. Retrieved 2016-01-23.
  39. ^ Gunnell, John, ed. (1992). Standard Catalog of American Cars, 1946-1975 (Third ed.). Krause Publications. p. 569. ISBN 9780873412049. Retrieved 2016-01-23.
  40. ^ Lamm, Michael (December 1972). "Mini-ponycars - Detroit thinks small again". Popular Mechanics. 138 (6): 177. Retrieved 2017-06-14.
  41. ^ Sessler, Peter; Sessler C., Nilda (2006). Ford Mustang Buyer's And Restoration Guide. Sams Technical Publishing. p. 83. ISBN 978-0-7906-1326-0. Retrieved 2016-01-23.
  42. ^ Vance, Bill (2006-07-16). "Motoring Memories: Ford Mustang II, 1974–1978". Autos.ca. Retrieved 2016-01-23.
  43. ^ Lapham, Edward (1979-01-08). "1979 financial outlook is cloudy". Automotive News. Retrieved 2016-01-23.
  44. ^ Cranswick, Marc (2001). Cars of American Motors: An Illustrated History. McFarland. p. 267. ISBN 978-0-7864-4672-8. Retrieved 2016-01-23.
  45. ^ Pearce, Al (2010-06-30). "NASCAR: Pony-car showdown set for Daytona". Autoweek.com. Retrieved 2016-01-23.
  46. ^ Ryan, Nate (2010-07-01). "Mustang more than a one-trick pony with Nationwide model". USA Today. Retrieved 2016-01-23.
  47. ^ Jensen, Tom (2010-06-30). "NNS: Pony Cars Welcomed, The Ford Mustang and Dodge Challenger are ready to race..." Nascar.speedtv.com. Archived from the original on 2013-06-02. Retrieved 2016-01-23.
  • Media related to Pony car at Wikimedia Commons


This article uses material from the Wikipedia article "Pony car", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer