An R-clip, also known as an R-pin, R-key, hairpin cotter pin,[1] hairpin cotter,[2] bridge pin,[2] hitch pin[3] or spring cotter pin,[4] is a fastener made of a springy material, commonly hardened metal wire, resembling the shape of the letter "R".
R-clips are commonly used to secure the ends of round shafts such as axles and clevis pins. The straight leg of the R-clip is pushed into a hole near one end of the shaft until the semicircular "belly" in the middle of the other, bent leg of the R-clip grips one side of the shaft resisting any force removing the R-clip from its hole. To assist insertion the end of the bent leg is angled away from the straight leg. This angled end rides the side of the shaft and opens the "belly" mouth enough to pass the widest part of the shaft as the R-clip is inserted.
There is also a double loop variety when a wider range of suitable shafts is required. It also spreads out the stresses more evenly for a longer life.[5]
This type of pin is usually made of round wire of a harder metal than is appropriate for traditional cotter pins.
R-clips are similar in function to split pins and linchpins. Compared to split pins, they are easier to remove and are re-usable.
This article uses material from the Wikipedia article "R-clip", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD