Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Alexander.stohr at the German language Wikipedia).
A shower is a place in which a person bathes under a spray of typically warm or hot water. Indoors, there is a drain in the floor. Most showers have temperature, spray pressure and adjustable showerhead nozzle.
The simplest showers have a swivelling nozzle aiming down on the user, while more complex showers have a showerhead connected to a hose that has a mounting bracket. This allows the showerer to spray the water at different parts of their body. A shower can be installed in a small shower stall or bathtub with a plastic shower curtain or door.
Showering is common in Western culture due to the efficiency of using it compared with a bathtub. Its use in hygiene is, therefore, common practice.[1] A shower uses less water on average than a bath: 80 litres for a shower compared with 150 litres for a bath.[2]
The original showers were neither indoor structures nor man-made but were common natural formations: waterfalls.[3] The falling water rinsed the bathers completely clean and was more efficient than bathing in a traditional basin, which required manual transport of both fresh and waste water. Ancient people began to reproduce these natural phenomena by pouring jugs of water, often very cold, over themselves after washing. There has been evidence of early upper class Egyptian and Mesopotamians having indoor shower rooms where servants would bathe them in the privacy of their own homes.[4] However, these were rudimentary by modern standards, having rudimentary drainage systems and water was carried, not pumped, into the room.
The ancient Greeks were the first people to have showers. Their aqueducts and sewage systems made of lead pipes allowed water to be pumped both into and out of large communal shower rooms used by elites and common citizens alike.[5] These rooms have been discovered at the site of the city Pergamum and can also be found represented in pottery of the era. The depictions are very similar to modern locker room showers, and even included bars to hang up clothing.[6] The ancient Romans also followed this convention; their famous bathhouses (Thermae) can be found all around the Mediterranean and as far out as modern-day England. The Romans not only had these showers but also believed in bathing multiple times a week, if not every day. The water and sewage systems developed by the Greeks and Romans broke down and fell out of use after the fall of the Roman Empire.
The first mechanical shower, operated by a hand pump, was patented in England in 1767 by William Feetham,[7] a stove maker from Ludgate Hill in London. His shower contraption used a pump to force the water into a vessel above the user's head and a chain would then be pulled to release the water from the vessel. Although the system dispensed with the servant labour of filling up and pouring out buckets of water, the showers failed to catch on with the rich as a method for piping hot water through the system was not available. The system would also recycle the same dirty water through every cycle.
This early start was greatly improved in the anonymously invented English Regency shower design of circa 1810 (there is some ambiguity among the sources).[3] The original design was over 10 feet (3 m) tall, and was made of several metal pipes painted to look like bamboo. A basin suspended above the pipes fed water into a nozzle that distributed the water over the user's shoulders. The water on the ground was drained and pumped back through the pipes into the basin, where the cycle would repeat itself.[citation needed] The original prototype was steadily improved upon in the following decades until it began to approximate the shower of today in its mode of operation. Hand-pumped models became fashionable at one point as well as the use of adjustable sprayers for different water flow. The reinvention of reliable indoor plumbing around 1850[8] allowed free-standing showers to be connected to a running water source, supplying a renewable flow of water.[9]
Modern showers were installed in the barracks of the French army in the 1870s as an economic hygiene measure, under the guidance of François Merry Delabost, a French doctor and inventor.[10]As surgeon-general at Bonne Nouvelle prison in Rouen, Delabost had previously replaced individual baths with mandatory communal showers for use by prisoners, arguing that they were more economical and hygienic.[11] First six, then eight shower stalls were installed. The water was heated by a steam engine and in less than five minutes, up to eight prisoners could wash simultaneously with only twenty liters of water. The French system of communal showers was adopted by other armies, the first being that of Prussia in 1879, and by prisons in other jurisdictions. They were also adopted by boarding schools, before being installed in public bathhouses. The first shower in a public bathhouse was in 1887 in Vienna, Austria. In France, public bathhouses and showers were established by Charles Cazalet, firstly in Bordeaux in 1893 and then in Paris in 1899.[12]
Domestic showers are most commonly stall showers or showers over a bathtub. A stall shower is a dedicated shower area which uses a door or curtain to contain water spray. The shower over a bathtub saves bathroom space and enables the area to be used for either a bath or a shower and commonly uses a sliding shower curtain to contain the water spray. Showers may also be in a wet room, in which there is no contained shower area, or in a dedicated shower room, which does not require containment of water spray. Most domestic showers have a single overhead shower head, which may be adjustable.[13]
Many modern athletic and aquatic facilities provide showers for use by patrons, commonly in gender segregated changing rooms. These can be in the form of individual stalls shielded by curtains or a door or communal shower rooms. The latter are generally large open rooms with any number of shower heads installed either directly into the walls or on posts throughout the shower area. Open showers are often provided at public swimming pools and at popular beaches.
Military forces around the world set up field showers to enable the washing away of dangerous residue from modern weapons such as caustic chemicals, deadly biological agents, and radioactive materials, which can harm forces on both sides of a conflict.[14]
A wet room is a bathroom without internal dedicated or raised areas which has an open shower. Structurally, a wet room requires the bathroom to have a gradient or slope towards a drain hole, and a foul air trap connecting the floor to the waste pipes.
Shower usage in the latter half of the 20th century sky-rocketed. Personal hygiene became a primary concern, and bathing every day or multiple times a day is common among Western cultures.[20] Showering is generally faster than bathing and can use less water. An average shower of four minutes at 2.5 gallons per minute uses about 10 US gallons (38 L) of water,[21] but modern low-flow shower heads are limited to only two gallons a minute (in the US), corresponding to 8 US gallons (30 L) for a four-minute shower.
Various measures can be taken to increase safety for those, especially elderly people, taking showers or baths.[22]
When a person takes a shower may indicate their social position. Blue collar workers have been found to be more likely to take a shower in the evening after work, whereas white collar workers have been found to shower in the morning before work.[23] An equal number of reasons can be offered for showering at night as for showering in the morning.[24] Contrary to myth, there are no adverse health effects from showering at night.[25]
Some people take more than one shower each day: in the morning, after working out, and at night. People also shower to cool off in hot weather.[26][better source needed] The ideal amount of showering may be less frequently than daily because showering, especially with hot water, can dry out and irritate the skin, remove beneficial bacteria, and cause small cracks that can lead to infection. According to some dermatologists, too much cleanliness for young children can lead to allergies or eczema.[27]
Used shower water can be employed as greywater.
Showering is mostly part of a daily routine primarily to promote cleanliness and prevent odour, disease and infection. Advances in science and medicine in the 19th century began to realize the benefit of regular bathing to an individual's health. As a result, most modern cultures encourage a daily personal hygiene regimen. Showering has also developed the reputation as a relaxing and generally therapeutic activity.[28]
Designs for shower facilities vary by location and purpose. There are free-standing showers, but also showers which are integrated into a bathtub. Showers are separated from the surrounding area through watertight curtains (shower curtain), sliding doors, or folding doors, or shower blinds, in order to protect the space from spraying water. Showers with a level entry wet room are becoming very popular, especially due to improvements in waterproofing systems and prefabricated components.
Places such as a swimming pool, a locker room, or a military facility have multiple showers. There may be communal shower rooms without divisions, or shower stalls (typically open at the top.)
Many types of showers are available, including complete shower units which are all encompassing showers that include the pan, walls, and often the shower head, as well as pieced together units in which the pan, shower head, and doors are purchased separately. Each type of shower poses different installation issues.
Though the installation requirements of each of shower will differ, the installation of a shower in general requires the laying of several water transportation pipes, including a pipe for hot water and for cold water, and a drainage pipe.
It is important that the wet areas of a bathroom be waterproof, and multiple layers of waterproofing can be employed. Grout is used to fill gaps between tiles, but grout and tile setting materials are generally porous. Tiles are generally waterproof, though a shower pan must be installed beneath them as a safety to prevent water leakage.[29] Thus small mosaic tiles offer less of a defense than large format tiles. Sub-tile waterproofing is important when tiles are being used. Best practice requires a waterproofing material to cover the walls and floor of the shower area that are then covered with tile, or in some countries with a sheet material like vinyl.
Some shower areas utilize a second emergency drain outside of the shower in case of overflow. In Australia and some European countries, plumbing codes require this second emergency drain (but not in the United Kingdom nor North America).[citation needed]
A shower head is a perforated nozzle that distributes water over solid angle a focal point of use, generally overhead the bather. A shower uses less water than a full immersion in a bath. Some shower heads can be adjusted to spray different patterns of water, such as massage, gentle spray, strong spray, and intermittent pulse or combination modes. Hard water may result in calcium and magnesium deposits clogging the head, reducing the flow and changing the spray pattern. For descaling, various acidic chemicals or brushes can be used or some heads have rubber-like jets that can be manually descaled. A homemade remedy is to immerse it in a solution of water and vinegar for a while, since the vinegar is able to dissolve limescale.
Some governments around the world set standards for water usage and regulate shower heads. For example, in the United States, residential and most commercial shower heads must flow no more than 9.5 liters per minute (2.5 gallons per minute) per the Department of Energy ruling 10 CFR 430. Low-flow shower heads, less than or equal 7.6 liters per minute (2.0 gallons per minute), can use water more efficiently by aerating the water stream, altering nozzles through advanced flow principles or by high-speed oscillation of the spray stream. USEPA administers a voluntary water saving program, WaterSense, which can certify low-flow shower heads.
Shower curtains are curtains used in bathtubs with a shower or shower enclosures. They are usually made from vinyl, cloth or plastic. The shower curtain has two main purposes: to provide privacy and to prevent water from flooding or spraying outside the shower area. Shower curtains usually surround the bath inside the tub or shower area and are held up with railings or curtain rods high on the wall or ceiling. To accommodate the different types of bathtub shapes, railings can come in different sizes and are flexible in their design. Some people use two shower curtains: one that is inside the tub, which is mainly functional or decorative as well, and an outer shower curtain, which is purely decorative. The bottom portion of the inner curtain often comes with magnetic discs or suction cups which adhere to the bathtub itself.
Shower doors are doors used in bathrooms that help keep water inside a shower or bathtub and are alternatives to shower curtains. They are available in many different styles such as framed or frameless, sliding or swing. They are usually constructed of aluminium, clear glass, plexi-glass or tempered glass. Shower doors can come in many different hardware finishes and glass patterns that can match other bathroom hardware such as faucets and shower heads. There are also shower doors that are in a neo angle design for use on shower pans that have the neo design as well. The design of the shower pan is extremely important as the shower door must be the type required for the pan in order to work. A shower door requires plastic lining along the edges of the door to protect against water leaking out.
This article uses material from the Wikipedia article "Shower", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art