powered by CADENAS

Social Share

Amazon

Impeller (8335 views - Electrical Engineering)

An impeller (also written as impellor or impellar) is a rotor used to increase (or decrease in case of turbines) the pressure and flow of a fluid.
Go to Article

Explanation by Hotspot Model

Youtube


    

Impeller

Impeller

Impeller

An impeller (also written as impellor[1] or impellar) is a rotor used to increase (or decrease in case of turbines) the pressure and flow of a fluid.

In pumps

An impeller is a rotating component of a centrifugal pump which transfers energy from the motor that drives the pump to the fluid being pumped by accelerating the fluid outwards from the center of rotation.[2] The velocity achieved by the impeller transfers into pressure when the outward movement of the fluid is confined by the pump casing. Impellers are usually short cylinders with an open inlet (called an eye) to accept incoming fluid, vanes to push the fluid radially, and a splined, keyed, or threaded bore to accept a drive-shaft.

The impeller made out of cast material in many cases may be called rotor, also. It is cheaper to cast the radial impeller right in the support it is fitted on, which is put in motion by the gearbox from an electric motor, combustion engine or by steam driven turbine. The rotor usually names both the spindle and the impeller when they are mounted by bolts.

Heart pumps in medicine

In a failing heart, mechanical circulatory devices often utilize a continuous axial-flow impeller pump design.[3]

Types

  • Open impeller
  • Semi-open impeller
  • Closed or shrouded impeller.

In centrifugal compressors

The main part of a centrifugal compressor is the impeller. An open impeller has no cover, therefore it can work at higher speeds. A compressor with a covered impeller can have more stages than one that has an open impeller.

In water jets

Some impellers are similar to small propellers but without the large blades. Among other uses, they are used in water jets to power high speed boats.

Since impellers have no large blades to turn, they can spin at much higher speeds than propellers. The water forced through the impeller is channelled by the housing, creating a water jet that propels the vessel forward. The housing is normally tapered into a nozzle to increase the speed of the water, which also creates a Venturi effect in which low pressure behind the impeller pulls more water towards the blades, tending to increase the speed.

To work efficiently, there must be a close fit between the impeller and the housing. The housing is normally fitted with a replaceable wear ring which tends to wear as sand or other particles are thrown against the housing side by the impeller.

Vessels using impellers are normally steered by changing the direction of the water jet.

Compare to propeller and jet aircraft engines.

In agitated tanks

Impellers in agitated tanks are used to mix fluids or slurry in the tank. This can be used to combine materials in the form of solids, liquids and gas. Mixing the fluids in a tank is very important if there are gradients in conditions such as temperature or concentration.

There are two types of impellers, depending on the flow regime created (see figure):

  • Axial flow impeller
  • Radial flow impeller

Radial flow impellers impose essentially shear stress to the fluid, and are used, for example, to mix immiscible liquids or in general when there is a deformable interface to break. Another application of radial flow impellers are the mixing of very viscous fluids.

Axial flow impellers impose essentially bulk motion, and are used on homogenization processes, in which increased fluid volumetric flow rate is important.

Impellers can be further classified principally into three sub-types

  • Propellers
  • Paddles
  • Turbines

All these can be discussed immediately after example.

Example

If one heats a pot of soup on the stove the pot will develop a temperature gradient, (warmest on the bottom and cooler at the surface). Mild agitation will increase the rate of heating by dissipating the heat through the entire pot. See: Law of cooling (which also applies to heating). Even more significant, agitation disturbs the soup directly in contact with the hotter pot surface. Highly turbulent flow at the warming surface is important to good heat transfer. This is the same effect as the "wind chill" factor where moving air and turbulent action on surfaces (like those on people) resulting in significantly enhanced heat transfer. In unusual circumstances, overly-severe agitation may decrease the rate of heating which defeats the purpose.

Propellers

Propellers are axial thrust-giving elements. These elements give a very high degree of swirling in the vessel. The flow pattern generated in the fluid resembles a helix.

In washing machines

Some constructions of top loading washing machines use impellers to agitate the laundry during washing.

Firefighting rank badge

Fire services in the United Kingdom and many countries of the Commonwealth use a stylized depiction of an impeller as a rank badge. Officers wear one or more on their epaulettes or the collar of their firefighting uniform as an equivalent to the "pips" worn by the army and police.

In medical devices

Impellers are an integral part of axial-flow pump (AFPs), used in ventricular assist devices to augment or fully replace cardiac function.[4]

In air pumps

Air pumps, such as the roots blower, use meshing impellers to move air through a system. Applications include blast furnaces, ventilation systems, and superchargers for internal combustion engines.

See also



This article uses material from the Wikipedia article "Impeller", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced