powered by CADENAS

Social Share

Amazon

Powerlifting (6373 views - Sports List)

Powerlifting is a strength sport that consists of three attempts at maximal weight on three lifts: squat, bench press, and deadlift. As in the sport of Olympic weightlifting, it involves the athlete attempting a maximal weight single lift of a barbell loaded with weight plates. Powerlifting evolved from a sport known as "odd lifts", which followed the same three-attempt format but used a wider variety of events, akin to strongman competition. Eventually odd lifts became standardized to the current three. In competition, lifts may be performed equipped or un-equipped (typically referred to as 'raw' lifting or 'classic' in the IPF specifically). Equipment in this context refers to a supportive bench shirt or squat/deadlift suit or briefs. In some federations, knee wraps are permitted in the equipped but not un-equipped division; in others, they may be used in both equipped and un-equipped lifting. Weight belts, knee sleeves, wrist wraps and special footwear may also be used, but are not considered when distinguishing equipped from un-equipped lifting.Competitions take place across the world. Powerlifting has been a Paralympic sport (bench press only) since 1984 and, under the IPF, is also a World Games sport. Local, national and international competitions have also been sanctioned by other federations operating independently of the IPF.
Go to Article

Explanation by Hotspot Model

Youtube


    

Powerlifting

Powerlifting

Powerlifting
The deadlift being performed by 2009 IPF World Champion Dean Bowring
First played 20th century or earlier, United States
Characteristics
Type

International Powerlifting Federation (IPF) weight classes:

  • Women: 47 kg, 52 kg, 57 kg, 63 kg, 72 kg, 84 kg, 84 kg+
  • Men: 59 kg, 66 kg, 74 kg, 83 kg, 93 kg, 105 kg, 120 kg, 120 kg+
Presence
Olympic Inclusion in process (currently only participates as a Paralympic sport)
World Games 1981 – present

Powerlifting is a strength sport that consists of three attempts at maximal weight on three lifts: squat, bench press, and deadlift. As in the sport of Olympic weightlifting, it involves the athlete attempting a maximal weight single lift of a barbell loaded with weight plates.[1] Powerlifting evolved from a sport known as "odd lifts", which followed the same three-attempt format but used a wider variety of events, akin to strongman competition. Eventually odd lifts became standardized to the current three.

In competition, lifts may be performed equipped or un-equipped (typically referred to as 'raw' lifting or 'classic' in the IPF specifically). Equipment in this context refers to a supportive bench shirt or squat/deadlift suit or briefs. In some federations, knee wraps are permitted in the equipped but not un-equipped division; in others, they may be used in both equipped and un-equipped lifting. Weight belts, knee sleeves, wrist wraps and special footwear may also be used, but are not considered when distinguishing equipped from un-equipped lifting.[2]

Competitions take place across the world. Powerlifting has been a Paralympic sport (bench press only) since 1984 and, under the IPF, is also a World Games sport. Local, national and international competitions have also been sanctioned by other federations operating independently of the IPF.

History

Early history

The roots of powerlifting are found in traditions of strength training stretching back as far as ancient Greek and Roman times. The modern sport originated in the United Kingdom and the United States in the 1950s. Previously, the weightlifting governing bodies in both countries had recognized various "odd lifts" for competition and record purposes. During the 1950s, Olympic weightlifting declined in the United States, while strength sports gained many new followers. In 1958, the AAU's National Weightlifting Committee decided to begin recognizing records for odd lifts. A national championship was tentatively scheduled for 1959, but never happened. The first genuine national "meet" was held in September 1964 under the auspices of the York Barbell Company. Ironically, York Barbell owner Bob Hoffman had been a longtime adversary of the sport, but his company was now making powerlifting equipment to make up for the sales it had lost on Olympic equipment.

During the late 1950s, Hoffman's influence on Olympic lifting and his predominately Olympic-based magazine Strength and Health were beginning to come under increasing pressure from Joe Weider's organization. In order to combat the growing influence of Weider, Hoffman started another magazine, Muscular Development, which would be focused more on bodybuilding and the fast-growing interest in odd lift competitions. The magazine's first editor was John Grimek. During the late 1950s and early 1960s, various odd lift events gradually developed into the specific lifts of the bench press, squat, and deadlift, and they were lifted in that order. Hoffman became more and more influential in the development of this new lifting sport and organized the Weightlifting Tournament of America in 1964, effectively the first USA National championships. In 1965, the first named USA National Championships were held. During the same period, lifting in Britain also had factions. In the late 1950s, because members of the ruling body (BAWLA) were only interested in the development of Olympic lifting, a breakaway organization called the Society of Amateur Weightlifters had been formed to cater for the interests of lifters who were not particularly interested in Olympic lifting.

Although at that time there were 42 recognized lifts, the "Strength Set" (biceps curl, bench press, and squat) soon became the standard competition lifts, and both organizations held Championships on these lifts (as well as on the Olympic lifts) until 1965. In 1966, the Society of Amateur Weightlifters rejoined BAWLA and, in order to fall into line with the American lifts, the biceps curl was dropped and replaced with the deadlift. The first British Championship was held in 1966. During the late 1960s and at the beginning of the 1970s, various friendly international contests were held. At the same time, in early November of each year and to commemorate Hoffman's birthday, a prestigious lifting contest was held. In 1971, it was decided to make this event the "World Weightlifting Championships". The event was held on the morning of November 6, 1971, in York, Pennsylvania. There was no such thing as teams and thus the event consisted of a large group of American lifters, four British lifters, and one lifter from the West Indies. All of the referees were American. Weights were in pounds. Lifting order was "rising bar", and the first lift was the bench press. There was no such thing as a bench shirt or squat suit, and various interpretations were held regarding the use and length of knee wraps and weightlifting belts. The IPF rules system did not exist yet, nor had world records been established.

Because of the lack of formalized rules, some disputes occurred. There was no 52 kg class, 100 kg class, or 125 kg class. At the first World Championships, one of the American super-heavyweights, Jim Williams, benched 660 lbs on his second attempt (no shirt), and almost locked out 680 lbs on a third attempt. Some other notable lifts were Larry Pacifico benching 515 lbs in the 90 kg class, John Kuc deadlifting 820 lbs, and Vince Anello attempting 800 lbs at 90 kg.[3] Hugh Cassidy and Williams both totaled 2,160 lbs, but Cassidy got the win because of a lower bodyweight in the Super heavyweight division.

In 1972 the 'second' AAU World Championships were held, this time over two days – 10 and 11 November. This time there were 8 lifters from Great Britain (two of whom, Ron Collins and John Pegler, did stints as Referees), six Canadians, two Puerto Ricans, three Zambians, and one from the West Indies. With 67 lifters in all, the other 47 were Americans. Lifts were still measured in pounds, the bench press was the first lift, and there were still no suits, power belts, or fancy wraps. New Zealand's Precious McKenzie won his 'second' world title with 550 kg at 56. Mike Shaw 'lost' his world title, won the previous year, to American Jack Keammerer. Ron Collins made up for his 'bomb' on the bench in 1971 and stormed to the 75 kg title. Pacifico just won against another American, Mel Hennessey, at 110 kg, both with enormous benches of 260 kg and 255 kg. At Super (over 110 kg) John Kuc beat Jim Williams with an incredible 2,350 lbs total (raw). Kuc squatting 905 lbs for a record squat and attempting a 397½ (875 lbs) deadlift again, and Williams benching a massive 307½ (675 lbs) – the greatest bench press ever at the time, before just missing with 317½ (700 lbs).[4] Jon Cole, the Super heavyweight winner of the US Senior Championships 1972 and holder of the greatest total at that time with 1,075 kg (2,370 lbs), didn't show up to take on Kuc.

IPF and after

The International Powerlifting Federation was formed immediately after the contest, and so none of the lifts could be yet registered as official world records. The 1973 Worlds was also held in York. This time there were only 47 entrants: one Swedish, one Puerto Rican (Peter Fiore, who was lifting for Zambia), two Canadians, one West Indian, eight British, and the rest Americans. The officiating became more international and included Tony Fitton and Terry Jordan from Britain, a Canadian, and a Zambian. American Bob Crist was the IPF President, and another American, Clarence Johnson, was Vice-President. 1973 was the first time that the lifts were done in the order now recognized – squat, bench press, deadlift (although still lifting in pounds). Precious Mackenzie won his third World title, easily beating American teenager Lamar Gant. 1974 was the first time that teams had to be selected in advance. With 74 entrants, this was the largest Worlds so far. The 52 kg class was introduced, and nine lifters entered. In 1975, the World Championships was held outside America for the first time, at the town hall in Birmingham, hosted by Vic Mercer. 82 lifters entered. Unusually for a competition, the super-heavyweights lifted first. This was because the television company filming the event was only interested in filming the "big guys". Hoffman sent over tons of equipment for this contest and did not take it back, and local legend says it is all still being used in Birmingham and the wider West Midlands region.

The establishment of the IPF in 1973 spurred the establishment of the EPF (European Powerlifting Federation) in 1974. Since it was closely associated with bodybuilding and women had been competing as bodybuilders for years, the new sport was opened to them very quickly. The first U. S. national championships for women were held in 1978 and the IPF added women's competition in 1979. In the USA, the Amateur Sports Act of 1978 required that each Olympic or potential Olympic sport must have its own national governing body by November 1980. As a result, the AAU lost control of virtually every amateur sport. The USPF was founded in 1980 as the new national governing body for American powerlifting. Soon, controversy over drug testing would cause powerlifting to splinter into multiple federations. In 1981, the American Drug Free Powerlifting Association (ADFPA), led by Brother Bennett, became the first federation to break away from the USPF, citing the need to implement effective drug testing in the sport.[5] Meanwhile, the IPF was moving towards adopting drug testing at international meets, and requiring member nations to implement drug testing at national meets as well. In 1982, drug testing was introduced to the IPF men's international championship, although the USPF championships that year did not have drug testing.[6]

The IPF's push for drug testing was resisted by some American lifters, and in 1982 Larry Pacifico and Ernie Frantz founded the American Powerlifting Federation (APF), which advertised its categorical opposition to all drug testing.[5] In 1987, the American Powerlifting Association (APA) and World Powerlifting Alliance (WPA) were formed by Scott Taylor. The APA and WPA offer both drug tested and non-tested categories in most of their competitions. Ultimately, the USPF failed to conform to IPF demands and was expelled from the international body in 1997, with the ADFPA, now named USA Powerlifting (USAPL), taking its place.[7] Despite the trend towards more and more federations, each with their own rules and standards of performance, some powerlifters have attempted to bring greater unity to the sport. For example, 100% RAW promoted unequipped competition and merged with another federation, Anti-Drug Athletes United (ADAU), in 2013.[8] The Revolution Powerlifting Syndicate (RPS), founded by Gene Rychlak in 2011, might also be considered a move towards greater unity, as the RPS breaks the tradition of charging lifters membership fees to a specific federation in addition to entry fees for each competition.[9] Also, some meet promoters have sought to bring together top lifters from different federations, outside existing federations' hierarchy of local, regional, national and international meets; a prominent example of this is the Raw Unity Meet (RUM), held annually since 2007.[10]

Developments in equipment and rules

As new equipment was developed, it came to distinguish powerlifting federations from one another. Weight belts and knee wraps (originally simple Ace bandages) predated powerlifting, but in 1983 John Inzer invented the first piece of equipment distinct to powerlifters—the bench shirt.[11] Bench shirts and squat/deadlift suits (operating on the same principle) became ubiquitous in powerlifting, but only some federations adopted the latest and most supportive canvas, denim, and multiply polyester designs, while others such as the IPF maintained more restrictive rules on which supportive equipment could be used.[12] The Monolift, a rack in which the bar catches swing out and eliminate the walkout portion of the squat, was invented by Ray Madden and first used in competition in 1992.[13] This innovation was adopted by some federations and forbidden in others. Other inventions included specialized squat bars and deadlift bars, moving away from the IPF standard of using the same bar for all three lifts.

The rules of powerlifting have also evolved and differentiated. For example, in ADFPA/USAPL competition, the "press" command on the bench press was used, not used,[14] and then used again, following a 2006 IPF motion to reinstate this rule.[15] IPF rules also mandate a "start" command at the beginning of the bench press. Many other federations, for example the Natural Athlete Strength Association (NASA), have never used the "start" command.[16] As a further example of diversifying rules of performance, in 2011 the Southern Powerlifting Federation (SPF) eliminated the "squat" command at the beginning of the squat.[17] Some federations also now allow the sumo variation of the deadlift, which varies with the feet being considerably wider apart and some tension taken off the lower spine being taken up by the legs. Many communities and federations do not class the sumo variation as a technical deadlift.[18]

Supportive equipment

In powerlifting, supportive equipment refers to supportive shirts, briefs, suits, and sometimes knee wraps made of materials that store elastic potential energy and thereby assist the three lifts contested in the sport: squat, bench press and deadlift.[19] Some federations allow single ply knee sleeves, which contestant can put on and off by himself, and wraps for wrists in raw competition, while some don't and there are also some federations that hold raw records with and without wraps like GPA. Straps are also used, as help with deadlift in case of a weak grip but are not allowed by any federations in official competitions. Belt is the only supportive equipment that is allowed by all federations in raw competition. The use of supportive equipment distinguishes 'equipped' and 'un-equipped' or 'raw' divisions in the sport, and 'equipped' and 'unequipped' records in the competition lifts. The wide differences between equipped and unequipped records in the squat and bench suggest that supportive equipment confers a substantial advantage to lifters in these disciplines.[20] This is less evident in the case of the deadlift, where the lack of an eccentric component to the lift minimizes how much elastic energy can be stored in a supportive suit. Supportive equipment should not be confused with the equipment on which the lifts are performed, such as a bench press bench or the barbell and discs; nor with personal accessories such as a weightlifting belt that may allow greater weight to be lifted, but by mechanisms other than storing elastic energy.

Principles of operation

Supportive equipment is used to increase the weight lifted in powerlifting exercises.[20][21][22] A snug garment is worn over a joint or joints (such as the shoulders or hips). This garment deforms during the downward portion of a bench press or squat, or the descent to the bar in the deadlift, storing elastic potential energy.[23] On the upward portion of each lift, the elastic potential energy is transferred to the barbell as kinetic energy, aiding in the completion of the lift.[19][24] Some claim that supportive equipment prevents injuries by compressing and stabilizing the joints over which it worn.[24] For example, the bench shirt is claimed to support and protect the shoulders.[20] Critics point out that the greater weights used with supportive equipment and the equipment's tendency to change the pattern of the movement may compromise safety, as in the case of the bar moving towards the head during the upward portion of the shirted bench press.[25]

Material and construction

Different materials are used in the construction of supportive equipment. Squat suits may be made of varying types of polyester, or of canvas. The latter fabric is less elastic, and therefore considered to provide greater 'stopping power' at the bottom of the movement but less assistance with the ascent.[22] Bench shirts may be made of polyester or denim,[21] where the denim again provides a less-elastic alternative to the polyester. Knee wraps are made of varying combinations of cotton and elastic.[26] Supportive equipment can be constructed in different ways to suit lifters' preferences. A squat or deadlift suit may be constructed for a wide or a narrow stance; and a bench shirt may be constructed with 'straight' sleeves (perpendicular to the trunk of the lifter) or sleeves that are angled towards the abdomen. The back of the bench shirt may be closed or open, and the back panel may or may not be of the same material as the front of the shirt. Similarly, 'hybrid' squat suits can include panels made from canvas and polyester, in an effort to combine the strengths of each material. When two or more panels overlay one another in a piece of supportive equipment, that equipment is described as 'multi-ply', in contrast to 'single-ply' equipment made of one layer of material throughout.[22]

Raw powerlifting

Unequipped or "raw" (often styled as RAW) or classic powerlifting has been codified in response to the proliferation and advancement of bench shirts and squat/deadlift suits. The AAU first began its raw division in 1994 and the term "raw" was coined by Al Siegal who later formed the ADAU in 1996. The 100% RAW federation was founded in 1999;[27] within a decade, many established federations came to recognize "raw" divisions in addition to their traditional (open) divisions permitting single-ply or multi-ply equipment. RAW during this time frame however was looked upon as a beginners stage by the elite lifters in powerlifting. In January 2008 the Raw Unity Meet (simply known as "RUM") was formed by Eric Talmant and Johnny Vasquez. This contest became the turning point in raw lifting. It was a crucial contest that gathered the best lifters under one roof regardless of gear worn to compete without equipment. Brian Schwab, Amy Weisberger, Beau Moore, Tony Conyers, Arnold Coleman and Dave Ricks were among the first Elite lifters to remove their equipment and compete raw. RUM spearheaded raw lifting into what it has become today. United Powerlifting Association (UPA) established a standard for raw powerlifting in 2008[28] and USAPL held the first Raw Nationals in the same year.[29] Eventually, IPF recognized raw lifting with the sanction of a "Classic 'Unequipped' World Cup" in 2012, and published its own set of standards for raw lifting.[30] By this time, the popularity of raw lifting has surged to the point where raw lifters came to predominate over equipped lifters in local meets.[31][32] Note that the IPF's use of the word 'classic' to describe raw powerlifting is differentiated from most other powerlifting federations' use of the word to differentiate between 'classic raw' and 'modern raw': classic raw is still unequipped but allows the use of knee wraps while modern raw allows knee sleeves at most. The IPF does not allow knee wraps in its unequipped competitions and would thus be considered 'modern raw' but the IPF does not recognize the word 'raw.'

The use of knee sleeves in unequipped powerlifting has brought about much debate as to whether certain neoprene knee sleeves can actually assist a lifter during the squat. Some lifters purposely wear knee sleeves which are excessively tight and have been known to use plastic bags and have others to assist them get their knee sleeves on. This led to the IPF mandating that lifters put on their knee sleeves unassisted.[33]

Equipped powerlifting

Equipped lifters compete separately from raw lifters. Equipped lifters will wear a squat suit, knee wraps, a bench shirt, and a deadlift suit. These four things are what separate equipped lifters and raw lifters. A squat suit is made of an elastic-like material, and a single-ply polyester layer. This allows a competitor to spring out of the bottom of a squat (called "pop out of the hole" in Powerlifting circles) by maintaining rigidity, keeping him or her upright and encouraging their hips to remain parallel with the floor. This allows lifters to lift more weight than would normally be possible without the suit. There are also multi-ply suits giving the lifter even more rigidity, like that of a traditional canvas suit, with the same pop as a single-ply suit or briefs.[34] During the squat, lifters also tend to wear knee wraps. Even though knee wraps will be a sub-classification of raw lifting it will still be worn by equipped lifters. A raw lifter who would squat in knee wraps will have the weight lifted noted as "in wraps" to distinguish this from the other raw lifters. Knee wraps are made out of the same, or very similar, elastic material as wrist wraps are made out of. They are wrapped around the lifters knees very tightly with the lifter usually not being able to do it himself and needing someone to assist them in doing so. The knee wraps are wrapped in a spiral or diagonal method. The knee wraps build elastic energy during the eccentric part of the squat and once the lifter has hit proper depth the lifter will start the concentric part of the movement releasing this elastic energy and using it to help them move the weight upwards. It gives the lifter more spring, or pop out of the hole of the squat resulting in a heavier and faster squat.

For the bench press, there are also single-ply and multi-ply bench shirts that work similarly to a squat suit. It acts as artificial pectoral muscles and shoulder muscles for the lifter. It resists the movement of the bench press by compressing and building elastic energy. When the bar is still and the official gives the command to press the compression and elastic energy of the suit aids in the speed of the lift, and support of the weight that the lifter would not be able to provide for himself without the bench shirt. In order to achieve proper tightness and fitting the lifter must be assisted when putting the bench shirt on for it is not possible to be done alone.

For the deadlift suit, there is single-ply and multi-ply as well. The elastic energy is built when the lifter goes down to set up and place their grip on the bar before lifting even starts. The deadlift suit aids in getting the weight off the floor, considered to be the first part of the movement, but not very helpful on the lockout portion of the deadlift, known as the second part of the movement.

Classes and categories

Weight Classes:

Most powerlifting federations use the following weight classes:[35][36][37]

Men: 52 kg, 56 kg, 60 kg, 67.5 kg, 75 kg, 82.5 kg, 90 kg, 100 kg, 110 kg, 125 kg, 140 kg, 140 kg+

Women: 44 kg, 48 kg, 52 kg, 56 kg, 60 kg, 67.5 kg, 75 kg, 82.5 kg, 90 kg, 90 kg +

However, in 2011, the IPF introduced the following new weight classes:

IPF Weight Classes:

Men: up to 53 kg (Sub-Junior/Junior), 59 kg, 66 kg, 74 kg, 83 kg, 93 kg, 105 kg, 120 kg, 120 kg+

Women: up to 43 kg (Sub-Junior/Junior), 47 kg, 52 kg, 57 kg, 63 kg, 72 kg, 84 kg, 84 kg +

Age categories

This depends on the federation generally but averages are as follows:

15-18 (Sub-Jr), 19-23 (Jr), Any age(Open), 40+(Masters)

The IPF uses the following age categories: sub-junior (18 and under), junior (19-23), open (24-39), masters 1 (40-49), masters 2 (50-59), masters 3 (60-69), masters 4 (70+). Age category is dependent on the year of the participant's birth. For example, if the participant turns 18 years old in January, he or she is still considered a Sub-junior until the end of that calendar year. Other federations typically break the Masters' categories down to 5-year increments, for example, 40-44, 45-49, 50-54, etc. Some federations also include a sub-master class from 35-39.

Grip

There are multiple types of grip in powerlifting. Not all are allowed in competitions. There are couple of classifications:

  • considering the position of the barbell in the hand
    • full grip - mostly used in squats, military press and push press
    • fingertip grip - mostly used in deadlift
  • considering the position of the thumb
    • regular grip
    • thumbless or suicide or false or monkey or open-hand grip - mostly used in squats and recreational bench press
    • hook grip - sometimes used in deadlift
  • considering the orientation of the palm
    • prone/pronated or overhand or double overhand grip - used in bench press and deadlift; the last term is almost exclusively used when talking about deadlift
    • reverse or supine/supinated or underhand grip - sometimes used in bench press
    • alternated or mixed grip - one hand is supinated and the other is pronated; often used in deadlift
  • considering the distance between hands - almost exclusively used when talking about bench press
    • wide grip
    • narrow grip
  • combinations
    • thumbless mixed grip - sometimes used in deadlift

Competition

A powerlifting competition takes place as follows:

Each competitor is allowed three to three attempts on each of the squat, bench press, and deadlift, depending on their standing and the organization they are lifting in. The lifter's best valid attempt on each lift counts toward the competition total. For each weightclass, the lifter with the highest total wins. If two or more lifters achieve the same total, the lighter lifter ranks above the heavier lifter.[38]Problem

Competitors are judged against other lifters of the same gender, weight class, and age. This helps to ensure that the accomplishments of lifters like Lamar Gant, who has deadlifted 5 times his bodyweight, are recognized alongside those of Eddie Hall, the current All-time deadlift world record holder.

Comparisons of lifters and scores across different weight classes can also be made using handicapping systems. World federations use the following ones: Wilks (IPF), Glossbrenner (WPC), Reshel (APF, GPC, GPA, WUAP, IRP), Outstanding Lifter (aka OL or NASA) (NASA), Schwartz/Malone, Siff; for cadet and junior categories Foster coefficient is mostly used, while for master categories (above 40 years old) McCulloch or Reshel coefficients. [39][40] Winner of a competition based on a official coefficient used by presiding world federation is called best lifter.

During the 2016 World Open Powerlifting Championships, the three best competitors were Fedosienko Sergey, Summer Blaine, and Olech Jaroslaw. The country with the most combined points was the Ukraine, who beat the next best team United States by close to 100 points. The 2016 championships did not see the same athletic stand out that the 2015 championships did by athlete Samuel Ogden from Ohio.[41]

Events

In a powerlifting competition, sometimes referred to as standard competition, there are three events: bench press, squat, and deadlift. Placing is achieved via combined total. Some variations of this are found at some meets such as "push-pull only" meets where lifters only compete in the bench press and deadlift, with the bench press coming first and the deadlift after. Single lift meets (or full meets) are often held, sometimes alongside a normal 3-lift event. This is most common in the bench press.

At a meet the events will follow in order: squat, then bench press, and the deadlift will be the final lift of the meet. If the federation also has an event for strict curls this will normally occur before the squat event.

There are also, though very rarely, endurance meets (or "for repetitions" meets) where lifters compete in number of repetitions of exercise with the same weight (most often bench press and most often the weight is equal to lifter's weight). WDFPF held such competitions.

Rules

Squat

There are two types depending on equipment used: conventional stand and monolift stand. In case of the former lift is called walked out squat and in case of the latter lift is called monolift squat. Very few federations allow monolift stand and one such is GPC.

The lift starts with the lifter standing erect and the bar loaded with weights resting on the lifter's shoulders. At the referee's command the lift begins. The lifter creates a break in the hips, bends his knees and drops into a squatting position with the hip crease (the top surface of the leg at the hip crease) below the top of the knee. The lifter then returns to an erect position. At the referee's command the bar is returned to the rack and the lift is completed.

  • After removing the bar from the racks while facing the front of the platform, the lifter may move forward or backward to establish the lifting position. The top of the bar not more than 3 cm below the top of the anterior deltoids. The bar shall be held horizontally across the shoulders with the hands and/or fingers gripping the bar, and the feet flat upon the platform with the knees locked.
  • The lifter shall wait in this position for the head referee's signal. The signal will be given as soon as the lifter is set and demonstrates control with the bar properly positioned. The head referee's signal shall consist of a downward movement of the arm and audible command "Squat".
  • Upon receiving the head referee's signal, the lifter must bend the knees and lower the body until the top surface of the legs at the hip joint is lower than the top of knees.
  • The lifter must recover at will, without double bouncing, to an upright position with the knees locked. The bar may stop, but there must be no downward motion during recovery. As soon as the lifter demonstrates a controlled final position, the head referee will give the signal indicating completion of the lift and to replace the bar.
  • The signal to replace the bar will consist of a backward motion of the arm and the audible command "Rack". The lifter must then make a reasonable attempt to return the bar to the racks.
  • The lifter shall face the front of the platform, towards the head referee.
  • The lifter shall not hold the collars or discs at any time during the performance of the lift. However, the edge of the hands gripping the bar may be in contact with the inner surface of the collar.
  • Not more than five and not less than two loaders/spotters shall be on the platform at any time.
  • The lifter may enlist the help of spotters in removing the bar from the racks; however, once the bar has cleared the racks, the spotters shall not physically assist the lifter with regards to actually getting into the proper set position. The spotters may assist the lifter to maintain control should the lifter stumble or demonstrate any evident instability.
  • The lifter will be allowed only one commencement signal per attempt.
  • The lifter may be given an additional attempt at the same weight at the head referee's discretion if failure in an attempt was due to any error by one or more of the spotters.

Causes for disqualification

  • Failure to observe the head referee's signals at the commencement or completion of a lift.
  • Double bouncing or more than one recovery attempt at the bottom of the lift.
  • Failure to assume an upright position with knees locked at the commencement and completion of the lift.
  • Movement of the feet laterally, backward or forward that would constitute a step or stumble.
  • Failure to bend the knees and lower the body until the surface of the legs at the hip joint is lower than the tops of the knees.
  • Any resetting of the feet after the squat signal.
  • Contact with the bar by the spotters between the referee's signals.
  • Contact of elbows or upper arms with the legs.
  • Failure to make a reasonable attempt to return the bar to the racks.
  • Any intentional dropping or dumping of the bar.

Bench press

With her or his back resting on the bench, the lifter takes the loaded bar at arm's length. The lifter lowers the bar to the chest. When the bar becomes motionless on the chest, the referee gives a press command. Then the referee will call 'Rack' and the lift is completed as the weight is returned to the rack.

  • The front of the bench must be placed on the platform facing the head referee.
  • The lifter must lie backward with shoulders and buttocks in contact with the flat bench surface. The lifter's shoes or toes must be in solid contact with the platform or surface. The position of the head is optional.
  • To achieve firm footing, a lifter of any height may use discs or blocks to build up the surface of the platform. Whichever method is chosen, the shoes must be in a solid contact with the surface. If blocks are used, they shall not exceed 45 cm x 45 cm.
  • Not more than five and not less than two loaders/spotters shall be in attendance. The lifter may enlist the help of one or more of the designated spotters or enlist a personal spotter in removing the bar from the racks. Only designated spotters may remain on the platform during the lift. The lift off must be to arms length and not down to the chest. A designated spotter, having provided a centre lift off, must immediately clear the area in front of the head referee and move to either side of the bar. If the personal spotter does not immediately leave the platform area and/or in any way distracts or impedes the head referees' responsibilities, the referees may determine that the lift is unacceptable, and be declared "no lift" by the referees and given three red lights.
  • The spacing of the hands shall not exceed 81 cm, measured between the forefingers. The bar shall have circumferential machine markings or tape indicating this maximum grip allowance. If the lifter should use an offset or unequal grip on the bar, whereby one hand is placed outside the marking or tape, it is the lifters responsibility to explain this to the head referee, and allow inspection of the intended grip prior to making an attempt. If this is not done until the lifter is on the platform for an official attempt, any necessary explanation and/or measurements will be done on the lifter's time for that attempt. The reverse or underhand grip is forbidden, as is a thumbless grip.
  • After receiving the bar at arms length, the lifter shall lower the bar to the chest and await the head referees' signal.
  • The signal shall be an audible command "Press" and given as soon as the bar is motionless on the chest. As long as the bar is not so low that it touches the lifter's belt, it is acceptable.
  • The lifter will be allowed only one commencement signal per attempt.
  • After the signal to commence the lift has been given, the bar is pressed upward. The bar shall not be allowed to sink into the chest or move downwards prior to the lifter's attempt to press upward. The lifter will press the bar to straight arm's length and hold motionless until the audible command "Rack" is given. Bar may move horizontally and may stop during the ascent, but may not move downward towards the chest.

Causes for disqualification

  • Failure to observe the referee's signals at the commencement or completion of the lift.
  • Any change in the elected position that results in the buttocks breaking contact with the bench or lateral movement of the hands (between the referee's signals). Any excessive movement or change of contact of the feet during the lift proper.
  • Allowing the bar to sink into the chest after receiving the referee's signal.
  • Pronounced uneven extension of the arms during or at the completion of the lift.
  • Any downward motion of the bar during the course of being pressed out.
  • Contact with the bar by the spotters between the referee's signals.
  • Any contact of the lifter's shoes with the bench or its supports.
  • Deliberate contact between the bar and the bar rest uprights during the lift to assist the completion of the press.
  • It is the responsibility of the lifter to inform any personally enlisted spotters to leave the platform as soon as the bar is secured at arms length. Such spotters shall not return to the platform upon completion or failure of the attempt. It is especially important for a spotter providing a centre lift off to leave the platform quickly so as not to impair the head referee's view. Failure of any personal spotters to leave the platform may cause disqualification of the lift.

Deadlift

In the deadlift the athlete grasps the loaded bar which is resting on the platform floor. The lifter pulls the weights off the floor and assumes an erect position. The knees must be locked and the shoulders back, with the weight held in the lifter's grip. At the referee's command the bar will be returned to the floor under the control of the lifter.

  • The bar must be laid horizontally in front of the lifter's feet, gripped with an optional grip in both hands, and lifted until the lifter is standing erect. The bar may stop but there must be no downward motion of the bar.
  • The lifter shall face the front of the platform.
  • On completion of the lift, the knees shall be locked in a straight position and the lifter shall be standing erect.
  • The head referee's signal shall consist of a downward movement of the arm and the audible command "Down". The signal will not be given until the bar is held motionless and the lifter is in an apparent finished position.
  • Any raising of the bar or any deliberate attempt to do so will count as an attempt.

Causes for disqualification

  • Any downward motion of the bar before it reaches the final position.
  • Failure to stand erect.
  • Failure to lock the knees straight at the completion of the lift.
  • Supporting the bar on the thighs during the performance of the lift. 'Supporting' is defined as a body position adopted by the lifter that could not be maintained without the counterbalance of the weight being lifted.
  • Movement of the feet laterally, backward or forward that would constitute a step or stumble.
  • Lowering the bar before receiving the head referee's signal.
  • Allowing the bar to return to the platform without maintaining control with both hands.

Training

Powerlifters practice weight training to improve performance in the three competitive lifts—the squat, bench press and deadlift. Weight training routines used in powerlifting are extremely varied. For example, some methods call for the use of many variations on the contest lifts, while others call for a more limited selection of exercises and an emphasis on mastering the contest lifts through repetition.[42] While many powerlifting routines invoke principles of sports science, such as specific adaptation to imposed demand (SAID principle),[43] there is some controversy around the scientific foundations of particular training methods, as exemplified by the debate over the merits of "speed work," or training to attain maximum acceleration of submaximal weights.[44]

In addition to weight training, powerlifters may pursue other forms of training to improve their performance. For example, aerobic exercise may be used to improve endurance during drawn-out competitions and support recovery from weight training sessions.[45]

Common set & rep schemes are based on a percentage of the lifter's 1RM (1 Rep Maximum). For example, 5 sets of 5 reps (5x5) at 75% of the 1RM. Rest periods between sets range from 2–5 minutes based on the lifter's ability to recover fully for the next set.[46]

Federations

Prominent international federations include:

Of these federations, the oldest and most prominent is the IPF. It comprises federations from over 100 countries located on six continents. The IPF is the federation responsible for coordinating participation in the World Games, an international event affiliated with the International Olympic Committee.The IPF has many affiliates, one of these being USAPL. Specifically, the USAPL regulates all ages of lifters from the high school level to ages 40+ within the United States.[48] The next-oldest federation is the WPC, formed as the international companion to the APF after its split from the USPF.

Different federations have different rules and different interpretations of the rules, leading to a myriad of variations. Differences arise on the equipment eligible, clothing, drug testing and aspects of allowable technique. The 100% Raw Federation allows no supportive gear to be worn by the lifter while the IPF, AAU, NASA, USAPL and the ADFPF only allow a single-ply tight polyester squat suit, deadlift suit and bench shirt, wraps for knees and wrists, and a belt in the equipped divisions. Other federations, such as the APF, APA, IPA, SPF, WPC, AWPC and WPO, allow opened or closed back bench shirts, multi-ply gear, and a wide array of gear materials such as canvas, denim, polyester etc.

The USPA was founded in 2010 by Steve Denison based on a lifter friendly environment. It's explosive growth (holding over 225 competitions each year worldwide) has been attributed to a strict adherence to the rules, without the politics. Both the USPA, and the IPL (International Powerlifting League) now rank among the largest, and most respected Organizations in both the US, and World, in the sport of powerlifting.[49]

The IPF has suspended entire member nations' federations, including the Russian Federation, Ukraine, Kazakhstan, Iran, India and Uzbekistan, for repeated violations of the IPF's anti-doping policies.[50] However Russia, Ukraine and Kazakhstan did not serve their full suspension.

Rank and classification

There are several classifications in powerlifting determining rank. These typically include Elite, Master, Class I,II,III,IV. The Elite standard is considered to be within the top 1% of competing powerlifters. Several standards exist, including the United States Powerlifting Association classifications,[51] the IPF/USAPL (single-ply) classifications,[52] the APF (multi-ply) classifications,[53] and the Anti-Drug Athletes United (ADAU, raw) classifications.[54] Countries in the former Soviet Union use a somewhat different nomenclature for the top classes, distinguishing among Masters of sport, International Class; Masters of Sport; and Candidates for Master of Sport.

The Master classification should not be confused with the Master age division, which refers to athletes who are at least 40 years old.[55]

American high schools

In the United States, powerlifting is not a popular sport in schools, although relatively more popular in the South and in the Upper Midwest. Texas, Oklahoma, Wisconsin, Mississippi, Louisiana and Ohio have the most successful programs.[56]

Gyms

Powerlifting gyms range from commercial fitness centers to private clubs. Some gyms gain fame due to their association with a training methodology (e.g., Westside Barbell[57]), federation (e.g., Lexen Xtreme[58] and the Xtreme Power Coalition [XPC][59]), or publication (e.g., SuperTraining Gym[60] and Power magazine[61]). Other gyms are notable for their association with champion powerlifters, for example Quads Gym and Ed Coan.[62] Other notable powerlifters operate their own gyms, such as Scot Mendelson's F.I.T., Dan Green's Boss Barbell and Žydrūnas Savickas.

Global database

The global meet results are available in a searchable web database.

World champions

See: List of world championships medalists in powerlifting (men) or List of world championships medalists in powerlifting (women)

See also



This article uses material from the Wikipedia article "Powerlifting", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Sports List

Air sports
• Aerobatics
• Air racing
• Cluster ballooning
• Hopper ballooning

Wingsuit flying
• Gliding
• Hang gliding
• Powered hang glider
• Human powered aircraft
• Model aircraft
• Parachuting
• Banzai skydiving
• BASE jumping
• Skydiving
• Skysurfing
• Wingsuit flying
• Paragliding
• Powered paragliding
• Paramotoring
• Ultralight aviation

Archery
• Field archery
• Flight archery
• Gungdo
• Indoor archery
• Kyūdō
• Popinjay
• Target archery

Ball-over-net games
• Badminton
• Ball badminton
• Biribol
• Bossaball
• Fistball
• Footbag net
• Football tennis
• Footvolley
• Hooverball
• Jianzi
• Padel
• Peteca
• Pickleball
• Platform tennis
• Sepak takraw
• Sipa
• Throwball
• Volleyball
• Beach volleyball
• Water volleyball
• Paralympic volleyball
• Wallyball
• Ringo


Basketball family
• Basketball
• Beach basketball
• Deaf basketball
• Streetball
• Water basketball
• Wheelchair basketball
• Cestoball
• Korfball
• Netball
• Fastnet
• Indoor netball
• Ringball
• Slamball

Bat-and-ball (safe haven)
• Baseball
• Softball
• Slow pitch
• Fast-pitch softball
• 16-inch softball
• Bat and trap
• British baseball – four posts
• Brännboll – four bases
• Corkball – four bases (no base-running)
• Cricket – two creases
• Indoor cricket
• Limited overs cricket
• One Day International
• Test cricket
• Twenty20
• Danish longball
• Kickball
• Kilikiti
• Lapta – two salos (bases)
• The Massachusetts Game – four bases
• Matball
• Oina
• Old cat – variable
• Over-the-line – qv
• Palant
• Pesäpallo – four bases
• Punchball
• Rounders – four bases or posts
• Scrub baseball – four bases (not a team game per se)
• Stickball – variable
• Stool ball – two stools
• Tee-ball
• Town ball – variable
• Vigoro – two wickets
• Wireball
• Wiffleball

Baton twirling
• Baton twirling

Acro sports
• Ballet
• Dancing
• Cheerleading
• Gymnastics

Performance sports
• Drum corps
• Marching band

Board sports

• Skateboarding
• Scootering
• Casterboarding
• Freeboard (skateboard)
• Longboarding
• Streetboarding
• Skysurfing
• Streetluge
• Snowboarding
• Mountainboarding
• Sandboarding
• Snowkiting
• Surfing
• Wakesurfing
• Bodyboarding
• Riverboarding
• Skimboarding
• Windsurfing
• Wakeboarding
• Kneeboarding
• Paddleboarding

Catch games
• Dodgeball
• Ga-ga
• Keep away
• Kin-Ball
• Newcomb ball
• Quidditch
• Rundown (a.k.a. Pickle)
• Yukigassen

Climbing

• Abseiling
• Aid climbing
• Ice climbing
• Mixed climbing
• Mountaineering
• Rock climbing
• Bouldering
• Deep-water soloing
• Sport climbing
• Traditional climbing
• Other
• Canyoning (Canyoneering)
• Coasteering
• Hiking
• Rope climbing
• Pole climbing

Cycling

• Artistic cycling
• BMX
• Cyclo-cross
• Cross-country mountain biking
• Cycle polo
• Cycle speedway
• Downhill mountain biking
• Dirt jumping
• Enduro mountain biking
• Freestyle BMX
• Hardcourt Bike Polo
• Road bicycle racing
• Track cycling
• Underwater cycling

Skibob
• Skibobbing

Unicycle

• Mountain unicycling
• Unicycling
• Unicycle basketball
• Unicycle hockey
• Unicycle trials
Combat sports: wrestling and martial arts
• Aiki-jūjutsu
• Aikido
• Jujutsu
• Judo
• Brazilian jiu-jitsu
• Sambo (martial art)
• Sumo
• Wrestling
• Amateur wrestling
• Greco-Roman wrestling
• Freestyle wrestling
• Folk wrestling
• Boli Khela
• Collar-and-elbow
• Cornish wrestling
• Dumog
• Glima
• Gouren
• Kurash
• Lancashire wrestling
• Catch wrestling
• Malla-yuddha
• Mongolian wrestling
• Pehlwani
• Professional wrestling
• Schwingen
• Shuai jiao
• Ssireum
• Varzesh-e Pahlavani
• Yağlı Güreş
• Greek wrestling

Striking

• Choi Kwang-Do
• Cockfighting
• Boxing
• Bokator
• Capoeira
• Fujian White Crane
• Karate
• Kenpō
• Kickboxing
• Lethwei
• Muay Thai
• Pradal serey
• Sanshou
• Savate
• Shaolin Kung Fu
• Sikaran
• Silat
• Subak
• Taekkyeon
• Taekwondo
• Taidō
• Tang Soo Do
• Wing Chun
• Zui quan

Mixed or hybrid
• Baguazhang
• Bando
• Bartitsu
• Bujinkan
• Hapkido
• Hwa Rang Do
• Jeet Kune Do
• Kajukenbo
• Kalaripayattu
• Krav Maga
• Kuk Sool Won
• Marine Corps Martial Arts Program
• Mixed martial arts
• Northern Praying Mantis
• Ninjutsu
• Pankration
• Pencak Silat
• Sanshou
• Shidōkan Karate
• Shōrin-ryū Shidōkan
• Shoot boxing
• Shootfighting
• Shorinji Kempo
• Systema
• T'ai chi ch'uan
• Vajra-mushti
• Vale tudo
• Vovinam
• Xing Yi Quan
• Zen Bu Kan Kempo

Weapons
• Axe throwing
• Battōjutsu
• Boffer fighting
• Eskrima
• Egyptian stick fencing
• Fencing
• Gatka
• Hojōjutsu
• Iaidō
• Iaijutsu
• Jōdō
• Jogo do pau
• Jūkendō
• Jittejutsu
• Kendo
• Kenjutsu
• Krabi–krabong
• Kung fu
• Kyūdō
• Kyūjutsu
• Modern Arnis
• Naginatajutsu
• Nguni stick-fighting
• Okinawan kobudō
• Shurikenjutsu
• Silambam
• Sōjutsu
• Sword fighting
• Wushu
• Kumdo
• Wing Chun


Skirmish
• Airsoft
• Laser tag
• Paintball


Cue sports
• Carom billiards
• Three-cushion
• Five-pins
• Balkline and straight rail
• Cushion caroms
• Four-ball (yotsudama)
• Artistic billiards
• Novuss (and cued forms of carrom)
• Pocket billiards (pool)
• Eight-ball
• Blackball (a.k.a. British eight-ball pool)
• Nine-ball
• Straight pool (14.1 continuous)
• One-pocket
• Three-ball
• Seven-ball
• Ten-ball
• Rotation
• Baseball pocket billiards
• Cribbage (pool)
• Bank pool
• Artistic pool
• Trick shot competition
• Speed pool
• Bowlliards
• Chicago
• Kelly pool
• Cutthroat
• Killer
• Russian pyramid
• Snooker
• Sinuca brasileira
• Six-red snooker
• Snooker plus
• Hybrid carom–pocket games
• English billiards
• Bottle pool
• Cowboy
• Obstacle variations
• Bagatelle
• Bar billiards
• Bumper pool
• Table Sports
• Foosball


Equine sports
• Buzkashi
• Barrel racing
• Campdrafting
• Cirit
• Charreada
• Chilean rodeo
• Cross country
• Cutting
• Dressage
• Endurance riding
• English pleasure
• Equitation
• Eventing
• Equestrian vaulting
• Gymkhana
• Harness racing
• Horse racing
• Horseball
• Hunter
• Hunter-jumpers
• Jousting
• Pato
• Reining
• Rodeo
• Show jumping
• Steeplechase
• Team penning
• Tent pegging
• Western pleasure


Fishing
• Angling
• Big-game fishing
• Casting
• Noodling
• Spearfishing
• Sport fishing
• Surf fishing
• Rock fishing
• Fly fishing
• Ice fishing

Flying disc sports

• Beach ultimate
• Disc dog
• Disc golf
• Disc golf (urban)
• Dodge disc
• Double disc court
• Flutterguts
• Freestyle
• Freestyle competition
• Goaltimate
• Guts
• Hot box
• Ultimate

Football

• Ancient games
• Chinlone
• Cuju
• Episkyros
• Harpastum
• Kemari
• Ki-o-rahi
• Marn Grook
• Woggabaliri
• Yubi lakpi
• Medieval football
• Ba game
• Caid
• Calcio Fiorentino
• Camping (game)
• Chester-le-Street
• Cnapan
• Cornish hurling
• Haxey Hood
• Knattleikr
• La soule
• Lelo burti
• Mob football
• Royal Shrovetide Football
• Uppies and Downies
• Association football
• Jorkyball
• Paralympic football
• Powerchair Football
• Reduced variants
• Five-a-side football
• Beach soccer
• Futebol de Salão
• Futsal
• Papi fut
• Indoor soccer
• Masters Football
• Street football
• Freestyle football
• Keepie uppie
• Swamp football
• Three sided football
• Australian football
• Nine-a-side footy
• Rec footy
• Metro footy
• English school games
• Eton College
• Field game
• Wall game
• Harrow football
• Gaelic football
• Ladies' Gaelic football
• Gridiron football
• American football
• Eight-man football
• Flag football
• Indoor football
• Arena football
• Nine-man football
• Six-man football
• Sprint football
• Touch football
• Canadian football
• Street football (American)
• Rugby football
• Beach rugby
• Rugby league
• Masters Rugby League
• Mod league
• Rugby league nines
• Rugby league sevens
• Tag rugby
• Touch football
• Wheelchair rugby league
• Rugby union
• American flag rugby
• Mini rugby
• Rugby sevens
• Tag rugby
• Touch rugby
• Rugby tens
• Snow rugby
• Hybrid codes
• Austus
• Eton wall game
• International rules football
• Samoa rules
• Speedball
• Universal football
• Volata


Golf

• Miniature golf
• Match play
• Skins game
• Speed golf
• Stroke play
• Team play
• Shotgun start

Gymnastics

• Acrobatic gymnastics
• Aerobic gymnastics
• Artistic gymnastics
• Balance beam
• Floor
• High bar
• Parallel bars
• Pommel horse
• Still rings
• Uneven bars
• Vault
• Juggling
• Rhythmic gymnastics
• Ball
• Club
• Hoop
• Ribbon
• Rope
• Rope jumping
• Slacklining
• Trampolining
• Trapeze
• Flying trapeze
• Static trapeze
• Tumbling

Handball family
• Goalball
• Hitbal
• Tchoukball
• Team handball
• Beach handball
• Czech handball
• Field handball
• Torball
• Water polo

Hunting

• Beagling
• Big game hunting
• Deer hunting
• Fox hunting
• Hare coursing
• Wolf hunting

Ice sports
• Bandy
• Rink bandy
• Broomball
• Curling
• Ice hockey
• Ringette
• Ice yachting
• Figure skating


Kite sports
• Kite buggy
• Kite fighting
• Kite landboarding
• Kitesurfing
• Parasailing
• Snow kiting
• Sport kite (Stunt kite)

Mixed discipline
• Adventure racing
• Biathlon
• Duathlon
• Decathlon
• Heptathlon
• Icosathlon
• Modern pentathlon
• Pentathlon
• Tetrathlon
• Triathlon

Orienteering family
• Geocaching
• Orienteering
• Rogaining
• Letterboxing
• Waymarking

Pilota family
• American handball
• Australian handball
• Basque pelota
• Jai alai
• Fives
• Eton Fives
• Rugby Fives
• Frisian handball
• Four square
• Gaelic handball
• Jeu de paume
• Palla
• Patball
• Valencian pilota

Racquet (or racket) sports
• Badminton
• Ball badminton
• Basque pelota
• Frontenis
• Xare
• Beach tennis
• Fives
• Matkot
• Padel
• Paleta Frontón
• Pelota mixteca
• Pickleball
• Platform tennis
• Qianball
• Racketlon
• Racquetball
• Racquets
• Real tennis
• Soft tennis
• Speed-ball
• Speedminton
• Squash
• Hardball squash
• Squash tennis
• Stické
• Table tennis
• Tennis
Remote control
• Model aerobatics
• RC racing
• Robot combat
• Slot car racing

Rodeo-originated
• Bullriding
• Barrel Racing
• Bronc Riding
• Saddle Bronc Riding
• Roping
• Calf Roping
• Team Roping
• Steer Wrestling
• Goat Tying

Running
• Endurance
• 5K run
• 10K run
• Cross-country running
• Half marathon
• Marathon
• Road running
• Tower running
• Ultramarathon
• Sprint
• Hurdles

Sailing / Windsurfing
• Ice yachting
• Land sailing
• Land windsurfing
• Sailing
• Windsurfing
• Kiteboarding
• Dinghy sailing

Snow sports
• Alpine skiing
• Freestyle skiing
• Nordic combined
• Nordic skiing
• Cross-country skiing
• Telemark skiing
• Ski jumping
• Ski touring
• Skijoring
• Speed skiing

Sled sports

• Bobsleigh
• Luge
• Skibobbing
• Skeleton
• Toboggan

Shooting sports
• Clay pigeon shooting
• Skeet shooting
• Trap shooting
• Sporting clays
• Target shooting
• Field target
• Fullbore target rifle
• High power rifle
• Benchrest shooting
• Metallic silhouette
• Practical shooting
• Cowboy action shooting
• Metallic silhouette shooting
Stacking
• Card stacking
• Dice stacking
• Sport stacking

Stick and ball games
• Hornussen

Hockey
• Hockey
• Ball hockey
• Bando
• Bandy
• Rink bandy
• Broomball
• Moscow broomball
• Field hockey
• Indoor field hockey
• Floorball
• Ice hockey

Ice hockey 
 • Pond hockey
• Power hockey
• Ringette
• Sledge hockey
• Underwater ice hockey
• Roller hockey
• Inline hockey
• Roller hockey (Quad)
• Skater hockey
• Rossall Hockey
• Spongee
• Street hockey
• Underwater hockey
• Unicycle hockey

Hurling and shinty
• Cammag
• Hurling
• Camogie
• Shinty
• Composite rules shinty-hurling

Lacrosse
• Lacrosse
• Box lacrosse
• Field lacrosse
• Women's lacrosse
• Intercrosse


Polo
• Polo
 • Bicycle polo
• Canoe polo
• Cowboy polo
• Elephant polo
• Horse polo
• Segway polo
• Yak polo

Street sports
• Free running
• Freestyle footbag
• Freestyle football
• Powerbocking
• Parkour
• Scootering
• Street workout

Tag games

• British bulldogs (American Eagle)
• Capture the flag
• Hana Ichi Monme
• Hide and seek
• Jugger
• Kabaddi
• Kho kho
• Kick the can
• Oztag
• Red rover
• Tag

Walking
• Hiking
• Backpacking (wilderness)
• Racewalking
• Bushwhacking
• Walking

Wall-and-ball
• American handball
• Australian handball
• Basque pelota
• Butts Up
• Chinese handball
• Fives
• Gaelic handball
• International fronton
• Jorkyball
• Racquetball
• Squash
• Squash tennis
• Suicide (game)
• Valencian frontó
• Wallball
• Wallyball

Aquatic & paddle sports
• Creeking
• Flyak
• Freeboating
• Sea kayaking
• Squirt boating
• Surf kayaking
• Whitewater kayaking

Rafting
• Rafting
• White water rafting

Rowing
• Rowing (sport)
• Gig racing
• Coastal and ocean rowing
• Surfboat
• Single scull
Other paddling sports
• Dragon boat racing
• Stand up paddle boarding
• Water polo
• Canoe polo
• Waboba

Underwater
• Underwater football
• Underwater rugby
• Underwater hockey

Competitive swimming
• Backstroke
• Breaststroke
• Butterfly stroke
• Freestyle swimming
• Individual medley
• Synchronized swimming
• Medley relay

Kindred activities
• Bifins (finswimming)
• Surface finswimming

Subsurface and recreational
• Apnoea finswimming
• Aquathlon (underwater wrestling)
• Freediving
• Immersion finswimming
• Scuba diving
• Spearfishing
• Snorkelling
• Sport diving (sport)
• Underwater hockey
• Underwater orienteering
• Underwater photography (sport)
• Underwater target shooting
Diving
• Cliff diving
• Diving

Weightlifting
• Basque traditional weightlifting
• Bodybuilding
• Highland games
• Olympic weightlifting
• Powerlifting
• Strength athletics (strongman)
• Steinstossen

Motorized sports
• Autocross (a.k.a. Slalom)
• Autograss
• Banger racing
• Board track racing
• Demolition derby
• Desert racing
• Dirt track racing
• Drag racing
• Drifting
• Folkrace
• Formula racing
• Formula Libre
• Formula Student
• Hillclimbing
• Ice racing
• Kart racing
• Land speed records
• Legends car racing
• Midget car racing
• Monster truck
• Mud bogging
• Off-road racing
• Pickup truck racing
• Production car racing
• Race of Champions
• Rally raid
• Rallycross
• Rallying
• Regularity rally
• Road racing
• Short track motor racing
• Snowmobile racing
• Sports car racing
• Sprint car racing
• Street racing
• Stock car racing
• Time attack
• Tractor pulling
• Touring car racing
• Truck racing
• Vintage racing
• Wheelstand competition

Motorboat racing
• Drag boat racing
• F1 powerboat racing
• Hydroplane racing
• Jet sprint boat racing
• Offshore powerboat racing
• Personal water craft

Motorcycle racing
• Auto Race
• Board track racing
• Cross-country rally
• Endurance racing
• Enduro
• Freestyle motocross
• Grand Prix motorcycle racing
• Grasstrack
• Hillclimbing
• Ice racing
• Ice speedway
• Indoor enduro
• Motocross
• Motorcycle drag racing
• Motorcycle speedway
• Off-roading
• Rally raid
• Road racing
• Superbike racing
• Supercross
• Supermoto
• Supersport racing
• Superside
• Track racing
• Trial
• TT racing
• Free-style moto

Marker sports
• Airsoft
• Archery
• Paintball
• Darts

Musical sports
• Color guard
• Drum corps
• Indoor percussion
• Marching band

Fantasy sports
• Quidditch
• Hunger Games(Gladiating)
• Pod Racing
• Mortal Kombat(MMA)

Other
• Stihl Timbersports Series
• Woodsman

Overlapping sports
• Tennis
• Polocrosse
• Badminton
• Polo

Skating sports
• Aggressive inline skating
• Artistic roller skating
• Figure skating
• Freestyle slalom skating
• Ice dancing
• Ice skating
• Inline speed skating
• Rinkball
• Rink hockey
• Roller derby
• Roller skating
• Short track speed skating
• Skater hockey
• Speed skating
• Synchronized skating

Freestyle skiing
• Snowboarding
• Ski flying
• Skibob
• Snowshoeing
• Skiboarding