powered by CADENAS

Social Share

Amazon

Facial tissue (3564 views - Interior Design)

Facial tissue, paper handkerchief, and Kleenex refers to a class of soft, absorbent, disposable papers that are suitable for use on the face. They are disposable alternatives for cloth handkerchiefs. The terms are commonly used to refer to the type of paper tissue, usually sold in boxes, that is designed to facilitate the expulsion of nasal mucus from the nose (nose-blowing) although it may refer to other types of facial tissues including napkins and wipes. Facial tissue is often referred to as a "tissue", or (in the United States) by the generic trademark "Kleenex" which popularized the invention and its use.
Go to Article

Explanation by Hotspot Model

Youtube


    

Facial tissue

Facial tissue

Facial tissue

Facial tissue, paper handkerchief, and Kleenex refers to a class of soft, absorbent, disposable papers that are suitable for use on the face. They are disposable alternatives for cloth handkerchiefs. The terms are commonly used to refer to the type of paper tissue, usually sold in boxes, that is designed to facilitate the expulsion of nasal mucus from the nose (nose-blowing) although it may refer to other types of facial tissues including napkins and wipes.

Facial tissue is often referred to as a "tissue", or (in the United States) by the generic trademark "Kleenex" which popularized the invention and its use.

Manufacture

Facial tissue and paper handkerchiefs are made from the lowest basis weights tissue paper (14 18 g/m2). The surface is often made smoother by light calendering. These paper types consist usually of 2–3 plies. Because of high quality requirements the base tissue is normally made entirely from pure chemical pulp, but might contain added selected recycled fiber.[1] The tissue paper might be treated with softeners, lotions or added perfume to get the right properties or "feeling". The finished facial tissues or handkerchiefs are folded and put in pocket-size packages or a box dispenser.

History

The first unbleached bamboo facial tissues were invented by Alps Group Pte Ltd Singapore under the brand of Cloversoft. This invention was first retailed in Singapore and Asia in September 2014.

A few months on, Alps Group Pte Ltd came up with white bamboo tissues under Dr Blanc. Alps Group Pte Ltd is the first company to use bamboo to turn them into tissues. They have now created wet wipes using unbleached bamboo. All the wet wipes in the market are made from plastic.

Alps Group Pte Ltd has achieved another milestone now to have created the world's first bamboo facial tissues that are packaged in Kraft paper as opposed to the conventional plastic packaging. This is retailed in Singapore and Asia in September 2018.

Facial tissue has been used for centuries in Japan, in the form of washi (和紙) or Japanese tissue, as described in this 17th-century European account of the voyage of Hasekura Tsunenaga:

"They blow their noses in soft silky papers the size of a hand, which they never use twice, so that they throw them on the ground after usage, and they were delighted to see our people around them precipitate themselves to pick them up."[2]

In 1924, facial tissues as they are known today were first introduced by Kimberly-Clark as Kleenex. It was invented as a means to remove cold cream. Early advertisements linked Kleenex to Hollywood makeup departments and sometimes included endorsements from movie stars (Helen Hayes and Jean Harlow) who used Kleenex to remove their theatrical makeup with cold cream. It was the customers that started to use Kleenex as a disposable handkerchief, and a reader review in 1926 by a newspaper in Peoria, Illinois found that 60% of the users used it for blowing their nose. The other 40% used it for various reasons, including napkins and toilet paper.[3]

Kimberly-Clark also introduced pop-up, colored, printed, pocket, and 3-ply facial tissues.[4]

Brands

See also



This article uses material from the Wikipedia article "Facial tissue", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art