powered by CADENAS

Social Share

Amazon

Graphics tablet (6355 views - Consumer products)

A graphic tablet (also known as a digitizer, drawing tablet, drawing pad, digital drawing tablet, pen tablet, or digital art board) is a computer input device that enables a user to hand-draw images, animations and graphics, with a special pen-like stylus, similar to the way a person draws images with a pencil and paper. These tablets may also be used to capture data or handwritten signatures. It can also be used to trace an image from a piece of paper which is taped or otherwise secured to the tablet surface. Capturing data in this way, by tracing or entering the corners of linear poly-lines or shapes, is called digitizing.The device consists of a flat surface upon which the user may "draw" or trace an image using the attached stylus, a pen-like drawing apparatus. The image is displayed on the computer monitor, though some graphic tablets now also incorporate an LCD screen for a more realistic or natural experience and usability. Some tablets are intended as a replacement for the computer mouse as the primary pointing and navigation device for desktop computers.
Go to Article

Explanation by Hotspot Model

Youtube


    

Graphics tablet

Graphics tablet

A graphic tablet (also known as a digitizer, drawing tablet, drawing pad, digital drawing tablet, pen tablet, or digital art board) is a computer input device that enables a user to hand-draw images, animations and graphics, with a special pen-like stylus, similar to the way a person draws images with a pencil and paper. These tablets may also be used to capture data or handwritten signatures. It can also be used to trace an image from a piece of paper which is taped or otherwise secured to the tablet surface. Capturing data in this way, by tracing or entering the corners of linear poly-lines or shapes, is called digitizing.[1]

The device consists of a flat surface upon which the user may "draw" or trace an image using the attached stylus, a pen-like drawing apparatus. The image is displayed on the computer monitor, though some graphic tablets now also incorporate an LCD screen for a more realistic or natural experience and usability.

Some tablets are intended as a replacement for the computer mouse as the primary pointing and navigation device for desktop computers.

History

The first electronic handwriting device was the Telautograph, patented by Elisha Gray in 1888.[2]

The first graphic tablet resembling contemporary tablets and used for handwriting recognition by a computer was the Stylator in 1957.[3] Better known (and often misstated as the first digitizer tablet) is the RAND Tablet[4] also known as the Grafacon[5] (for Graphic Converter), introduced in 1964. The RAND Tablet employed a grid of wires under the surface of the pad that encoded horizontal and vertical coordinates in a small magnetic signal. The stylus would receive the magnetic signal, which could then be decoded back as coordinate information.

The acoustic tablet, or spark tablet, used a stylus that generated clicks with a spark plug. The clicks were then triangulated by a series of microphones to locate the pen in space.[6] The system was fairly complex and expensive, and the sensors were susceptible to interference by external noise.

Digitizers were popularized in the mid-1970s and early 1980s by the commercial success of the ID (Intelligent Digitizer) and BitPad manufactured by the Summagraphics Corp.[7] The Summagraphics digitizers were sold under the company's name but were also private labeled for HP, Textronix, Evans and Sutherland and several other graphic system manufacturers. The ID model was the first graphics tablet to make use of what was at the time, the new Intel microprocessor technology. This embedded processing power allowed the ID models to have twice the accuracy of previous models while still making use of the same foundation technology. Key to this accuracy improvement were two US Patents issued to Stephen Domyan, Robert Davis, and Edward Snyder. The Bit Pad model was the first attempt at a low cost graphics tablet with an initial selling price of $555 when other graphics tablets were selling in the $2,000 to $3,000 price range. This lower cost opened up the opportunities for would be entrepreneurs to be able to write graphics software for a multitude of new applications. These digitizers were used as the input device for many high-end CAD (Computer Aided Design) systems as well as bundled with PCs and PC-based CAD software like AutoCAD.

Summagraphics also made an OEM version of its BitPad which was sold by Apple Computer as the Apple Graphic Tablet accessory to their Apple II. These tablets used a magnetostriction technology which used wires made of a special alloy stretched over a solid substrate to accurately locate the tip of a stylus or the center of a digitizer cursor on the surface of the tablet. This technology also allowed Proximity or "Z" axis measurement.[8]

The first home computer graphic tablet was the KoalaPad. Though originally designed for the Apple II, the Koala eventually broadened its applicability to practically all home computers with graphic support, examples of which include the TRS-80 Color Computer, Commodore 64, and Atari 8-bit family. Competing tablets were eventually produced; the tablets produced by Atari were generally considered to be of high quality.[9]

In 1981, musician Todd Rundgren created the first color graphic tablet software for personal computers, which was licensed to Apple as the Utopia Graphic Tablet System.[10]

In the 1980s, several vendors of graphic tablets began to include additional functions, such as handwriting recognition and on-tablet menus.[11][12]

Characteristics

Typically tablets are characterized by size of the device, drawing area, its resolution size («active area», which is measured in lpi), number of buttons and types and number of interfaces: bluetooth, usb; etc.[13] The actual drawing accuracy is restricted to pen's nib size.[14]

Types

There have been many attempts to categorize the technologies that have been used for graphic tablets:

Passive tablets
Passive tablets,[15] most notably those manufactured by Wacom and Parblo, for example, make use of electromagnetic induction technology, where the horizontal and vertical wires of the tablet operate as both transmitting and receiving coils (as opposed to the wires of the RAND Tablet which only transmit). The tablet generates an electromagnetic signal, which is received by the LC circuit in the stylus. The wires in the tablet then change to a receiving mode and read the signal generated by the stylus. Modern arrangements also provide pressure sensitivity and one or more buttons, with the electronics for this information present in the stylus. On older tablets, changing the pressure on the stylus nib or pressing a button changed the properties of the LC circuit, affecting the signal generated by the pen, which modern ones often encode into the signal as a digital data stream. By using electromagnetic signals, the tablet is able to sense the stylus position without the stylus having to even touch the surface, and powering the pen with this signal means that devices used with the tablet never need batteries. Activslate 50, the model used with Promethean white boards, also uses a hybrid of this technology.[16]
Active tablets
Active tablets differ in that the stylus used contains self-powered electronics that generate and transmit a signal to the tablet. These styluses rely on an internal battery rather than the tablet for their power, resulting in a bulkier stylus. Eliminating the need to power the pen means that such tablets may listen for pen signals constantly, as they do not have to alternate between transmit and receive modes, which can result in less jitter.
Optical tablets
Optical tablets operate by a very small digital camera in the stylus and then doing pattern matching on the image of the paper. The most successful[citation needed] example is the technology developed by Anoto.
Acoustic tablets
Early models were described as spark tablets—a small sound generator was mounted in the stylus, and the acoustic signal picked up by two microphones placed near the writing surface. Some modern designs are able to read positions in three dimensions.[17][18]
Capacitive tablets
These tablets have also been designed to use an electrostatic or capacitive signal. Scriptel's designs are one example of a high-performance tablet detecting an electrostatic signal. Unlike the type of capacitive design used for touchscreens, the Scriptel design is able to detect the position of the pen while it is in proximity to or hovering above the tablet. Many multi-touch tablets use capacitive sensing.[19][20]

For all these technologies, the tablet can use the received signal to also determine the distance of the stylus from the surface of the tablet, the tilt (angle from vertical) of the stylus, and other information in addition to the horizontal and vertical positions, such as clicking buttons of the stylus or the rotation of the stylus.

Compared to touchscreens, a graphic tablet generally offers much higher precision, the ability to track an object which is not touching the tablet, and can gather much more information about the stylus, but is typically more expensive, and can only be used with the special stylus or other accessories.

Some tablets, especially inexpensive ones aimed at young children, come with a corded stylus, using technology similar to older RAND tablets.

Pucks

After styluses, pucks are the most commonly used tablet accessory. A puck is a mouse-like device that can detect its absolute position and rotation. This is opposed to a mouse pointing device, which can only sense its relative velocity on a surface (most tablet drivers are capable of allowing a puck to emulate a mouse in operation, and many pucks are marketed as a "mouse"). Pucks range in size and shape; some are externally indistinguishable from a mouse, while others are a fairly large device with dozens of buttons and controls. Professional pucks often have a reticle or loupe which allows the user to see the exact point on the tablet's surface targeted by the puck, for detailed tracing and computer aided design (CAD) work.

Embedded LCD tablets

Some graphics tablets incorporate an LCD into the tablet itself, allowing the user to draw directly on the display surface.

Graphic tablet/screen hybrids offer advantages over both standard PC touchscreens and ordinary graphic tablets. Unlike touchscreens, they offer pressure sensitivity, and their input resolution is generally higher.[citation needed] While their pressure sensitivity and resolution are typically no better than those of ordinary tablets, they offer the additional advantage of directly seeing the location of the physical pen device relatively to the image on the screen. This often allows for increased accuracy and a more tactile, "real" feeling to the use of the device.

The graphic tablet manufacturer Wacom holds many intellectual property patents on key technologies for graphic tablets,[21] which forces competitors to use other technologies or license Wacom's patents. The displays are often sold for thousands of dollars. For instance, the Wacom Cintiq series ranges from just below US$1,000 to over US$2,000.

Some commercially available graphic tablet-screen hybrids include:

There have also been do-it-yourself projects where conventional used LCD monitors and graphics tablets have been converted to a graphics tablet-screen hybrid.[22][23]

Uses

Graphic tablets, because of their stylus-based interface and ability to detect some or all of pressure, tilt, and other attributes of the stylus and its interaction with the tablet, are widely considered to offer a very natural way to create computer graphics, especially two-dimensional computer graphics. Indeed, many graphic packages can make use of the pressure (and, sometimes, stylus tilt or rotation) information generated by a tablet, by modifying the brush size, shape, opacity, color, or other attributes based on data received from the graphic tablet.

In East Asia, graphic tablets, known as "pen tablets", are widely used in conjunction with input-method editor software (IMEs) to write Chinese, Japanese, and Korean characters (CJK). The technology is popular and inexpensive and offers a method for interacting with the computer in a more natural way than typing on the keyboard, with the pen tablet supplanting the role of the computer mouse. Uptake of handwriting recognition among users who use alphabetic scripts has been slower.

Graphic tablets are commonly used in the artistic world. Using a pen-like stylus on a graphic tablet combined with a graphics-editing program, such as Illustrator or Photoshop by Adobe Systems, or CorelDraw, gives artists a lot of precision when creating digital drawings or artwork. Photographers can also find working with a graphic tablet during their post processing can really speed up tasks like creating a detailed layer mask or dodging and burning.

Educators make use of tablets in classrooms to project handwritten notes or lessons and to allow students to do the same, as well as providing feedback on student work submitted electronically. Online teachers may also use a tablet for marking student work, or for live tutorials or lessons, especially where complex visual information or mathematical equations are required. Students are also increasingly using them as note-taking devices, especially during university lectures while following along with the lecturer.

Tablets are also popular for technical drawings and CAD, as one can typically put a piece of paper on them without interfering with their function.

Finally, tablets are gaining popularity as a replacement for the computer mouse as a pointing device.[when?] They can feel more intuitive to some users than a mouse, as the position of a pen on a tablet typically corresponds to the location of the pointer on the GUI shown on the computer screen. Those artists using a pen for graphic work will as a matter of convenience use a tablet and pen for standard computer operations rather than put down the pen and find a mouse.

Graphic tablets are available in various sizes and price ranges; A6-sized tablets being relatively inexpensive and A3-sized tablets far more expensive. Modern tablets usually connect to the computer via a USB or HDMI interface.

Manufacturers

Similar devices

Interactive whiteboards offer high-resolution wall size graphic tablets up to 95" along with options for pressure and multiple input. These are becoming commonplace in schools and meeting rooms around the world.[27]

Touch screens like those found on some tablet computers, iPads, and the Nintendo DS are operated in similar ways, but they usually use either optical grids or a pressure-sensitive film instead, and therefore they do not need a special pointing device.

A graphic tablet is also used for Audio-Haptic products where blind or visually impaired people touch swelled graphics on a graphic tablet and get audio feedback from that.[28] The product that is using this technology is called Tactile Talking Tablet or T3.

See also



This article uses material from the Wikipedia article "Graphics tablet", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library