In 3D computer graphics, Polygonal modeling is an approach for modeling objects by representing or approximating their surfaces using polygons. Polygonal modeling is well suited to scanline rendering and is therefore the method of choice for real-time computer graphics. Alternate methods of representing 3D objects include NURBS surfaces, subdivision surfaces, and equation-based representations used in ray tracers. See polygon mesh for a description of how polygonal models are represented and stored.
The basic object used in mesh modeling is a vertex, a point in three-dimensional space. Two vertices connected by a straight line become an edge. Three vertices, connected to each other by three edges, define a triangle, which is the simplest polygon in Euclidean space. More complex polygons can be created out of multiple triangles, or as a single object with more than 3 vertices. Four sided polygons (generally referred to as quads)[1][2] and triangles are the most common shapes used in polygonal modeling. A group of polygons, connected to each other by shared vertices, is generally referred to as an element. Each of the polygons making up an element is called a face.
In Euclidean geometry, any three non-collinear points determine a plane. For this reason, triangles always inhabit a single plane. This is not necessarily true of more complex polygons, however. The flat nature of triangles makes it simple to determine their surface normal, a three-dimensional vector perpendicular to the triangle's surface. Surface normals are useful for determining light transport in ray tracing, and are a key component of the popular Phong shading model. Some rendering systems use vertex normals instead of face normals to create a better-looking lighting system at the cost of more processing. Note that every triangle has two face normals, which point to opposite directions from each other. In many systems only one of these normals is considered valid – the other side of the polygon is referred to as a backface, and can be made visible or invisible depending on the programmer’s desires.
Many modeling programs do not strictly enforce geometric theory; for example, it is possible for two vertices to have two distinct edges connecting them, occupying exactly the same spatial location. It is also possible for two vertices to exist at the same spatial coordinates, or two faces to exist at the same location. Situations such as these are usually not desired and many packages support an auto-cleanup function. If auto-cleanup is not present, however, they must be deleted manually.
A group of polygons which are connected by shared vertices is referred to as a mesh. In order for a mesh to appear attractive when rendered, it is desirable that it be non-self-intersecting, meaning that no edge passes through a polygon. Another way of looking at this is that the mesh cannot pierce itself. It is also desirable that the mesh not contain any errors such as doubled vertices, edges, or faces. For some purposes it is important that the mesh be a manifold – that is, that it does not contain holes or singularities (locations where two distinct sections of the mesh are connected by a single vertex).
Although it is possible to construct a mesh by manually specifying vertices and faces, it is much more common to build meshes using a variety of tools. A wide variety of 3D graphics software packages are available for use in constructing polygon meshes.
One of the more popular methods of constructing meshes is box modeling, which uses two simple tools:
A second common modeling method is sometimes referred to as inflation modeling or extrusion modeling. In this method, the user creates a 2D shape which traces the outline of an object from a photograph or a drawing. The user then uses a second image of the subject from a different angle and extrudes the 2D shape into 3D, again following the shape’s outline. This method is especially common for creating faces and heads. In general, the artist will model half of the head and then duplicate the vertices, invert their location relative to some plane, and connect the two pieces together. This ensures that the model will be symmetrical.
Another common method of creating a polygonal mesh is by connecting together various primitives, which are predefined polygonal meshes created by the modeling environment. Common primitives include:
Finally, some specialized methods of constructing high or low detail meshes exist. Sketch based modeling is a user-friendly interface for constructing low-detail models quickly, while 3D scanners can be used to create high detail meshes based on existing real-world objects in almost automatic way. These devices are very expensive, and are generally only used by researchers and industry professionals but can generate high accuracy sub-millimetric digital representations.
There is a very large number of operations which may be performed on polygonal meshes. Some of these roughly correspond to real-world manipulations of 3D objects, while others do not.
Polygonal mesh operations:
Creations - Create new geometry from some other mathematical object
Loft - generate a mesh by creating a shape along two or more profile curves
Extrude - creates a surface by sweeping a profile curve or polygon surface along a straight or linear line
Revolve - generate a mesh by revolving (rotating) a shape around an axis
Marching cubes - algorithm to construct a mesh from an implicit function
Binary Creations - Create a new mesh from a binary operation of two other meshes
Add - boolean addition of two or more meshes
Subtract - boolean subtraction of two or more meshes
Intersect - boolean intersection
Union - boolean union of two or more meshes
Attach - attach one mesh to another (removing the interior surfaces)
Chamfer - create a beveled surface which smoothly connects two surfaces
Deformations - Move only the vertices of a mesh
Deform - systematically move vertices (according to certain functions or rules)
Weighted Deform - move vertices based on localized weights per vertex
Morph - move vertices smoothly between a source and target mesh
Bend - move vertices to "bend" the object
Twist - move vertices to "twist" the object
Manipulations - Modify the geometry of the mesh, but not necessarily topology
Displace - introduce additional geometry based on a "displacement map" from the surface
Simplify - systematically remove and average vertices
Subdivide - smooth a course mesh by subdividing the mesh (Catmull-Clark, etc.)
Convex Hull - generate another mesh which minimally encloses a given mesh (think shrink-wrap)
Cut - create a hole in a mesh surface
Stitch - close a hole in a mesh surface
Measurements - Compute some value of the mesh
Volume - compute the 3D volume of a mesh (discrete volumetric integral)
Surface Area - compute the surface area of a mesh (discrete surface integral)
Collision Detection - determine if two complex meshes in motion have collided
Fitting - construct a parametric surface (NURBS, bicubic spline) by fitting it to a given mesh
Point-Surface Distance - compute distance from a point to the mesh
Line-Surface Distance - compute distance from a line to the mesh
Line-Surface Intersection - compute intersection of line and the mesh
Cross Section - compute the curves created by a cross-section of a plane through a mesh
Centroid - compute the centroid, geometric center, of the mesh
Center-of-Mass - compute the center of mass, balance point, of the mesh
Circumcenter - compute the center of a circle or sphere enclosing an element of the mesh
Incenter - compute the center of a circle or sphere enclosed by an element of the mesh
Once a polygonal mesh has been constructed, further steps must be taken before it is useful for games, animation, etc. The model must be texture mapped to add colors and texture to the surface and it must be given a skeleton for animation. Meshes can also be assigned weights and centers of gravity for use in physical simulation.
To display a model on a computer screen outside of the modeling environment, it is necessary to store that model in one of the file formats listed below, and then use or write a program capable of loading from that format. The two main methods of displaying 3D polygon models are OpenGL and Direct3D. Both of these methods can be used with or without a 3D accelerated graphics card.
There are many disadvantages to representing an object using polygons. Polygons are incapable of accurately representing curved surfaces, so a large number of them must be used to approximate curves in a visually appealing manner. The use of complex models has a cost in lowered speed. In scanline conversion, each polygon must be converted and displayed, regardless of size, and there are frequently a large number of models on the screen at any given time. Often, programmers must use multiple models at varying levels of detail to represent the same object in order to cut down on the number of polygons being rendered.
The main advantage of polygons is that they are faster than other representations. While a modern graphics card can show a highly detailed scene at a frame rate of 60 frames per second or higher, surface modelers, the main way of displaying non-polygonal models, are incapable of achieving an interactive frame rate (10 frame/s or higher) with a similar amount of detail. With sprites, another alternative to polygons, every required pose must be created individually, while a single polygonal model can perform any movement if the appropriate motion data is applied, and can be viewed from any angle.[3]
A variety of formats are available for storing 3D polygon data. The most popular are:
This article uses material from the Wikipedia article "Polygonal modeling", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,file,format,converter,import,export,translate,material,3dprinting,rendering,threejs,webgl,opengl,.ply,.stl,.obj,.mtl