Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Unkown).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2010) (Learn how and when to remove this template message) |
A utility knife is a knife used for general or utility purposes.[1] The utility knife was originally a fixed blade knife with a cutting edge suitable for general work such as cutting hides and cordage, scraping hides, butchering animals, cleaning fish, and other tasks. Craft knives are tools mostly used for crafts. Today, the term "utility knife" also includes small folding or retractable-blade knives suited for use in the general workplace or in the construction industry.
There is also a utility knife for kitchen use, which is between a chef's knife and paring knife in size.
The fixed-blade utility knife was developed some 500,000 years ago, when human ancestors began to make knives made of stone.[1] These knives were general-purpose tools, designed for cutting and shaping wooden implements, scraping hides, preparing food, and for other utilitarian purposes.[1]
By the 19th century the fixed-blade utility knife had evolved into a steel-bladed outdoors field knife capable of butchering game, cutting wood, and preparing campfires and meals. With the invention of the backspring, pocket-size utility knives were introduced[when?] with folding blades and other folding tools designed to increase the utility of the overall design. The folding pocketknife and utility tool is typified by the Camper or Boy Scout pocketknife, the U.S. folding utility knife, the Swiss Army Knife, and by multi-tools fitted with knife blades. The development of stronger locking blade mechanisms for folding knives—as with the Spanish navaja, the Opinel, and the Buck 110 Folding Hunter[citation needed]—significantly increased the utility of such knives when employed for heavy-duty tasks such as preparing game or cutting through dense or tough materials.
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (July 2012) (Learn how and when to remove this template message) |
The fixed or folding blade utility knife is popular for both indoor and outdoor use. One of the most popular types of workplace utility knife is the retractable or folding utility knife (also known as a Stanley knife, box cutter, X-Acto knife, or by various other names). These types of utility knives are designed as multi-purpose cutting tools for use in a variety of trades and crafts. Designed to be lightweight and easy to carry and use, utility knives are commonly used in factories, warehouses, construction projects, and other situations where a tool is routinely needed to mark cut lines, trim plastic or wood materials, or to cut tape, cord, strapping, cardboard, or other packaging material.
In British, Australian and New Zealand English, along with Dutch and Austrian German, a utility knife frequently used in the construction industry is known as a Stanley knife.[2] This name is a genericised trademark named after Stanley Works, a manufacturer of such knives. In Israel and Switzerland, these knives are known as Japanese knives. In Brazil they are known as estiletes or cortadores Olfa (the latter, being another genericised trademark).[citation needed] In Portugal and Canada they are also known as X-Acto (yet another genericised trademark). In India, the Philippines, France, Iraq, Italy, Egypt, and Germany, they are simply called cutter.[citation needed] In the Flemish region of Belgium it is called cuttermes(je) (cutter knife).[citation needed] In general Spanish, they are known as cortaplumas (penknife, when it comes to folding blades);[citation needed] in Spain, Mexico, and Costa Rica, they are colloquially known as cutters; in Argentina and Uruguay the segmented fixed-blade knives are known as "Trinchetas".[citation needed] In Turkey, they are known as maket bıçağı (which literally translates as model knife).[3]
Other names for the tool are box cutter or boxcutter, razor blade knife, razor knife, carpet knife, pen knife, stationery knife, sheetrock knife, or drywall knife.
Utility knives may use fixed, folding, or retractable or replaceable blades, and come in a wide variety of lengths and styles suited to the particular set of tasks they are designed to perform. Thus, an outdoors utility knife suited for camping or hunting might use a broad 75 to 130 millimetres (3–5 in) fixed blade, while a utility knife designed for the construction industry might feature a replaceable utility or razor blade for cutting packaging, cutting shingles, marking cut lines, or scraping paint.
Large fixed-blade utility knives are most often employed in an outdoors context, such as fishing, camping, or hunting. Outdoor utility knives typically feature sturdy blades from 100 to 150 millimetres (4–6 in) in length, with edge geometry designed to resist chipping and breakage.
The term "utility knife" may also refer to small fixed-blade knives used for crafts, model-making and other artisanal projects. These small knives feature light-duty blades best suited for cutting thin, lightweight materials. The small, thin blade and specialized handle permit cuts requiring a high degree of precision and control.
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (July 2012) (Learn how and when to remove this template message) |
The largest construction or workplace utility knives typically feature retractable and replaceable blades, made of either die-cast metal or molded plastic. Some use standard razor blades, others specialized double-ended utility blades. The user can adjust how far the blade extends from the handle, so that, for example, the knife can be used to cut the tape sealing a package without damaging the contents of the package. When the blade becomes dull, it can be quickly reversed or switched for a new one. Spare or used blades are stored in the hollow handle of some models, and can be accessed by removing a screw and opening the handle. Other models feature a quick-change mechanism that allows replacing the blade without tools, as well as a flip-out blade storage tray. The blades for this type of utility knife come in both double- and single-ended versions, and are interchangeable with many, but not all, of the later copies. Specialized blades also exist for cutting string, linoleum, and other materials.
Another style is a snap-off utility knife that contains a long, segmented blade that slides out from it. As the endmost edge becomes dull, it can be broken off the remaining blade, exposing the next section, which is sharp and ready for use. The snapping is best accomplished with a blade snapper that is often built-in, or a pair of pliers, and the break occurs at the score lines, where the metal is thinnest. When all of the individual segments are used, the knife may be thrown away, or, more often, refilled with a replacement blade. This design was introduced by Japanese manufacturer Olfa Corporation in 1956 as the world's first snap-off blade and was inspired from analyzing the sharp cutting edge produced when glass is broken and how pieces of a chocolate bar break into segments.
Another utility knife often used for cutting open boxes consists of a simple sleeve around a rectangular handle into which single-edge utility blades can be inserted. The sleeve slides up and down on the handle, holding the blade in place during use and covering the blade when not in use. The blade holder may either retract or fold into the handle, much like a folding-blade pocketknife. The blade holder is designed to expose just enough edge to cut through one layer of corrugated fiberboard, to minimize chances of damaging contents of cardboard boxes.
Most utility knives are not well suited to use as offensive weapons, with the exception of some outdoor-type utility knives employing longer blades. However, even small razor-blade type utility knives may sometimes find use as slashing weapons. The 9-11 commission report stated passengers in cell phone calls reported knives or "box-cutters" were used as weapons, (also Mace or a bomb), in hi-jacking airplanes in the September 11, 2001 terrorist attacks against the United States, though the exact design of the knives used is unknown.[4][5] Two of the hijackers were known to have purchased Leatherman knives, which feature a 4" locking blade which were not prohibited on U.S. flights at the time. Those knives were not found in the possessions the two hijackers left behind.[6] Similar cutters, including paper cutters, have also been known to be used as a lethal weapon.[7]
Small work-type utility knives have also been used to commit robbery and other crimes. In June 2004, a Japanese student was slashed to death with a segmented-type utility knife.
In the United Kingdom, the law was changed[when?] to raise the age limit for purchasing knives, including utility knives, from 16 to 18.[8]
This article uses material from the Wikipedia article "Utility knife", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted