powered by CADENAS

Social Share

Amazon

Hipot (2593 views - Electrical Engineering)

Hipot is an abbreviation for high potential. Traditionally, hipot is a term given to a class of electrical safety testing instruments used to verify electrical insulation in finished appliances, cables or other wired assemblies, printed circuit boards, electric motors, and transformers. Under normal conditions, any electrical device will produce a minimal amount of leakage current due to the voltages and internal capacitance present within the product. Yet due to design flaws or other factors, the insulation in a product can break down, resulting in excessive leakage current flow. This failure condition can cause shock or death to anyone that comes into contact with the faulty product. A hipot test (also called Dielectric Withstanding Voltage (DWV) test) verifies that the insulation of a product or component is sufficient to protect the operator from electrical shock. In a typical hipot test, high voltage is applied between a product's current-carrying conductors and its metallic shielding. The resulting current that flows through the insulation, known as leakage current, is monitored by the hipot tester. The theory behind the test is that if a deliberate over-application of test voltage does not cause the insulation to break down, the product will be safe to use under normal operating conditions—hence the name, Dielectric Withstanding Voltage test. In addition to over-stressing the insulation, the test can also be performed to detect material and workmanship defects, most importantly small gap spacings between current-carrying conductors and earth ground. When a product is operated under normal conditions, environmental factors such as humidity, dirt, vibration, shock and contaminants can close these small gaps and allow current to flow. This condition can create a shock hazard if the defects are not corrected at the factory. No other test can uncover this type of defect as well as the Dielectric Withstand test. Three types of hipot tests are commonly used. These three tests differ in the amount of voltage applied and the amount (or nature) of acceptable current flow: Dielectric Breakdown Test. The test voltage is increased until the dielectric fails, or breaks down, allowing too much current to flow. The dielectric is often destroyed by this test so this test is used on a random sample basis. This test allows designers to estimate the breakdown voltage of a product's design and to see where the breakdown occurred. Dielectric Withstand Test. A standard test voltage is applied (below the established Breakdown Voltage) and the resulting leakage current is monitored. The leakage current must be below a preset limit or the test is considered to have failed. This test is non-destructive providing that it does not fail and is usually required by safety agencies to be performed as a 100% production line test on all products before they leave the factory. Insulation Resistance Test. This test is used to provide a quantifiable resistance value for all of a product's insulation. The test voltage is applied in the same fashion as a standard hipot test, but is specified to be Direct Current (DC). The voltage and measured current value are used to calculate the resistance of the insulation.
Go to Article

Explanation by Hotspot Model

Hipot

Hipot

Hipot is an abbreviation for high potential. Traditionally, hipot is a term given to a class of electrical safety testing instruments used to verify electrical insulation in finished appliances, cables or other wired assemblies, printed circuit boards, electric motors, and transformers.

Under normal conditions, any electrical device will produce a minimal amount of leakage current due to the voltages and internal capacitance present within the product. Yet due to design flaws or other factors, the insulation in a product can break down, resulting in excessive leakage current flow. This failure condition can cause shock or death to anyone that comes into contact with the faulty product.

A hipot test (also called Dielectric Withstanding Voltage (DWV) test) verifies that the insulation of a product or component is sufficient to protect the operator from electrical shock. In a typical hipot test, high voltage is applied between a product's current-carrying conductors and its metallic shielding. The resulting current that flows through the insulation, known as leakage current, is monitored by the hipot tester. The theory behind the test is that if a deliberate over-application of test voltage does not cause the insulation to break down, the product will be safe to use under normal operating conditions—hence the name, Dielectric Withstanding Voltage test.

In addition to over-stressing the insulation, the test can also be performed to detect material and workmanship defects, most importantly small gap spacings between current-carrying conductors and earth ground. When a product is operated under normal conditions, environmental factors such as humidity, dirt, vibration, shock and contaminants can close these small gaps and allow current to flow. This condition can create a shock hazard if the defects are not corrected at the factory. No other test can uncover this type of defect as well as the Dielectric Withstand test.

Three types of hipot tests are commonly used. These three tests differ in the amount of voltage applied and the amount (or nature) of acceptable current flow:

Dielectric Breakdown Test. The test voltage is increased until the dielectric fails, or breaks down, allowing too much current to flow. The dielectric is often destroyed by this test so this test is used on a random sample basis. This test allows designers to estimate the breakdown voltage of a product's design and to see where the breakdown occurred.

Dielectric Withstand Test. A standard test voltage is applied (below the established Breakdown Voltage) and the resulting leakage current is monitored. The leakage current must be below a preset limit or the test is considered to have failed. This test is non-destructive providing that it does not fail and is usually required by safety agencies to be performed as a 100% production line test on all products before they leave the factory.

Insulation Resistance Test. This test is used to provide a quantifiable resistance value for all of a product's insulation. The test voltage is applied in the same fashion as a standard hipot test, but is specified to be Direct Current (DC). The voltage and measured current value are used to calculate the resistance of the insulation.

Hipot tester

A hipot tester is an electronic device used to verify the electrical insulation in a device or other wired assembly that could subject someone to a shock if it failed. It generally consists of:

  1. A source of high voltage,
  2. A current meter,
  3. A switching matrix used to connect the high voltage source and the current meter to all of the contact points in a cable.

Hipot testers may also have a microcontroller and a display to automate the testing process and display the testing results.

A hipot tester can be very similar to a cable tester and often the two are combined into a single device.

In a typical wired assembly a hipot test should connect all circuits in common to ground. Then, one by one the tester will disconnect a given circuit from ground and connect that circuit to high voltage . The current that flows is monitored to verify that it is low enough.

External links



This article uses material from the Wikipedia article "Hipot", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced