Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 4.0 (Alex1380).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (April 2011) (Learn how and when to remove this template message) |
Cable carriers, also known as drag chains, energy chains, or cable chains depending on the manufacturer, are guides designed to surround and guide flexible electrical cables and hydraulic or pneumatic hoses connected to moving automated machinery. They reduce wear and stress on cables and hoses, prevent entanglement, and improve operator safety.
Cable carriers may be arranged to accommodate horizontal, vertical, rotary and three-dimensional movements.
Steel carriers were introduced to the market for the first time in the 1950s. Their inventor Dr Gilbert Waninger and Dr Waldrich, the owner of the Kabelschlepp, recognized the great potential of these chains at an early stage.
Until then flexibles such as cables and hydraulic hoses had simply been allowed to hang loose from machines, resulting in damage and rapid wear.[1] Nowadays, plastic (specifically, polypropylene or PP) cable carriers are also widely used.
As of 2007 there were more than seven manufacturers worldwide, including igus, Brevetti Stendalto, EKD Gelenkrohr, FESMA, Murrplastik, Tsubaki Kabelschlepp, CPSYSTEM, Metreel, M Buttkereit, Gortrac and Cavotec.
Most carriers have a rectangular cross section, inside which the cables lie. Cross bars along the length of the carrier can be opened from the outside, so that cables can be easily inserted and plugs connected. Internal separators in the carrier separate the cables. Cables can also be held in place with an integrated strain relief. Mounting brackets fix the ends of the carrier to the machine.
Besides only bending in one plane due to the rigid jointed structure, cable carriers also often only permit bending in one direction. In combination with rigid mounting of the ends of the carrier, this can entirely prevent the enclosed cables from flopping in undesired directions and becoming tangled or crushed.
Today cable carriers are available in many different styles, sizes, prices and performance ranges. Some of the following variants are:
Cable carriers are often used with special highly flexible cables to extend the cables' service life.
Cable carriers are used anywhere where there is moving automation involving the transferral of energy, data, liquids or gases. Examples include machine tools, cranes, car washes, medical and laboratory equipment, automatic warehousing, forklifts, industrial robots, offshore oil rigs and stage technology.
http://www.thefabricator.com/article/default/the-evolution-of-cable-carriers
This article uses material from the Wikipedia article "Cable carrier", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD