This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2007) (Learn how and when to remove this template message) |
Tie down straps (also called ratchet straps, lashing straps or tie downs) are fasteners used to hold down cargo or equipment during transport. Tie down straps are essentially webbing that is outfitted with tie down hardware. This hardware allows the tie down strap to attach to the area surrounding the cargo or equipment, loop over the cargo or equipment, and/or attach to the cargo or equipment. It usually also includes a method of tensioning the strap, such as a ratchet.
Two common types of tie down straps are loop straps and two-piece straps.
Loop straps, like their name implies, are a single piece of webbing that is looped around the item to be protected and the two endpoints are brought together at the tie down fastener for fastening and providing tension.
Two-piece tie down straps is a single assembly that is constructed out of two separate pieces of webbing each with their own hardware that is fastened at one end to the area surrounding the equipment to be protected and connected to each other, typically at the fastener.
Tie Down webbing is available in single ply and double ply strengths and is used to make 1,2,3, and 4 inches Tie Down Straps. [1]
Webbing with linking device is a product used for fastening of goods with truck, trailer, pallets, boxes, containers etc. This is also known as Ratchet lashing, Ratchet straps, Ratchet tie down, tie down straps, lashing with webbing etc.
Custom ratchet straps can have hooks such as J hooks, D hooks, E track fittings, and with S hooks being the most popular industry standard. [2]
This article uses material from the Wikipedia article "Tie down straps", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted