powered by CADENAS

Social Share

Argentine ant (7522 views - Insects)

The Argentine ant, Linepithema humile (formerly Iridomyrmex humilis), is an ant native to northern Argentina, Uruguay, Paraguay, Bolivia and southern Brazil. It is an invasive species that has been established in many Mediterranean climate areas, inadvertently introduced by humans to many places, including South Africa, New Zealand, Japan, Easter Island, Australia, Europe, Hawaii, and the continental United States.
Go to Article

Explanation by Hotspot Model

Argentine ant

Argentine ant

Argentine ant
Scientific classification
Kingdom: Animalia
Phylum: Arthropoda
Class: Insecta
Order: Hymenoptera
Family: Formicidae
Subfamily: Dolichoderinae
Tribe: Dolichoderini
Genus: Linepithema
Species: L. humile
Binomial name
Linepithema humile
(Mayr, 1868)

The Argentine ant, Linepithema humile (formerly Iridomyrmex humilis), is an ant native to northern Argentina, Uruguay, Paraguay, Bolivia and southern Brazil. It is an invasive species that has been established in many Mediterranean climate areas,[1] inadvertently introduced by humans to many places, including South Africa, New Zealand, Japan, Easter Island, Australia, Europe, Hawaii, and the continental United States.[2][3]

Description

The worker ants are 1.6–2.8 millimetres (0.06–0.11 in) long[4][5][dubious ] and can easily squeeze through cracks and holes as small as 1 millimetre (0.04 in) in size. Queens are 4.2–6.4 millimetres (0.17–0.25 in) long,[4] much smaller than other species of ants. These ants will set up quarters in the ground, in cracks in concrete walls, in spaces between boards and timbers, even among belongings in human dwellings. In natural areas, they generally nest shallowly in loose leaf litter or beneath small stones, due to their poor ability to dig deeper nests. However, if a deeper nesting ant species abandons their nest, Argentine ant colonies will readily take over the space.[citation needed]

Typical size of worker ants found in Southern California.
These markers can help identify Argentine ants.

German entomologist Gustav L. Mayr identified the first specimens of Hypoclinea humilis in the vicinity of Buenos Aires, Argentina in 1866. This species was shortly transferred to the genus Iridomyrmex, and finally to Linepithema in the early 1990s.

Distribution

The native range of Argentine ants is limited to around major waterways in the lowland areas of the Paraná River drainage. They have recently spread into parts of Argentina, Brazil, Chile, Colombia, Ecuador, and Peru.[6] The species has become established in at least 15 countries throughout the world, on six continents, as well as many oceanic islands.[7]

Global "mega-colony"

According to research published in Insectes Sociaux in 2009, it was discovered that ants from three Argentine ant supercolonies in America, Europe, and Japan, that were previously thought to be separate, were in fact most likely to be genetically related. The three colonies in question were one in Europe, stretching 6,000 km (3,700 mi) along the Mediterranean coast, the "Californian large" colony, stretching 900 km (560 mi) along the coast of California, and a third on the west coast of Japan.[8][9]

Based on a similarity in the chemical profile of hydrocarbons on the cuticles of the ants from each colony, and on the ants' non-aggressive and grooming behaviour when interacting, compared to their behaviour when mixing with ants from other super-colonies from the coast of Catalonia in Spain and from Kobe in Japan, researchers concluded that the three colonies studied actually represented a single global super-colony.[8][9]

The researchers stated that "enormous extent of this population is paralleled only by human society", and had probably been spread and maintained by human travel.[8][9]

Behavior

They have been extraordinarily successful, in part, because different nests of the introduced Argentine ants seldom attack or compete with each other, unlike most other species of ant. In their introduced range, their genetic makeup is so uniform that individuals from one nest can mingle in a neighboring nest without being attacked. Thus, in most of their introduced range, they form supercolonies. "Some ants have an extraordinary social organization, called unicoloniality, whereby individuals mix freely among physically separated nests. This type of social organization is not only a key attribute responsible for the ecological domination of these ants, but also an evolutionary paradox and a potential problem for kin selection theory because relatedness between nest mates is effectively zero."[10] The Very Large Colony, which covers territory from San Diego to beyond San Francisco, may have a population of nearly one trillion individuals.[11]

Conflict does occur between members of different supercolonies. In 1997, UC San Diego researchers observed fighting between different Argentine ants kept in lab, and in 2004 scientists began to map out the boundaries of the different supercolonies that clashed in San Diego. On the border of the Very Large Colony and the Lake Hodges Colony thirty million ants die each year on a battlefront that covers miles.[12]

In contrast, native populations are more genetically diverse, genetically differentiated (among colonies and across space), and form colonies that are much smaller than the supercolonies that dominate the introduced range. Argentine ants in their native South America also co-exist with many other species of ants, and do not attain the high population densities that characterize introduced populations.[13]

In a series of experiments, ants of the same colony were isolated and fed different diets. The hydrocarbons from the diet were eventually incorporated into the cuticle of the subjects. Those that had the same diet appeared to recognize one another as kin. Those who had at least some overlap in dietary composition also appeared to react non-aggressively to one another. These interactions contrasts drastically with the groups that fed on completely different sources, such as those who lived off flies and those that fed on grasshoppers. The groups appeared to have incorporated hydrocarbons that were not similar to the others and created an unfamiliar identity cue. These groups reacted violently towards each other. This suggests that dietary factors affect the recognition cues for colony members.[14][15]

Reproduction and seasonal colony trends

Like workers in many other ant species, Argentine ant workers are unable to lay reproductive eggs but can direct the development of eggs into reproductive females; the production of males appears to be controlled by the amount of food available to the larvae.[16] Argentine ant colonies almost invariably have many reproductive queens, as many as eight for every 1,000 workers. The queens seldom or never disperse in winged form. Instead, colonies reproduce by budding off into new units. As few as ten workers and a single queen can establish a new colony.[citation needed]

The seasonal low occurs in mid-winter, when 90% of a representative colony consisted of workers and the remainder of queens, and no reproductive activity and minimal birthing. Eggs are produced in late-winter, nearly all of which hatch into sexual forms by May. Mating occurs after the females emerge. Worker production increases steadily from mid-March to October, after which their numbers are not replenished; thus, their numbers drop steadily over the winter months.[17]

Colonies in the Argentine ant’s native habitat are kept within a range of ten to one hundred meters by colonies of interspecific and intraspecific rivals. As the colonies expand, they appear to form fluctuating territory borders, which contract and expand on a seasonal and conditional basis. There is an expansive push outward in the summer months, with a retreating motion in the winter. This has to do with soil moisture and temperature conditions.[18] At the edges of these borders are either rival L. humile colonies or other obstacles that prevent further expansion, such as an inhospitable environment for nesting.[18]

Impact

The ants are ranked among the world's 100 worst animal invaders.[19] In its introduced range, the Argentine ant often displaces most or all native ants. This can, in turn, imperil other species in the ecosystem, such as native plants that depend on native ants for seed dispersal, or lizards that depend on native ants for food. For example, the recent severe decline in coastal horned lizards in southern California is closely tied to Argentine ants displacing native ant species on which the lizards feed.[20]

Argentine ants sometimes tend aphid colonies,[21] and their protection of this plant pest from predators and parasitoids can cause problems in agricultural areas.[22] In return for this protection, the ants benefit by feeding off an excretion known as honeydew. Thus, when Argentine ants invade an agricultural area, the population densities of these plant parasites increase and so does the damage they cause to crops.[citation needed]

Pest control

Argentine ants are a common household pest, often entering structures in search of food or water (particularly during dry or hot weather), or to escape flooded nests during periods of heavy rainfall. When they invade a kitchen, it is not uncommon to see two or three queens foraging along with the workers. Eliminating a single queen does not stop the colony's ability to breed.[citation needed]

Borate-sucrose water baits are toxic to Argentine ants, when the bait is 25% sucrose water, with 0.5-1.0% boric acid or borate salts. [23] [24]

Due to their nesting behavior and presence of numerous queens in each colony, it is generally impractical to spray Argentine ants with pesticides or to use boiling water as with mound building ants. Spraying with pesticides has occasionally stimulated increased egg-laying by the queens, compounding the problem. Pest control usually requires exploiting their omnivorous dietary habits, through use of slow-acting poison bait (e.g. fipronil, hydramethylnon sulfuramid), which will be carried back to the nest by the workers, eventually killing all the individuals, including the queens. It may take four to five days to eradicate a colony in this manner.[citation needed]

Researchers from the University of California, Irvine, have developed a way to use the scent of Argentine ants against them.[25] The exoskeletons of the ants are covered with a hydrocarbon-laced secretion. They made a compound that is different, but similar, to the one that coats the ants. If the chemical is applied to an ant, the other members of the colony will kill it.[26] The chemical method may be effective in combination with other methods.[citation needed]

Another approach for a large scale control of the Argentine ant has been proposed by researchers from Japan, who showed that it is possible to disrupt its trails with synthetic pheromones.[27] This has been confirmed in various later trials by a New Zealand-led team in Hawaii [28] and by researchers from Victoria University of Wellington who showed that this approach is beneficial for other local ant species.[29]

  1. ^ Neil D. Tsutsui; Andrew V. Suarez; David A. Holway; Ted J. Case (2001). "Relationships among native and introduced populations of the Argentine ant (Linepithema humile) and the source of introduced populations" (PDF). Molecular Ecology. 10 (9): 2151–2161. PMID 11555258. doi:10.1046/j.0962-1083.2001.01363.x. Archived from the original (PDF) on 2013-02-07. 
  2. ^ Hartley, Stephen; Harris, Richard; Lester, Philip J. (2006-09-01). "Quantifying uncertainty in the potential distribution of an invasive species: climate and the Argentine ant". Ecology Letters. 9 (9): 1068–1079. ISSN 1461-0248. doi:10.1111/j.1461-0248.2006.00954.x. 
  3. ^ Roura-Pascual, Núria; Hui, Cang; Ikeda, Takayoshi; Leday, Gwénaël; Richardson, David M.; Carpintero, Soledad; Espadaler, Xavier; Gómez, Crisanto; Guénard, Benoit (2011-01-04). "Relative roles of climatic suitability and anthropogenic influence in determining the pattern of spread in a global invader". Proceedings of the National Academy of Sciences. 108 (1): 220–225. ISSN 0027-8424. PMC 3017164. PMID 21173219. doi:10.1073/pnas.1011723108. 
  4. ^ a b "Argentine ants". Orkin. Retrieved December 2015.  Check date values in: |access-date= (help)
  5. ^ Eric P. Benson; Patricia A. Zungoli; Jennifer S. Nauman. "Argentine Ants". Clemson University, College of Agriculture, Forestry and Life Science. 
  6. ^ Alexander L. Wild (2004). "Taxonomy and distribution of the Argentine ant, Linepithema humile (Hymenoptera: Formicidae)" (PDF). Annals of the Entomological Society of America. 97 (6): 1204–1215. doi:10.1603/0013-8746(2004)097[1204:TADOTA]2.0.CO;2. 
  7. ^ Andrew V. Suarez; David A. Holway; Ted J. Case (2001). "Patterns of spread in biological invasions dominated by long-distance jump dispersal: Insights from Argentine ants". Proceedings of the National Academy of Sciences. 98 (3): 1095–1100. Bibcode:2001PNAS...98.1095S. JSTOR 3054827. PMC 14714. PMID 11158600. doi:10.1073/pnas.98.3.1095. 
  8. ^ a b c Walker, Matt (1 July 2009). "Ant mega-colony takes over world". Earth News. BBC News. Archived from the original on 2 July 2009. Retrieved 2 July 2009. 
  9. ^ a b c Sunamura, E.; Espadaler, X.; Sakamoto, H.; Suzuki, S.; Terayama, M.; Tatsuki, S. (2009-03-04). "Intercontinental union of Argentine ants: behavioral relationships among introduced populations in Europe, North America, and Asia". Insectes Sociaux. 56 (2): 143–147. ISSN 0020-1812. doi:10.1007/s00040-009-0001-9. 
  10. ^ Tatiana Giraud; Jes S. Pedersen; Laurent Keller (2002). "Evolution of supercolonies: the Argentine ants of southern Europe". Proceedings of the National Academy of Sciences. 99 (9): 6075–6079. Bibcode:2002PNAS...99.6075G. JSTOR 3058627. PMC 122904. PMID 11959924. doi:10.1073/pnas.092694199. 
  11. ^ Moffett, Mark (2010). Adventures Among Ants: A Global Safari with a Cast of Trillions. Berkeley and Los Angeles, CA: University of California Press. p. 204. ISBN 978-0-520-26199-0. 
  12. ^ Moffett, Mark (2010). Adventures Among Ants: A Global Safari with a Cast of Trillions. Berkeley and Los Angeles, CA: University of California Press. pp. 203–205. ISBN 978-0-520-26199-0. 
  13. ^ "Success of introduced Argentine ants tied to reduced genetic variation". University of California, San Diego. Retrieved 2015-08-25. 
  14. ^ "Diet-Related Modification of Cuticular Hydrocarbon Profiles of the Argentine Ant, Linepithema humile, Diminishes Intercolony Aggression". Journal of Chemical Ecology. 31: 829–843. 2005-05-25. doi:10.1007/s10886-005-3547-7. Retrieved 2015-08-25. 
  15. ^ "Large scale unicoloniality: the population and colony structure of the invasive Argentine ant (Linepithema humile) in New Zealand". Insectes Sociaux. 54: 275–282. 2007-06-12. doi:10.1007/s00040-007-0942-9. Retrieved 2015-08-25. 
  16. ^ L. Passera; L. Keller; J. P. Suzzoni (March 1988). "Control of brood male production in the Argentine ant Iridomyrmex humilis (Mayr)". Insectes Sociaux. 35 (1): 19–33. doi:10.1007/BF02224135. 
  17. ^ Markin, George P. (1969). "The Seasonal Life Cycle of the Argentine Ant In Southern California". Annals of the Entomological Society of America. 63 (5): 1238. 
  18. ^ a b "Linking Temporal and Spatial Scales in the Study of an Argentine Ant Invasion". Biological Invasions. 8: 501–507. doi:10.1007/s10530-005-6411-3. Retrieved 2015-08-25. 
  19. ^ "Super ant colony hits Australia". BBC News. 14 August 2004. 
  20. ^ "Proliferation of Argentine ants in California linked to decline in coastal horned lizards". Science Daily. March 5, 2002. 
  21. ^ C. M. Bristow (1991). "Are ant–aphid associations a tritrophic interaction? Oleander aphids and Argentine ants". Oecologia. 87 (4): 514–521. JSTOR 4219728. doi:10.1007/BF00320414. 
  22. ^ Crystal D. Grover; Kathleen C. Dayton; Sean B. Menke; David A. Holway (2008). "Effects of aphids on foliar foraging by Argentine ants and the resulting effects on other arthropods" (PDF). Ecological Entomology. 33 (1): 101–106. doi:10.1111/j.1365-2311.2007.00942.x. Archived from the original (PDF) on 2011-04-01. 
  23. ^ Klotz, John H.; Greenberg, Les; Amrhein, Christopher; Rust, Michael K. (August 2000). "Toxicity and Repellency of Borate-Sucrose Water Baits to Argentine Ants (Hymenoptera: Formicidae)" (PDF). Household and Structural Insects. Retrieved 2017-01-15. 
  24. ^ Klotz, John H.; Rust, Michael K.; Amrhein, Christopher; Krieger, Robert (September 2004). "In search of the 'sweet spot'" (PDF). Pest Control. Retrieved 2017-01-15. 
  25. ^ Perlman, David (2006-09-15). "Ants' own chemical may control them". SFGate. Retrieved 2015-08-25. 
  26. ^ Rivenburg, Roy (September 15, 2006). "UCI makes ants go ape by giving them B.O.". Los Angeles Times. 
  27. ^ US patent 8,278,360 B2, Sadahiro Tatsuki; Mamoru Terayama & Yasutoshi Tanaka et al., "Behavior-disrupting agent and behavior-disrupting method of Argentine ant", published 2012-10-02, assigned to Shin-Etsu Chemical Co Ltd 
  28. ^ David M Suckling; R. W. Peck; L. M. Manning; L. D. Stringer; J. Cappadonna; A. M. El-Sayed (2008). "Disruption of Foraging by a Dominant Invasive Species to Decrease Its Competitive Ability". Journal of Chemical Ecology. 34 (12): 1602–9. PMID 19034574. doi:10.1007/s10886-008-9566-4. 
  29. ^ Fabian L. Westermann; David M. Suckling; Philip J. Lester (2014). "Disruption of Foraging by a Dominant Invasive Species to Decrease Its Competitive Ability" (PDF). PLoS One. 9 (3): e90173. Bibcode:2014PLoSO...990173W. PMC 3942413. PMID 24594633. doi:10.1371/journal.pone.0090173. 


This article uses material from the Wikipedia article "Argentine ant", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Insects

3D data - 3D model - 3D library - beetle bug insect