powered by CADENAS

Social Share

Rove beetle (3506 views - Insects)

The rove beetles are a family (Staphylinidae) of beetles, primarily distinguished by their short elytra (wing covers) that typically leave more than half of their abdomens exposed. With roughly 63,000 species in thousands of genera, the group is currently recognized as the largest extant family of beetles. It is an ancient group, with fossilized rove beetles known from the Triassic, 200 million years ago, and possibly even earlier if the genus Leehermania proves to be a member of this family. They are an ecologically and morphologically diverse group of beetles, and commonly encountered in terrestrial ecosystems. One well-known species is the devil's coach horse beetle. For some other species, see list of British rove beetles.
Go to Article

Explanation by Hotspot Model

Rove beetle

Rove beetle

Rove beetle

Rove beetles
Rove beetles of western Eurasia
Scientific classification
Kingdom: Animalia
Phylum: Arthropoda
Class: Insecta
Order: Coleoptera
Suborder: Polyphaga
Infraorder: Staphyliniformia
Superfamily: Staphylinoidea
Family: Staphylinidae
Lameere, 1900
Subfamilies

The rove beetles are a family (Staphylinidae) of beetles, primarily distinguished by their short elytra (wing covers) that typically leave more than half of their abdomens exposed. With roughly 63,000 species in thousands of genera, the group is currently recognized as the largest extant family of beetles. It is an ancient group, with fossilized rove beetles known from the Triassic, 200 million years ago, and possibly even earlier if the genus Leehermania proves to be a member of this family.[1] They are an ecologically and morphologically diverse group of beetles, and commonly encountered in terrestrial ecosystems.

One well-known species is the devil's coach horse beetle. For some other species, see list of British rove beetles.

Anatomy

As might be expected for such a large family, considerable variation exists among the species. Sizes range from <1 to 35 mm (1.4 in), with most in the 2–8 mm range, and the form is generally elongated, with some rove beetles being ovoid in shape. Colors range from yellow and red to reddish-brown to brown to black to iridescent blue and green. The antennae usually have 11 segments and are filiform, with moderate clubbing in some genera. The abdomen may be very long and flexible, and some rove beetles superficially resemble earwigs.

Some members of Paederina (specifically the genus Paederus), a subtribe of Paederinae, contain a potent vesicant in their haemolymph which can produce a skin irritation called dermatitis linearis.[2] which in English has unfortunately acquired the inaccurate name Paederus dermatitis. The irritant pederin is highly toxic, more potent than cobra venom.[3]

Ecology

Rove beetles are known from every type of habitat in which beetles occur, and their diets include just about everything except the living tissues of higher plants, but now including higher plants with the discovery of the diet of Himalusa thailandensis. Most rove beetles are predators of insects and other invertebrates, living in forest leaf litter and similar decaying plant matter. They are also commonly found under stones, and around freshwater margins. Almost 400 species are known to live on ocean shores that are submerged at high tide [4] although these are much fewer than 1% of the worldwide total of Staphylinidae. These include the pictured rove beetle;.[5] Other species have adapted to live as inquilines in ant and termite colonies, and some live in mutualistic relationships with mammals whereby they eat fleas and other parasites, benefiting the host. A few species, notably those of the genus Aleochara, are scavengers and carrion feeders, or are parasitoids of other insects, particularly of certain fly pupae.

Although rove beetles' appetites for other insects would seem to make them obvious candidates for biological control of pests, and empirically they are believed to be important controls in the wild, experiments using them have not been notably successful. Greater success is seen with those species (genus Aleochara) that are parasitoids.

Rove beetles of the genus Stenus are very interesting insects. They are specialist predators of small invertebrates such as collembola. Their labium can shoot out from the head using blood pressure. The thin rod of the labium ends in a pad of bristly hairs and hooks and between these hairs are small pores that exude an adhesive glue-like substance, which sticks to prey.[6]

Systematics

Classification of the 63,000 (as of 2015) staphylinid species is ongoing and controversial, with some workers proposing an organization of as many as 10 separate families, but the current favored system is one of 31 subfamilies, about 100 tribes (some grouped into supertribes), and about 3,200 genera. About 400 new species are being described each year, and some estimates suggest three-quarters of tropical species are as yet undescribed.

  1. ^ Chatzimanolis, Stylianos; Grimaldi, David A.; Engel, Michael S.; Fraser, Nicholas C. (2012). "Leehermania prorova, the Earliest Staphyliniform Beetle, from the Late Triassic of Virginia (Coleoptera: Staphylinidae)". American Museum Novitates. 3761 (3761): 1–28. doi:10.1206/3761.2. 
  2. ^ Capinera, John L; J. Howard Frank (2008). "Dermatitis linearis". Encyclopedia of entomology. Springer. pp. 1179–. ISBN 978-1-4020-6242-1. The 28 species thus far shown to produce such a toxin belong to three of the 14 genera of Paederina, namely Paederus, Paederidus, and Megalopaederus 
  3. ^ "Ectoparasites". Institute of Tropical Medicine, Antwerp. Retrieved 2007-06-04. 
  4. ^ J.H. Frank & K.-J. Ahn (2011). "Coastal Staphylinidae (Coleoptera): A worldwide checklist, biogeography and natural history". ZooKeys. 107: 1–98. PMC 3392188. PMID 22792029. doi:10.3897/zookeys.107.1651. 
  5. ^ P. C. Craig (1970). "The behavior and distribution of the intertidal sand beetle, Thinopinus pictus (Coleoptera: Staphylinidae)". Ecology. 51 (6): 1012–1017. JSTOR 1933627. doi:10.2307/1933627. 
  6. ^ Piper, Ross (2007), Extraordinary Animals: An Encyclopedia of Curious and Unusual Animals, Greenwood Press.

Important works on Staphylinidae

For the Palaearctic fauna, the most up-to-date works are:

  • Lohse, G.A. (1964) Familie: Staphylinidae. In: Freude, H., Harde, K.W. & Lohse, G.A. (Eds.), Die Käfer Mitteleuropas. Band 4, Staphylinidae I (Micropeplinae bis Tachyporinae). Krefeld: Goecke & Evers Verlag, 264 pp.
  • Lohse, G.A. (1974) Familie: Staphylinidae. In: Freude, H., Harde, K.W. & Lohse, G.A. (Eds.), Die Käfer Mitteleuropas. Band 5, Staphylinidae II (Hypocyphtinae und Aleocharinae). Pselaphidae. Krefeld: Goecke & Evers Verlag, 381 pp.
  • Lohse, G.A. (1989) Ergänzungen und Berichtigungen zu Freude-Harde-Lohse "Die Käfer Mitteleuropas" Band 5 (1974), pp. 185–243 In: Lohse, G.A. & Lucht, W.H. (Eds.), Die Käfer Mitteleuropas. 1. Supplementband mit Katalogteil. Krefeld: Goecke & Evers Verlag, pp. 185–243.

Regional works

Europe

  • Lott, D.A. (2009). The Staphylinidae (rove beetles) of Britain and Ireland. Part 5: Scaphidiinae, Piestinae, Oxytelinae. Handbooks for the identification of British insects, vol. 12, part 5. St Albans: Royal Entomological Society. British and Irish fauna only
  • Tronquet, M. (2006). Catalogue iconographique des Coléoptères des Pyrénées-Orientales. Vol. 1: Staphylinidae. Supplément au Tome XV de la Revue de l’Association Roussillonnaise d’Entomologie. Perpignan: Association Roussillonnaise d’Entomologie.Extensively illustrated

Dog

This article uses material from the Wikipedia article "Rove beetle", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Insects

3D data - 3D model - 3D library - beetle bug insect