Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 4.0 (http://muzyczny.pl).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Headphones" – news · newspapers · books · scholar · JSTOR (April 2017) (Learn how and when to remove this template message) |
Headphones (or head-phones in the early days of telephony and radio) are a pair of small loudspeaker drivers worn on or around the head over a user's ears. They are electroacoustic transducers, which convert an electrical signal to a corresponding sound. Headphones let a single user listen to an audio source privately, in contrast to a loudspeaker, which emits sound into the open air for anyone nearby to hear. Headphones are also known as earspeakers, earphones[1] or, colloquially, cans.[2] Circumaural ('around the ear') and supra-aural ('over the ear') headphones use a band over the top of the head to hold the speakers in place. The other type, known as earbuds or earpieces[1] consist of individual units that plug into the user's ear canal. In the context of telecommunication, a headset is a combination of headphone and microphone. Headphones connect to a signal source such as an audio amplifier, radio, CD player, portable media player, mobile phone, video game console, or electronic musical instrument, either directly using a cord, or using wireless technology such as Bluetooth, DECT or FM radio. The first headphones were developed in the late 19th century for use by telephone operators, to keep their hands free. Initially the audio quality was mediocre and a step forward was the invention of high fidelity headphones.[3]
Headphones are made in a range of different audio reproduction quality capabilities. Headsets designed for telephone use typically cannot reproduce sound with the high fidelity of expensive units designed for music listening by audiophiles. Headphones that use cables typically have either a 1/4 inch (6.35mm) or 1/8 inch (3.5mm) phone jack for plugging the headphones into the audio source. Some stereo earbuds are wireless, using Bluetooth connectivity to transmit the audio signal by radio waves from source devices like cellphones and digital players.[4] Due to the spread of wireless devices in recent years headphones are increasingly used by people in public places such as sidewalks, grocery stores, and public transit. Headphones are also used by people in various professional contexts, such as audio engineers mixing sound for live concerts or sound recordings and DJs, who use headphones to cue up the next song without the audience hearing, aircraft pilots and call center employees. The latter two types of employees use headphones with an integrated microphone.
Headphones originated from the telephone receiver earpiece, and were the only way to listen to electrical audio signals before amplifiers were developed. The first truly successful set was developed in 1910 by Nathaniel Baldwin, who made them by hand in his kitchen and sold them to the United States Navy.[5][6]
These early headphones used moving iron drivers,[7] with either single-ended or balanced armatures. The common single-ended type used voice coils wound around the poles of a permanent magnet, which were positioned close to a flexible steel diaphragm. The audio current through the coils varied the magnetic field of the magnet, exerting a varying force on the diaphragm, causing it to vibrate, creating sound waves. The requirement for high sensitivity meant that no damping was used, so the frequency response of the diaphragm had large peaks due to resonance, resulting in poor sound quality. These early models lacked padding, and were often uncomfortable to wear for long periods. Their impedance varied; headphones used in telegraph and telephone work had an impedance of 75 ohms. Those used with early wireless radio had more turns of finer wire to increase sensitivity. Impedance of 1000 to 2000 ohms was common, which suited both crystal sets and triode receivers. Some very sensitive headphones, such as those manufactured by Brandes around 1919, were commonly used for early radio work.
In early powered radios, the headphone was part of the vacuum tube's plate circuit and carried dangerous voltages. It was normally connected directly to the positive high voltage battery terminal, and the other battery terminal was securely grounded. The use of bare electrical connections meant that users could be shocked if they touched the bare headphone connections while adjusting an uncomfortable headset.
In 1958, John C. Koss, an audiophile and jazz musician from Milwaukee, produced the first stereo headphones.[8][7] Previously, headphones were used only by the US navy, telephone and radio operators, and individuals in similar industries.[7]
Smaller earbud type earpieces, which plugged into the user's ear canal, were first developed for hearing aids. They became widely used with transistor radios, which commercially appeared in 1954 with the introduction of the Regency TR-1. The most popular audio device in history, the transistor radio changed listening habits, allowing people to listen to radio anywhere. The earbud uses either a moving iron driver or a piezoelectric crystal to produce sound. The 3.5 mm radio and phone connector, which is the most commonly used in portable application today, has been used at least since the Sony EFM-117J transistor radio, which was released in 1964.[9][10] Its popularity was reinforced with its use on the Walkman portable tape player in 1979.
Headphones may be used with stationary CD and DVD players, home theater, personal computers, or portable devices (e.g., digital audio player/MP3 player, mobile phone). Cordless headphones are not connected to their source by a cable. Instead, they receive a radio or infrared signal encoded using a radio or infrared transmission link, such as FM, Bluetooth or Wi-Fi. These are powered receiver systems, of which the headphone is only a component. Cordless headphones are used with events such as a Silent disco or Silent Gig.
In the professional audio sector, headphones are used in live situations by disc jockeys with a DJ mixer, and sound engineers for monitoring signal sources. In radio studios, DJs use a pair of headphones when talking to the microphone while the speakers are turned off to eliminate acoustic feedback while monitoring their own voice. In studio recordings, musicians and singers use headphones to play or sing along to a backing track or band. In military applications, audio signals of many varieties are monitored using headphones.
Wired headphones are attached to an audio source by a cable. The most common connectors are 6.35 mm (¼″) and 3.5 mm phone connectors. The larger 6.35 mm connector is more common on fixed location home or professional equipment. The 3.5 mm connector remains the most widely used connector for portable application today. Adapters are available for converting between 6.35 mm and 3.5 mm devices.
Electrical characteristics of dynamic loudspeakers may be readily applied to headphones, because most headphones are small dynamic loudspeakers.
Headphones are available with high or low impedance (typically measured at 1 kHz). Low-impedance headphones are in the range 16 to 32 ohms and high-impedance headphones are about 100-600 ohms. As the impedance of a pair of headphones increases, more voltage (at a given current) is required to drive it, and the loudness of the headphones for a given voltage decreases. In recent years, impedance of newer headphones has generally decreased to accommodate lower voltages available on battery powered CMOS-based portable electronics. This has resulted in headphones that can be more efficiently driven by battery-powered electronics. Consequently, newer amplifiers are based on designs with relatively low output impedance.
The impedance of headphones is of concern because of the output limitations of amplifiers. A modern pair of headphones is driven by an amplifier, with lower impedance headphones presenting a larger load. Amplifiers are not ideal; they also have some output impedance that limits the amount of power they can provide. To ensure an even frequency response, adequate damping factor, and undistorted sound, an amplifier should have an output impedance less than 1/8 that of the headphones it is driving (and ideally, as low as possible). If output impedance is large compared to the impedance of the headphones, significantly higher distortion is present.[11] Therefore, lower impedance headphones tend to be louder and more efficient, but also demand a more capable amplifier. Higher impedance headphones are more tolerant of amplifier limitations, but produce less volume for a given output level.
Historically, many headphones had relatively high impedance, often over 500 ohms so they could operate well with high-impedance tube amplifiers. In contrast, modern transistor amplifiers can have very low output impedance, enabling lower-impedance headphones. Unfortunately, this means that older audio amplifiers or stereos often produce poor-quality output on some modern, low-impedance headphones. In this case, an external headphone amplifier may be beneficial.
Sensitivity is a measure of how effectively an earpiece converts an incoming electrical signal into an audible sound. It thus indicates how loud the headphones are for a given electrical drive level. It can be measured in decibels of sound pressure level per milliwatt (dB (SPL)/mW) or decibels of sound pressure level per volt (dB (SPL) / V).[12] Unfortunately, both definitions are widely used, often interchangeably. As the output voltage (but not power) of a headphone amplifier is essentially constant for most common headphones, dB/mW is often more useful if converted into dB/V using Ohm's law:
Alternatively, online calculators can be used.[13] Once the sensitivity per volt is known, the maximum volume for a pair of headphones can be easily calculated from the maximum amplifier output voltage. For example, for a headphone with a sensitivity of 100 dB (SPL)/V, an amplifier with an output of 1 root mean square (RMS) voltage produces a maximum volume of 100 dB.
Pairing high sensitivity headphones with power amplifiers can produce dangerously high volumes and damage headphones. The maximum sound pressure level is a matter of preference, with some sources recommending no higher than 110 to 120 dB. In contrast, the American Occupational Safety and Health Administration recommends an average SPL of no more than 85 dB(A) to avoid long-term hearing loss, while the European Union standard EN 50332-1:2013 recommends that volumes above 85 dB(A) include a warning, with an absolute maximum volume (defined using 40–4000 Hz noise) of no more than 100 dB to avoid accidental hearing damage.[14] Using this standard, headphones with sensitivities of 90, 100 and 110 dB (SPL)/V should be driven by an amplifier capable of no more than 3.162, 1.0 and 0.3162 RMS volts at maximum volume setting, respectively to reduce the risk of hearing damage.
The sensitivity of headphones is usually between about 80 and 125 dB/mW and usually measured at 1 kHz.[15]
Headphone size can affect the balance between fidelity and portability. Generally, headphone form factors can be divided into four separate categories: circumaural (over-ear), supra-aural (on-ear), earbud and in-ear.
Circumaural headphones (sometimes called full size headphones or over-ear headphones) have circular or ellipsoid earpads that encompass the ears. Because these headphones completely surround the ear, circumaural headphones can be designed to fully seal against the head to attenuate external noise. Because of their size, circumaural headphones can be heavy and there are some sets that weigh over 500 grams (1 lb). Ergonomic headband and earpad design is required to reduce discomfort resulting from weight. These are commonly used by drummers in recording.
Supra-aural headphones or on-ear headphones have pads that press against the ears, rather than around them. They were commonly bundled with personal stereos during the 1980s. This type of headphone generally tends to be smaller and lighter than circumaural headphones, resulting in less attenuation of outside noise. Supra-aural headphones can also lead to discomfort due to the pressure on the ear as compared to circumaural headphones that sit around the ear. Comfort may vary due to the earcup material.
Both circumaural and supra-aural headphones can be further differentiated by the type of earcups:
Open-back headphones have the back of the earcups open. This leaks more sound out of the headphone and also lets more ambient sounds into the headphone, but gives a more natural or speaker-like sound, due to including sounds from the environment.
Closed-back (or sealed) styles have the back of the earcups closed. They usually block some of the ambient noise. Closed-back headphones usually can produce stronger low frequencies than open-back headphones.
Semi-open headphones, have a design that can be considered as a compromise between open-back headphones and closed-back headphones. Some[who?] believe the term "semi-open" is purely there for marketing purposes. There is no exact definition for the term semi-open headphone. Where the open-back approach has hardly any measure to block sound at the outer side of the diaphragm and the closed-back approach really has a closed chamber at the outer side of the diaphragm, a semi-open headphone can have a chamber to partially block sound while letting some sound through via openings or vents.
Earphones are very small headphones that are fitted directly in the outer ear, facing but not inserted in the ear canal. Earphones are portable and convenient, but many people consider them uncomfortable.[16] They provide hardly any acoustic isolation and leave room for ambient noise to seep in; users may turn up the volume dangerously high to compensate, at the risk of causing hearing loss.[16][17] On the other hand, they let the user be better aware of their surroundings. Since the early days of the transistor radio, earphones have commonly been bundled with personal music devices. They are sold at times with foam pads for comfort. (The use of the term earbuds, which has been around since at least 1984, did not hit its peak until after 2001, with the success of Apple's MP3 player.[18])
In-ear headphones, also known as in-ear monitors (IEMs) or canalphones, are small headphones with similar portability to earbuds that are inserted in the ear canal itself. IEMs are higher-quality in-ear headphones and are used by audio engineers and musicians as well as audiophiles.
The outer shells of in-ear headphones are made up of a variety of materials, such as plastic, aluminum, ceramic and other metal alloys. Because in-ear headphones engage the ear canal, they can be prone to sliding out, and they block out much environmental noise. Lack of sound from the environment can be a problem when sound is a necessary cue for safety or other reasons, as when walking, driving, or riding near or in vehicular traffic.[19]
Generic or custom-fitting ear canal plugs are made from silicone rubber, elastomer, or foam. Custom in-ear headphones use castings of the ear canal to create custom-molded plugs that provide added comfort and noise isolation.[16]
This type combines advantages of earbuds and in-ear headphones – depending on the environment and requirements of the user, they provide passive noise reduction for quality mode (conversation or active music listening) or they give control over the sound environment around user in comfort mode (stand by or background voice/music listening).[citation needed]
A headset is a headphone combined with a microphone. Headsets provide the equivalent functionality of a telephone handset with hands-free operation. Among applications for headsets, besides telephone use, are aviation, theatre or television studio intercom systems, and console or PC gaming. Headsets are made with either a single-earpiece (mono) or a double-earpiece (mono to both ears or stereo). The microphone arm of headsets is either an external microphone type where the microphone is held in front of the user's mouth, or a voicetube type where the microphone is housed in the earpiece and speech reaches it by means of a hollow tube.
Telephone headsets connect to a fixed-line telephone system. A telephone headset functions by replacing the handset of a telephone. Headsets for standard corded telephones are fitted with a standard 4P4C commonly called an RJ-9 connector. Headsets are also available with 2.5 mm jack sockets for many DECT phones and other applications. Cordless bluetooth headsets are available, and often used with mobile telephones. Headsets are widely used for telephone-intensive jobs, in particular by call centre workers. They are also used by anyone wishing to hold telephone conversations with both hands free.
For older models of telephones, the headset microphone impedance is different from that of the original handset, requiring a telephone amplifier for the telephone headset. A telephone amplifier provides basic pin-alignment similar to a telephone headset adaptor, but it also offers sound amplification for the microphone as well as the loudspeakers. Most models of telephone amplifiers offer volume control for loudspeaker as well as microphone, mute function and switching between headset and handset. Telephone amplifiers are powered by batteries or AC adaptors.
Unwanted sound from the environment can be reduced by excluding sound from the ear by passive noise isolation, or, often in conjunction with isolation, by active noise cancellation.
Passive noise isolation is essentially using the body of the earphone, either over or in the ear, as a passive earplug that simply blocks out sound. The headphone types that provide most attenuation are in-ear canal headphones and closed-back headphones, both circumaural and supra aural. Open-back and earbud headphones provide some passive noise isolation, but much less than the others. Typical closed-back headphones block 8 to 12 dB, and in-ears anywhere from 10 to 15 dB. Some models have been specifically designed for drummers to facilitate the drummer monitoring the recorded sound while reducing sound directly from the drums as much as possible. Such headphones claim to reduce ambient noise by around 25 dB.
Active noise-cancelling headphones use a microphone, amplifier, and speaker to pick up, amplify, and play ambient noise in phase-reversed form; this to some extent cancels out unwanted noise from the environment without affecting the desired sound source, which is not picked up and reversed by the microphone. They require a power source, usually a battery, to drive their circuitry. Active noise cancelling headphones can attenuate ambient noise by 20 dB or more, but the active circuitry is mainly effective on constant sounds and at lower frequencies, rather than sharp sounds and voices. Some noise cancelling headphones are designed mainly to reduce low-frequency engine and travel noise in aircraft, trains, and automobiles, and are less effective in environments with other types of noise.
Headphones use various types of transducer to convert electrical signals to sound.
The moving coil driver, more commonly referred to as a "dynamic" driver is the most common type used in headphones. It consists of a stationary magnet element affixed to the frame of the headphone, which sets up a static magnetic field. The magnet in headphones is typically composed of ferrite or neodymium. A voice coil, a light coil of wire, is suspended in the magnetic field of the magnet, attached to a diaphragm, typically fabricated from lightweight, high-stiffness-to-mass-ratio cellulose, polymer, carbon material, paper or the like. When the varying current of an audio signal is passed through the coil, it creates a varying magnetic field that reacts against the static magnetic field, exerting a varying force on the coil causing it and the attached diaphragm to vibrate. The vibrating diaphragm pushes on the air to produce sound waves.
Electrostatic drivers consist of a thin, electrically charged diaphragm, typically a coated PET film membrane, suspended between two perforated metal plates (electrodes). The electrical sound signal is applied to the electrodes creating an electrical field; depending on the polarity of this field, the diaphragm is drawn towards one of the plates. Air is forced through the perforations; combined with a continuously changing electrical signal driving the membrane, a sound wave is generated. Electrostatic headphones are usually more expensive than moving-coil ones, and are comparatively uncommon. In addition, a special amplifier is required to amplify the signal to deflect the membrane, which often requires electrical potentials in the range of 100 to 1000 volts.
Due to the extremely thin and light diaphragm membrane, often only a few micrometers thick, and the complete absence of moving metalwork, the frequency response of electrostatic headphones usually extends well above the audible limit of approximately 20 kHz. The high frequency response means that the low midband distortion level is maintained to the top of the audible frequency band, which is generally not the case with moving coil drivers. Also, the frequency response peakiness regularly seen in the high frequency region with moving coil drivers is absent. Well-designed electrostatic headphones can produce significantly better sound quality than other types.[citation needed]
Electrostatic headphones require a voltage source generating 100 V to over 1 kV, and are on the user's head. Since the invention of insulators, there's no actual danger. They do not need to deliver significant electric current, which further limits the electrical hazard to the wearer in case of fault.
An electret driver functions along the same electromechanical means as an electrostatic driver. However the electret driver has a permanent charge built into it, whereas electrostatics have the charge applied to the driver by an external generator. Electret and electrostatic headphones are relatively uncommon. Original electrets were also typically cheaper and lower in technical capability and fidelity than electrostatics. Patent applications from 2009-2013 have been approved that show by using different materials, i.e. a "Fluorinated cyclic olefin electret film", Frequency response chart readings can reach 50 kHz at 100db. When these new improved electrets are combined with a traditional dome headphone driver, headphones can be produced that are recognised by the Japan Audio Society as worthy of joining the Hi Res Audio program. US patents 8,559,660 B2. 7,732,547 B2.7,879,446 B2.7,498,699 B2.
Orthodynamic (also known as Planar Magnetic) headphones use similar technology to electrostatic headphones, with some fundamental differences. They operate similarly to Planar Magnetic Loudspeakers.
An orthodynamic driver consists of a relatively large membrane that contains an embedded wire pattern. This membrane is suspended between two sets of permanent, oppositely aligned, magnets. A current passed through the wires embedded in the membrane produces a magnetic field that reacts with the field of the permanent magnets to induce movement in the membrane, which produces sound.
A balanced armature is a sound transducer design primarily intended to increase the electrical efficiency of the element by eliminating the stress on the diaphragm characteristic of many other magnetic transducer systems. As shown schematically in the first diagram, it consists of a moving magnetic armature that is pivoted so it can move in the field of the permanent magnet. When precisely centered in the magnetic field there is no net force on the armature, hence the term 'balanced.' As illustrated in the second diagram, when there is electric current through the coil, it magnetizes the armature one way or the other, causing it to rotate slightly one way or the other about the pivot thus moving the diaphragm to make sound.
The design is not mechanically stable; a slight imbalance makes the armature stick to one pole of the magnet. A fairly stiff restoring force is required to hold the armature in the 'balance' position. Although this reduces its efficiency, this design can still produce more sound from less power than any other[clarification needed]. Popularized in the 1920s as Baldwin Mica Diaphragm radio headphones, balanced armature transducers were refined during World War II for use in military sound powered telephones. Some of these achieved astonishing electro-acoustic conversion efficiencies, in the range of 20% to 40%, for narrow bandwidth voice signals.
Today they are typically used only in in-ear headphones and hearing aids, where their high efficiency and diminutive size is a major advantage.[20] They generally are limited at the extremes of the hearing spectrum (e.g. below 20 Hz and above 16 kHz) and require a better seal than other types of drivers to deliver their full potential. Higher-end models may employ multiple armature drivers, dividing the frequency ranges between them using a passive crossover network. A few combine an armature driver with a small moving-coil driver for increased bass output.
The earliest loudspeakers for radio receivers used balanced armature drivers for their cones.[21]
The thermoacoustic effect generates sound from the audio frequency Joule heating of the conductor, an effect that is not magnetic and does not vibrate the speaker. In 2013 a carbon nanotube thin-yarn earphone based on the thermoacoustic mechanism was demonstrated by a research group in Tsinghua University.[22] The as-produced CNT thin yarn earphone has a working element called CNT thin yarn thermoacoustic chip. Such a chip is composed of a layer of CNT thin yarn array supported by the silicon wafer, and periodic grooves with certain depth are made on the wafer by micro-fabrication methods to suppress the heat leakage from the CNT yarn to the substrate.[citation needed]
Transducer technologies employed much less commonly for headphones include the Heil Air Motion Transformer (AMT); Piezoelectric film; Ribbon planar magnetic; Magnetostriction and Plasma-ionisation. The first Heil AMT headphone was marketed by ESS Laboratories and was essentially an ESS AMT tweeter from one of the company's speakers being driven at full range. Since the turn of the century, only Precide of Switzerland have manufactured an AMT headphone. Piezoelectric film headphones were first developed by Pioneer, their two models used a flat sheet of film that limited the maximum volume of air movement. Currently, TakeT produces a piezoelectric film headphone shaped similarly to an AMT transducer but, which like the Precide driver, has a variation in the size of transducer folds over the diaphragm. It additionally incorporates a two way design by its inclusion of a dedicated tweeter/supertweeter panel. The folded shape of a diaphragm allows a transducer with a larger surface area to fit within smaller space constraints. This increases the total volume of air that can be moved on each excursion of the transducer given that radiating area.
Magnetostriction headphones, sometimes sold under the label Bonephones, work by vibrating against the side of head, transmitting sound via bone conduction. This is particularly helpful in situations where the ears must be unobstructed, or for people who are deaf for reasons that don't affect the nervous apparatus of hearing. Magnetostriction headphones though, are limited in their fidelity compared to conventional headphones that rely on the normal workings of the ear. Additionally, in the early 1990s, a French company called Plasmasonics tried to market a plasma-ionisation headphone. There are no known functioning examples left.
Headphones can prevent other people from hearing the sound, either for privacy or to prevent disturbing others, as in listening in a public library. They can also provide a level of sound fidelity greater than loudspeakers of similar cost. Part of their ability to do so comes from the lack of any need to perform room correction treatments with headphones. High-quality headphones can have an extremely flat low-frequency response down to 20 Hz within 3 dB. While a loudspeaker must use a relatively large (often 15" or 18") speaker driver to reproduce low frequencies, headphones can accurately reproduce bass and sub-bass frequencies with speaker drivers only 40-50 millimeters wide (or much smaller, as is the case with in-ear monitor headphones). Headphones' impressive low-frequency performance is possible because they are so much closer to the ear that they only need to move relatively small volumes of air.
Marketed claims such as 'frequency response 4 Hz to 20 kHz' are usually overstatements; the product's response at frequencies lower than 20 Hz is typically very small.[23] Headphones are also useful for video games that use 3D positional audio processing algorithms, as they allow players to better judge the position of an off-screen sound source (such as the footsteps of an opponent or their gun fire).
Although modern headphones have been particularly widely sold and used for listening to stereo recordings since the release of the Walkman, there is subjective debate regarding the nature of their reproduction of stereo sound. Stereo recordings represent the position of horizontal depth cues (stereo separation) via volume and phase differences of the sound in question between the two channels. When the sounds from two speakers mix, they create the phase difference the brain uses to locate direction. Through most headphones, because the right and left channels do not combine in this manner, the illusion of the phantom center can be perceived as lost. Hard panned sounds are also heard only in one ear rather than from one side.
Binaural recordings use a different microphone technique to encode direction directly as phase, with very little amplitude difference below 2 kHz, often using a dummy head. They can produce a surprisingly lifelike spatial impression through headphones. Commercial recordings almost always use stereo recording, rather than binaural, because loudspeaker listening is more common than headphone listening.
It is possible to change the spatial effects of stereo sound on headphones, to better approximate the presentation of speaker reproduction, by using frequency-dependent cross-feed between the channels.
Headsets can have ergonomic benefits over traditional telephone handsets. They allow call center agents to maintain better posture without needing to hand-hold a handset or tilt their head sideways to cradle it.[24]
Using headphones at a sufficiently high volume level may cause temporary or permanent hearing impairment or deafness. The headphone volume often has to compete with the background noise, especially in loud places such as subway stations, aircraft, and large crowds. Extended periods of exposure to high sound pressure levels created by headphones at high volume settings may be damaging;[25][26] however, one hearing expert found that "fewer than 5% of users select volume levels and listen frequently enough to risk hearing loss."[27] Some manufacturers of portable music devices have attempted to introduce safety circuitry that limited output volume or warned the user when dangerous volume was being used, but the concept has been rejected by most of the buying public, which favors the personal choice of high volume. Koss introduced the "Safelite" line of cassette players in 1983 with such a warning light. The line was discontinued two years later for lack of interest.
The government of France has imposed a limit on all music players sold in the country:[28] they must not be capable of producing more than 100dBA (the threshold of hearing damage during extended listening is 80 dB, and the threshold of pain, or theoretically of immediate hearing loss, is 130 dB).[29] Motorcycle and other power-sport riders benefit by wearing foam earplugs when legal to do so to avoid excessive road, engine, and wind noise, but their ability to hear music and intercom speech is actually enhanced when doing so. The ear can normally detect 1-billionth of an atmosphere of sound pressure level,[30] hence it is incredibly sensitive. At very high sound pressure levels, muscles in the ear tighten the tympanic membrane and this leads to a small change in the geometry of the ossicles and stirrup that results in lower transfer of force to the oval window of the inner ear (the acoustic reflex).[31]
The risk of hearing damage also depends on the exposure time. The higher the volume, the faster hearing loss occurs. According to OSHA work safety guidelines, workers should be exposed to 90dBA noise for a maximum of 8 hours to avoid hearing loss. An increase to just 95dBA cuts the safe exposure to only 4 hours. But there is little specific consensus on the safe level of exposure. NIOSH has an 8-hour recommended exposure limit set to 85dBA. Additionally, an increase to 93dBA instead of 95dBA halves the safe exposure time to 4 hours.[32]
Some studies have found that people are more likely to raise volumes to unsafe levels while performing strenuous exercise.[33] A Finnish study[34] recommended that exercisers should set their headphone volumes to half of their normal loudness and only use them for half an hour.
Noise cancelling headphones can be considered dangerous because of a lack of awareness the listener may have with their environment. Noise cancelling headphones are so effective that a person may not be able to hear oncoming traffic or pay attention to people around them. There is also a general danger that music in headphones can distract the listener and lead to dangerous situations.[35]
The usual way of limiting sound volume on devices driving headphones is by limiting output power. This has the additional undesirable effect of being dependent of the efficiency of the headphones; a device producing the maximum allowed power may not produce adequate volume when paired with low-efficiency, high-impedance equipment, while the same amount of power can reach dangerous levels with very efficient earphones.
This article uses material from the Wikipedia article "Headphones", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library