An insulation monitoring device monitors the ungrounded system between an active phase conductor and earth. It is intended to give an alert (light and sound) or disconnect the power supply when the resistance between the two conductors drops below a set value, usually 50 kΩ (sample of IEC standard for medical applications). The main advantage is that the ungrounded or floating system allows a continuous operation of important consumers such as medical, chemical, military, etc.
Some manufacturers of monitors for these systems are capable of handling VFDs (Variable Frequency (Speed) Drives). Most, however are not due to issues with the DC-portions of the VFDs.
Most monitors work by injecting low level dc on the line and detecting. Some manufacturers use a patented AMP-monitoring principle (Adapted Measuring Pulse)[citation needed]
This electronics-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Insulation monitoring device", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD